== Purpose ==
This article describes the configuration of the PWR wake-up pins for a usage in Linux.
The PWR Wake-up pins are used to wake-up from Standby from an external device.
This article does not describe how to configure a wake-up pin to use it internally in OPTEE.
1. Overview[edit source]
- Button: one external device plugged to a wake-up pin. Could also be a PMIC.
- PWR: PWR internal peripheral
- OPTEE PWR IRQ driver: driver in charge of PWR peripheral that provides access to the wake-up pin via an interrupts interface.
- OPTEE PWR IRQ user driver: PWR IRQ consumer used to enable one wake-up pin and forward events as notifications to the non-secure world.
- OPTEE notification: stack in charge of communication with the non secure world.
- Linux Linaro optee driver: stack in charge of communication with secure world. Transform OPTEE notifications to interrupts.
- GPIO keys: Linux driver using a wake-up pin handled by OPTEE. Could be any driver able to handle Linux interrupts.
2. Wake-up pin configuration[edit source]
2.1. OPTEE configuration[edit source]
Wake-up pins are configured in OPTEE via device-tree. A pwr-irq-user can be instantiated to handle the desired wake-up pin and send a OPTEE notification to Linux in case of event.
2.2. Linux configuration[edit source]
Linux does not handle wake-up pin, but it can handle an OPTEE notification as an interrupt. This is configured via device-tree.
3. Example with wake-up pin 2[edit source]
In the example below, the wake-up pin number 2 is configured by OPTEE, forwarded as notification number 4 to Linux, and used by "gpio-keys" driver in Linux to generate a key-press.
OPTEE device tree:
wakeup_button: wakeup-button { compatible = "st,stm32mp1,pwr-irq-user"; st,wakeup-pin-number = <2>; st,notif-it-id = <4>; status = "okay"; };
Linux device tree:
wake_up { compatible = "gpio-keys"; status = "okay"; button { label = "wake-up"; linux,code = <KEY_WAKEUP>; interrupts-extended = <&optee 4>; status = "okay"; }; };
4. References[edit source]