The STM32MP135x-DK Discovery kit (STM32MP135F-DK
) constitutes a flexible and complete solution for evaluating the capabilities of the STM32MP135 line
microprocessor devices.
All useful information to start with the STM32MP135x-DK Discovery kit is accessible through the links provided below.
1. Supported software distribution[edit source]
Only one software distribution is supported with STM32MP135x-DK Discovery kit :
- The STM32MPU Embedded Software distribution[1].
Take also a look at the latest STM32 MPU ecosystem release note for complementary information.
For this distribution, three software Packages are delivered:
- the Starter Package
- the Developer Package
- the Distribution Package
Note that the Which Package better suits your needs article provides hints for selecting the most appropriate Package.
These Packages provide you with the software packages (image, source code) and the tools that are needed to start using the STM32MP135x-DK Discovery Kits boards.
![]() | ||
Starter Package | Developer Package | Distribution Package |
|
Note: these developments require a host PC running the OpenSTLinux SDK, and optionally an IDE |
|
2. Hardware description[edit source]
The STM32MP135x-DK - hardware description article describes the board, and provides indications on how to:
- assemble the board
- configure the hardware switches
- connect the board to external material
It also contains a short introduction of the board hardware components and connectors.
Board description |
---|
![]() STM32MP135x-DK - hardware description |
3. References[edit source]