STM32MP135x-DK - software distributions

Revision as of 17:01, 7 November 2022 by Registered User
Applicable for STM32MP13x lines

The STM32MP135x-DK Discovery kit More info green.png (STM32MP135F-DK More info green.png) constitutes a flexible and complete solution for evaluating the capabilities of the STM32MP135 line More info.png microprocessor devices.

All useful information to start with the STM32MP135x-DK Discovery kit More info green.png is accessible through the links provided below.

1. Supported software distribution[edit source]

Only one software distribution is supported with STM32MP135x-DK Discovery kit More info green.png:

  • The STM32MPU Embedded Software distribution[1].

Take also a look at the latest STM32 MPU ecosystem release note for complementary information.

For this distribution, three software Packages are delivered:

  • the Starter Package
  • the Developer Package
  • the Distribution Package

Note that the Which Package better suits your needs article provides hints for selecting the most appropriate Package.

The STM32MP135x-DK Discovery kit More info green.png includes the software packages (image, source code) and the tools needed to get started.


ST logo.png STM32MPU Embedded Software distribution[1]
Starter Package Developer Package Distribution Package
  • to evaluate the board capabilities
  • to run examples
  • to modify the pieces of software delivered as source code in this Package (for example the Linux® kernel)
  • to add custom applications in the user space (delivered as binary in this Package)

Note: these developments require a host PC running the OpenSTLinux SDK, and optionally an IDE

  • to create a custom distribution

2. Hardware description[edit source]

A brief article (see link below) describes the board, and provides indications on how to:

  • assemble the board
  • configure the hardware switches
  • connect the board to external material

It also contains a short introduction of the board hardware components and connectors.

Board description
STM32MP135x-DK - hardware description
STM32MP135x-DK - hardware description

3. References[edit source]