The STM32MP135x-DK Discovery kit (STM32MP135F-DK
) constitutes a flexible and complete solution for evaluating the capabilities of the STM32MP13 microprocessor devices.
All useful information in order to start with these boards is accessible through links provided here below.
1. Supported software distribution[edit source]
Only one software distribution is supported in these boards:
- The STM32MPU Embedded Software distribution[1]. You might also take a look at the latest STM32MP13 ecosystem release note.
For this distribution, three software Packages are delivered : the Starter Package, the Developer Package, the Distribution Package.
Note that the Which Package better suits your needs article provides hints for selecting the most appropriate Package.
The STM32MP135x-DK Discovery kit include the software packages (image, source code) and the tools needed to get started.
![]() | ||
Starter Package | Developer Package | Distribution Package |
|
Note: these developments require a host PC running the OpenSTLinux SDK, and optionally an IDE |
|
2. Hardware description[edit source]
A brief article (see link below) describes the board, and provides indications on how to:
- assemble the board
- configure hardware switches
- connect the board to external material
It also contains a short introduction of the board hardware components and connectors.
Board description |
---|
![]() STM32MP135x-DKx - hardware description |
3. References[edit source]