1. Article purpose[edit source]
This article explains how to configure the DDRCTRL and DDRPHYC internal peripherals from the first stage bootloader.
The configuration is performed using the device tree mechanism that provides a hardware description of the DDR subsystem (DDR controler and DDR PHY peripheral), and embeds the configuration used by the first stage bootloader to initialize the DDR before loading the second stage bootloader.
The DDR settings are only used in the device tree of the boot chain FSBL, that is, in the TF-A device tree for OpenSTLinux official delivery (or in SPL only for the DDR tuning tool).
2. DT bindings documentation[edit source]
The DDR subsystem is a 'memory-controller' device represented by the device tree bindings documented below:
- TF-A: docs/devicetree/bindings/memory-controllers/st,stm32mp1-ddr.txt"[1]
- U-Boot: doc/device-tree-bindings/memory-controllers/st,stm32mp1-ddr.txt"[2]
3. DT configuration[edit source]
This hardware description is a combination of the STM32 microprocessor device tree files (.dtsi extension) and board device tree files (.dts extension). See the Device tree for an explanation of the device-tree file split.
STM32CubeMX can be used to generate this DDR board device tree. Refer to How to configure the DT using STM32CubeMX for more details.
3.1. DT configuration (STM32 level)[edit source]
The STM32MP1 DDR node is located in stm32mp15-ddr.dtsi[3] (see Device tree for further explanation).
/ { ... soc { ... ddr: ddr@5a003000{ compatible = "st,stm32mp1-ddr"; reg = <0x5A003000 0x550 0x5A004000 0x234>; clocks = <&rcc_clk AXIDCG>, <&rcc_clk DDRC1>, <&rcc_clk DDRC2>, <&rcc_clk DDRPHYC>, <&rcc_clk DDRCAPB>, <&rcc_clk DDRPHYCAPB>; clock-names = "axidcg", "ddrc1", "ddrc2", "ddrphyc", "ddrcapb", "ddrphycapb"; status = "okay"; }; }; };
3.2. DT configuration (board level)[edit source]
The next attributes provide the DDR information and DDR settings; the values used by the FSBL to initialize the registers of the DDR subsystem (the DDR controller and the DDR PHY).
These value are generated by DDR tools included in STM32CubeMX.
The board configuration defines each configuration needed (DDR_...) and includes the STM32-level device tree.
3.2.1. info[edit source]
- st,mem-name: name for the DDR configuration, a simple string for information
- st,mem-speed: DDR expected speed in kHz
- st,mem-size: DDR mem size in bytes (used in SSBL and FSBL)
3.2.2. Controller register values[edit source]
- st,ctl-reg: controller values depending on the DDR type (DDR3/LPDDR2/LPDDR3):
- st,ctl-timing: controller values depending on the DDR frequency and timing parameters:
- st,ctl-map: controller values depending on the address mapping:
- st,ctl-perf: controller values depending on performance and scheduling:
3.2.3. phy register values[edit source]
- st,phy-reg: phy values depending on the DDR type: (DDR3/LPDDR2/LPDDR3):
- st,phy-timing: phy values depending on the DDR frequency and timing parameters:
- st,phy-cal: phy cal depending on the DDR calibration or tuning. This parameter is optional: when it is absent, the built-in PHY calibration is done (default behavior); when it is present:
3.2.3.1. st,phy-cal value and DDR tuning[edit source]
By default, the st,phy-cal property is absent in device tree and the built-in PHY calibration is executed by the DDR driver to determine value of registers DXnDQTR and DXnDQSTR (with n = byte for 0 to 4).
When st,phy-cal is present in device tree (e.g. when DDR_PHY_CAL_SKIP is defined), the built-in PHY calibration is skipped and the driver use the device tree value of registers DXnDQTR and DXnDQSTR: they described the fine step delays used for DQ/DQS pin deskew and for eye centering. These optimal values are determined by the STM32CubeMX DDR Tuning Tool calibration result.
This DDR tuning is expected only during the bring-up of a new design and only when the build-in calibration is not enough to determine the optimal values for the above registers; the following procedure may be used:
- run multiple tuning on the same board (with power ON/OFF cycle or reset), the line DQ/DQS delays are expected to be stable (1step max), otherwise a noise issue on PCB may be suspected.
- run tuning on multiple boards to determine best value, board to board variations are expected to be low (1 step in typical case, 2 step in worst cases)
Then the best value is saved in the device tree and apply to all boards.
See #How to configure the DT using STM32CubeMX and the dedicated application note[4] for further information.
3.3. DT configuration examples[edit source]
3.3.1. Simple example[edit source]
You can add the DDR configuration node with :
/ {
...
soc {
ddr: ddr@5a003000{
compatible = "st,stm32mp1-ddr";
reg = <0x5A003000 0x550
0x5A004000 0x234>;
clocks = <&rcc_clk AXIDCG>,
<&rcc_clk DDRC1>,
<&rcc_clk DDRC2>,
<&rcc_clk DDRPHYC>,
<&rcc_clk DDRCAPB>,
<&rcc_clk DDRPHYCAPB>;
clock-names = "axidcg",
"ddrc1",
"ddrc2",
"ddrphyc",
"ddrcapb",
"ddrphycapb";
st,mem-name = "DDR3 2x4Gb 533MHz";
st,mem-speed = <533000>;
st,mem-size = <0x40000000>;
st,ctl-reg = <
0x00040401 /*MSTR*/
0x00000010 /*MRCTRL0*/
0x00000000 /*MRCTRL1*/
0x00000000 /*DERATEEN*/
0x00800000 /*DERATEINT*/
0x00000000 /*PWRCTL*/
0x00400010 /*PWRTMG*/
0x00000000 /*HWLPCTL*/
0x00210000 /*RFSHCTL0*/
0x00000000 /*RFSHCTL3*/
0x00000000 /*CRCPARCTL0*/
0xC2000040 /*ZQCTL0*/
0x02050105 /*DFITMG0*/
0x00000202 /*DFITMG1*/
0x07000000 /*DFILPCFG0*/
0xC0400003 /*DFIUPD0*/
0x00000000 /*DFIUPD1*/
0x00000000 /*DFIUPD2*/
0x00000000 /*DFIPHYMSTR*/
0x00000001 /*ODTMAP*/
0x00000000 /*DBG0*/
0x00000000 /*DBG1*/
0x00000000 /*DBGCMD*/
0x00000000 /*POISONCFG*/
0x00000010 /*PCCFG*/
>;
st,ctl-timing = <
0x0080008A /*RFSHTMG*/
0x121B2414 /*DRAMTMG0*/
0x000D041B /*DRAMTMG1*/
0x0607080E /*DRAMTMG2*/
0x0050400C /*DRAMTMG3*/
0x07040407 /*DRAMTMG4*/
0x06060303 /*DRAMTMG5*/
0x02020002 /*DRAMTMG6*/
0x00000202 /*DRAMTMG7*/
0x00001005 /*DRAMTMG8*/
0x000D041B /*DRAMTMG14*/
0x06000600 /*ODTCFG*/
>;
st,ctl-map = <
0x00080808 /*ADDRMAP1*/
0x00000000 /*ADDRMAP2*/
0x00000000 /*ADDRMAP3*/
0x00001F1F /*ADDRMAP4*/
0x07070707 /*ADDRMAP5*/
0x0F070707 /*ADDRMAP6*/
0x00000000 /*ADDRMAP9*/
0x00000000 /*ADDRMAP10*/
0x00000000 /*ADDRMAP11*/
>;
st,ctl-perf = <
0x00001201 /*SCHED*/
0x00001201 /*SCHED*/1
0x01000001 /*PERFHPR1*/
0x08000200 /*PERFLPR1*/
0x08000400 /*PERFWR1*/
0x00010000 /*PCFGR_0*/
0x00000000 /*PCFGW_0*/
0x02100B03 /*PCFGQOS0_0*/
0x00800100 /*PCFGQOS1_0*/
0x01100B03 /*PCFGWQOS0_0*/
0x01000200 /*PCFGWQOS1_0*/
0x00010000 /*PCFGR_1*/
0x00000000 /*PCFGW_1*/
0x02100B03 /*PCFGQOS0_1*/
0x00800000 /*PCFGQOS1_1*/
0x01100B03 /*PCFGWQOS0_1*/
0x01000200 /*PCFGWQOS1_1*/
>;
st,phy-reg = <
0x01442E02 /*PGCR*/
0x10400812 /*ACIOCR*/
0x00000C40 /*DXCCR*/
0xF200001F /*DSGCR*/
0x0000000B /*DCR*/
0x00010000 /*ODTCR*/
0x0000007B /*ZQ0CR1*/
0x0000CE81 /*DX0GCR*/
0x0000CE81 /*DX1GCR*/
0x0000CE81 /*DX2GCR*/
0x0000CE81 /*DX3GCR*/
>;
st,phy-timing = <
0x0022A41B /*PTR0*/
0x047C0740 /*PTR1*/
0x042D9C80 /*PTR2*/
0x369477D0 /*DTPR0*/
0x098A00D8 /*DTPR1*/
0x10023600 /*DTPR2*/
0x00000830 /*MR0*/
0x00000000 /*MR1*/
0x00000208 /*MR2*/
0x00000000 /*MR3*/
>;
status = "okay";
};
The optional node st,phy-cal allows to use a calibration result when it is present, for example:
/ {
...
soc {
ddr: ddr@5a003000{
compatible = "st,stm32mp1-ddr";
...
st,phy-cal = <
0x40000000 /*DX0DLLCR*/
0xFFFFFFFF /*DX0DQTR*/
0x3DB02000 /*DX0DQSTR*/
0x40000000 /*DX1DLLCR*/
0xFFFFFFFF /*DX1DQTR*/
0x3DB02000 /*DX1DQSTR*/
0x40000000 /*DX2DLLCR*/
0xFFFFFFFF /*DX2DQTR*/
0x3DB02000 /*DX2DQSTR*/
0x40000000 /*DX3DLLCR*/
0xFFFFFFFF /*DX3DQTR*/
0x3DB02000 /*DX3DQSTR*/
>;
...
};
3.3.2. STM32CubeMX configuration file[edit source]
STM32CubeMX generates a .dtsi file with the needed values as defines (named DDR_...), and includes the #Generic DDR dtsi file "stm32mp15-ddr.dtsi"[3]: as this dtsi file is preprocessed during FSBL compilation, it generates a correct device tree.
For example the file fdts/stm32mp15-ddr3-1x4Gb-1066-binG.dtsi is:
/ SPDX-License-Identifier: GPL-2.0+ OR BSD-3-Clause
/*
* File generated by STMicroelectronics STM32CubeMX DDR Tool for MPUs
* DDR type: DDR3 / DDR3L
* DDR width: 16bits
* DDR density: 4Gb
* System frequency: 533000Khz
* Relaxed Timing Mode: false
* Address mapping type: RBC
*
* Save Date: 2020.02.20, save Time: 18:45:20
*/
#define DDR_MEM_NAME "DDR3-DDR3L 16bits 533000Khz"
#define DDR_MEM_SPEED 533000
#define DDR_MEM_SIZE 0x20000000
#define DDR_MSTR 0x00041401
#define DDR_MRCTRL0 0x00000010
#define DDR_MRCTRL1 0x00000000
#define DDR_DERATEEN 0x00000000
#define DDR_DERATEINT 0x00800000
.....
#define DDR_DX2DQSTR 0x3DB02000
#define DDR_DX3GCR 0x0000CE80
#define DDR_DX3DLLCR 0x40000000
#define DDR_DX3DQTR 0xFFFFFFFF
#define DDR_DX3DQSTR 0x3DB02000
#include "stm32mp15-ddr.dtsi"
NB: the calibration values (DXnDLLCR, DXnDQTR, DXnDQSTR, with n in 1...3) are not used when DDR_PHY_CAL_SKIP is not defined
3.3.3. Generic DDR dtsi file[edit source]
The dtsi file used with DDR_ defines for STM32MP15x lines is stm32mp15-ddr.dtsi
// SPDX-License-Identifier: GPL-2.0+ OR BSD-3-Clause
/*
* Copyright (C) 2018, STMicroelectronics - All Rights Reserved
*/
/ {
soc {
ddr: ddr@5a003000{
compatible = "st,stm32mp1-ddr";
reg = <0x5A003000 0x550
0x5A004000 0x234>;
clocks = <&rcc AXIDCG>,
<&rcc DDRC1>,
<&rcc DDRC2>,
<&rcc DDRPHYC>,
<&rcc DDRCAPB>,
<&rcc DDRPHYCAPB>;
clock-names = "axidcg",
"ddrc1",
"ddrc2",
"ddrphyc",
"ddrcapb",
"ddrphycapb";
st,mem-name = DDR_MEM_NAME;
st,mem-speed = <DDR_MEM_SPEED>;
st,mem-size = <DDR_MEM_SIZE>;
st,ctl-reg = <
DDR_MSTR
DDR_MRCTRL0
DDR_MRCTRL1
DDR_DERATEEN
DDR_DERATEINT
DDR_PWRCTL
DDR_PWRTMG
DDR_HWLPCTL
DDR_RFSHCTL0
DDR_RFSHCTL3
DDR_CRCPARCTL0
DDR_ZQCTL0
DDR_DFITMG0
DDR_DFITMG1
DDR_DFILPCFG0
DDR_DFIUPD0
DDR_DFIUPD1
DDR_DFIUPD2
DDR_DFIPHYMSTR
DDR_ODTMAP
DDR_DBG0
DDR_DBG1
DDR_DBGCMD
DDR_POISONCFG
DDR_PCCFG
>;
st,ctl-timing = <
DDR_RFSHTMG
DDR_DRAMTMG0
DDR_DRAMTMG1
DDR_DRAMTMG2
DDR_DRAMTMG3
DDR_DRAMTMG4
DDR_DRAMTMG5
DDR_DRAMTMG6
DDR_DRAMTMG7
DDR_DRAMTMG8
DDR_DRAMTMG14
DDR_ODTCFG
>;
st,ctl-map = <
DDR_ADDRMAP1
DDR_ADDRMAP2
DDR_ADDRMAP3
DDR_ADDRMAP4
DDR_ADDRMAP5
DDR_ADDRMAP6
DDR_ADDRMAP9
DDR_ADDRMAP10
DDR_ADDRMAP11
>;
st,ctl-perf = <
DDR_SCHED
DDR_SCHED1
DDR_PERFHPR1
DDR_PERFLPR1
DDR_PERFWR1
DDR_PCFGR_0
DDR_PCFGW_0
DDR_PCFGQOS0_0
DDR_PCFGQOS1_0
DDR_PCFGWQOS0_0
DDR_PCFGWQOS1_0
DDR_PCFGR_1
DDR_PCFGW_1
DDR_PCFGQOS0_1
DDR_PCFGQOS1_1
DDR_PCFGWQOS0_1
DDR_PCFGWQOS1_1
>;
st,phy-reg = <
DDR_PGCR
DDR_ACIOCR
DDR_DXCCR
DDR_DSGCR
DDR_DCR
DDR_ODTCR
DDR_ZQ0CR1
DDR_DX0GCR
DDR_DX1GCR
DDR_DX2GCR
DDR_DX3GCR
>;
st,phy-timing = <
DDR_PTR0
DDR_PTR1
DDR_PTR2
DDR_DTPR0
DDR_DTPR1
DDR_DTPR2
DDR_MR0
DDR_MR1
DDR_MR2
DDR_MR3
>;
#ifdef DDR_PHY_CAL_SKIP
st,phy-cal = <
DDR_DX0DLLCR
DDR_DX0DQTR
DDR_DX0DQSTR
DDR_DX1DLLCR
DDR_DX1DQTR
DDR_DX1DQSTR
DDR_DX2DLLCR
DDR_DX2DQTR
DDR_DX2DQSTR
DDR_DX3DLLCR
DDR_DX3DQTR
DDR_DX3DQSTR
>;
#endif
status = "okay";
};
};
};
4. How to configure the DT using STM32CubeMX[edit source]
The STM32CubeMX tool can be used to configure the STM32MPU device and get the corresponding platform configuration device tree files.
The STM32CubeMX supports all the defines described in the above DT bindings documentation paragraph with a generated included file "stm32mp15-mx.dtsi"; it is included in the mx dts file before the #Generic DDR dtsi file . Refer to the STM32CubeMX user manual and the dedicated application note[4] for further information.
See also How_to_create_your_board_device_tree#DDR configuration with STM32CubeMX DDR Tuning Tool.
If you want to use the STM32CubeMX DDR Tuning Tool calibration result, add in the generated files "stm32mp15-mx.dtsi" the line:
#define DDR_PHY_CAL_SKIP
5. References[edit source]
Please refer to the following links for additional information:
- ↑ docs/devicetree/bindings/memory-controllers/st,stm32mp1-ddr.txt TF-A DDR binding information file
- ↑ doc/device-tree-bindings/memory-controllers/st,stm32mp1-ddr.txt U-Boot DDR binding information file
- ↑ 3.0 3.1 fdts/stm32mp15-ddr.dtsi (for TF-A): STM32MP157C device tree files
- ↑ 4.0 4.1 AN5168 - DDR configuration on STM32MP1 Series MPU