1. Introduction[edit source]
This article explain how to set up a Point-to-Point connection to the STM32 MPU board, especially in case of a proxy is also setup on the PC for accessing the Internet.
2. Setting up network[edit source]
To set up the connection
- go to Windows -> Preferences -> General -> Network Connections
- select "Manual" in the Active Provider field, and:
- adjust your proxy setup with Edit... in Proxy entries
- configure a new Proxy bypass with Add Host... giving the IP address of the STM32 MPUtarget.
![Network Setting in STM32CubeIDE Network Setting in STM32CubeIDE](/stm32mpu/nsfr_img_auth.php/thumb/c/c7/CubeIDE-Proxy.png/500px-CubeIDE-Proxy.png)