1. Framework purpose[edit source]
The purpose of this article is to explain how to handle the STM32 Arm® Cortex® MPUs low-power modes:
- Low-power modes available on the device
- Linux software overview for Power Management (on/off support, Suspend / Resume, Idle behavior, policy and control)
- How to enter and exit a platform low-power mode
2. Software overview[edit source]
The Linux® Power Management (PM) is spitted in:
- Static PM or System-Wide Power Management:
- power off
- suspend framework, used to trigger a low-power mode entry/exit sequence.
- Dynamic PM or Working-State Power Management or Active Power Management based on other frameworks:
- CPUfreq, Devfreq
- OPP with link to thermal framework
- Genpd (performance states)
- Runtime PM: dynamically disable the resources of the peripherals (clocks and power supply when applicable) in case of inactivity (see power/runtime_pm.html).
- Clocks
- Regulators
Refer to power and in admin-guide/pm for more details.
The OpenSTLinux power management support is based on Arm® interface standards:
2.1. STM32MP1 series[edit source]
On STM32MP1 series, the "System-Wide Power Management" is supported:
The user application issues a suspend request to the kernel. This request is handled by the suspend Framework, which notifies all the device drivers to prepare for low-power entry. It then calls the PSCI service.
2.2. STM32MP2 series[edit source]
When the user application sent a suspend request to the kernel (static), it is treated by the suspend framework with the PSCI suspend support.
For OS initiated low power more (dynamic), the inactivity is managed by CPUIdle with PSCI driver and low power mode is selected with generic power domains (GenPD).
2.3. Component description[edit source]
Kernel components for low power:
- Dynamic PM: CPU Idle and device Idle with Runtime PM
- CPUFreq: DVFS for CPU (see the page How to change the CPU frequency for details)
- Suspend framework: this framework schedules the overall sequence by stopping all the ongoing tasks
- GenPD: domain framework, based on runtime PM
- GenPD driver: this driver is used for low-power mode selection according to the activated wakeup sources.
- PSCI library: this is a set of standardized functions to request a low-power service to the secure monitor
- Clock framework
- RCC driver: this driver handles the circuit non-secure clocks
- Regulator framework
- SCMI framework: including SCMI drivers for secure resource as clock, regulators, reset, performance domain
Secure monitor components (TF-A BL31 on AArch64 platforms, OP-TEE on AArch32 platforms) :
- PSCI library: this is a set of standardized functions handling the low-power services
- Low power driver: the role of this driver is to choose the low-power mode according to the programmed wakeup source(s)
- PWR driver: this driver is responsible for configuring the low-power mode
- RCC driver: this driver handles the circuit secure clocks
Secure world components (OP-TEE):
- SCMI stack: SCMI stack with access to secure resources, clock with RCC driver, regu with PWR driver and STPMIC driver
2.4. API description[edit source]
The suspend process is triggered from the user space through standard commands (see next chapter for details).
The system sleep control file is the state file, located under: /sys/power/
Further details can be found in admin-guide/pm/sleep-states.html and in power/interface.html.
The sysfs ABI are described in sysfs-power and sysfs-devices-power.
The device power API are described in driver-api/pm/index.html, in particular in driver-api/pm/devices.html.
3. Configuration[edit source]
The objective of this chapter is to explain how to configure the Linux kernel and device tree to have the Power Management (PM) framework activated.
3.1. Kernel configuration[edit source]
The Power Management framework is activated by default in ST deliveries.
It can be deactivated through the kernel menuconfig using Power management options/Suspend to RAM and standby: Menuconfig or how to configure kernel .
3.2. Device tree configuration[edit source]
3.2.1. STM32MP1 series[edit source]
The default system low-power mode mapping can be modified through the secure monitor device tree, as described OP-TEE page.
Below an example in OP-TEE core/arch/arm/dts/stm32mp135f-dk.dts
&pwr_regulators { system_suspend_supported_soc_modes = < STM32_PM_CSLEEP_RUN STM32_PM_CSTOP_ALLOW_LP_STOP STM32_PM_CSTOP_ALLOW_LPLV_STOP STM32_PM_CSTOP_ALLOW_LPLV_STOP2 STM32_PM_CSTOP_ALLOW_STANDBY_DDR_SR >; system_off_soc_mode = <STM32_PM_SHUTDOWN>; };
3.2.2. STM32MP2 series[edit source]
The Soc device tree describes the PSCI topology in sub-nodes of cpus/domain-idle-states
:
- for Linux, only the mode supported with S2IDLE and PSCI OS initiated mode in arch/arm64/boot/dts/st/stm32mp251.dtsi : the Stop1 modes
- for TF-A all the low power modes in fdts/stm32mp251.dtsi
The selected PSCI power level is indicated to OP-TEE with Secure-EL1 Payload Dispatcher (SPD) PSCI hooks. The STPMIC25 driver in OP-TEE configures the regulators for the expected low power mode as describes in device tree with regulator-state-XXX subnodes, see PMIC page for details and OP-TEE device tree example in core/arch/arm/dts/stm32mp257f-ev1.dts .
The unsupported low power modes must be deleted in your board device-tree for TF-A BL31 and for Linux, and also its references in power domaine nodes with domain-idle-states.
For example on board without PMIC, if the regulator controlled by PWR_LP pins forces the reduced voltage on VDDCORE and VDDCPU, the LP-Stop1 and LP-Stop2 can not be supported.
- in TF-A device tree
/ { cpus { domain-idle-states { /delete-node/ lp-stop1; /delete-node/ lp-stop2; }; }; };
- in Linux device tree (CLUSTER_PD
domain-idle-states = <&STOP1>, <&LP_STOP1>;
for CLUSTER_PD in arch/arm64/boot/dts/st/stm32mp251.dts ):
/ { cpus { domain-idle-states { /delete-node/ domain-lp-stop1; }; }; }; &CLUSTER_PD { domain-idle-states = <&STOP1>; };
4. How to use the framework[edit source]
The power framework is managed with userfs API.
For Weston OpenSTLinux distribution, the direct access to sysfs must be avoided and must be replaced by systemctl
command.
- Suspend-to-RAM (S2RAM or deep)
echo mem > /sys/power/state
- The mode 'deep' for S2RAM is default at boot, you can force it with
echo deep > /sys/power/mem_sleep echo mem > /sys/power/state
- or with
SuspendState=mem
in /etc/systemd/sleep.conf
systemctl suspend
- Suspend-to-Idle (S2Idle or freeze)
echo freeze > /sys/power/state
- The mode 'deep' for S2RAM is default at boot for mem power state, you can force it with
echo s2idle > /sys/power/mem_sleep echo mem > /sys/power/state
- or with
SuspendState=freeze
in /etc/systemd/sleep.conf
systemctl suspend
- Power-Off
shutdown -P now systemctl poweroff
In OpenSTLinux, the low power modes are selected with devices activity and activated wake up.
Family | Linux mode | low power mode |
---|---|---|
STM32MP1 series | deep | Stop LPLV-Stop Standby |
freeze | not supported | |
power off | Standby (DDR off) | |
STM32MP2 series | freeze | Stop1 LP-Stop1 LPLV-Stop1 |
deep | Stop2 LP-Stop2 LPLV-Stop2 Standby1 | |
power off | Standby1 VBAT |
See next chapter for details.
4.1. Low-power modes on STM32MP1 series[edit source]
Refer to STM32MP13 reference manuals, STM32MP15 reference manuals or STM32MP25 reference manuals for the full description of low-power modes.
The modes are handled by the RCC and the PWR peripherals.
Only the Suspend-to-RAM (S2RAM) target is supported for STM32MP1 series: the whole system activity is stopped and a low-power mode is entered. The software selects the deepest mode according to the activated wakeup source(s).
STM32MP1 series STMicroelectronics deliveries propose a default mapping of the low-power modes for each type of board, this default mapping can be changed thanks to the device tree as explain in the previous paragraph.
4.1.1. On STM32MP13x lines
[edit source]
The table below summarizes the device hardware states corresponding to each low-power mode.
MPU mode | Platform mode | VDDCORE state | VDDCPU state | Clocks state |
---|---|---|---|---|
CRun | Run | On | On | On |
CStop | Stop/LPLV-Stop | On/Retention | On/Retention | Off/Off |
CStandby | Stop/LPLV-Stop/LPLVL-STOP2/Standby | On/Retention/Retention/Off | On/Retention/Off/Off | Off/Off/Off/Off |
The following tables give the list of wake-up sources available in each mode.
Platform mode | Available wake-up sources |
---|---|
Stop | BOR, PVD, AVD, Vbat mon, Temp mon, HSE CSS, LSE CSS, RTC, TAMP, USBH, OTG, ETH, USART, I2C, SPI, DTS, LPTIM, IWDG, GPIO, Wakeup pins (from PWR) |
LPLV-Stop LPLV-Stop2 |
BOR, PVD, AVD, Vbat mon, Temp mon, LSE CSS, RTC, TAMP, USART, I2C, SPI, DTS, LPTIM, IWDG, GPIO, Wakeup pins (from PWR) |
Standby | BOR, Vbat mon, Temp mon, LSE CSS, RTC, TAMP, IWDG, Wakeup pins (from PWR) |
4.1.2. On STM32MP15x lines
[edit source]
The AN5109 low-power application note also gives much more information on these modes, including:
- the detailed description of the operating modes,
- the low-power mode entry and exit sequences,
- the low-power mode control registers.
- the wake-up sources and the software mechanism that ensures the consistency between the low-power mode and the activated wake-up source,
The table below summarizes the device hardware states corresponding to each low-power mode.
The term "subsystem" either refers to Arm® Cortex®-A7 (also called MPU) or to Arm® Cortex®-M4 (also called MCU). A mode prefixed by 'C' corresponds to a subsystem mode.
Level | Mode | VDDCORE state | Subsystem Clocks state |
---|---|---|---|
MPU Subsystem | MPU CRun | on | on |
MPU CStop | on | off | |
MPU CStandby | on | off | |
MCU Subsystem | MCU CRun | on | on |
MCU CStop | on | off |
A platform mode is the combination of MPU and MCU modes.
MPU mode | MCU mode | Platform mode | VDDCORE state | Clocks state |
---|---|---|---|---|
CRun/CStop/CStandby | CRun | Run | On | On |
CStop/CStandby | CStop | Stop (LPDS = 0) | On | Off |
CStop/CStandby | CStop | LP-Stop or LPLV-Stop (LPDS = 1) | Retention | Off |
CStandby | CStop MCU PDDS = 1 |
Standby | Off | Off |
The following tables give the list of wake-up sources available in each mode.
Plaform mode | Available wake-up sources |
---|---|
Stop | BOR, PVD, AVD, Vbat mon, Temp mon, LSE CSS, RTC, TAMP, USB, CEC, ETH, USART, I²C, SPI, LPTIM, IWDG, GPIO, Wakeup pins (from PWR) |
LPLV-Stop | BOR, PVD, AVD, Vbat mon, Temp mon, LSE CSS, RTC, TAMP, IWDG, GPIO, Wakeup pins (from PWR) |
Standby | BOR, Vbat mon, Temp mon, LSE CSS, RTC, TAMP, IWDG, Wakeup pins (from PWR) |
This list of Wake-up capability peripheral for each mode is defined in the Table 35. Functionalities depending on system operating mode of the STM32MP15 reference manuals.
4.2. Low-power modes on STM32MP2 series[edit source]
The AN5726 Guidelines for using low-power modes on STM32MP2 MPU also gives much more information on these modes and on associated the wake-up sources.
System mode | Linux Command | Power consumption | Wake-up time | VDDCPU | VDDCORE | DDR state |
---|---|---|---|---|---|---|
Stop1 | freeze (s2idle) |
Medium | Low | ON | ON | SR, VTT on |
LP-Stop1 | Medium | Low | SR, VTT off | |||
LPLV-Stop1 | Medium | Medium | ON (reduced) | ON (reduced) | ||
Stop2 | mem (deep) |
Low | Low | OFF | ON | SR, VTT off |
LP-Stop2 | Low | Medium | ||||
LPLV-Stop2 | Low | Medium | ON (reduced) | |||
Standby1 | Low | High | OFF | |||
Standby2 | shutdown | Very-Low | High | Off | ||
VBAT | Very-Low | Very-High |
OpenSTLinux sets the DDR in Self Refresh mode (SR) in all the low-power modes except power off and for LP-Stop1 and LP-Stop2 modes, the DDR VTT supply is switched off on STMicroelectronics reference design thought the PWR_LP signal connected to PWRCTRL1 pin of STPMIC25.
This list of Wake-up capability peripheral for each mode is defined in the Table 94. Functionalities depending on system operating mode of the STM32MP25 reference manuals.
The following tables give the list of wake-up sources available in each mode.
Plaform mode | Available wake-up sources |
---|---|
Stop1/2 and LP-Stop1/2 |
Group1 : Group2 + HPDMAx (x = 1, 2, 3), HSI frequency monitoring, USB, UCPD1, ETHx (x = 1,2), USARTx (x = 1 to 9), I2Cx (x = 1 to 7), I3Cx (x = 1 to 3), SPIx (x = 1 to 7), DTS, LPTIMx (x = 1, 2) |
LPLV-Stop1/2 | Group2 : Group3 + PVD, PVM, GPIOs |
Standby1 | Group3 : Group4 + CPU3, DBG, LPDMA, LPUART1[note 1], I2C8[note 1], I3C4[note 1], SPI8[note 1], ADF1[note 1], LPTIMy (y = 3, 4, 5), WWDG2, MBOX2, HSEM, GPIOZ |
Standby2 | Group4 : Group5 + 6 x WKUP pins |
VBAT | Group5 : BOR, VBATH/VBATL, TEMPH/TEMPL, LSE CSS, RTC/auto wake-up, tamper pins, IWDGx |
4.2.1. PSCI topology[edit source]
The low power modes for STM32MP2 use the PSCI stack in TF-A BL31, including the PSCI OSI mode.
The PSCI topology is defined in TF-A PM driver: plat/st/stm32mp2/stm32mp2_pm.c .
Each low power more is associated to a PSCI State-id, which uses the ARM Recommended StateID Encoding with OS initiated support, based on the PSCI state system topology defined in plat/st/stm32mp2/include/platform_def.h with:
PLAT_MAX_PWR_LVL
= 4, for Core(0), D1(1), D1LPLV(2), D2(3), D2_LPLV(3)PLAT_MIN_SUSPEND_PWR_LVL
=2, limit level forPSCI_CPU_SUSPEND
supportPLAT_NUM_PWR_DOMAINS
= 6 (2 cores and 4 power level)
and with the power domain states:
STM32MP_LOCAL_STATE_RUN
(0)STM32MP_LOCAL_STATE_RET
(1)STM32MP_LOCAL_STATE_LP
(2)STM32MP_LOCAL_STATE_OFF
(3)
For PSCI suspend requests, STM32MP25 supports 5 power levels in the PSCI topology to handle the regulators configuration done in OP-TEE for STPMIC2, in particular to differentiate the tension for LP and the LPLV modes.
The composite PSCI State-id are used in PSCI_CPU_SUSPEND
requests and in device tree (for S2Idle and for OS initiated support) and for used internal in TF-A BL31 for PSCI_CPU_SUSPEND
request (Deep).
PSCI request | Name | State-id | PState | D2_LPLV | D2 | D1_LPLV | D1 | Core |
---|---|---|---|---|---|---|---|---|
PSCI_CPU_SUSPEND | Sleep (WFI) | 0x00000001 | STANDBY | RUN | RUN | RUN | RUN | RET |
Stop1 | 0x00000011 | STANDBY | RUN | RUN | RUN | RET | RET | |
LP-Stop1 | 0x00000021 | STANDBY | RUN | RUN | RUN | LP | RET | |
LPLV-Stop1 | 0x00000211 | STANDBY | RUN | RUN | LP | RET | RET | |
PSCI_SYSTEM_SUSPEND | Stop2 | 0x40001333 | POWERDOWN | RUN | RET | OFF | OFF | OFF |
LP-Stop2 | 0x40002333 | POWERDOWN | RUN | LP | OFF | OFF | OFF | |
LPLV-Stop2 | 0x40023333 | POWERDOWN | LP | OFF | OFF | OFF | OFF | |
Standby | 0x40002333 | POWERDOWN | OFF | OFF | OFF | OFF | OFF |
4.2.2. PSCI in Linux (PSCI_CPU_SUSPEND)[edit source]
In Linux the power domain and associated low power modes for OS initiated mode are described in SoC device tree (in arch/arm64/boot/dts/st/stm32mp251.dtsi and in arch/arm64/boot/dts/st/stm32mp253.dtsi ) using the hierarchical model as described in Documentation/devicetree/bindings/arm/psci.yaml .
/ { cpus { idle-states { entry-method = "psci"; CPU_PWRDN: cpu-power-down { compatible = "arm,idle-state"; arm,psci-suspend-param = <0x00000001>; }; }; domain-idle-states { STOP1: domain-stop1 { compatible = "domain-idle-state"; arm,psci-suspend-param = <0x00000011>; }; LP_STOP1: domain-lp-stop1 { compatible = "domain-idle-state"; arm,psci-suspend-param = <0x0000021>; }; LPLV_STOP1: domain-lplv-stop1 { compatible = "domain-idle-state"; arm,psci-suspend-param = <0x00000211>; }; }; }; psci { compatible = "arm,psci-1.0"; method = "smc"; CPU_PD0: power-domain-cpu0 { #power-domain-cells = <0>; domain-idle-states = <&CPU_PWRDN>; power-domains = <&CLUSTER_PD>; }; CPU_PD1: power-domain-cpu1 { #power-domain-cells = <0>; domain-idle-states = <&CPU_PWRDN>; power-domains = <&CLUSTER_PD>; }; CLUSTER_PD: power-domain-cluster { #power-domain-cells = <0>; domain-idle-states = <&STOP1>, <&LP_STOP1>; power-domains = <&RET_PD>; }; RET_PD: power-domain-retention { #power-domain-cells = <0>; domain-idle-states = <&LPLV_STOP1>; }; };
This power domain hierarchy is used in generic power domain (GenPD) for S2IDLE request and for dynamic power management, based PSCI OS initiated mode PM runtime: Linux kernel selects the lowest possible low power mode with the associated PSCI State Id, according the state of each power domain (device in the power domain is running, wake-up source is activated) and which respects the OS constraint (wake-up latency in OS initiated mode for example).
The devices are assigned to a domain in Soc device tree according the Table 94. Functionalities depending on system operating mode of the reference manuals (autonomous mode is not managed in OpenSTLinux).
- CLUSTER_PD for peripherals not functional in "Stop1/2 and LP-Stop1/2"
- RET_PD for peripherals not functional in "LPLV-Stop1/2"
The EXTI1 driver manages also the activated wake up source: LPLV-Stop1 mode is not not allowed for Group2 wake up source.
4.2.3. PSCI in TF-A (PSCI_SYSTEM_SUSPEND)[edit source]
For deep
request the PSCI_SYSTEM_SUSPEND is sent to T-FA when the secondary core is stopped and all the process are frozen. The activated wake-up are consolidated in TF-A BL31 to select the lowest POWERDOWN supported mode in stm32_get_sys_suspend_power_state() .
If a low power mode is not supported by a board design, it must be removed in TF-A BL31 device tree.
You can limit the maximum supported mode with wake-up sources, but you can't force Stop2 mode by Linux command if LP-Stop2 is supported (same functionalities, same supported wake-up sources).
To debug purpose, you can force the selected mode in stm32_get_sys_suspend_power_state()
, for example:
/* Search the max supported POWERDOWN modes <= max_pwr_state */
for (i = ARRAY_SIZE(stm32mp_supported_pwr_states) - 1U; i > 0U; i--) {
pwr_state = stm32mp_supported_pwr_states[i];
if ((pwr_state != 0U) && (pwr_state <= max_pwr_state) &&
(psci_get_pstate_type(pwr_state) == PSTATE_TYPE_POWERDOWN)) {
break;
}
}
pwr_state = PWRSTATE_STOP2;
state_id = psci_get_pstate_id(pwr_state);
or remove some states in TF-A device tree , for example remove LP-Stop2 mode to allow Stop2 selection:
/ { cpus { domain-idle-states { /delete-node/ lp-stop2; }; }; };
4.3. How to enter and exit low-power modes[edit source]
4.3.1. System-Wide Power Management[edit source]
The platform selects the allowed modes depending on the required wakeup source and the coprocessor state.
So you need:
- Activate the MCU needed wakeup source(s) and call the expected low-power mode for MCU side
or stop the MCU firmware - Activate the MPU needed wakeup source(s) and call the expected low-power mode for MPU side
4.3.1.1. MCU side[edit source]
Please refer to Coprocessor power management for Arm® Cortex®-M commands or the MCU firmware can also be stopped before entering in low power (it is mandatory if this firmware is running in DDR).
4.3.1.2. MPU side[edit source]
The wakeup source(s) activation (device dependent) is done in the corresponding Linux driver (see the 'wakeup' attribute in sysfs) and it is possible to check the state of each wakeup source by displaying this attribute.
Then the low-power mode request is done by issuing the following command:
echo mem > /sys/power/state
When systemd[3] is used, for example on the Weston OpenSTLinux configuration, the low-power mode is safely entered with the systemctl
command:
systemctl suspend
In this case, the configuration file /etc/systemd/sleep.conf [4] map the Weston power state to the kernel power state (in /sys/power/state). The OpenSTlinux configuration is:
[Sleep] SuspendMode= HibernateMode= HybridSleepMode= SuspendState=mem HibernateState=mem HybridSleepState=mem
To exploit the “freeze” mode:
[Sleep] SuspendState=freeze
4.3.1.3. Example[edit source]
- entering/exiting MPU CStop mode
Enable at least one wakeup source from table 2.1 in CStop category, for example USART4 on STM32MP15:
echo enabled > /sys/devices/platform/soc/40010000.serial/tty/ttySTM0/power/wakeup echo enabled > /sys/devices/platform/soc/40010000.serial/power/wakeup
Call the low-power entry:
echo mem > /sys/power/state
or systemd function:
systemctl suspend
The MPU is now in CStop mode, and can be woken up by sending a character to the console.
4.3.2. Active Power Management[edit source]
This mode is only supported on STM32MP2 platform with PSCI OS initiated support.
The active power management is based on driver activity, with device PM runtime and GenPD, so you need to stop ALL the STM32MP25 peripherals activity, including console to allow low power modes.
5. Source code location[edit source]
The source files are located inside the Linux kernel.
- power core:
- power drivers:
- drivers/base/power
- GENPD driver: domain.c
- CPUIdle driver: drivers/cpuidle/
- PSCI drivers:
- STM32MP specific driver:
- drivers/soc/st/stm32_pm_domain.c for STM32MP1 series
- drivers/base/power
- bindings:
For the framework used in Linux power management, see the associated pages:
And drivers in other software component for each internal peripheral or external component are described in the associated pages:
6. How to trace and debug[edit source]
The suspend/resume process execution is logged in the MPU console. It gives useful information on the platform state (sleeping or active).
root@stm32mp1:~# echo mem > /sys/power/state [ 1072.267571] PM: suspend entry (deep) [ 1072.269687] PM: Syncing filesystems ... done. [ 1072.279114] Freezing user space processes ... (elapsed 0.008 seconds) done. [ 1072.292835] OOM killer disabled. [ 1072.296046] Freezing remaining freezable tasks ... (elapsed 0.001 seconds) done. [ 1072.303431] Suspending console(s) (use no_console_suspend to debug) [ 1072.332520] dwc2 49000000.usb-otg: suspending usb gadget configfs-gadget [ 1072.332537] dwc2 49000000.usb-otg: dwc2_hsotg_ep_disable: called for ep0 [ 1072.332546] dwc2 49000000.usb-otg: dwc2_hsotg_ep_disable: called for ep0 [ 1072.468536] Disabling non-boot CPUs ... [ 1072.507876] CPU1 killed. [ 1072.509635] Enabling non-boot CPUs ... [ 1072.510508] CPU1 is up [ 1072.527553] dwmac4: Master AXI performs any burst length [ 1072.527583] stm32-dwmac 5800a000.ethernet eth0: No Safety Features support found [ 1072.527621] stm32-dwmac 5800a000.ethernet eth0: ERROR failed to create debugfs directory [ 1072.527631] stm32-dwmac 5800a000.ethernet eth0: stmmac_hw_setup: failed debugFS registration [ 1072.588234] dwc2 49000000.usb-otg: resuming usb gadget configfs-gadget [ 1072.738469] OOM killer enabled. [ 1072.741575] Restarting tasks ... done. [ 1072.752596] PM: suspend exit
Get more debug information from the console with the following commands:
echo N > /sys/module/printk/parameters/console_suspend
This command allows to see the last linux kernel trace and also the PSCI stack traces, in OP-TEE for STM32MP1 and the the TF-A BL31 traces for STM32MP2 (which indicate the selected low power mode).
You can also activate the dynamic debug in Linux:
echo "func pm_dev_dbg +p" > /sys/kernel/debug/dynamic_debug/control
echo "func pm_pr_dbg +p" > /sys/kernel/debug/dynamic_debug/control echo "func dpm_show_time +p" > /sys/kernel/debug/dynamic_debug/control echo "func s2idle_loop +p" > /sys/kernel/debug/dynamic_debug/control
And use power sysfs sysfs-devices-power, for example:
echo 1 > /sys/power/pm_debug_messages echo 0 > /sys/power/pm_async
You can also activate PM_DEBUG and PM_TRACE.
To go further see the kernel documentation power/basic-pm-debugging.rst and power/s2ram.rst.
It is also possible to monitor the hardware signals related to the system low-power modes thanks to the HDP internal peripheral.
Please refer to HDP Linux driver for its configuration.
7. To go further[edit source]
Refer to reference manual for a detailed description of low-power modes and peripheral wakeup sources:
The next application notes gives additional information on the hardware settings used for low-power management:
8. References[edit source]
- ↑ Arm Power State Coordination Interface (PSCI):
https://developer.arm.com/documentation/den0022 - ↑ Arm System Control and Management Interface Platform Design Document (SCMI) specification:
https://developer.arm.com/documentation/den0056 - ↑ systemd: https://systemd.io/
- ↑ https://manpages.debian.org/jessie/systemd/systemd-sleep.conf.5.en.html