How to use U-Boot stm32key command

Revision as of 19:26, 2 April 2024 by Registered User
Applicable for STM32MP13x lines, STM32MP15x lines, STM32MP25x lines

1. Purpose[edit source]

In this article, the stm32key U-Boot command is used to illustrate and experiment the steps to provision the keys in the correct OTP needed to activate secure boot features: authentication and encryption.

It also allows setting the device directly to the CLOSED state.

Warning white.png Warning
Concerning the STM32MP25x lines More info.png, this article have not been updated yet.

1.1. Prerequisite[edit source]

All the required keys must be generated to provision the OTP.

The OTP write support must be activated in OP-TEE STM32MP BSEC PTA with CFG_STM32_BSEC_WRITE.

In ecosystem release ≤ v4.1.0 , this configuration is activated only on OP-TEE debug release with:

CFG_STM32_BSEC_WRITE ?= $(CFG_TEE_CORE_DEBUG)

The command stm32key is not functional by default with the release version of OP-TEE.

Warning white.png Warning
Make sure that a device with secure boot enabled is used: this is mentioned in the chip part number, for STM32MP13 and STM32MP15. Otherwise, the device becomes permanently unusable.

2. stm32key command[edit source]

U-Boot in OpenSTLinux embeds a stm32key command that can be called from U-Boot command-line interface to manage the keys in OTPs.

  stm32key help
 stm32key - Manage key on STM32
 
 Usage:
 stm32key list: list the supported key with description
 stm32key select [<key>]: Select the key identified by <key> or display the key used for read/fuse command
 stm32key read [<addr> | -a ]: Read the curent key at <addr> or current / all (-a) key in OTP
 stm32key fuse [-y] <addr>: Fuse the current key at addr in OTP
 stm32key close [-y]: Close the device, force use of PKH stored in OTP

The optional option -y is used to skip the confirmation message.

The name of the used <key> is

  • for STM32MP13x lines More info.png: PKHTH for authentication and EDMK for encryption
  stm32key list
 PKHTH: Hash of the 8 ECC Public Keys Hashes Table (ECDSA is the authentication algorithm)
 	OTP24..32
 EDMK: Encryption/Decryption Master Key"
 	OTP92..95
  • for STM32MP15x lines More info.png: PKH for authentication
  stm32key list
 PKH: Hash of the ECC Public Key (ECDSA is the authentication algorithm)
 	OTP24..32

3. Authentication keys provisioning[edit source]

The key provisioning is the first step to enable the authentication: burn the keys in OTPs with the key hash output file from STM32 KeyGen.

3.1. Select keys[edit source]

Key is selected with the command stm32key select <key>, with <key>=

  • PKHTH for STM32MP13x lines More info.png
  stm32key select PKHTH
 PKHTH selected
  • PKH for STM32MP15x lines More info.png
  stm32key select PKH
 PKH selected

3.2. Load keys file in DDR[edit source]

The keys hash file, output file from STM32 KeyGen, must be available in DDR before proceeding with the stm32key command;
this file is loaded at ${loadaddr} = 0xc4000000 in the next examples.

The file publicKeysHash.bin (for STM32MP15x lines More info.png) or publicKeysHashHashes.bin (for STM32MP13x lines More info.png) can be loaded from a filesystem partition on a storage device by using the load command (see documentation). For example, the file publicKeysHash.bin is in the bootfs (partition 7) on SD™ card (mmc0):

  load mmc 0#bootfs ${loadaddr} publicKeysHash.bin

or

  load mmc 0:7 0xc4000000 publicKeysHash.bin
 32 bytes read in 50 ms (0 Bytes/s)

3.3. Verify keys file in DDR[edit source]

Once the publicKeysHash.bin (for STM32MP15x lines More info.png) or publicKeysHashHashes.bin (for STM32MP13x lines More info.png) file is loaded in DDR, you can verify the content of the file with the command:

  stm32key read ${loadaddr} 

Example for STM32MP13x lines More info.png with PKHTH

 stm32key read ${loadaddr} 
 Read PKHTH at 0xc4000000
 PKHTH OTP 24: [c4000000] 27051956
 PKHTH OTP 25: [c4000004] b56aef2d
 PKHTH OTP 26: [c4000008] 6215263c
 PKHTH OTP 27: [c400000c] 00000439
 PKHTH OTP 28: [c4000010] 00000000
 PKHTH OTP 29: [c4000014] 00000000
 PKHTH OTP 30: [c4000018] 72429173
 PKHTH OTP 31: [c400001c] 05020600

Example for STM32MP15x lines More info.png with PKH

 stm32key read ${loadaddr} 
 Read PKH at 0xc4000000
 PKH OTP 24: [c4000000] 27051956
 PKH OTP 25: [c4000004] b56aef2d
 PKH OTP 26: [c4000008] 6215263c
 PKH OTP 27: [c400000c] 00000439
 PKH OTP 28: [c4000010] 00000000
 PKH OTP 29: [c4000014] 00000000
 PKH OTP 30: [c4000018] 72429173
 PKH OTP 31: [c400001c] 05020600

3.4. Key provisioning[edit source]

To write and lock the keys in OTP, you use the command:

  stm32key fuse ${loadaddr} 
Warning white.png Warning
Verify the keys before to confirm the operation; It is an irreversible operation!

3.5. Verify keys file in OTP[edit source]

After the previous command, the device contains the keys to authenticate images and it can be verified with the command:

  stm32key read

Result for STM32MP13x lines More info.png with PKHTH

 stm32key read
 PKHTH OTP 24: 27051956 lock : 50000000
 PKHTH OTP 25: b56aef2d lock : 50000000
 PKHTH OTP 26: 6215263c lock : 50000000
 PKHTH OTP 27: 00000439 lock : 50000000
 PKHTH OTP 28: 00000000 lock : 50000000
 PKHTH OTP 29: 00000000 lock : 50000000
 PKHTH OTP 30: 72429173 lock : 50000000
 PKHTH OTP 31: 05020600 lock : 50000000

Result for STM32MP15x lines More info.png with PKH

 stm32key read
 PKH OTP 24: 27051956 lock : 50000000
 PKH OTP 25: b56aef2d lock : 50000000
 PKH OTP 26: 6215263c lock : 50000000
 PKH OTP 27: 00000439 lock : 50000000
 PKH OTP 28: 00000000 lock : 50000000
 PKH OTP 29: 00000000 lock : 50000000
 PKH OTP 30: 72429173 lock : 50000000
 PKH OTP 31: 05020600 lock : 50000000

4. Encryption Decryption Master Key provisioning[edit source]

The EDMK key provisioning is the first step to enable the image decryption.

It is only available on STM32MP13x lines More info.png.

4.1. Select EDMK[edit source]

Key is selected with the command stm32key select <key>, with <key>=

  • EDMK for STM32MP13x lines More info.png
  stm32key select EDMK
 EDMK selected

4.2. Load EDMK file in DDR[edit source]

The keys file must be available in DDR before proceeding the stm32key command;
this file is loaded at ${loadaddr} = 0xc4000000 in the next examples.

The file edmk.bin can be loaded from a filesystem partition on a storage device by using the load command (see documentation). For example, the file edmk.bin is in the bootfs (partition 7) on SD™ card (mmc0):

  load mmc 0#bootfs ${loadaddr}  edmk.bin

or

  load mmc 0:7 0xc4000000 edmk.bin
 32 bytes read in 50 ms (0 Bytes/s)

4.3. Verify EDMK in DDR[edit source]

Then you can verify the content of keys files loaded in DDR with the command: stm32key read <addr>

Result for STM32MP13x lines More info.png with EDMK and ${loadaddr }=0xc4000000

  stm32key read ${loadaddr} 
  Read EDMK at 0xc4000000
  EDMK OTP 92: [c4000000] 27051956
  EDMK OTP 93: [c4000004] b56aef2d
  EDMK OTP 94: [c4000008] 6215263c
  EDMK OTP 95: [c400000c] 00000439

4.4. EDMK provisioning[edit source]

To write and lock the EDMK in OTP, you use the command with the same address:

  stm32key fuse ${loadaddr} 
Warning white.png Warning
Verify keys before to confirm the operation, it is a irreversible operation !

4.5. Verify EDMK in OTP[edit source]

After the previous command, the device contains the keys to decrypt the images and it can be verified with the command:

  stm32key read

Result for STM32MP13x lines More info.png with EDMK

 stm32key read
 EDMK OTP 92: 00000000 lock : 50000000
 EDMK OTP 93: 00000000 lock : 50000000
 EDMK OTP 94: 00000000 lock : 50000000
 EDMK OTP 95: 00000000 lock : 50000000

Warning: the content of the key cannot be read. It is masked, but the lock property can be verified to ensure that the key has been written.

5. Closing the device[edit source]

Once the authentication process is confirmed in ROM code and in TF-A, the device can be closed to ensure that only signed images can be used.

This operation is performed with the U-Boot command:

  stm32key close
Warning white.png Warning
This must not be done on STM32MP13x or STM32MP15x devices without secure boot enabled; Otherwise, the device becomes bricked and cannot be used anymore