How to configure OP-TEE

Revision as of 16:51, 19 December 2023 by Registered User (→‎Bare Environment)
Applicable for STM32MP13x lines, STM32MP15x lines, STM32MP25x lines


1. Purpose[edit source]

This article describes the configuration and process used for building several OP-TEE components from sources and deploying them the target.

The build example is based on the OpenSTLinux Developer Package or Distribution Package, and also presents build instructions for a bare environment.

2. Overview[edit source]

OP-TEE is a trusted execution environment for Arm®v7-A and Arm®v8-A platforms. OP-TEE is made of several components described in OP-TEE architecture overview.

OP-TEE components generate boot images and files stored in the filesystem embedded in the target.

  • OP-TEE OS generates 3 boot image files to be loaded in the platform boot media, in the predefined partitions. The generated boot images include a STM32 binary header enabling the use of the authenticated boot and flash programming facilities.
  • OP-TEE client (package optee_client) can be built to generate non-secure services for the OP-TEE OS. The files generated from optee_client build are stored in the embedded filesystem.
  • OP-TEE project releases other packages intended for test and demonstration. These can be built and embedded in the target filesystem. Building optee_examples and optee_test generates client and trusted applications together with libraries which are all stored in the target filesystem. Note the OP-TEE Linux driver is built into the Linux kernel image and is part of the OP-TEE ecosystem.

OP-TEE can be embedded as BL32 in the STM32 MPU platforms for the ST trusted configuration.

Warning white.png Warning
OP-TEE boot images must be embedded in the FIP binary that is loaded by BL2 and can be automatically authentified

3. OP-TEE core configuration[edit source]

OP-TEE services STM32MP13x lines More info.png STM32MP15x lines More info.png
(OP-TEE in SYSRAM)
STM32MP15x lines More info.png
(OP-TEE in DDR)
STM32MP25x lines More info.png
SCMI services
PSCI services N.A
Oscillator calibration service
Random generation service
Wakeup source management
Power Domain service
OTP access services
NVMEM provisioning services
User Trusted application support
Trustworthiness of secure services
OPP request management
Remote proc services

3.1. SCMI services[edit source]

SCMI services STM32MP13x lines More info.png STM32MP15x lines More info.png
(OP-TEE in SYSRAM)
STM32MP15x lines More info.png
(OP-TEE in DDR)
STM32MP25x lines More info.png
Clock management
Reset management
Performance management
Regulator management

3.2. PSCI services[edit source]

PSCI services STM32MP13x lines More info.png STM32MP15x lines More info.png
(OP-TEE in SYSRAM)
STM32MP15x lines More info.png
(OP-TEE in DDR)
STM32MP25x lines More info.png
System reset N.A
CPU hotplug N.A
Low power N.A
Info white.png Information
On STM32MP25x lines More info.png, the PSCI services are handled by secure monitor level firmware that is TF-A/BL31

3.3. STM32MP13x lines More info.png[edit source]

OP-TEE OS is loaded in DDR. Thanks to DDRMCE, the DDR area is encrypted.

3.4. STM32MP15x lines More info.png[edit source]

Warning white.png Warning
Enabling OP-TEE secure services in STM32MP15x lines More info.png for ecosystem release ≥ v5.0.0 More info.png

Before ecosystem release v5.0.0 More info.png , OP-TEE for STM32MP15x lines More info.png default configuration builds OP-TEE so that the firmware and the Trusted Applications execute in secure SYSRAM insternal secure memory.
With ecosystem release ≥ v5.0.0 More info.png OP-TEE OS for STM32MP15x lines More info.png default configuration makes it loaded in DDR, relaxed from hardware contraints of running in the secure SYSRAM. Because the DDR is not encrypted, OP-TEE cannot enforce trustworthiness of its secure services. Therefore this default configuration disables OP-TEE support for Trusted Applications and secure services. This default configuration only embeds support for power management and system services.

From ecosystem release v5.0.0 More info.png , OP-TEE for STM32MP15x lines More info.png, one can enable back OP-TEE secure services by changing the components build configuration switches so that OP-TEE executes in the secure SYSRAM, refer to Details on build directives.

When OP-TEE is running in SYSRAM:

OP-TEE OS requires more than 256Ko RAM to execute. STM32MP15x lines More info.png SYSRAM is only 256Ko large therefore OP-TEE core, when executing from SYSRAM must enable its pager mode (configuration switch CFG_WITH_PAGER=y) to extend secure memory using virtual memory means and paging on demand mechanisms to save secure data into DDR, protected by hash tables and software encryption keys.

When so, OP-TEE boot image is made of 2 binary images: one (the unpaged part) is loaded at the beginning of the SYSRAM by the FSBL, the second (the pageable part) is loaded in DDR by the FSBL, in a DDR area that can be accessed by the CPU secure world.

OP-TEE OS manages low power mode by saving an encrypted image of the SYSRAM content in DDR before it is suspended. OP-TEE restores this content back into the SYSRAM when it resumes from the suspended state. This sequence is achieved using CPU instructions and encryption keys saved in the secure and retained backup SRAM.

For more information on OP-TEE's pager implementation and integration, one can refer to the OP-TEE documenation related to pager [1]

3.5. STM32MP25x lines More info.png[edit source]

OP-TEE OS is loaded in DDR, in memory areas protected thanks to RISAF memory region encryption and secure level management.

4. Build with the Distribution Package[edit source]

The Distribution Package provides means to build the following OP-TEE components from their related bitbake target:

 bitbake optee-os-stm32mp                # OP-TEE core firmware
 bitbake optee-os-sdk-stm32mp            # OP-TEE development kit for Trusted Applications
 bitbake optee-client                    # OP-TEE client
 bitbake optee-test                      # OP-TEE test suite (optional)
 bitbake optee-examples                  # TA and CA examples

Distribution Package build process includes fetching the source files, compiling them and installing them to the target images.

The Yocto recipes for the OP-TEE packages can be found in:

meta-st/meta-st-stm32mp/recipes-security/optee/optee-os-stm32mp*
meta-st/meta-st-openstlinux/recipes-security/optee/optee-client*
meta-st/meta-st-openstlinux/recipes-security/optee/optee-examples*
meta-st/meta-st-openstlinux/recipes-security/optee/optee-test*

5. Build with the Developer Package or a Bare Environment[edit source]

Both Developer Package and bare build environments expect you to fetch/download the OP-TEE package source file trees in order to build the embedded binary images.

The instruction set below assumes all OP-TEE package source trees are available in the base directory referred as <sources>/. The source files are available from the github repositories:

 cd <sources>/
 git clone https://github.com/STMicroelectronics/optee_os.git
 git clone https://github.com/OP-TEE/optee_client.git
 git clone https://github.com/OP-TEE/optee_test.git
 git clone https://github.com/linaro-swg/optee_examples.git
 ls -1 <sources>/
optee_client
optee_examples
optee_os
optee_test
 
Warning white.png Warning
Pay attention to use a consistent tag version for all optee components eg 3.12.0 for DV3.1
Warning white.png Warning
The STM32 MPU platform may not be fully merged in the official OP-TEE repository [2] hence the URL provided above refers to the ST distribution [3]



STM32MP25x lines More info.png require an extra source tree for the implementation of the SCMI server embedded in OP-TEE core:

 git clone https://github.com/STMicroelectronics/SCP-firmware.git

STM32MP25x lines More info.png may also need an extra source tree for some device tree files (DTS file) that define specific board configuration settings:

 git clone https://github.com/STMicroelectronics/dt-stm32mp.git

5.1. Initialize the cross compile environment[edit source]

The compilation toolchain provided by the Developer Package can be used, refer to Setup Cross Compile Environment.

Alternatively other bare toolchains can be used to build the OP-TEE secure parts. In such case, the instructions below expect the toolchain to be part of the PATH and its prefix is defined by CROSS_COMPILE. One can use something like:

 export PATH=<path-to-toolchain>:$PATH
 export CROSS_COMPILE=<toolchain-prefix>-

5.2. Build OP-TEE OS[edit source]

5.2.1. Developer Package SDK[edit source]

The OP-TEE OS can be built from the Developer Package Makefile.sdk script that is present in the tarball. It automatically sets the proper configuration for the OP-TEE OS build. To build from shell command:

 make -f $PWD/../Makefile.sdk CFG_EMBED_DTB_SOURCE_FILE=<board_dts_file_name>.dts

5.2.2. Bare environment[edit source]

Alternatively one can also build OP-TEE OS based a bare cross compilation toolchain. OP-TEE OS builds with a Makefile and needs some configuration directives, in first place PLATFORM and CFG_EMBED_DTB_SOURCE_FILE.

PLATFORM defines the OP-TEE platform, stm32mp1 or stm32mp2.

CFG_EMBED_DTB_SOURCE_FILE defines the target platform device tree file name, from <optee-os>/core/arch/arm/dts/.

For example, building for stm32mp157c-ev1 target:

 cd <optee-os>
 make PLATFORM=stm32mp1 \
           CFG_EMBED_DTB_SOURCE_FILE=stm32mp157c-ev1.dts \
           CFG_TEE_CORE_LOG_LEVEL=2 O=build all

STM32MP25x lines More info.png requires an extra configuration switch CFG_SCP_FIRMWARE, with the absolute path of the SCP-firmware component source file tree. SCP-firmware is the SCMI server reference implementation embedded for SCMI services.

For example, building for stm32mp257f-dk target:

 cd <optee-os>
 make PLATFORM=stm32mp2 ARCH=arm \
           CFG_EMBED_DTB_SOURCE_FILE=stm32mp257f-dk.dts \
           CFG_SCP_FIRMWARE=<SCP-Firmware absolute path> \
           CFG_TEE_CORE_LOG_LEVEL=2 O=build all

Using the External device tree:


For some boards, ST provides extra device tree configurations in a dedicated git repository: optee/stm32mp257f-ev1-ca35tdcid-ostl.dts . You can use the git submodule command or simply clone the repository below:

 git clone https://github.com/STMicroelectronics/dt-stm32mp.git

or

 git submodule add https://github.com/STMicroelectronics/dt-stm32mp.git core/arch/arm/dts/external-dt

If the external device tree source tree is located at core/arch/arm/dts/external-dt, please ignore the rest of this subchapter, this is the default path for the external device tree.

You'll then need to compile OP-TEE and specify the external device tree path in the CFG_EXT_DTS config switch. Example for the STM32MP257F-EV1 Evaluation board More info green.png with OSTL config:

 make PLATFORM=stm32mp2 ARCH=arm \
           CFG_EXT_DTS=<PATH_TO_EXTERNAL_DT>/optee
           CFG_EMBED_DTB_SOURCE_FILE=stm32mp257f-ev1-ca35tdcid-ostl.dts \
           CFG_SCP_FIRMWARE=<SCP-Firmware absolute path> \
           CFG_TEE_CORE_LOG_LEVEL=2 \
           O=build all

5.2.3. Generated Files[edit source]

The 3 OP-TEE boot images are generated at following paths:

<optee-os>/build/core/tee-header_v2.bin
<optee-os>/build/core/tee-pageable_v2.bin
<optee-os>/build/core/tee-pager_v2.bin

The configuration directives used for the build are available in this file:

<optee-os>/build/conf.mk

The build also generates a development kit used to build Trusted Application binaries, in 32bit and/or 64bit:

<optee-os>/build/export-ta_arm32/
<optee-os>/build/export-ta_arm64/

5.2.4. Details on build directives[edit source]

Mandatory directives to build OP-TEE OS:

  • PLATFORM=<platform>
    • Ex: PLATFORM=stm32mp1 for STM32MP1 series
    • Ex: PLATFORM=stm32mp2 for STM32MP2 series
  • CFG_EMBED_DTB_SOURCE_FILE=<device-tree-source-file>: in-tree (core/arch/arm/dts/ ) device tree filename with its .dts extension.
    • Ex: CFG_EMBED_DTB_SOURCE_FILE=stm32mp157f-dk2.dts

Mandatory directives to build OP-TEE OS for STM32MP2 series:

  • CFG_SCP_FIRMWARE=<SCP-Firmware absolute path>


OP-TEE generic optional directives commonly used, described in OP-TEE OS mk/config.mk file:

  • CFG_CORE_HEAP_SIZE=<VALUE>: define the byte size of OP-TEE core memory allocation pool
  • CFG_NUM_THREADS=<VALUE>: define the number of TEE threads provisioned in OP-TEE
  • CFG_REE_FS={n|y}: disable/enable OP-TEE REE filsystem based secure storage area
  • CFG_RPMB_FS={n|y}: disable/enable OP-TEE eMMC/RPMB based secure storage area
  • CFG_RPMB_FS_DEV_ID=<VALUE>: define the mmcblk block device used by REE for eMMC/RPMB accesses
    (e.g. "1" on stm32mp157x-ev1 boards)
  • CFG_WITH_USER_TA={n|y}: disable/enable support for Trusted Applications in OP-TEE secure memory (default is y)


OP-TEE generic optional debugging and test directives commonly used, described in OP-TEE OS mk/config.mk file:

  • CFG_TEE_CORE_DEBUG={n|y}: disable/enable debug support
  • CFG_TEE_CORE_LOG_LEVEL={0|1|2|3|4}: define OP-TEE core trace level (0: no trace, 4: overflow of traces) (default is 2: info)
  • CFG_TEE_CORE_TA_LEVEL={0|1|2|3|4}: define OP-TEE Trusted Applications (TAs) trace level (default is 1: error)
  • CFG_TEE_CORE_TA_TRACE={n|y}: disable/enable TAs trace message at define OP-TEE core level (default is y)
  • CFG_UNWIND={n|y}: disable/enable stack unwind debug trace messages
  • CFG_ENABLE_EMBEDDED_TESTS={n|y}; disable/enable embedded test, used by xtest tool (default is y)
  • CFG_WITH_STATS={n|y}: disable/enable OP-TEE statistics retrieve from the Stats PTA service.
  • CFG_WERROR={n|y}: disable/enable build error trigger on OP-TEE build warning occurences.
  • CFG_TA_GPROF_SUPPORT={n|y}: disable/enable profiling of Trusted Application implementation based on gprof standard tool
  • CFG_FTRACE_SUPPORT={n|y}: disable/enable function trace support in Trusted Applications based on ftrace standard tool
  • CFG_SYSCALL_FTRACE={n|y}: disable/enable support for ftrace syscall graph generation


OP-TEE optional directives commonly used on STM32MP1 series and STM32MP2 series:

  • CFG_EXT_DTS=<PATH_TO_EXTERNAL_DT>
    • Needed if using the External device tree and its source tree is not located at core/arch/arm/dts/external-dt
  • CFG_STM32_EARLY_CONSOLE_UART={0|1|2|...}: define the USART instance used for early console trace messages (default is 4)
  • CFG_STM32_BSEC_WRITE={n|y}: disable/enable the program/write fuses capabilities (default n to avoid briking the chip)


OP-TEE optional directives specific to STM32MP15x lines More info.png ecosystem release ≥ v5.0.0 More info.png :

  • CFG_STM32MP1_OPTEE_IN_SYSRAM={n|y}: See warning section below and STM32MP15x lines for details (default is n).
    Note that when CFG_STM32MP1_OPTEE_IN_SYSRAM=n, CFG_WITH_USER_TA default value is n,
    and when CFG_STM32MP1_OPTEE_IN_SYSRAM=y, CFG_WITH_USER_TA default value is y.
  • CFG_STM32MP15_HUK={n|y}: disable/enable reading of OP-TEE's HUK (Hardware Unique Key) from BSEC fuses.
  • CFG_STM32_HUK_FROM_DT={n|y}: disable/enable reading of HUK location in BSEC fuses from OP-TEE's embedded Device Tree.
  • CFG_STM32_HUK_TESTKEY={n|y}: disable/enable use of a test (default is y)
    Supersedes CFG_OTP_HW_TESTKEY used in before ecosystem release v5.0.0 More info.png .


Info white.png Information

For ecosystem release ≤ v3.0.0 compatibility:
It is still possible to generate the the STM32 binary files with an option flag:
CFG_STM32MP15x_STM32IMAGE=1: Generate the STM32 files for ecosystem release ≤ v3.0.0 compatibility.


Warning white.png Warning

"To enable OP-TEE secure service for STM32MP15x lines More info.png on ecosystem release ≥ v5.0.0 More info.png , one must configure OP-TEE to execute in secure SYSRAM. TF-A boot loader must also be configured to load OP-TEE in internal SYSRAM, not is DDR.
To make OP-TEE for STM32MP15x lines More info.png to execute in SYSRAM, one shall:

  • enable OP-TEE configuration switch CFG_STM32MP1_OPTEE_IN_SYSRAM=y
  • enable TF-A configuration switch STM32MP1_OPTEE_IN_SYSRAM=1 for both TF-A BL2 and TF-A FIP images.

Note: internal memory size constrains the debug support level that can be provided.

5.2.5. Troubleshoot[edit source]

The Developer Package toolchain may report dependency error in the traces such as:

 make PLATFORM=stm32mp1 ...
arm-ostl-linux-gnueabi-ld.bfd: unrecognized option '-Wl,-O1' 
arm-ostl-linux-gnueabi-ld.bfd: use the --help option for usage information
core/arch/arm/kernel/link.mk:165: recipe for target 'build/arm-plat-stm32mp1/core/tee.elf' failed
make: *** [build/arm-plat-stm32mp1/core/tee.elf] Error 1

This is linked to default CFLAGS and LDFLAGS exported by SDK. Just remove them from the environment and rebuild

 unset -v CFLAGS LDFLAGS 

Other reported issues:

 make PLATFORM=stm32mp1 ...
arm-openstlinux_weston-linux-gnueabi-ld.bfd: cannot find libgcc.a: No such file or directory

To overcome the issue, add the directive CFLAGS32=--sysroot=$SDKTARGETSYSROOT or CFLAGS64=--sysroot=$SDKTARGETSYSROOT, depending on target architecture. For example, :

 cd <optee-os>
 make PLATFORM=stm32mp1 \
           CFG_EMBED_DTB_SOURCE_FILE=stm32mp157c-ev1.dts \
           CFG_TEE_CORE_LOG_LEVEL=2 \
           CFLAGS32=--sysroot=${SDKTARGETSYSROOT} \
           O=build all

5.3. Build commands for other OP-TEE components[edit source]

This section describes how the several OP-TEE components (excluding OP-TEE OS described in above section) can be built. All those components generate files targeting the embedded Linux OS based filesystem (i.e the rootfs). These files are the secure Trusted Applications (TAs) binaries as well as non-secure Client Applications (CAs), libraries and test files.

There are several ways to build the OP-TEE components. The examples given below refer to OP-TEE client, test and examples source file tree paths as <optee-client>, <optee-test> and <optee-examples>.

Building these components expect, at least for the trusted applications, that the OP-TEE OS was built and the generated TA development kit is available at <optee-os>/build/export-ta_arm32/.

It is recommended to use CMake for building the Linux userland part whereas secure world binaries (TAs) must be build from their GNU makefiles as the OP-TEE project has not yet ported the secure world binaries build process over CMake.

5.3.1. Build the secure components[edit source]

Build the TAs: This step expects OP-TEE OS is built to generate the 32bit TA development kit. Assuming OP-TEE OS was built at path <optee-os>/build, the TA development kit is available from path <optee-os>/build/export-ta_arm32/.

Instructions below build and copy the Trusted Application binaries to a local ./target/ directory that can be used to populate the target filesystem.

 export TA_DEV_KIT_DIR=$PWD/optee_os/build/export-ta_arm32
 mkdir -p ./target/lib/optee_armtz
 for f in optee_test/ta/*/Makefile; do \
            make -C `dirname $f` O=build; \
            cp -f `dirname $f`/build/*.ta ./target/lib/optee_armtz; \
      done

Content in local directory ./target/ are the TA binary files:

 tree target/
target
└── lib
  └── optee_armtz
   ├── 614789f2-39c0-4ebf-b235-92b32ac107ed.ta
   ├── 731e279e-aafb-4575-a771-38caa6f0cca6.ta
   └── (...)

These files need to be copied to the the target filesystem.

5.3.2. Build the non-secure components[edit source]

Download the OP-TEE source files in a base directory and create a CMakeLists.txt file in the base directory that lists all package to be built through CMake. For example:

 ls
optee_client
optee_examples
optee_os
optee_test
CMakeLists.txt
 cat CMakeLists.txt
add_subdirectory (optee_client)
add_subdirectory (optee_test)
add_subdirectory (optee_examples)
 

From base directory, run cmake then make. The example below also creates the tree file system ./target/ that is populated with files generated that need to be installed in the target file system.
Note this examples also sets the toolchain environment:

 cmake -DOPTEE_TEST_SDK=$PWD/optee_os/build/export-ta_arm32 \
            -DCMAKE_INSTALL_PREFIX=  -DCMAKE_BUILD_TYPE=Release -DBUILD_SHARED_LIBS=y
 make
 make DESTDIR=target install 

Note the empty CMAKE_INSTALL_PREFIX value to get thing installed from root /, not from /usr/. DESTDIR=target makes the embedded files be populated in the local ./target/ directory.

Note also that stm32mp1 expects tool tee-supplicant to be located in directory /usr/bin whereas CMake installs it in directory /usr/sbin. To overcome this issue, one can build a link to the effective location, i.e:

 ln -s ../bin/tee-supplicant target/sbin/tee-supplicant

Once done, local directory ./target/ contains the files to be copied in the target filesystem.

 tree target/
target/
├── bin
│   ├── benchmark
│   ├── optee_example_acipher
│   ├── optee_example_aes
│   ├── optee_example_hello_world
│   ├── optee_example_hotp
│   ├── optee_example_random
│   ├── optee_example_secure_storage
│   ├── tee-supplicant
│   └── xtest
├── include
│   ├── tee_bench.h
│   ├── tee_client_api_extensions.h
│   ├── tee_client_api.h
│   └── teec_trace.h
├── lib
│   ├── libteec.so -> libteec.so.1
│   ├── libteec.so.1 -> libteec.so.1.0.0
│   └── libteec.so.1.0.0
│   └── optee_armtz
│       └── (...)                 # This directory was previously filled with TAs
└── sbin
    └── tee-supplicant -> ../bin/tee-supplicant

6. Update OP-TEE boot images[edit source]

OP-TEE boot images are part of the FIP binary.
The next step to deploy the OP-TEE OS is to update the FIP binary following the FIP update process.

7. Update OP-TEE Linux files[edit source]

7.1. Update on board[edit source]

The other OP-TEE images are stored in the target filesystem.

For example, if using an SD card as target boot media, the card can be plugged in its PC card reader and the images copied. The files can be simply copied into the mounted rootfs.

7.2. Update in a SD card[edit source]

The OP-TEE files that need to be copied to the target filesystem were installed in a local directory ./target/.

They can now be copied to the target SD card rootfs partition once the SD card is plugged to the host computer and its filesystems are mounted in the host, i.e

 cp -ar target/* /media/$USERNAME/rootfs/

8. Update your boot device (including SD card on the target)[edit source]

Refer to the STM32CubeProgrammer documentation to update your target.

9. References[edit source]