This article lists documents that apply to the STM32 MPU ecosystem release of the STM32MP25x lines . Those documents are generally referenced into other wiki pages.
All the resources for the STM32MP2 series are located in the STM32MP2 series web page.
Reference | Name | Link | |
---|---|---|---|
Application notes | |||
AN5489 | AN5489 - Getting started with STM32MP25xx lines hardware development | AN5489.pdf | |
AN5723 | AN5723 - Guidelines for DDR memory configuration on STM32MP2 MPUs | AN5723.pdf | |
AN5724 | AN5724 - Guidelines for DDR memory routing on STM32MP2 MPUs | AN5724.pdf | |
AN5718 | AN5718 - Migrating from STM32MP15x lines to STM32MP25x lines MPUs | AN5718.pdf | |
AN5726 | AN5726 - Guidelines for using low-power modes on STM32MP2 MPUs | *AN5726.pdf | |
AN5827 | AN5827 - Guidelines for entering RMA state on MPU series | Under preparation | |
AN5727 | AN5727 - How to use STPMIC25 for a wall adapter powered application on STM32MP25x lines MPUs | Under preparation | |
AN5730 | AN5730 - Guidelines for measuring system power consumption on STM32MP2 MPUs | Under preparation | |
AN6115 | AN6115 - How to connect STPMIC25 unused pins | AN6115.pdf | |
AN6116 | AN6116 - STPMIC25 BOM details | AN6116.pdf | |
AN6128 | AN6128 - STPMIC25 PCB layout guidelines | AN6128.pdf | |
Datasheets[1] | |||
DS14284 | STM32MP25xC/F Datasheet | DS14284.pdf | |
DS14285 | STM32MP25xA/D Datasheet | DS14285.pdf | |
DS14278 | STPMIC25 datasheet |
DS14278.pdf | |
Errata sheets | |||
ES0598 | STM32MP25x ErrataSheet | ES0598.pdf | |
Reference manuals[1] | |||
RM0457 | STM32MP25 reference manual (STM32MP25xx advanced Arm®-based 32/64-bit MPUs) |
RM0457.pdf | |
Boards schematics | |||
PM0264 | STM32 Cortex®-M33 MCUs and MPUs programming manual | PM0264.pdf | |
Boards schematics | |||
MB1936 schematics | STM32MP257F-EV1 board revD schematics with STM32MP25F RevB 18x18 package | [1] | |
B-CAMS-IMX schematics | Camera module bundle schematics | [2] | |
B-LVDS7-WSVGA schematics | LVDS TFT LCD module schematics | [3] | |
STM32MP25F-DK schematics | STM32MP257F-DK board schematics example with STM32MP25F RevY 14x14 package | [4] | |
DDR routing examples schematics | Additional DDR memory routing examples | * | |
User manuals | |||
UM3359 | STM32MP2357F-EV1 User Manual | UM3359.pdf | |
UM3354 | B-CAMS-IMX Camera module bundle User Manual | UM3354.pdf |
- ↑ 1.0 1.1 The part numbers are specified in STM32MP25 microprocessor part numbers