1. Article purpose[edit source]
The purpose of this article is to explain how to configure the DFSDM internal peripheral when the peripheral is assigned to Linux® OS, and in particular:
- How to configure the DFSDM peripheral to enable filters and associated channels
- How to configure the board, e.g. serial interface input/output pins
The configuration is performed using the device tree mechanism.
It is used by the DFSDM Linux driver which registers the relevant information in IIO and ALSA frameworks.
If the peripheral is assigned to another execution context, refer to How to assign an internal peripheral to a runtime context article for guidelines on peripheral assignment and configuration.
2. DT bindings documentation[edit source]
The DFSDM maybe used as various functions: ADC and DMIC (for audio).
Each one is represented by a separate compatible string, documented in STM32 DFSDM device tree bindings[1].
The external analog frontend (e.g. sigma-delta modulator) is documented in Device-Tree bindings for sigma delta modulator[2]
3. DT configuration[edit source]
This hardware description is a combination of STM32 microprocessor and board device tree files. See Device tree for more explanations on device tree file split.
The STM32CubeMX can be used to generate the board device tree. Refer to How to configure the DT using STM32CubeMX for more details.
3.1. DT configuration (STM32 level)[edit source]
DFSDM nodes are declared in stm32mp151.dtsi[3] for STM32MP15x lines , and stm32mp131.dtsi[4] for STM32MP13x lines .
- DT root node ('dfsdm') describes the ADC hardware block parameters such as registers area, clocks.
- DT child nodes ('dfsdm0', 'dfsdm1', ...) describe each filter independently: compatible string, interrupts, DMAs.
dfsdm: dfsdm@4400d000 { compatible = "st,stm32mp1-dfsdm"; ... /* common resources in 'dfsdm' root node. */ dfsdm0: filter@0 { compatible = "st,stm32-dfsdm-adc"; /* can either be st,stm32-dfsdm-(adc or dmic) */ ... /* private resources in 'dfsdm0' child node. */ } dfsdm1: filter@1 { ... }
3.2. DT configuration (board level)[edit source]
Follow the sequences described in the below chapters to configure and enable the DFSDM on your board.
3.2.1. Common resources for all DFSDM filters[edit source]
Configure the 'dfsdm' DT root node:
- Enable the DT root node for the DFSDM, by setting status = "okay".
- Configure the pins in use via pinctrl, by setting pinctrl-0, pinctrl-1 and pinctrl-names.
- Configure the SPI clock output frequency, by setting spi-max-frequency (optional: only for SPI master mode).
- Configure the audio clock to be used, by setting clocks and clock-names (optional: to use more accurate clock for audio).
&dfsdm { clocks = <&rcc DFSDM_K>, <&rcc ADFSDM_K>; clock-names = "dfsdm", "audio"; };
3.2.2. Private resources for each DFSDM filter[edit source]
Configure the filter(s) DT child node(s):
- Enable the DT child node(s) for the DFSDM filter(s) in use, by setting status = "okay".
- Override the compatible string by setting "st,stm32-dfsdm-dmic" (optional: only for audio digital microphone).
- Enable the channel(s), by setting st,adc-channels = <0 1 2...>.
- Configure the channel(s) by setting st,adc-channel-names, st,adc-channel-types (e.g. SPI or manchester) and st,adc-channel-clk-src (e.g. external or internal).
- Configure the filter order, by setting st,filter-order.
3.2.3. Additional configuration for DFSDM ADC[edit source]
The DFSDM ADC device has an external analog front-end, the sigma delta modulator.
Configure the external sigma delta modulator for each channel (optional, not needed for audio digital microphone):
- Add your_sd_modulator DT node in the board dts file (see the generic sd-modulator[2] example here after).
- Add io-channels = <&your_sd_modulator> to the DFSDM filter child node in order to assign it to the filter channel(s).
3.2.4. Additional configuration for DFSDM audio[edit source]
Additional child nodes must be added for audio soundcard configuration.
3.3. DT configuration examples[edit source]
3.4. DFSDM ADC DT configuration example[edit source]
The example below shows how to configure the DFSDM ADC channel 1, assigned to DFSDM filter 0:
- Declare pins used in pinctrl DT node (see Pinctrl device tree configuration):
- Configure PB13 as DFSDM CLKOUT alternate function (AF3 by default, ANALOG for low-power mode).
- Configure PC3 as DFSDM DATA1 alternate function (AF3 by default, ANALOG for low-power mode).
dfsdm_clkout_pins_a: dfsdm-clkout-pins-0 { pins { pinmux = <STM32_PINMUX('B', 13, AF3)>; /* DFSDM_CKOUT */ bias-disable; drive-push-pull; slew-rate = <1>; }; }; dfsdm_clkout_sleep_pins_a: dfsdm-clkout-sleep-pins-0 { pins { pinmux = <STM32_PINMUX('B', 13, ANALOG)>; /* DFSDM_CKOUT */ }; };
dfsdm_data1_pins_a: dfsdm-data1-pins-0 { pins { pinmux = <STM32_PINMUX('C', 3, AF3)>; /* DFSDM_DATA1 */ }; }; dfsdm_data1_sleep_pins_a: dfsdm-data1-sleep-pins-0 { pins { pinmux = <STM32_PINMUX('C', 3, ANALOG)>; /* DFSDM_DATA1 */ }; };
- Add sd-modulator[2] in the board dts file.
sd_adc1: adc-1 {
compatible = "sd-modulator";
#io-channel-cells = <0>;
};
- Configure and enable DFSDM, configure channel 1 to use SPI (rising edge), associate it to filter0.
&dfsdm { pinctrl-names = "default", "sleep"; pinctrl-0 = <&dfsdm_clkout_pins_a &dfsdm_data1_pins_a>; /* default pins */ pinctrl-1 = <&dfsdm_clkout_sleep_pins_a &dfsdm_data1_sleep_pins_a>; /* sleep pins for low-power mode */ spi-max-frequency = <2048000>; /* desired maximum clock rate */ status = "okay"; dfsdm0: filter@0 { st,adc-channels = <1>; /* Assign channel 1 to this filter */ st,adc-channel-names = "in1"; /* Give it a name */ st,adc-channel-types = "SPI_R"; /* SPI data on rising edge */ st,adc-channel-clk-src = "CLKOUT_F"; /* internal clock source used for conversion */ io-channels = <&sd_adc1>; /* phandle to the external sd-modulator */ st,filter-order = <1>; status = "okay"; }; };
3.5. DFSDM audio DT configuration example[edit source]
Two microphones can be multiplexed on the same DFSDM input line, where one microphone is sampled on the SPI clock rising edges, and the other on the SPI clock falling edges. By convention rising edge corresponds to the left channel and falling edge to the right channel. For a given DFSDM input line DATAn, the left channel is fed to the DFSDM channel n, while the right channel is fed to the DFSDM channel n-1. For each channel a muxer allows to select either the left or right channel. The st,adc-alt-channel DT property is used to configure this channel input muxer.
A full example of DFSDM DT configuration for audio can be found in Soundcard_configuration#Static_configuration_2 DT sample.
4. How to configure the DT using STM32CubeMX[edit source]
The STM32CubeMX tool can be used to configure the STM32MPU device and get the corresponding platform configuration device tree files.
The STM32CubeMX may not support all the properties described in the above DT bindings documentation paragraph. If so, the tool inserts user sections in the generated device tree. These sections can then be edited to add some properties and they are preserved from one generation to another. Refer to STM32CubeMX user manual for further information.
5. References[edit source]
Please refer to the following links for additional information:
- ↑ Documentation/devicetree/bindings/iio/adc/st,stm32-dfsdm-adc.yaml , STM32 DFSDM device tree bindings
- ↑ 2.0 2.1 2.2 Documentation/devicetree/bindings/iio/adc/sigma-delta-modulator.yaml , Generic Device-Tree bindings for sigma delta modulator
- ↑ arch/arm/boot/dts/stm32mp151.dtsi , STM32MP151 device tree file
- ↑ arch/arm/boot/dts/stm32mp131.dtsi , STM32MP131 device tree file