1. Article purpose[edit source]
The purpose of this article is to
- briefly introduce the BSEC peripheral and its main features
- indicate the level of security supported by this hardware block
- explain how each instance can be allocated to the three runtime contexts and linked to the corresponding software components
- explain, when necessary, how to configure the BSEC peripheral.
2. Peripheral overview[edit source]
The BSEC peripheral is used to control an OTP (one time programmable) fuse box, used for on-chip non-volatile storage for device configuration and security parameters.
2.1. Features[edit source]
Refer to STM32MP15 reference manuals for the complete list of features, and to the software components, introduced below, to see which features are implemented.
2.2. Security support[edit source]
The BSEC is a secure peripheral.
3. Peripheral usage and associated software[edit source]
3.1. Boot time[edit source]
The BSEC is configured at boot time to set up platform security.
3.2. Runtime[edit source]
3.2.1. Overview[edit source]
The BSEC instance is a system peripheral and is controlled by the Arm® Cortex®-A7 secure:
3.2.2. Software frameworks[edit source]
Internal peripherals software table template
| Security | BSEC | OP-TEE BSEC driver | Linux NVMEM framework | | |- |}
3.2.3. Peripheral configuration[edit source]
The configuration is based on Device tree, please refer to BSEC device tree configuration article.
It can be applied by the firmware running in a secure context, done in TF-A or in OP-TEE.
It can also be configured by Linux® kernel, please refer to NVMEM overview article.
3.2.4. Peripheral assignment[edit source]
Internal peripherals assignment table template
| rowspan="1" | Security | rowspan="1" | BSEC | BSEC | ✓ | ✓ | | |-
|}
4. How to go further[edit source]
5. References[edit source]