This article explains the way STM32CubeIDE is managing Yocto SDK provided by OpenSTLinux.
1. Overview[edit source]
Two flavors are proposed for installing Yocto SDK:
- the Yocto SDK is already installed on the host machine, after a download of the STM32MP1 OpenSTLinux Developer Package. In that case, only a setup is needed for STM32CubeIDE to use it.
- the Yocto SDK is not present on the host platform, it can be installed via STM32CubeIDE:
- embedded inside the STM32CubeIDE; Yocto SDK removal is managed by STM32CubeIDE
- on host platform disk, outside STM32CubeIDE scope; Yocto SDK removal under final user responsibility
2. Using already installed Yocto SDK[edit source]
We suppose here
3. Installing Yocto SDK from STM32CubeIDE[edit source]
.