1. Article purpose[edit source]
The purpose of this article is to:
- briefly introduce the DDRCTRL and DDRPHYC peripherals and their main features
- indicate the level of security supported by those hardware blocks
- explain how they can be allocated to the three runtime contexts and linked to the corresponding software components
- explain, when necessary, how to configure the DDRCTRL and DDRPHYC peripherals
2. Peripheral overview[edit source]
DDRCTRL and DDRPHYC peripherals are used to configure the physical interface to the external DDR memory.
2.1. Features[edit source]
Refer to STM32MP15 reference manuals for the complete features list, and to the software components, introduced below, to know which features are really implemented.
2.2. Security support[edit source]
DDRCTRL and DDRPHYC are secure aware (under ETZPC control).
The access to the DDR memory can be filtered via TZC controller: for instance, it is possible to forbid the access from the Cortex®-M4 to the DDR region used by the Cortex®-A7.
3. Peripheral usage and associated software[edit source]
3.1. Boot time[edit source]
DDRCTRL and DDRPHYC are kept secure and used by the FSBL to initialize the access to the DDR where it loads the SSBL (U-Boot) for execution.
STMicroelectronics wants to make the DDR memory configuration as easy as possible, for this reason a DDR tuning function is available in STM32CubeMX tool in order to generate the device tree that is given to the FSBL to perform this initialization.
3.2. Runtime[edit source]
3.2.1. Overview[edit source]
DDRCTRL and DDRPHYC are accessed at runtime by the secure monitor (from the FSBL or OP-TEE) to put the DDR in self-refresh state before going into Stop or Standby low power mode.
On Standby exit, the ROM code loads the FSBL that configures again the DDRCTRL and DDRPHYC before proceeding with the wake up procedure, till Linux.
The TZC controller is configured by TF-A to split the DDR in two regions :
- the first region, the biggest one, is reserved for Linux (Cortex-A7 non-secure context)
- the second one, 32 MB wide, is dedicated for OP-TEE (Cortex-A7 secure context). This area is used by its pager as a cache area from where it can load trusted applications that are authenticated in the SYSRAM internal memory before execution.
This split is visible in the overall memory mapping.
3.2.2. Software frameworks[edit source]
Internal peripherals software table template
| Core/RAM | DDR via DDRCTRL | Memory mapping | Memory mapping | | |- |}
3.2.3. Peripheral configuration[edit source]
The configuration is applied during boot time by the FSBL (see Boot chains overview): TF-A or U-Boot SPL.
The configuration by itself (values for DDRCTL and DDRPHY registers) is generated via STM32CubeMX tool in the device tree for the FSBL, according to the DDR configuration (type, size, frequency, speed grade).
3.2.4. Peripheral assignment[edit source]
Internal peripherals assignment table template
| rowspan="1" | Core/RAM | rowspan="1" | DDR via DDRCTRL | DDR | ✓ | ✓ | | |-
|}
4. How to go further[edit source]
Device tree binding of DDR node:
- available in U-boot source : doc/device-tree-bindings/ram/st,stm32mp1-ddr.txt