SYSRAM internal memory

Revision as of 17:28, 31 October 2023 by Registered User (→‎On {{MicroprocessorDevice | device=2}})
Applicable for STM32MP13x lines, STM32MP15x lines

1. Article purpose[edit source]

The purpose of this article is to:

  • briefly introduce the SYSRAM internal memory peripheral and its main features,
  • indicate the peripheral instances assignment at boot time and their assignment at runtime (including whether instances can be allocated to secure contexts),
  • list the software frameworks and drivers managing the peripheral,
  • explain how to configure the peripheral.

2. Peripheral overview[edit source]

The SYSRAM peripheral is an internal memory peripheral. It is physically located near the Arm® Cortex-A to optimize the core performance.

  • STM32MP13x lines More info.png SYSRAM is 128-Kbyte wide
  • STM32MP15x lines More info.png SYSRAM is 256-Kbyte wide
  • STM32MP2 series SYSRAM is 256-Kbyte wide

On STM32MP1 series, the SYSRAM is protected by ETZPC firewall. SYSRAM access are secure by default and can be split into 2 memory regions with a 4-Kbyte granularity:

  • a low secure region
  • a high non-secure region

On STM32MP2 series, the SYSRAM is protected by RISAB memory firewall, allowing to create some 4-Kbyte granularity memory regions with different access rights to share SYSRAM between the different execution contexts of the platform. By default, SYSRAM access is defined as Cortex-A35 secure.

Refer to the STM32 MPU reference manuals for the complete list of features, and to the software frameworks and drivers, introduced below, to see which features are implemented.

3. Peripheral usage[edit source]

This chapter is applicable in the scope of the OpenSTLinux BSP running on the Arm® Cortex®-A processor(s), and the STM32CubeMPU Package running on the Arm® Cortex®-M processor.

3.1. Boot time assignment[edit source]

3.1.1. On STM32MP13x lines More info.png[edit source]

The ROM code leaves the SYSRAM secure when it jumps to the entry point of the FSBL that it just loaded into the SYSRAM.
The FSBL does not have to keep any context in SYSRAM when it jumps to the SSBL: each boot stage is independent from the other.

Click on How to.png to expand or collapse the legend...

Check boxes illustrate the possible peripheral allocations supported by STM32 MPU Embedded Software:

  • means that the peripheral can be assigned to the given boot time context.
  • means that the peripheral is assigned by default to the given boot time context and that the peripheral is mandatory for the STM32 MPU Embedded Software distribution.
  • means that the peripheral can be assigned to the given boot time context, but this configuration is not supported in STM32 MPU Embedded Software distribution.
  • is used for system peripherals that cannot be unchecked because they are hardware connected in the device.

The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possibilities might be described in STM32 MPU reference manuals.

Domain Peripheral Boot time allocation Comment How to.png
Instance Cortex-A7
secure
(ROM code)
Cortex-A7
secure
(TF-A BL2)
Cortex-A7
non-secure
(U-Boot)
Core/RAM SYSRAM SYSRAM

3.1.2. On STM32MP15x lines More info.png[edit source]

The ROM code mainly configures the SYSRAM as a secure peripheral during its execution. It uses 9 Kbytes located at the beginning of the SYSRAM to store its read and write data. Among them, it stores the boot context in the first 512 bytes of SYSRAM: this boot context contains several information (such as the selected boot device) and pointers to the ROM code exported services (used for secure boot authentication). The ROM code loads the FSBL just after the boot context, into the remaining 247 Kbytes of SYSRAM, and eventually branches the Cortex®-A7 core 0 execution to this FSBL.
The FSBL code can use the whole SYSRAM, but it must take care not to overwrite the boot context before taking it into account.


Click on How to.png to expand or collapse the legend...

Check boxes illustrate the possible peripheral allocations supported by STM32 MPU Embedded Software:

  • means that the peripheral can be assigned to the given boot time context.
  • means that the peripheral is assigned by default to the given boot time context and that the peripheral is mandatory for the STM32 MPU Embedded Software distribution.
  • means that the peripheral can be assigned to the given boot time context, but this configuration is not supported in STM32 MPU Embedded Software distribution.
  • is used for system peripherals that cannot be unchecked because they are hardware connected in the device.

The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possibilities might be described in STM32 MPU reference manuals.

Domain Peripheral Boot time allocation Comment How to.png
Instance Cortex-A7
secure
(ROM code)
Cortex-A7
secure
(TF-A BL2)
Cortex-A7
non-secure
(U-Boot)
Core/RAM SYSRAM SYSRAM

3.1.3. On STM32MP2 series[edit source]

The ROM code leaves the SYSRAM secure when it jumps to the entry point of the FSBL that it just loaded into the SYSRAM.
The FSBL does not have to keep any context in SYSRAM when it jumps to the next boot stages: each boot stage is independent from the other.

Click on How to.png to expand or collapse the legend...

  • means that the peripheral can be assigned to the given boot time context.
  • means that the peripheral is assigned by default to the given boot time context and that the peripheral is mandatory for the STM32 MPU Embedded Software distribution.
  • means that the peripheral can be assigned to the given boot time context, but this configuration is not supported in STM32 MPU Embedded Software distribution.
  • is used for system peripherals that cannot be unchecked because they are hardware connected in the device.

The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possibilities might be described in STM32MP25 reference manuals.

Domain Peripheral Boot time allocation Comment How to.png
Instance Cortex-A35
secure
(ROM code)
Cortex-A35
secure
(TF-A BL2)
Cortex-A35
non-secure
(U-Boot)
Core/RAM SYSRAM SYSRAM

3.2. Runtime assignment[edit source]

3.2.1. On STM32MP13x lines More info.png[edit source]

In OSTL distribution, the SYSRAM runtime mapping is the one reached at the end of the boot. It is consequently fully secure and can contain a secure monitor functions provided by OP-TEE secure OS to handle low power modes.

STM32MP13 embeds an on-the-fly DDR cyphering engine, the DDRMCE internal peripheral, allowing to put OP-TEE secure OS sensitive code inside the external DDR, instead of the SYSRAM.

You may decide to split the SYSRAM at runtime. In this case:

  • set the SYSRAM bottom secure, for a Cortex®-A7 secure monitor or a secure OS (such as OP-TEE)

and

  • set the SYSRAM top non-secure, for instance for using in Linux® as reserved memory


Click on How to.png to expand or collapse the legend...

STM32MP13 internal peripherals

Check boxes illustrate the possible peripheral allocations supported by STM32 MPU Embedded Software:

  • means that the peripheral can be assigned to the given runtime context.
  • means that the peripheral is assigned by default to the given runtime context and that the peripheral is mandatory for the STM32 MPU Embedded Software distribution.
  • means that the peripheral can be assigned to the given runtime context, but this configuration is not supported in STM32 MPU Embedded Software distribution.
  • is used for system peripherals that cannot be unchecked because they are hardware connected in the device.

Refer to How to assign an internal peripheral to an execution context for more information on how to assign peripherals manually or via STM32CubeMX.
The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possibilities might be described in STM32MP13 reference manuals.

Domain Peripheral Runtime allocation Comment How to.png
Instance Cortex-A7
secure
(OP-TEE)
Cortex-A7
non-secure
(Linux)
Core/RAM SYSRAM SYSRAM Shareable (multiple choices supported)

Secure section required for low power entry and exit

3.2.2. On STM32MP15x lines More info.png[edit source]

In OSTL distribution, the SYSRAM runtime mapping is the one reached at the end of the boot. It is consequently fully secure and can contain a secure OS (like OP-TEE).

You may decide to split the SYSRAM at runtime. In this case:

  • set the SYSRAM bottom secure, for a Cortex®-A7 secure monitor or a secure OS (such as OP-TEE)

and

  • set the SYSRAM top non-secure, for instance for using in Linux® as reserved memory


Click on How to.png to expand or collapse the legend...

STM32MP15 internal peripherals

Check boxes illustrate the possible peripheral allocations supported by STM32 MPU Embedded Software:

  • means that the peripheral can be assigned to the given runtime context.
  • means that the peripheral is assigned by default to the given runtime context and that the peripheral is mandatory for the STM32 MPU Embedded Software distribution.
  • means that the peripheral can be assigned to the given runtime context, but this configuration is not supported in STM32 MPU Embedded Software distribution.
  • is used for system peripherals that cannot be unchecked because they are hardware connected in the device.

Refer to How to assign an internal peripheral to an execution context for more information on how to assign peripherals manually or via STM32CubeMX.
The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possiblities might be described in STM32MP15 reference manuals.

Domain Peripheral Runtime allocation Comment How to.png
Instance Cortex-A7
secure
(OP-TEE)
Cortex-A7
non-secure
(Linux)
Cortex-M4

(STM32Cube)
Core/RAM SYSRAM SYSRAM Shareable (multiple choices supported)

Secure section required for low power entry and exit

3.2.3. On STM32MP25x lines More info.png[edit source]

In OSTL distribution, the SYSRAM runtime mapping is split into two regions.

  • one Cortex-A35 secure region dedicated to secure monitor which handles Cortex-A35 cluster
  • one Cortex-A35 non-secure region assigned to Linux kernel for HPDMA linked list management

As SYSRAM is used by ROM code during D1Standby exit low power sequence, it is not advise to assign SYSRAM to Cortex-M33 except if product doesn't plan to support Run2 and (LPLV)Stop2 low power modes.


Click on How to.png to expand or collapse the legend...

STM32MP25 internal peripherals

Check boxes illustrate the possible peripheral allocations supported by STM32 MPU Embedded Software:

  • means that the peripheral can be assigned to the given runtime context.
  • means that the peripheral is assigned by default to the given runtime context and that the peripheral is mandatory for the STM32 MPU Embedded Software distribution.
  • means that the peripheral can be assigned to the given runtime context, but this configuration is not supported in STM32 MPU Embedded Software distribution.
  • is used for system peripherals that cannot be unchecked because they are hardware connected in the device.

The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possibilities might be described in STM32MP25 reference manuals.

Domain Peripheral Runtime allocation Comment How to.png
Instance Cortex-A35
secure
(OP-TEE /
TF-A BL31)
Cortex-A35
non-secure
(Linux)
Cortex-M33
secure
(TF-M)
Cortex-M33
non-secure
(STM32Cube)
Cortex-M0+
Warning.png
(STM32Cube)
Core/RAM SYSRAM SYSRAM BL31

OP-TEE

Cortex-A35 secure section required for low power entry and exit

4. Software frameworks and drivers[edit source]

Thus, below are listed the software frameworks and drivers managing the XXX peripheral for the embedded software components listed in the above tables.

5. How to assign and configure the peripheral[edit source]

The peripheral assignment can be done via the STM32CubeMX graphical tool (and manually completed if needed).
This tool also helps to configure the peripheral:

  • partial device trees (pin control and clock tree) generation for the OpenSTLinux software components,
  • HAL initialization code generation for the STM32CubeMPU Package.

The configuration is applied by the firmware running in the context in which the peripheral is assigned.