TF-A BL2 Trusted Board Boot

Revision as of 15:40, 6 June 2022 by Registered User (→‎RoT)
Applicable for STM32MP13x lines, STM32MP15x lines

1. Article purpose[edit source]

The main purpose of this article is to explain how the the Trusted Board Boot support is managed in the Trusted Firmware-A component and the STM32 MPU specific implementation.

2. Overview[edit source]

Trusted Firmware-A as a strong focus on security management. It defines a reference implementation of secure software and implements the Trusted Board Boot requirements[1] specified by Arm®. TF-A BL2 implements an authentication framework that uses a defined Chain of Trust (CoT) based on Arm® TBBR requirements to achieve a secure boot.


The authentication framework is enabled using a dedicated Trusted Firmware-A build flag in the BL2 command line:
TRUSTED_BOARD_BOOT=1

3. Chain of Trust (CoT)[edit source]

To manage the Trusted Board Boot requirements, Trusted Firmware-A manages a Public Key Infrastructure (PKI) model so called Chain of Trust.

The Chain of Trust is following X509.v3[2] certificate standard adding some specific extensions and relies on a public key infrastructure (PKI) generating self-signed certificates. The Root of Trust of this chain is based on a Root of Trust Public Key (ROTPK).

Chain of Trust manages 2 certificate types:

  • Key certificate used to verify public keys which have been used to sign content certificates.
  • Content certificate used to store the hash of a boot loader image.

Both certificates contains a non volatile counter value that can be used for anti-rollback protection.

TF-A BL2 implements a default certificate chain to describe the PKI topology. It uses the firmware configuration framework to register into TF-A BL2 the chaining implementation based on default device tree include fdts/cot_descriptors.dtsi . It describes the chain of trust following the specified bindings.

Once generated, all the certificates will be part of the FIP which will be updatable independently.

The certificate generation uses the default Trusted Firmware-A certificate creation tool.

4. Authentication Framework[edit source]

Trusted Firmware-A design an authentication framework to centralize all secure mecanism relying on Authentication Module(AM), Image Parser Module (IPM) and Crypto Module (CM). This generic framework based on certificate chain of trust is responsible of:

  • Allocating memory for loaded image
  • Identify the image and load it
  • Check the integrity
  • Authenticate / [ Decrypt ] the image
  • Extract the CoT information if needed to authenticate next image in CoT.

A reference implementation as been integrated in Trusted Firmware-A using mbedTLS[3] for:

  • the Image Parser Module(IPM) using x509.v3 certificate (Image Parser Library (IPL))
  • the Crypto Module(CM) with a dedicated (Cryptographic Library (CL)

5. STM32 MPU implementation[edit source]

5.1. CoT[edit source]

STM32 MPU uses the standard Arm&regTBBR PKI implementation by including the generic fdts/cot_descriptors.dtsi in the TF-A BL2 device tree board file.

Caption
Warning white.png Warning
This CoT description is defined in the BL2 device tree so it cannot be changed without any TF-A BL2 update

5.1.1. Define a custom CoT[edit source]

It is possible to update the CoT by changing the chain of certificate. This must be done accordingly at:

5.2. RoT[edit source]

The Root of Trust Public Key (ROTPK) used as reference for the chain of trust is located in the STM32MP1 OTP.
The STM32MP1 platform plat_get_rotpk_info implementation is made in : plat/st/common/stm32mp_trusted_boot.c .

On STM32MP15x lines More info.png, the hash of the public key used is located in the PKH section of OTP.

On STM32MP13x lines More info.png, the key revocation mecanism allows multiple root key definitions on the platform.
The public key hash used is located in the Trusted Firmware-A BL2 STM32 header which is located in SRAM3. The multiple public key hashes are used to generate the final hash store in the PKHTH section of OTP which is controlled to confirm key integrity.

Warning white.png Warning
Because the default implementation uses the same public key as the ROM Code, Trusted Firmware-A BL2 doesn't manage key revocation.

5.2.1. Define a custom RoT[edit source]

It is possible to change the ROTPK to have a dedicated public key for the CoT by changing the following:

 static int get_rotpk_hash(void *cookie, uint8_t *hash, size_t len)
 {
   if (cookie != NULL) {
      return -EINVAL;
   }
   return copy_hash_from_otp(<New_OTP_define>, hash, len);
 }

5.3. Non volatile counters[edit source]

Each certificate embeds a non volatile counter value that is checked to control anti-rollback mechanism.
There are 2 non volatile counters: - Trusted Non volatile counter - Non trusted volatile counter

On STM32MP1, TAMP monotonic counter is used to store the backup value which requires backup battery to maintain the content. It is mandatory to align the same value between trusted and non trusted value as only one counter is used as reference.

5.4. STM32 FW Encryption[edit source]

On STM32MP13x lines More info.png, it is possible to encrypt binary in the FIP.

The binary that can be encrypted must be defined in the plat/st/common/stm32mp_fconf_io.c .

Trusted Firmware-A provides a tool to manage the firmware encryption.

The current implementation is to use the same key as the ROM Code which is located in EDMK section of OTP.

5.4.1. Define a custom Encryption Key[edit source]

A new decryption key can be defined by updating:

5.5. STM32 Crypto Library (CL)[edit source]

The STM32MP1 platform supports ECDSA based certificate with SHA256 signature.
A dedicated Cryptographic Library was implemented for STM32 MPU to use hardware accelerators plat/st/common/stm32mp_crypto_lib.c . It requires mbedTLS API to parse ASN1 certificate.

The Cryptographic Library (CL) defined the functions to:

  • On STM32MP15x lines More info.png:
    • Verify a digital signature : ECDSA based authentication (P256NIST or BRAINPOOL_P256T1) uses HASH and ROM Code secure services.
    • Verify a HASH : HASH calculation uses HASH
  • On STM32MP13x lines More info.png:
    • ECDSA based authentication (P256NIST or BRAINPOOL_P256T1) uses HASH and PKA hardware accelerators.
    • Verify a HASH : HASH calculation uses HASH
    • Decrypt and verify a binary using SAES (Limited to AES GCM mode)

5.6. STM32 MPU build options[edit source]

To manage the Trusted Board Boot, TF-A_BL2 must be built using TRUSTED_BOARD_BOOT=1.

When TRUSTED_BOARD_BOOT=1 has been set, the FIP must embed all the certificates.

It is possible to directly generate the FIP with all the necessary certificates using specific build flags GENERATE_COT=1.

It is also possible to specify external keys otherwise, missing keys will be generated by the tool.

Description Makefile Flag certificate creation tool args
Root public key (Mandatory) ROT_KEY --rot-key
Algorithm used for key generation KEY_ALG --key-alg
Algorithm used for hash HASH_ALG --hash-alg
Trusted word key TRUSTED_WORLD_KEY --trusted-world-key
Non Trusted word key NON_TRUSTED_WORLD_KEY --non-trusted-world-key
Trusted Firmware Non volatile counter TFW_NVCTR_VAL --tfw-nvctr
Non Trusted Firmware Non volatile counter NTFW_NVCTR_VAL --ntfw-nvctr
Trusted key certificate TRUSTED_KEY_CERT --trusted-key-cert


Warning white.png Warning
The content of each certificate is different and requires all arguments to regenerate it. The FIP is directly constructed with the correct output

6. References[edit source]