The article is written specifically for helping to transfer any file from a Working PC to the STM32MP157C-DK2 using "Tera Term" (http://tera-term.en.lo4d.com/). Please download and install Tera-Term on your Windows PC and follow below steps -
- Plug the power cable to power-up the STM32MP157C-DK2 board.
- Connect the Discovery Kit to your PC via USB micro B type cable through CN11.
- Check the Virtual COM port number visible in the device manager. For example, in the snapshot below, the COM port number is 14.
- Open Tera-Term on your PC and select the COM port (as found in step 3 above). The baud rate should be 115200 baud. The virtual terminal (remote access) will appear as shown in below snapshot.
- To transfer a file from host PC to Discovery Kit,click on File menu on top left corner of the Tera-Tem window and go to File>>Transfer>>ZMODEM>>Send. Refer to below snapshot –
- Select the file from pop up window (example in snapshot below) to be transferred and click on the ‘Open’ tab.
- A progress bar will show the status of file transfer. Snapshot below-
- The transferred file will be available at location : /home/root on the discovery board