Template:ArticleMainWriter Template:ArticleApprovedVersion
1. Purpose[edit source]
This article gives an example of a driver that controls GPIOs from kernel space.
Sample source files are provided as examples: kernel module (driver), device tree and Makefile.
This example is available for STM32MP15_Evaluation_boards or STM32MP15_Discovery_kits
2. Code[edit source]
2.1. Objective[edit source]
Sample gpiolib usage code that makes an LED blink for 20 seconds.
2.2. Device tree[edit source]
dummy_device { compatible = "st,dummy"; status = "okay"; greenled-gpios = <&gpioa 14 0>; };
See GPIO_device_tree_configuration for more details of GPIO use in a device tree.
2.3. Kernel module code[edit source]
#include <linux/module.h> #include <linux/kernel.h> #include <linux/delay.h> #include <linux/gpio/consumer.h> #include <linux/platform_device.h> struct gpio_desc *red, *green; static int gpio_init_probe(struct platform_device *pdev) { int i = 0; printk("GPIO example init\n"); /* "greenled" label is matching the device tree declaration. OUT_LOW is the value at init */ green = devm_gpiod_get(&pdev->dev, "greenled", GPIOD_OUT_LOW); /* blink of the green led */ while (i < 10) { ssleep(1); gpiod_set_value(green, 1); ssleep(1); gpiod_set_value(green, 0); i++; } return(0); } static int gpio_exit_remove(struct platform_device *pdev) { printk("GPIO example exit\n"); return(0); } /* this structure does the matching with the device tree */ /* if it does not match the compatible field of DT, nothing happens */ static struct of_device_id dummy_match[] = { {.compatible = "st,dummy"}, {/* end node */} }; static struct platform_driver dummy_driver = { .probe = gpio_init_probe, .remove = gpio_exit_remove, .driver = { .name = "dummy_driver", .owner = THIS_MODULE, .of_match_table = dummy_match, } }; module_platform_driver(dummy_driver); MODULE_AUTHOR("Bernard Puel"); MODULE_DESCRIPTION("Gpio example"); MODULE_LICENSE("GPL"); MODULE_ALIAS("platform:dummy_driver");
2.4. Kernel module build[edit source]
See Adding_external_out-of-tree_Linux_kernel_modules for further information on module compilation.
2.5. Kernel module use[edit source]
scp dummy_driver.ko root@<board ip address>:/lib/modules/
- Update dependency descriptions for loadable kernel modules, and synchronize the data on disk with memory
/sbin/depmod -a sync
- Insert the kernel module example into the Linux kernel
modprobe dummy_driver [18167.821725] dummy_driver: GPIO example init