![]() |
Coming soon |
1. Article purpose[edit source]
This article aims to explain how to use the secure display hardware feature thanks to:
- the STM32 LTDC internal peripheral
- the following secure hardware internal peripherals:
- on STM32MP13x lines
, the STM32 ETZPC internal peripheral
- on STM32MP25x lines
, the STM32 RIFSC internal peripheral
- on STM32MP13x lines
- the STM32 OP-TEE framework and its related libutee library[1] that offers services to Trusted Applications (TA) including the Trusted User Interface (TUI) API
This article also explains how to configure and use a Trusted User Interface / Trusted Application example for demonstrating the secure display hardware feature.
2. Prerequisites[edit source]
To run the Trusted User Interface / Trusted Application example, required hardware boards and software stacks are listed below:
- On STM32MP13x lines
: The STM32MP135x-DK Discovery kit
- On STM32MP25x lines
: The STM32MP257x-EV1 Evaluation board
or the STM32MP257x-DK Discovery kit
- A display panel or the HDMI interface
- An OpenSTLinux distribution
3. LTDC Secure layer description[edit source]
On STM32MP13x lines , the LTDC internal periphal supports 2 layers: layer 2 can be set as secure (under ETZPC control), whereas the layer 1 is always non-secure.
On STM32MP25x lines , the LTDC internal peripheral supports 3 layers: layer 3 can be set as secure (under RIFSC internal peripheral control), whereas layer 1 and layer 2 are always non-secure, with grouped regs and additional interrupt set:
- The RIFSC RISUP differentiates the access right of accesses performed toward the following RIF protected peripheral ID:
- "LTDC common": LTDC common registers, about panel info, synchronization, interface
- "LTDC_L1L2" (layer 1 and 2): for the window of any two default applications
- "LTDC_L3": LTDC layer 3, for the window of a potentially secure application, or any default application if there is no secure layer
- "LTDC_ROT": LTDC rotation, with information about the rotation buffers
- The RIFSC RIMU differentiates the bus transactions emitted by the following AXI masters:
- "RIMU_L1L2": read access only for layer 1 and 2, always non-protected
- "RIMU_L3": read access only for layer 3, potentially protected
- "RIMU_ROT": write of blended pixels, and read of to-be-rotated pixels, potentially protected, because containing blended pixels of the protected layer 3
4. Related softwares and Configurations[edit source]
4.1. Device Tree[edit source]
4.2. OP-TEE[edit source]
header file of LTDC HAL module
4.3. Linux kernel[edit source]
...
/*
* Check the security of layer 2.
* Do not expose this layer to the user (do not create a plan)
* if this one is reserved for secure application.
*/
if (of_device_is_compatible(dev->of_node, "st,stm32mp25-ltdc")) {
ret = stm32_rifsc_check_access_by_id(STM32MP25_RIFSC_LTDC_L2_ID);
if (ret)
ldev->caps.nb_layers--;
}
...
Check the number of DRM/KMS layers are exposed to the userland with next commands:
.
modetest -p
![]() |
add modetest results |
4.4. Userland Trusted Application example[edit source]
5. Debug and Traces[edit source]
6. How to run the TUI TA example[edit source]
Boot the board, then use the optee-tui-client binary example, using the following command examples.
Get the optee-tui-client help and usage:
optee-tui-client
Usage:
--print-screen-info
--blank-screen <color> (value in ARGB format, ex. 0xFF112233)
--display-image <x>,<y>,<width>,<height>,<path> (file in raw ARGB format)
--draw-pin-pad
Get the display information:
optee-tui-client --print-screen-info D/TA: TA_InvokeCommandEntryPoint:160 result: 0 D/TA: TA_InvokeCommandEntryPoint:160 result: 0 width: 1024 height: 600 width DPI: 160 height DPI: 160 color depth: 0 D/TA: TA_InvokeCommandEntryPoint:160 result: 0
Set a background color on the secure layer to a given color (100% red in the below example):
optee-tui-client --blank-screen 0xFF0000 D/TA: TA_InvokeCommandEntryPoint:160 result: 0 D/TA: TA_InvokeCommandEntryPoint:160 result: 0 Hit Ctrl-C to quit ^C
Start the application example with the pin pad use case:
optee-tui-client --draw-pin-pad D/TA: TA_InvokeCommandEntryPoint:160 result: 0 D/TA: TA_InvokeCommandEntryPoint:160 result: -65529 TEEC_InvokeCommand 7 failed with code 0xffff0007 origin 0x4
7. How to go further[edit source]
You may be interested in the following related articles: