X-LINUX-RT expansion package

Revision as of 10:42, 19 June 2024 by Registered User (→‎Software prerequisites)
Applicable for STM32MP13x lines, STM32MP15x lines, STM32MP25x lines

1. Article purpose[edit source]

Purpose of this article is to:

  • introduce the X-LINUX-RT expansion package
  • define the hardware & software deliverables to use the X-LINUX-RT package,
  • describe all steps to integrate the X-LINUX-RT package and associated expected results
  • give some use case examples enabled by the X-LINUX-RT package
RT Expansion Package In STM32MPU Embedded Software.png

2. X-LINUX-RT expansion package description[edit source]

2.1. Overview[edit source]

X-LINUX-RT is an STM32 MPU OpenSTLinux Expansion Package that targets the real-time (RT) feature in the Linux® kernel.
An RT system is a system that responds to a request in a time lapse and not as fast as possible. It targets​:

  • Determinism​
  • LATENCY but not SPEED

For a better understanding about real-time Linux, refer to the Linux RT foundation website[1].
The X-LINUX-RT Expansion Package is mainly designed to be used with Yocto and the OpenSTLinux Distribution Package. However, the following chapters show how to use it either with the OpenSTLinux Distribution Package or with the Developer Package.

2.2. Main software modifications[edit source]

2.2.1. Linux kernel configuration[edit source]

The Linux kernel configuration must be modified to enable:

  • CONFIG_PREEMPT_RT : RT feature in kernel
  • CONFIG_HIGH_RES_TIMERS : high resolution timer support

2.2.2. OP-Tee OS board device trees[edit source]

Power management is not "compliant" with a real-time context as it changes the system behavior. Because there is no more frequency scaling, and to ensure an optimal lifetime for the microprocessor, the frequency is fixed following the recommended industrial profile.

    • 900 MHz for STM32MP13x lines More info.png
    • 650 MHz for STM32MP15x lines More info.png
    • 1.2 GHz for STM32MP25x lines More info.png

2.3. Versioning[edit source]

If any, precise here the version of the X-LINUX-NAME expansion package to use

  • X-LINUX-NAME package software
    • names of software,
    • revision number.

2.4. Associated licenses[edit source]

3. Prerequisites[edit source]

3.1. Hardware prerequisites[edit source]

  • STM32 MPU Board


3.2. Software prerequisites[edit source]

The X-LINUX-RT Expansion Package runs with OpenSTLinux from ecosystem release v5.0.0 More info.png to v5.1.0 More info.png.

4. Software setup[edit source]

4.1. How to get software[edit source]

X-LINUX-RT Expansion Package is delivered in a git repository on Github.

For ecosystem release v5.1.0 More info.png :

pushd <Distribution Package installation directory>/layers/meta-st
git clone -b mickledore https://github.com/STMicroelectronics/meta-st-x-linux-rt.git
cd meta-st-x-linux-rt
git reset --hard openstlinux-6.1-yocto-mickledore-mpu-v24.06.26
popd

For ecosystem release v5.0.0 More info.png only:

pushd <Distribution Package installation directory>/layers/meta-st
git clone -b mickledore https://github.com/STMicroelectronics/meta-st-x-linux-rt.git
cd meta-st-x-linux-rt
git reset --hard openstlinux-6.1-yocto-mickledore-mp1-v23.06.21
popd

4.1.1. How to install developer package[edit source]

4.1.2. How to install distribution package[edit source]

  • Clone the meta-st-x-linux-rt git repositories

For ecosystem release v5.1.0 More info.png :

pushd <Distribution Package installation directory>/layers/meta-st
git clone -b mickledore https://github.com/STMicroelectronics/meta-st-x-linux-rt.git
cd meta-st-x-linux-st-rt
git reset --hard openstlinux-6.1-yocto-mickledore-mpu-v24.06.26
popd

For ecosystem release v5.0.0 More info.png only:

pushd <Distribution Package installation directory>/layers/meta-st
git clone -b mickledore https://github.com/STMicroelectronics/meta-st-x-linux-rt.git
cd meta-st-x-linux-st-rt
git reset --hard openstlinux-6.1-yocto-mickledore-mp1-v23.06.21
popd
  • Source the build environment with the correct board and layer

For STM32MP13x lines More info.png:

DISTRO=openstlinux-weston MACHINE=stm32mp13-rt source layers/meta-st/scripts/envsetup.sh

For STM32MP15x lines More info.png:

DISTRO=openstlinux-weston MACHINE=stm32mp1-rt source layers/meta-st/scripts/envsetup.sh

For STM32MP2 series (for ecosystem release v5.1.0 More info.png ):

DISTRO=openstlinux-weston MACHINE=stm32mp2-rt source layers/meta-st/scripts/envsetup.sh
  • Build the image
bitbake st-image-weston
Info white.png Information
Note that building the image might take a long time depending on the host computer performance.

5. How to run RT feature ...[edit source]

To check that the RT feature is enabled and functional, the following commands can be executed.

5.1. Use cases execution and expected results[edit source]

5.1.1. Check the Linux kernel version[edit source]

 uname -s -r -v
Without the RT feature
Linux 6.1.82 #1 SMP PREEMPT Fri Mar 15 14:04:26 UTC 2024
With the RT feature
Linux 6.1.82-rt27 #1 SMP PREEMPT_RT Fri Mar 15 18:27:50 UTC 2024

5.1.2. Cyclictest[edit source]

Cyclictest accurately and repeatedly measures the difference between the time at which a thread is intended to wake up and the time at which it actually wakes up.
For a better understanding of cyclictest, refer to the cyclictest webpage in the Linux RT foundation website[2].

For example, the following command can be used:

 cyclictest --mlockall -t -a --priority=99 --interval=200 --distance=0 -l 1000
Without the RT feature
policy: fifo: loadavg: 1.96 0.65 0.23 4/186 1671          

T: 0 ( 1667) P:99 I:200 C:   1000 Min:     21 Act:   40 Avg:   33 Max:     103
T: 1 ( 1668) P:99 I:200 C:    882 Min:     21 Act:   58 Avg:   42 Max:     187
With the RT feature
policy: fifo: loadavg: 3.18 1.17 0.43 1/226 1776          

T: 0 ( 1775) P:99 I:200 C:   1000 Min:     21 Act:   24 Avg:   28 Max:      90
T: 1 ( 1776) P:99 I:200 C:    842 Min:     20 Act:   42 Avg:   23 Max:      48

Note: OPTEE HSI cyclic calibration was desactivated for this test

5.2. Use case restrictions[edit source]

Latency can be improved by disabling some features or services:

* weston
* systemd
* netdata
* OPTEE HSI cyclic calibration

A new distribution named openstlinux-rt is provided. This distribution is using SysVInit instead of Systemd, no Weston, no OPTEE HSI cyclic calibration and no netdata services.

To select it, run following command:

DISTRO=openstlinux-rt MACHINE=<your machine> source layers/meta-st/scripts/envsetup.sh

RT performances are improved.

 cyclictest --mlockall -t -a --priority=99 --interval=200 --distance=0 -l 1000
WARN: stat /dev/cpu_dma_latency failed: No such file or directory
policy: fifo: loadavg: 0.55 0.62 0.36 1/133 648          

T: 0 (  647) P:99 I:200 C:   1000 Min:     17 Act:   18 Avg:   21 Max:      45
T: 1 (  648) P:99 I:200 C:    781 Min:     17 Act:   23 Avg:   18 Max:      36

6. References[edit source]