GPIO internal peripheral

Revision as of 19:48, 7 December 2023 by Registered User
Applicable for STM32MP13x lines, STM32MP15x lines, STM32MP25x lines

1. Article purpose[edit source]

The purpose of this article is to:

  • briefly introduce the GPIO peripheral and its main features,
  • indicate the peripheral instances assignment at boot time and their assignment at runtime (including whether instances can be allocated to secure contexts),
  • list the software frameworks and drivers managing the peripheral,
  • explain how to configure the peripheral.

2. Peripheral overview[edit source]

The GPIO peripheral is used to configure the device IO ports, also called pins or pads.

On STM32MP13x lines More info.png, each GPIO instance controls 16 pins (for GPIOA to GPIOG), 15 pins (for GPIOH) or 8 pins (for GPIOI).
On STM32MP15x lines More info.png, each GPIO instance controls 16 pins (for GPIOA to GPIOJ) or 8 pins (for GPIOK and GPIOZ).
On STM32MP25x lines More info.png, each GPIO instance controls 16 pins (for GPIOA/B/D/E/F/G/I/J), 14 pins (for GPIOC), 12 pins (for GPIOH), 10 pins (for GPIOZ) or 8 pins (for GPIOK).

Every IO port implements the logic shown in the image below, taken from reference manual [1].

  • The IO pin (on the right) is the physical connection to a chip external ball, soldered on the PCB. The link between each GPIO pin and each ball of the package is given in the datasheet [2].
  • The Read and Write accesses allow the processor (Arm® Cortex®-A7 for STM32MP1 series or Arm® Cortex®-M4 for STM32MP15x lines More info.png) to configure the peripheral, control the IO pin and get its status.
  • Alternate function (AF) links allow to connect the IO port to an internal peripheral digital line. In such a case, the IO direction is given by the line purpose: for instance, UART transmit line (TX) is an output.
  • Analog links allow to connect the IO port to an internal peripheral analog line. In such a case, the IO direction is given by the line purpose: for instance, ADC input line is an input.

IO port.png

Note:
  • the pull-up and pull-down resistors are disabled (by hardware) in analog mode.
  • at reset, all pins are set in analog input mode to protect the device and minimize the power consumption. All unused pins should be kept in this state.


The pin configuration done by the software consists in:

  • setting the pin mode in the GPIOx_MODER register:
    • input or output if the pin is used as general purpose (GPIO), controlled by software.
    • analog.
    • alternate function (AF).
  • selecting the alternate function in the GPIOx_AFRH/L register (only when the pin mode is AF):
    • each IO port can support up to 16 alternate functions that are documented in the datasheet [2].
  • setting the pin characteristics:
    • no pull-up and no pull-down or pull-up or pull-down in the GPIOx_PUPDR register, needs to be selected to be coherent with the hardware schematics.
    • push-pull or open-drain in the GPIOx_OTYPER register, needs to be selected to be coherent with the hardware schematics.
    • output speed in the GPIOx_OSPEEDR register needs to be tuned to achieve the expected level of performance (rising and falling times) while limiting electromagnetic interferences (EMI) and overconsumption. As example, the table below summarizes the maximum achievable frequency for each supported IO voltage and a 30pF load:
  • On STM32MP13x lines More info.png:
GPIOx_OSPEEDR Meaning VDD=3v3 VDD=1v8
HSLV OFF
VDD=1v8
HSLV ON
b00 Low speed 21 MHz 5 MHz 23 MHz
b01 Medium speed 44 MHz 15 MHz 44 MHz
b10 High speed 100 MHz 37 MHz 90 MHz
b11 Very high speed 166 MHz 50 MHz 133 MHz
  • On STM32MP15x lines More info.png:
GPIOx_OSPEEDR Meaning VDD=3v3 VDD=1v8
HSLV OFF
VDD=1v8
HSLV ON
b00 Low speed 24 MHz 11 MHz 22 MHz
b01 Medium speed 83 MHz 28 MHz 79 MHz
b10 High speed 125 MHz 66 MHz 101 MHz
b11 Very high speed 150 MHz 70 MHz 111 MHz
  • On STM32MP25x lines More info.png:
GPIOx_OSPEEDR Meaning VDD=3v3 VDD=1v8
VRSEL OFF
VDD=1v8
VRSEL ON
b00 Low speed 45 MHz 20 MHz 45 MHz
b01 Medium speed 70 MHz 25 MHz 70 MHz
b10 High speed 100 MHz 30 MHz 100 MHz
b11 Very high speed 120 MHz 45 MHz 120 MHz
Notes:
  • More information is available in the IO speed settings chapter of the "Getting started with..." [3].
  • There are different IO types with different characteristics: for instance, all pads are not able to achieve 150 MHz while supplied at 3.3V. Refer to the datasheet [2] to get the characteristics for each pin.
  • On STM32MP1 series, when supplied with VDD=1.8V, it is possible to enable the high speed low voltage (HSLV) pad mode for FTH (Five volt Tolerant High speed) and FTE (Five volt Tolerant Extended high speed) IO types on some peripherals via SYSCFG HSLVEN bits. Warning: As it could be destructive if used when VDD>2.7V, thanks to carefully read the HSLVEN bits documentation in reference manuals [1], especially the management of the OTP bit PRODUCT_BELOW_2V5 (STM32MP1 series) and lock mechanism (for STM32MP13x lines More info.png only).
  • On STM32MP2 series, IOs could be configured either 1.8V or 3.3V compliance modes.
    • In 1.8V mode, IOs are not 3.3V tolerant
    • In 3.3V mode, IOs are not 5V tolerant
    • By default, all IOs are in 3.3V mode, working in non-optimal condition when supplied with VDD=1.8V. It is responsibility of bootchain to configure IOs mode according to product configuration by setting PWR VRSEL bits for each IO domain.
    • Warning: PWR VRSEL bits have effect only if associated HSLV OTP bit have been programmed.
    • Warning: Enabling 1.8V mode when VDD=3.3V will damage IOs

The table below shows all possible characteristics combinations for each pin mode:

pin mode GPIOx_PUPDR GPIOx_OTYPER GPIOx_OSPEEDR
analog
 
Not applicable Not applicable Not applicable
input (GPIO or AF)
 
no pull-up and no pull-down
or pull-down
or pull-up
Not applicable Not applicable
output (GPIO or AF)
or bi-directional (AF)
push-pull
or open-drain
cf. the table above
Note:
  • 'Not applicable' means that setting this register has no effect but, in any case, there is no risk for the device.
  • On the other hand, leaving a register not initialized whereas it should be, may lead to an unpredictable behavior!

GPIO access configuration

  • On STM32MP13x lines More info.png, any IOs from all GPIO banks can be unitary defined as secure or non-secure.
  • On STM32MP15x lines More info.png, only IOs from GPIOZ can be unitary defined as secure or non-secure.
  • On STM32MP25x lines More info.png, GPIO are RIF-aware, that means it is possible to assign each GPIO to one execution context define by:
  • a security level
  • a privilege level
  • a CID
For more information about RIF please refer to Resource Isolation Framework overview.

Refer to the STM32 MPU reference manuals [1] for the complete list of features, and to the software frameworks and drivers, introduced below, to see which features are implemented.

3. Peripheral usage[edit source]

This chapter is applicable in the scope of the OpenSTLinux BSP running on the Arm® Cortex®-A processor(s), and the STM32CubeMPU Package running on the Arm® Cortex®-M processor.

3.1. Boot time assignment[edit source]

The STM32CubeMX tool allows to configure in one place the GPIO configuration for boot time and runtime, so it is highly recommended to use it to generate your device tree. Moreover, STM32CubeMX integrates all the information documented in the datasheet [2], making this configuration step straightforward.

Since a GPIO configuration is done via atomic registers read and write, concurrent accesses from different cores must be avoided.

  • On STM32MP15x lines More info.png all GPIO configurations are done by the Arm® Cortex®-A7.
  • On STM32MP25x lines More info.png, GPIO configurations could be done by the different execution contexts as soon as RIF configuration has been applied by main processor (TDCID) secure OS.

The strategy is to progressively initialize the GPIO all along the boot chain, as soon as one boot component needs to use them:

  • Most of the GPIOs used by the ROM code are directly defined in the ROM code but it is possible to change some pins muxing via dedicated words in BSEC.
  • The other boot components are relying on a common binding[4] in the device tree to get the pins configuration:
    • The FSBL configures both secure and non-secure pins according to peripherals firewall configuration.
    • The Secure OS configures pins firewall protection and secure pins for secure peripherals
    • The SSBL and Linux pinctrl only configure non-secure pins.
      • On STM32MP15x lines More info.png, Linux also initializes the GPIO used by the coprocessor, via its resource manager.
3.1.1. On STM32MP13x lines More info.png[edit source]

Click on How to.png to expand or collapse the legend...

Check boxes illustrate the possible peripheral allocations supported by STM32 MPU Embedded Software:

  • means that the peripheral can be assigned to the given boot time context.
  • means that the peripheral is assigned by default to the given boot time context and that the peripheral is mandatory for the STM32 MPU Embedded Software distribution.
  • means that the peripheral can be assigned to the given boot time context, but this configuration is not supported in STM32 MPU Embedded Software distribution.
  • is used for system peripherals that cannot be unchecked because they are hardware connected in the device.

The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possibilities might be described in STM32 MPU reference manuals.

Domain Peripheral Boot time allocation Comment How to.png
Instance Cortex-A7
secure
(ROM code)
Cortex-A7
secure
(TF-A BL2)
Cortex-A7
non-secure
(U-Boot)
Core/IOs GPIO GPIOA-I The pins can individually be secured
3.1.2. On STM32MP15x lines More info.png[edit source]

Click on How to.png to expand or collapse the legend...

Check boxes illustrate the possible peripheral allocations supported by STM32 MPU Embedded Software:

  • means that the peripheral can be assigned to the given boot time context.
  • means that the peripheral is assigned by default to the given boot time context and that the peripheral is mandatory for the STM32 MPU Embedded Software distribution.
  • means that the peripheral can be assigned to the given boot time context, but this configuration is not supported in STM32 MPU Embedded Software distribution.
  • is used for system peripherals that cannot be unchecked because they are hardware connected in the device.

The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possibilities might be described in STM32 MPU reference manuals.

Domain Peripheral Boot time allocation Comment How to.png
Instance Cortex-A7
secure
(ROM code)
Cortex-A7
secure
(TF-A BL2)
Cortex-A7
non-secure
(U-Boot)
Core/IOs GPIO GPIOA-K (*) The pins cannot be secured

(*): despite they cannot be secured, the pins can be used by the secure context

GPIOZ The pins can individually be secured

3.1.1. On STM32MP2 series[edit source]

Click on How to.png to expand or collapse the legend...

  • means that the peripheral can be assigned to the given boot time context.
  • means that the peripheral is assigned by default to the given boot time context and that the peripheral is mandatory for the STM32 MPU Embedded Software distribution.
  • means that the peripheral can be assigned to the given boot time context, but this configuration is not supported in STM32 MPU Embedded Software distribution.
  • is used for system peripherals that cannot be unchecked because they are hardware connected in the device.

The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possibilities might be described in STM32MP25 reference manuals.

Domain Peripheral Boot time allocation Comment How to.png
Instance Cortex-A35
secure
(ROM code)
Cortex-A35
secure
(TF-A BL2)
Cortex-A35
non-secure
(U-Boot)
Core/IOs GPIO Info.png GPIOA-K Shareable at internal peripheral level thanks to the RIF: see the boot time allocation per feature
GPIOZ Shareable at internal peripheral level thanks to the RIF: see the boot time allocation per feature

The below table shows the possible boot time allocations for the features of the GPIO instances.

Feature Boot time allocation Info.png Comment
Cortex-A35
secure
(ROM code)
Cortex-A35
secure
(TF-A BL2)
Cortex-A35
non-secure
(U-Boot)
GPIOA-K IOy
GPIOZ IOy

3.2. Runtime assignment[edit source]

The GPIO configuration must not be done from different cores to avoid concurrent accesses, but this is not the case for the GPIO using: each core can manipulate IO on its own since dedicated set/clear registers are available for that.

Nevertheless, beyond the boot time, the GPIO configuration also evolves at runtime: while entering in low power mode, some GPIOs may be put back to analog input mode in order to reduce the power consumption.
On STM32MP1 series, this is done in two times:

  1. the Arm® Cortex®-A non-secure takes care of the non-secure pins with Linux IOs pins frameworks.
  2. the Arm® Cortex®-A secure takes care of the secure pins behind PSCI secure services.

On wakeup, the boot chain restores the GPIO configuration similarly to what is done at boot time.
On STM32MP25x lines More info.png, thanks to the RIF, each SW component shall take care of its pins during low power entry and exit sequences.


3.2.1. On STM32MP13x lines More info.png[edit source]

Click on How to.png to expand or collapse the legend...

STM32MP13 internal peripherals

Check boxes illustrate the possible peripheral allocations supported by STM32 MPU Embedded Software:

  • means that the peripheral can be assigned to the given runtime context.
  • means that the peripheral is assigned by default to the given runtime context and that the peripheral is mandatory for the STM32 MPU Embedded Software distribution.
  • means that the peripheral can be assigned to the given runtime context, but this configuration is not supported in STM32 MPU Embedded Software distribution.
  • is used for system peripherals that cannot be unchecked because they are hardware connected in the device.

Refer to How to assign an internal peripheral to an execution context for more information on how to assign peripherals manually or via STM32CubeMX.
The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possibilities might be described in STM32MP13 reference manuals.

Domain Peripheral Runtime allocation Comment How to.png
Instance Cortex-A7
secure
(OP-TEE)
Cortex-A7
non-secure
(Linux)
Core/IOs GPIO GPIOA-I The pins can individually be secured
3.2.2. On STM32MP15x lines More info.png[edit source]

Click on How to.png to expand or collapse the legend...

STM32MP15 internal peripherals

Check boxes illustrate the possible peripheral allocations supported by STM32 MPU Embedded Software:

  • means that the peripheral can be assigned to the given runtime context.
  • means that the peripheral is assigned by default to the given runtime context and that the peripheral is mandatory for the STM32 MPU Embedded Software distribution.
  • means that the peripheral can be assigned to the given runtime context, but this configuration is not supported in STM32 MPU Embedded Software distribution.
  • is used for system peripherals that cannot be unchecked because they are hardware connected in the device.

Refer to How to assign an internal peripheral to an execution context for more information on how to assign peripherals manually or via STM32CubeMX.
The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possiblities might be described in STM32MP15 reference manuals.

Domain Peripheral Runtime allocation Comment How to.png
Instance Cortex-A7
secure
(OP-TEE)
Cortex-A7
non-secure
(Linux)
Cortex-M4

(STM32Cube)
Core/IOs GPIO GPIOA-K (*) The pins can individually be shared

(*): despite they cannot be secured, the pins can be used by the secure context

GPIOZ The pins can individually be secured or shared

3.2.1. On STM32MP25x lines More info.png[edit source]

Click on How to.png to expand or collapse the legend...

STM32MP25 internal peripherals

Check boxes illustrate the possible peripheral allocations supported by STM32 MPU Embedded Software:

  • means that the peripheral can be assigned to the given runtime context.
  • means that the peripheral is assigned by default to the given runtime context and that the peripheral is mandatory for the STM32 MPU Embedded Software distribution.
  • means that the peripheral can be assigned to the given runtime context, but this configuration is not supported in STM32 MPU Embedded Software distribution.
  • is used for system peripherals that cannot be unchecked because they are hardware connected in the device.

The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possibilities might be described in STM32MP25 reference manuals.

Domain Peripheral Runtime allocation Comment How to.png
Instance Cortex-A35
secure
(OP-TEE /
TF-A BL31)
Cortex-A35
non-secure
(Linux)
Cortex-M33
secure
(TF-M)
Cortex-M33
non-secure
(STM32Cube)
Cortex-M0+
Warning.png
(STM32Cube)
Core/IOs GPIO Info.png GPIOA-K OP-TEE
TF-A BL31
Shareable at internal peripheral level thanks to the RIF: see the runtime allocation per feature
GPIOZ OP-TEE
TF-A BL31
Shareable at internal peripheral level thanks to the RIF: see the runtime allocation per feature

The below table shows the possible runtime allocations for the features of the GPIO instances.

Feature Runtime allocation Info.png Comment
Cortex-A35
secure
(OP-TEE /
TF-A BL31)
Cortex-A35
non-secure
(Linux)
Cortex-M33
secure
(TF-M)
Cortex-M33
non-secure
(STM32Cube)
Cortex-M0+
Warning.png
(STM32Cube)
GPIOA-K IOy OP-TEE
TF-A BL31
GPIOZ IOy OP-TEE
TF-A BL31

4. Software frameworks and drivers[edit source]

Below are listed the software frameworks and drivers managing the GPIO peripheral for the embedded software components listed in the above tables.

5. How to assign and configure the peripheral[edit source]

The peripheral assignment can be done via the STM32CubeMX graphical tool (and manually completed if needed).
This tool also helps to configure the peripheral:

  • partial device trees (pin control and clock tree) generation for the OpenSTLinux software components,
  • HAL initialization code generation for the STM32CubeMPU Package.

The configuration is applied by the firmware running in the context in which the peripheral is assigned.

In Linux kernel, each GPIO bank is declared as a "gpio-controller" in the device tree and each pin can then be used via two different consumer frameworks:

6. References[edit source]

  1. 1.0 1.1 1.2 Reference manuals: STM32MP15 | STM32MP13 | STM32MP25
  2. 2.0 2.1 2.2 2.3 Datasheets: STM32MP13 | STM32MP15 | STM32MP25
  3. Application Note (Getting started with ... hardware development):
  4. Documentation/devicetree/bindings/pinctrl/st,stm32-pinctrl.yaml