1. Overview[edit source]
gst-transcoder (gst-transcoder-1.0) is a GStreamer command line utility available with GStreamer-1.X.
This utility transcodes audio / video multimedia content using complex GStreamer elements such as decodebin and encodebin into various audio / video multimedia content. It takes as an input either individual files or URL.
2. Usage[edit source]
gst-transcoder accepts the following options:
gst-transcoder-1.0 --help
Usage:
gst-transcoder [OPTION?] <source uri> <destination uri> [<encoding format>[/<encoding profile name>]]
gst-transcoder-1.0 transcodes a stream defined by its first <input-uri>
argument to the place defined by its second <output-uri> argument
into the format described in its third <encoding-format> argument,
or using the given <output-uri> file extension.
The <encoding-format> argument:
===============================
If the encoding format is not defined, it will be guessed with
the given <output-uri> file extension.
<encoding-format> describe the media format into which the
input stream is going to be transcoded. We have two different
ways of describing the format:
GstEncodingProfile serialization format
---------------------------------------
GStreamer encoding profiles can be described with a quite extensive
syntax which is described in the GstEncodingProfile documentation.
The simple case looks like:
muxer_source_caps:videoencoder_source_caps:audioencoder_source_caps
Name and category of serialized GstEncodingTarget
-------------------------------------------------
Encoding targets describe well known formats which
those are provided in '.gep' files. You can list
available ones using the `--list-targets` argument.
Help Options:
-h, --help Show help options
--help-all Show all help options
--help-gst Show GStreamer Options
Application Options:
-c, --cpu-usage The CPU usage to target in the transcoding process
-l, --list-targets List all encoding targets
-s, --size set frame size (WxH or abbreviation)
-r, --audio-rate set audio sampling rate (in Hz)
-f, --framerate set video framerate as a fraction (24/1 for 24fps) or a single number (24 for 24fps))
-v, --video-encoder The video encoder to use.
3. List the available output profiles[edit source]
Use -l option to get the list of available destination multimedia content:
gst-transcoder-1.0 -l
dvd (device): Encoding target suitable for DVDs * Profiles: - dvd: This is an encoding profile usable for DVDs avi (file-extension): Default target for files with a .avi extension * Profiles: - default: Default profile for files with a .avi extension. mp3 (file-extension): Default target for files with a .mp3 extension * Profiles: - default: Default profile for files with a .mp3 extension. oga (file-extension): Default target for files with a .ogg and friends extension * Profiles: - default: Default target for files with a .ogg and friends extension ogv;ogg (file-extension): Default target for files with a .ogg and friends extension * Profiles: - default: Default target for files with a .ogg and friends extension webm (file-extension): Default target for files with a .webm extension * Profiles: - default: Default profile for files with a .webm extension. Audio stream can be either vorbis (default) or opus depending on what is available on the system. Video stream will be either in vp8 (default) or vp9.
4. Examples[edit source]
4.1. Basic transcoding[edit source]
Transcode from H264/AAC encapsulated in mp4 container to VP8/Vorbis encapsulated in webm container:
gst-transcoder-1.0 big_buck_bunny_720p_H264_AAC_25fps_3400K_short.mp4 av_vp8_720p_vorbis.webm webm
Encoding to: Container: default: Default profile for files with a .webm extension. Audio stream can be either vorbis (default) or opus depending on what is available on the system. Video stream will be either in vp8 (def) - Audio: audio/x-vorbis; audio/x-opus - Video: video/x-vp8; video/x-vp9 Starting transcoding... 0:00:03.9 / 0:00:04.0 DONE.
Verification of encoded video details:
gst-discoverer-1.0 av_vp8_720p_vorbis.webm
container #0: WebM
audio #1: Vorbis
Channels: 2 (front-left, front-right)
Sample rate: 44100
Depth: 32
Bitrate: 112000
video #2: VP8
Width: 1280
Height: 720
Depth: 24
Frame rate: 25/1
Pixel aspect ratio: 1/1
Interlaced: false
4.2. Format change[edit source]
4.3. Resolution change[edit source]
gst-transcoder-1.0 gst-transcoder-1.0 big_buck_bunny_720p_H264_AAC_25fps_3400K_sh
ort.mp4 out.webm webm "video/webm:video/x-raw,width=960,height=540->video/x-vp8:audio/x-vorbis"