X-LINUX-AI Application

Revision as of 09:37, 7 June 2024 by Registered User

This article aims to give general information about the x-linux-ai-application. presenting its core features, potential applications, and benefits to users seeking to leverage its capabilities within STM32MPU.

1. Description[edit source]

The X-LINUX-AI Application is an advanced software solution crafted to enhance the management and utilization of AI (Artificial Intelligence) capabilities on devices powered by OpenSTLinux. This robust tool not only offers a comprehensive display of all available AI applications supported for each board but also excels in identifying the optimal AI application performance for specific hardware. By leveraging the X-LINUX-AI Application, users can achieve superior accuracies and maximize the potential of their AI endeavors.

2. How to install X-LINUX-AI Application[edit source]

Warning white.png Warning
The software package is provided AS IS, and by downloading it, you agree to be bound to the terms of the software license agreement (SLA0048). The detailed content licenses can be found here.

Make sure to install x-linux-ai-tool. you can follow this link <a href="https://wiki.st.com/stm32mpu-prepa-v5.1/wiki/X-LINUX-AI_Tool#X-LINUX-AI_Tool_installation">x-linux-ai-tool</a>

    x-linux-ai --install x-linux-ai-application

3. How to use X-LINUX-AI Application:[edit source]

Info white.png Information
The x-linux-ai-application binary can be found in the /usr/bin directory.
Usage:	x-linux-ai-application -[option] -r <use-case> --model-type <model-type> --language <language>

 -l --list            : list all the available applications
 -r --run <str>       : run application with a specific use case
 --model-type <str>   : run application with a specific model type
 --language <str>     : run application with a specific program language
 -h --help            : Show this help

3.1. Usage Example[edit source]

  • To display a list of all the available use cases:
    x-linux-ai-application -l
root@stm32mp25-revab:~# x-linux-ai-application -l

[installed]	object-detection
[not installed]	image-classification
[not installed]	face-recognition
[not installed]	semantic-segmentation
[not installed]	pose-estimation
  • To run x-linux-ai Application:
    x-linux-ai-application -r <use-case>
root@stm32mp25-revab:~# x-linux-ai-application -r object-detection


Running ...
Application: tflite-object-detection-python
File path: /usr/local/demo-ai/object-detection/tflite/launch_python_object_detection.sh


machine used = stm32mp257
user : weston
display resolution is :  1024  x  600
Vx delegate: allowed_cache_mode set to 1.
Vx delegate: device num set to 0.
Vx delegate: allowed_builtin_code set to 0.
Vx delegate: error_during_init set to 0.
Vx delegate: error_during_prepare set to 0.
Vx delegate: error_during_invoke set to 0.
Loading external delegate from /usr/lib/libvx_delegate.so.2
number of threads used in tflite interpreter :  2
camera preview mode activate
check if a CSI or USB camera is connected
/home/weston
dcmipp found
/home/weston
DCMIPP_SENSOR=imx335
main_postproc=/dev/v4l-subdev3
Mediacontroller graph:

V4L_DEVICE=video1
V4L2_CAPS=video/x-raw, format=RGB16, width=640, height=480
DCMIPP_SENSOR=imx335
MAIN_POSTPROC=/dev/v4l-subdev3
  • To run an application with a specific model type:
    x-linux-ai-application -r <use-case> --model-type <model-type>
root@stm32mp25-revab:~# x-linux-ai-application -r object-detection --model-type onnx


Running ...
Application: onnx-object-detection-python
File path: /usr/local/demo-ai/object-detection/onnx/launch_python_object_detection.sh


machine used = stm32mp257
user : weston
display resolution is :  1024  x  600
NN model used :  /usr/local/demo-ai/object-detection/models/coco_ssd_mobilenet/coco_ssd_mobilenet.onnx
Number threads used :  2
input shape [1, 300, 300, 3]
H,W,C 300 300 3
camera preview mode activate
check if a CSI or USB camera is connected
/home/weston
dcmipp found
/home/weston
DCMIPP_SENSOR=imx335
main_postproc=/dev/v4l-subdev3
Mediacontroller graph:

V4L_DEVICE=video1
V4L2_CAPS=video/x-raw, format=RGB16, width=640, height=480
DCMIPP_SENSOR=imx335
MAIN_POSTPROC=/dev/v4l-subdev3
  • To run an application with a specific program language:
    x-linux-ai-application -r <use-case> --language <program-language>
root@stm32mp25-revab:~# x-linux-ai-application -r object-detection --language cpp


Running ...
Application: tflite-object-detection-cpp
File path: /usr/local/demo-ai/object-detection/tflite/launch_bin_object_detection.sh


machine used = stm32mp257
user : weston
model file set to: /usr/local/demo-ai/object-detection/models/coco_ssd_mobilenet/coco_ssd_mobilenet.tflite
label file set to: /usr/local/demo-ai/object-detection/models/coco_ssd_mobilenet/labels_coco_ssd_mobilenet.txt
camera framerate set to: 30
camera frame width set to: 640
camera frame heightset to: 480
Inference launched on NPU with the delagate :/usr/lib/libvx_delegate.so.2
2 cpu core(s) available
EdgeTPU acceleration: not used
Delegate acceleration: used
Loaded model /usr/local/demo-ai/object-detection/models/coco_ssd_mobilenet/coco_ssd_mobilenet.tflite
Vx delegate: allowed_cache_mode set to 0.
Vx delegate: device num set to 0.
Vx delegate: allowed_builtin_code set to 0.
Vx delegate: error_during_init set to 0.
Vx delegate: error_during_prepare set to 0.
Vx delegate: error_during_invoke set to 0.
WARNING: Fallback unsupported op 32 to TfLite
check if a CSI or USB camera is connected
/home/weston
dcmipp found
display resolution is : 1024 x 600 
Display config <= 600p 
video source used : /dev/ 
camera pipeline configuration : ,framerate=30/1 
  • To run an application with a specific model type and program language:
    x-linux-ai-application -r <use-case> --model-type <model-type> --language <program-language>
root@stm32mp25-revab:~# x-linux-ai-application -r image-classification --model-type onnx --language python


Running ...
Application: onnx-image-classification-python
File path: /usr/local/demo-ai/image-classification/onnx/launch_python_image_classification.sh


machine used = stm32mp257
user : weston
display resolution is :  1024  x  600
NN model used :  /usr/local/demo-ai/image-classification/models/mobilenet/mobilenet_v3_large_100_224_quant.onnx
Number threads used :  2
input shape ['unk__1576', 224, 224, 3]
H,W,C 224 224 3
camera preview mode activate
check if a CSI or USB camera is connected
/home/weston
dcmipp found
/home/weston
DCMIPP_SENSOR=imx335
main_postproc=/dev/v4l-subdev3
Mediacontroller graph:

V4L_DEVICE=video1
V4L2_CAPS=video/x-raw, format=RGB16, width=640, height=480
DCMIPP_SENSOR=imx335
MAIN_POSTPROC=/dev/v4l-subdev3
Info white.png Information

If none of the x-linux-ai applications are installed, you can list all the available packages using the following command:
    x-linux-ai -l

Alternatively, if you wish to install the optimal AI application, it can be suggested by x-linux-ai-application while executing a use case. Here is an example:

root@stm32mp25-revab:~# x-linux-ai-application -r pose-estimation

[WARNING]: tflite-pose-estimation-python: is not yet installed
[INFO]: Can be installed using: `x-linux-ai --install tflite-pose-estimation-python`

x-linux-ai-application has selected tflite-pose-estimation-python as the best application for pose estimation, and you can install it using the provided command. .

Warning white.png Warning
To run the optimal application, it must be installed on the board. If it is not, x-linux-ai-application will attempt to find the best option among the installed applications. Therefore, ensure that all applications are installed to allow the selection of the most suitable one.