This article lists documents that apply to the STM32 MPU ecosystem release of the STM32MP25x lines . Those documents are generally referenced into other wiki pages.
All the resources for the STM32MP2 series are located in the STM32MP2 series web page.
The resources for ALPHA program are not located in ST.com but ST private Teamspace [1] except for the ones common with STM32MP1 series.
Reference | Name | Link | |
---|---|---|---|
Application notes | |||
AN5729 | Guidelines for Lifetime Usage Estimates on STM32MP2 MPUs | Not yet available (planned for the mass market launch) | |
AN5489 Rev0.3 | AN5489 Rev0.3 Getting started with STM32MP25xx lines hardware development | [2] | |
AN5723 Rev0.1 | AN5723 Rev0.1 - Guidelines for DDR memory configuration on STM32MP2 MPUs | [3] | |
AN5724 Rev0.1 | AN5724 Rev0.1 - Guidelines for DDR memory routing on STM32MP2 MPUs | [4] | |
AN5718 Rev.0.1 | AN5718 Rev.0.1 - Migrating from STM32MP15x lines to STM32MP25x lines MPUs | Not yet available | |
AN5726 Rev.0.1 | AN5726 Rev.0.1 - Guidelines for using low-power modes on STM32MP2 MPUs | Not yet available | |
AN5727 Rev.0.1 | AN5727 Rev.0.1 - How to use STPMIC25 for a wall adapter powered application on STM32MP25x lines MPUs | Not yet available | |
Datasheets[1] | |||
DS14284 | DS14284 datasheet for STM32MP251C/F, STM32MP253C/F, STM32MP255C/F, STM32MP257C/F) | [5] | |
DS14285 | DS14285 datasheet for STM32MP251A/D, STM32MP253A/D, STM32MP255A/D, STM32MP257A/D) | [6] | |
DS14278 | STPMIC25 datasheet |
Not yet available | |
Errata sheets | |||
ES0598 rev0.1 | STM32MP251x/3x/5x/7x device revA errata | [7] | |
ES0598 rev0.2 | STM32MP251x/3x/5x/7x device revB errata | Not yet available | |
Reference manuals[1] | |||
RM0457 | STM32MP257 reference manual rev2 (STM32MP25xx advanced Arm®-based 32/64-bit MPUs) |
[8] | |
STPMIC25 draft CTM 0.121 | STPMIC25 draft CTM (0.121) | [9] | |
Boards schematics | |||
MB1854 schematics | Camera expansion board schematics | [10] | |
MB1936 schematics | STM32MP257F-EV1 board schematics with STM32MP25F RevB 18x18 package | [11] | |
MB1605 schematics | STM32MP257F-DK board schematics example with STM32MP25F RevB 14x14 package | [12] | |
DDR routing examples schematics | DDR memory routing examples for STM32MP257F revB | [13] | |
User manuals | |||
UM_STM32MP257F-EV1 | STM32MP2357F-EV1 BETA User Manual | [14] | |
UM_STM32CubeIDE | How to build and debug secure project on STM32MP25 co-processor in STM32CubeIDE | [15] | |
Tools Release Notes | |||
RN_STM32CubeIDE | STM32CubeIDE STM32MP25 Beta Release Note | [16] | |
RN_STM32CubeMX | STM32CubeMX STM32MP25 Beta Release Note | [17] | |
RN_STM32CubeProg | STM32CubeProg STM32MP25 Beta Release Note | [18] |
- ↑ 1.0 1.1 The part numbers are specified in STM32MP25 microprocessor part numbers