1. Article purpose[edit source]
This article describes the FlashLayout file format.
This file is used as an input by STM32CubeProgrammer tool in order to:
- define the Flash memory partitions (see STM32_MPU_Flash_mapping)
- select the files used to boot (see Boot chain overview) and then populate each partition.
The embedded programming service processes this file on the device and interacts with STM32CubeProgrammer to update the Flash memory.
This is done by the stm32prog
command in U-Boot. This command is automatically executed for a serial boot (bootcmd on USB or UART boot). However you can launch it manually from the U-Boot console: this is useful if you want to perform a non-virgin board update front of STM32CubeProgrammer, without manipulating the boot pins.
See AN5275: USB DFU/USART protocols used in STM32MP1 Series bootloaders for protocol details and refer to STM32CubeProgrammer article to know how to use this tool.
The next chapters:
- describe the FlashLayout file format
- give Typical FlashLayout file
- give FlashLayout file to load and start kernel that can be used to load a Linux kernel for direct execution
- give some hints on the Using of the provided FlashLayout files that come as part of STM32 MPU ecosystem deliveries
The FSBL, SSBL definitions can be found in the Boot chain overview.
As explain in TF-A overview, the FIP file includes all the binaries loaded by FSBL=TF-A BL2:
SSBL=U-Boot, the non secure device tree, BL32 = OP-TEE or SP-MIN...
2. FlashLayout file format[edit source]
The FlashLayout is a text file with a tab-separated-value format (tsv). It includes the below elements:
- one line per partition or device
- seven columns, one for each field, provided in the following order:
The lines beginning with the '#' character are ignored and treated as comments.
The "Binary" last column is not used by U-Boot. It is used by STM32CubeProgrammer on the host computer to select the files to be sent to the target.
Several tabulations (<tab>) can be used to allow the correct column alignment in the editor. They are ignored by STM32CubeProgrammer and by U-Boot.
Empty fields are not allowed. The FlashLayout file format supports the none reserved word.
2.1. Examples[edit source]
Below some valid FlashLayout files:
#opt Id Name Type Device Offset Binary - 0x01 fsbl-boot Binary none 0x00000000 tf-a-usb.stm32 - 0x03 fip-boot FIP none 0x00000000 fip.bin P 0x04 fsbl1 Binary mmc0 0x00004400 tf-a-sdcard.stm32 P 0x05 fsbl2 Binary mmc0 0x00044400 tf-a-sdcard.stm32 P 0x06 metadata1 Binary mmc0 0x00084400 metadata.bin P 0x07 metadata2 Binary mmc0 0x000C4400 metadata.bin P 0x08 fip-a FIP mmc0 0x00104400 fip.bin PED 0x09 fip-b FIP mmc0 0x00504400 none PED 0x09 u-boot-env binary mmc0 0x00904400 none P 0x10 bootfs System mmc0 0x00984400 bootfs.ext4 P 0x11 vendorfs FileSystem mmc0 0x04984400 vendorfs.ext4 P 0x12 rootfs FileSystem mmc0 0x05984400 rootfs.ext4 P 0x13 userfs FileSystem mmc0 0x33984400 userfs.ext4
Above, the first line contains only header information. This is not mandatory, as shown below:
- 0x01 fsbl_boot Binary none 0x0 tf-a-usb.stm32
- 0x03 fip_boot FIP none 0x0 fip.bin
P 0x10 sdcard RawImage mmc0 0x0 sdcard.bin
2.2. Field1: Options[edit source]
The Options field defines the operations to perform with a combination of characters: - P D E provided in any order;
First select the line of the FlashLayout with '-' or 'P':
- '-' : none option, the partition or the device is not modified (mandatory if #Field5: Device = none)
- 'P' : Program the partition or the device
- U-Boot requests the binary to STM32CubeProgrammer and programs the partition or the Flash device.
- On the block devices (SD card or e•MMC), the GPT partitioning is performed if all partitions of the device are selected with P.
- For the 'P' option, two optional modifiers can be added:
- 'E' : Empty partition or device, update is not requested (associated "Id" is skipped)
- 'D' : Delete partition or device
The only supported combinations are the following (with character in any order):
- - : no action
- P : update = program the partition or the flash device
- PE : do not update (also EP) : allow the GPT partitioning with empty partition for the block device but equivalent to '-' for RAW flash device
- PD : delete and update (also DP)
- PDE : delete and keep empty (also PED / DPE / DEP / EPD / EDP)
All other combinations are invalid.
2.3. Field2: Id[edit source]
Id identifies in a unique way the "download phase" requested by the device to STM32CubeProgrammer.
It is used by the embedded programming service to identify the next binary that is downloaded to the device.
Their destination depends on the executed code:
- ROM code and TF-A (FSBL): binary loaded in RAM, to start the embedded programming service
- U-Boot(SSBL): the embedded programming service is running, the binary is populated in Flash memory by
stm32prog
command.
The FlashLayout supported ranges are :
Range | Partition |
---|---|
0x01 to 0x0F | Boot partitions with FIP header or with STM32 header: SSBL, FSBL, other (TEE, Cortex-M4 firmware) |
0x10 to 0xF0 | User partitions programmed without header (uimage, dtb, rootfs, vendorfs, userfs) |
All the other values are forbidden in FlashLayout file.
The Id 0x01 and 0x03 are reserved for binaries containing FSBL and SSBL respectively; the presence of these two Id in the FlashLayout file is mandatory to load the embedded service.
2.3.1. Reserved Id[edit source]
The reserved and allowed values in FlashLayout file are the following:
Code | Content | Description |
---|---|---|
0x01 | image containing FSBL | loaded by ROM code in embedded RAM |
0x03 | image containing SSBL | loaded by FSBL in external RAM for serial boot = FIP for OpenSTLinux |
For information some other Id are reserved and used for the communication between the embedded programming service and STM32CubeProgrammer, but they are forbidden in FlashLayout file.
Code | Virtual Partition or State |
---|---|
0x00 | FlashLayout |
0xF1 | Command GetPhase |
0xF2 | OTP |
0xF3 | SSP |
0xF4 | PMIC NVM |
0xFE | State = End of operation |
0xFF | State = Reset |
2.3.2. Using Id for boot partition[edit source]
Even if in the FlashLayout file, any other Id lower than 0x10 (boot partition with FIP header or STM32 header) can identify the binaries containing the FSBL and SSBL to be programmed in Flash memory, the recommended mapping is:
Code | Comment | Content | Description |
---|---|---|---|
0x01 | reserved | FSBL to boot | file containing FSBL with serial load support: loaded by ROM code |
0x03 | reserved | SSBL to boot | file containing SSBL with programming support : loaded by FSBL |
0x04 | FSBL to program 1 | file containing FSBL to program in Flash memory (first copy) | |
0x05 | FSBL to program 2 | file containing FSBL to program in Flash memory (second copy) | |
0x06 | metadata 1 | FBSL metadata to program in Flash memory (first copy) | |
0x07 | metadata 2 | FBSL metadata to program in Flash memory (second copy) | |
0x08 | SSBL to program 1 | file containing SSBL to program in Flash memory (first copy) | |
0x09 | SSBL to program 1 | file containing SSBL to program in Flash memory (second copy) |
It enables having different binaries loaded in RAM (with Reserved ID 0x1 and 0x3) and programmed in Flash memory, for example when an updated feature is deactivated in the binaries to be programmed in Flash memory (see example in #Load and program different binaries).
We also skip the Id 0x2 (not reserved) to have a more coherent order, as U-Boot requests and programs the partitions in Id order.
With OpenSTLinux binaries (FSBL=TF-A and the FIP contains SSBL=U-Boot) , this recommended mapping uses two ID (0x03 and 0x08) for the same FIP file used to boot and to program:
Code | Comment | File | Description |
---|---|---|---|
0x01 | reserved | tf-a-usb.stm32 | TF-A to boot with serial load support on usb |
0x03 | reserved | fip.bin | FIP image file to boot, including U-Boot |
0x04 | tf-a-<dev>.stm32 | TF-A for <dev> boot device to program: first copy | |
0x05 | tf-a-<dev>.stm32 | TF-A for <dev> boot device to program: second copy | |
... | ... | ... | ... |
0x08 | fip.bin | FIP file to program, including U-Boot (same FIP binary than FIP to boot) |
However the minimal mapping is, when the same FSBL and SSBL binaries can be loaded in RAM and programmed in Flash memory:
Code | Comment | Content | Description |
---|---|---|---|
0x01 | reserved | FSBL | file containing FSBL (first copy) to program in Flash memory, also used for serial boot, loaded by ROM code |
0x02 | default | FSBL | file containing FSBL second copy to program in Flash memory |
0x03 | reserved | SSBL | file containing SSBL programmed in Flash memory, also used for serial boot, loaded by FSBL |
2.4. Field3: Name[edit source]
Name of the alternate setting of the USB DFU[1] for U-Boot enumeration. This is a string descriptor that indicates the target memory segment (see Interface Descriptor in DFU spec [2])
This is also the name of the Block device GPT partition: SD card / e•MMC.
The requirements for the GPT partitions, only for device = mmc + instance, are:
- FSBL for SD card boot: the name must start with "fsbl"= fsbl, fsbl1, fsbl2... (ROM code requirement)
- FIP containing SSBL for e•MMC/SD card boot: the name must be:
- "fip" when firmware update is not supported in TF-A
- "fip-a" and "fip-b" for firmware update support in TF-A, see #GPT partuuid of FIP partition.
- a partition named "rootfs", see specific behavior described in #GPT partuuid of rootfs partition.
These requirements are not verified by U-Boot during the Flash programming. If they are not fulfilled, the ROM code or TF-A does not find the boot stage binary and the boot from Flash memory fails.
2.5. Field4: Type[edit source]
Type is only used in U-Boot to select the part of Flash memory to be updated:
- one partition
- all the #Hardware device = RawImage
The supported values are:
GPT | MTD | ||||
---|---|---|---|---|---|
Type | SD card | e•MMC | NAND Flash memory | NOR Flash memory | RAM |
Binary | x | x | x | x | x |
Binary(N) | fsbl | ||||
FIP | x | x | x | x | x |
FileSystem | x | x | x | x | dtb |
System | x | x | UBI | UBI | kernel |
RawImage | x | user data | x | x |
2.5.1. Block device GPT partition: SD card / e•MMC[edit source]
Refer to GPT standard for details [3].
The supported values, with associated partition type GUID (globally unique identifiers[4]), are:
- Binary : raw data / linux reserved
(GUID = 8DA63339-0007-60C0-C436-083AC8230908) - FIP : FIP partition
(GUID =19D5DF83-11B0-457b-BE2C-7559C13142A5)
see also #GPT partuuid of FIP partition - FileSystem : Linux filesystem data
(GUID = 0FC63DAF-8483-4772-8E79-3D69D8477DE4)
ext2/ext4/fat file system - System : FileSystem partition marked as bootable and used by U-Boot to find extlinux.conf configuration file (normally only one in the device, generic DISTRO feature)
For a Block device, the GPT header is updated only if all the partitions of this device are selected with the P option (full update).
2.5.2. Raw Flash device (NAND/NOR Flash memories) MTD partition[edit source]
The supported values are:
- Binary: raw data, skip bad block (partition erase is not needed)
- Binary(N): raw data, skip bad block. The loaded binary is repeated N times.
It is only supported for NAND Flash memories when the partition name starts with "fsbl". It is used to avoid disturbances during the first boot (uncorrectable ECC errors).
The first good block is read from NAND and duplicated N times in the same partition (write skip bad block). - FIP: raw data, skip bad block
- FileSystem: unspecified File system, raw data
- System : normally UBI volume, U-Boot erases all the blocks following the last data in the MTD partition to avoid mount errors.
2.5.3. Hardware device[edit source]
Export the associated device as one alternate setting by using Type=RawImage.
- For SD card, NOR and NAND Flash memories: all the devices
- For e•MMC: the user data area of e•MMC (see #Field6: Offset for access to the boot area partitions)
For RawImage, Offset=0x0 and PartId >= 0x10
2.5.4. RAM device (DDR)[edit source]
The supported values are:
- Binary: raw data
- FileSystem: device tree used in the
bootm
command - System : kernel image used in the
bootm
command (uImage.bin for example)
When a RAM device is present in the FlashLayout, the programming service will not reboot but start the loaded kernel image with the associated device tree (when present, when it is absent the U-Boot device tree is used).
2.6. Field5: Device[edit source]
Select the targeted device and the instance (starting at 0) as defined by U-Boot device tree:
- mmc + instance : mmc0, mmc1, mmc2
It is used for e•MMC or SD card on SDMMC. In the below examples:- SD card = mmc0 (SDMMC1)
- e•MMC = mmc1 (SDMMC2)
- nor + instance : nor0
It is used for NOR on QUADSPI. - nand + instance : nand0
It is used for parallel NAND Flash memories on FMC. - spi-nand + instance : spi-nand0
It is used for serial NAND Flash memories on QSPI. - none only used to load the programming service in RAM
It is allowed only for the reserved bootloaders partition (FSBL=0x1 and SSBL=0x3). In this case, the only allowed fields are: Type=Binary, Offset=0x0 and option=- - ram + instance : ram0
It is used for files loaded in RAM by the programming service, for example to load and execute kernel.
Several devices can be mixed in the same FlashLayout file.
2.7. Field6: Offset[edit source]
The supported values are:
- boot1: first boot area partition of e•MMC (offset is 0x0)
- boot2: second boot area partition of e•MMC (offset is 0x0)
- Offset in Bytes: offset in Flash memory area (in the user data area for e•MMC)
Refer to #Partition sizes for offset constraints.
2.8. Field7: Binary[edit source]
This file is used by STM32CubeProgrammer to find the file associated to each Id when it is requested by embedded programming service .
The file can be absent (Binary=none in the tsv file) only for skipped partitions tagged with the E option. In all other cases, this file is sent to U-Boot to update the Flash memory only for the partitions selected with the P option.
2.9. GPT partuuid[edit source]
For GPT on block device (SD card / e•MMC), U-Boot can also set a unique partition guid [4](PARTUUID) on one partition.
This partition PARTUUID is distinct from the filesystem UUID and it is persistent.
Refer to GPT standard for details. [3]
2.9.1. GPT partuuid of FIP partition[edit source]
If #Field4: Type = FIP and the GPT partition UUID is defined according the #Field3: Name value:
- fip-a : PARTUUID = "4FD84C93-54EF-463F-A7EF-AE25FF887087"
- fip-b : PARTUUID = "09C54952-D5BF-45AF-ACEE-335303766FB3"
These value are aligned with the metadata generated by TF-A tools and allow to support the firmware update in TF-A BL2.
2.9.2. GPT partuuid of rootfs partition[edit source]
If #Field3: Name = rootfs and for each targeted MMC instance with #Field5: Device:
- rmmc0: PARTUUID = "e91c4e10-16e6-4c0e-bd0e-77becf4a3582"
- rmmc1: PARTUUID = "491f6117-415d-4f53-88c9-6e0de54deac6"
- rmmc2: PARTUUID = "fd58f1c7-be0d-4338-8ee9-ad8f050aeb18"
This value can be used with the "root" argument in the kernel bootargs to identify the partition used for the "Root filesystem". For instance, "root=PARTUUID=e91c4e10-16e6-4c0e-bd0e-77becf4a3582" [5] starts with the partition named rootfs on mmc0.
2.10. Partition operations[edit source]
To update only one partition, use the same FlashLayout file, keep the #Field1: Options=P for the partition to update and change the others to -.
And to delete only one partition, add the DE option on the corresponding line.
To update fip partition (based on #Examples):
- 0x01 fsbl-boot Binary none 0x00000000 tf-a-usb.stm32 - 0x03 fip-boot FIP none 0x00084400 fip.bin - 0x04 fsbl1 Binary mmc0 0x00004400 tf-a-sdcard.stm32 - 0x05 fsbl2 Binary mmc0 0x00044400 tf-a-sdcard.stm32 P 0x06 fip FIP mmc0 0x00084400 fip.bin - 0x10 bootfs System mmc0 0x00484400 bootfs.ext4 - 0x11 vendorfs FileSystem mmc0 0x04484400 vendorfs.ext4 - 0x12 rootfs FileSystem mmc0 0x05484400 rootfs.ext4 - 0x13 userfs FileSystem mmc0 0x33E84400 userfs.ext4
To delete fip partition:
- 0x01 fsbl-boot Binary none 0x00000000 tf-a-usb.stm32 - 0x03 fip-boot Binary FIP 0x00084400 fip.bin - 0x04 fsbl1 Binary mmc0 0x00004400 tf-a-sdcard.stm32 - 0x05 fsbl2 Binary mmc0 0x00044400 tf-a-sdcard.stm32 PDE 0x06 fip FIP mmc0 0x00084400 fip.bin - 0x10 bootfs System mmc0 0x00484400 bootfs.ext4 - 0x11 vendorfs FileSystem mmc0 0x04484400 vendorfs.ext4 - 0x12 rootfs FileSystem mmc0 0x05484400 rootfs.ext4 - 0x13 userfs FileSystem mmc0 0x33E84400 userfs.ext4
2.11. Partition sizes[edit source]
The partitions are contiguous (no holes in Flash memory).
The last partition continues until the end of the selected Flash memory.
To reduce the size of the last partition, use an 'Empty' partition and leave it unused.
All the partitions need to be present in the FlashLayout file, even if they are not selected or empty.
Then the offset and size of each partition are compared with:
- pre-existing GPT partitioning, for updates on block devices (e•MMC or SD card)
- predefined partitioning for MTD devices (NOR and NAND): see mtdparts environment variable in U-Boot for more information.
In case of partition size error, compare the existing partition size in U-Boot with the offset in the FlashLayout file.
2.11.1. GPT partition sizes[edit source]
Each GPT partition must be aligned to:
- 512 bytes (LBA)
- e•MMC erase group size
The first partition starts after 17 Kbytes (default size of GPT header for 128 entries in U-Boot).
Prior to updating partitions in a block device, check the partition size by executing the U-Boot command "part list" on the selected device:
part list mmc 0 Partition Map for MMC device 0 -- Partition Type: EFI Part Start LBA End LBA Name Attributes Type GUID Partition GUID 1 0x00000022 0x00000221 "fsbl1" attrs: 0x0000000000000000 type: 8da63339-0007-60c0-c436-083ac8230908 guid: 35b71598-cc09-43f0-b9e2-f2a4037202ee 2 0x00000222 0x00000421 "fsbl2" attrs: 0x0000000000000000 type: 8da63339-0007-60c0-c436-083ac8230908 guid: 3a8bb930-75b1-473a-819b-0749b62893f7 3 0x00000422 0x00002421 "fip" attrs: 0x0000000000000000 type: 8da63339-0007-60c0-c436-083ac8230908 guid: 1014bf09-4e50-418c-82a3-807576a5f25c 4 0x00002422 0x00022421 "bootfs" attrs: 0x0000000000000004 type: 0fc63daf-8483-4772-8e79-3d69d8477de4 type: linux guid: 6a1a0147-cc61-41ed-b0a7-e8fed794d4ab 5 0x00022422 0x0002a421 "vendorfs" attrs: 0x0000000000000000 type: 0fc63daf-8483-4772-8e79-3d69d8477de4 type: linux guid: 28f351bb-f287-4223-9c35-c318e0d669b1 6 0x0002a422 0x001aa421 "rootfs" attrs: 0x0000000000000000 type: 0fc63daf-8483-4772-8e79-3d69d8477de4 type: linux guid: e91c4e10-16e6-4c0e-bd0e-77becf4a3582 7 0x001aa422 0x01dacbdc "userfs" attrs: 0x0000000000000000 type: 0fc63daf-8483-4772-8e79-3d69d8477de4 type: linux guid: 3c26f1ba-c7cd-4b58-ae90-340bfe9b02bd
Warning: Start and end are indicated in multiple of LBA (512 bytes by default).
To check the e•MMC erase group size in U-Boot, select the mmc device (here 1) and use the command "mmc info" in U-Boot.
mmc dev 1 switch to partitions #0, OK mmc1(part 0) is current device mmc info Device: STM32 SD/MMC Manufacturer ID: 11 OEM: 100 Name: 004GA Bus Speed: 52000000 Mode: MMC High Speed (52MHz) Rd Block Len: 512 MMC version 5.0 High Capacity: Yes Capacity: 3.7 GiB Bus Width: 8-bit Erase Group Size: 512 KiB HC WP Group Size: 4 MiB User Capacity: 3.7 GiB WRREL Boot Capacity: 2 MiB ENH RPMB Capacity: 512 KiB ENH Boot area 0 is not write protected Boot area 1 is not write protected
2.11.2. MTD partition sizes[edit source]
Each MTD partition must be aligned to the device erase block size (NOR/NAND Flash memory).
In U-Boot shell, this size is verified with the command nand
or sf
, for example :
nand info Device 0: nand0, sector size 256 KiB Page size 4096 b OOB size 224 b Erase size 262144 b subpagesize 4096 b options 0x00084200 bbt options 0x00060000
sf probe SF: Detected mx25l51235f with page size 256 Bytes, erase size 64 KiB, total 64 MiB
For MTD, the U-Boot uses the mtdparts variable.
Execute the U-Boot command mtdparts
or mtd
to know the current value:
mtdparts mtd list
By default on ST board, the mtdpart variable is built dynamically in board_mtdparts_default() under CONFIG_SYS_MTDPARTS_RUNTIME
with the STMicroelectronics configs:
- CONFIG_MTDPARTS_NAND0_BOOT = "512k(fsbl1),512k(fsbl2),512k(metadata1),512k(metadata2),4m(fip-a1),4m(fip-a2),4m(fip-b1),4m(fip-b2)"
- CONFIG_MTDPARTS_NOR0_BOOT = "256k(fsbl1),256k(fsbl2),256k(metadata1),256k(metadata2),4m(fip-a1),4m(fip-a2),4m(fip-b1),4m(fip-b2),512k(u-boot-env)"
- CONFIG_MTDPARTS_SPINAND0_BOOT = "512k(fsbl1),512k(fsbl2),512k(metadata1),512k(metadata2),4m(fip-a1),4m(fip-a2),4m(fip-b1),4m(fip-b2)"
On NAND Flash, the last partition 'UBI' uses the remaining space with several UBI volumes for OpenSTLinux:
uboot_config, uboot_config_r, boot, rootfs, vendorfs, and userfs ("boot" is the volume name expected by U-Boot).
On NOR Flash, the last partition named 'nor_user', is a free MTD partition which uses the remaining space.
We align each partition size on max supported erase block size (512 Kbytes on NAND and 256 Kbytes on NOR).
To change the MTP partitioning on NOR and NAND Flash memories, update these configurations in your U-Boot defconfig as explained in U-Boot and in 'MTD partitions in U-Boot' or override this behavior in your board.
2.11.3. NOR MTD partition on ST boards[edit source]
The default MTD partitions used on the ST boards with OpenSTLinux for NOR boot is:
mtd list
SF: Detected mx66l51235l with page size 256 Bytes, erase size 64 KiB, total 64 MiB
List of MTD devices:
* nor0
- device: mx66l51235l@0
- parent: spi@58003000
- driver: jedec_spi_nor
- path: /soc/spi@58003000/mx66l51235l@0
- type: NOR flash
- block size: 0x10000 bytes
- min I/O: 0x1 bytes
- 0x000000000000-0x000004000000 : "nor0"
- 0x000000000000-0x000000040000 : "fsbl1"
- 0x000000040000-0x000000080000 : "fsbl2"
- 0x000000080000-0x0000000c0000 : "metadata1"
- 0x0000000c0000-0x000000100000 : "metadata2"
- 0x000000100000-0x000000500000 : "fip-a"
- 0x000000500000-0x000000900000 : "fip-b"
- 0x000000900000-0x000000980000 : "u-boot-env"
- 0x000000980000-0x000004000000 : "nor_user"
* nor1
- device: mx66l51235l@1
- parent: spi@58003000
- driver: jedec_spi_nor
- path: /soc/spi@58003000/mx66l51235l@1
- type: NOR flash
- block size: 0x10000 bytes
- min I/O: 0x1 bytes
- 0x000000000000-0x000004000000 : "nor1"
mtdparts SF: Detected mx66l51235l with page size 256 Bytes, erase size 64 KiB, total 64 MiB device nor0 <nor0>, # parts = 8 #: name size offset mask_flags 0: fsbl1 0x00040000 0x00000000 0 1: fsbl2 0x00040000 0x00040000 0 2: metadata1 0x00040000 0x00080000 0 3: metadata2 0x00040000 0x000c0000 0 4: fip-a 0x00400000 0x00100000 0 5: fip-b 0x00400000 0x00500000 0 6: u-boot-env 0x00080000 0x00900000 0 7: nor_user 0x03680000 0x00980000 0 active partition: nor0,0 - (fsbl1) 0x00040000 @ 0x00000000 defaults: mtdids : nor0=nor0 mtdparts: mtdparts=nor0:256k(fsbl1),256k(fsbl2),256k(metadata1),256k(metadata2),4m(fip-a),4m(fip-b),512k(u-boot-env),-(nor_user)
This default partitioning is compatible for any NOR device, as we align each partition size on max supported erase block size on = 256 Kbytes.
2.11.4. NAND MTD partition on ST boards[edit source]
The default MTD partitions used on the ST boards with OpenSTLinux for NAND boot is:
mtd list List of MTD devices: * nand0 - type: NAND flash - block size: 0x40000 bytes - min I/O: 0x1000 bytes - OOB size: 224 bytes - OOB available: 118 bytes - ECC strength: 8 bits - ECC step size: 512 bytes - bitflip threshold: 6 bits - 0x000000000000-0x000040000000 : "nand0" - 0x000000000000-0x000000080000 : "fsbl1" - 0x000000080000-0x000000100000 : "fsbl2" - 0x000000100000-0x000000180000 : "metadata1" - 0x000000180000-0x000000200000 : "metadata2" - 0x000000200000-0x000000600000 : "fip-a1" - 0x000000600000-0x000000a00000 : "fip-a2" - 0x000000a00000-0x000000e00000 : "fip-b1" - 0x000000e00000-0x000001200000 : "fip-b2" - 0x000001200000-0x000040000000 : "UBI"
mtdparts device nand0 <nand0>, # parts = 9 #: name size offset mask_flags 0: fsbl1 0x00080000 0x00000000 0 1: fsbl2 0x00080000 0x00080000 0 2: metadata1 0x00080000 0x00100000 0 3: metadata2 0x00080000 0x00180000 0 4: fip-a1 0x00400000 0x00200000 0 5: fip-a2 0x00400000 0x00600000 0 6: fip-b1 0x00400000 0x00a00000 0 7: fip-b2 0x00400000 0x00e00000 0 8: UBI 0x3ee00000 0x01200000 0 active partition: nand0,0 - (fsbl1) 0x00080000 @ 0x00000000 defaults: mtdids : nand0=nand0,nor0=nor0 mtdparts: mtdparts=nand0:512k(fsbl1),512k(fsbl2),512k(metadata1),512k(metadata2),4m(fip-a1),4m(fip-a2),4m(fip-b1),4m(fip-b2),- (UBI);nor0:256k(fsbl1),256k(fsbl2),256k(metadata1),256k(metadata2),4m(fip-a),4m(fip-b),512k(u-boot-env),-(nor_user)
This default partitioning is compatible for any NAND device, as we align each partition size on max supported erase block size on NAND = 512 Kbytes.
3. Typical FlashLayout file[edit source]
This chapter describes the Layout file for the typical OpenSTLinux boot use cases based on STM32_MPU_Flash_mapping.
Data are presented in tables for better readability despite the Layout file is plain text.
In the next examples, the boot chain of OpenSTLinux is used together with the following files:
- FSBL = TF-A with 2 different binary
- FSBL to boot with serial boot over USB = tf-a-usb.stm32
TF-A BL2 with STM32CubeProgrammer USB support, replaced by tf-a-uart.stm32 when UART is used - FSBL to program = tf-a-<dev>.stm32 (TF-A with boot from <dev> support, <dev> = emmc, sdcard, nand, spinand, nor)
- FSBL to boot with serial boot over USB = tf-a-usb.stm32
- TF-A metadata binary for FIP update support = 'metadata.bin
- FIP file containing SSBL = fip.bin, it includes secure monitor, from TF-A = SPMIN or from OP-TEE, SSBL=U-Boot binary and device tree.
3.1. NOR Flash memory and SD card[edit source]
NOR Flash memory in RAW, containing the bootloaders, use the MTD partitions for OpenSTLinux:
- 2 for TF-A : 2 copy for failsafe update
- 2 for TF-A metadata for FIP update support: 2 copy for failsafe update
- 2 for FIP : file in the first slot (fip-a), the second is empty (fip-b), reserved for FIP update support
- 1 for U-Boot environment
SD card using GPT: several EXT4 partitions.
In this next NOR flashlayout for the STMicroelectronics boards, we align each partition on max supported erase block size of NOR 256 Kbytes, based on default MTD partition on NOR but the size of these MTD partitions can be optimized for NOR with lower erase block size.
Opt | Part | Name | Type | Device | Offset | Binary |
---|---|---|---|---|---|---|
- | 0x01 | fsbl-boot | Binary | none | 0x0 | tf-a-usb.stm32 |
- | 0x03 | fip-boot | Binary | none | 0x0 | fip.bin |
P | 0x04 | fsbl1 | Binary | nor0 | 0x00000000 | tf-a-nor.stm32 |
P | 0x05 | fsbl2 | Binary | nor0 | 0x00040000 | tf-a-nor.stm32 |
P | 0x06 | metadata1 | Binary | nor0 | 0x00080000 | metadata.bin |
P | 0x07 | metadata2 | Binary | nor0 | 0x000C0000 | metadata.bin |
P | 0x08 | fip-a | Binary | nor0 | 0x00100000 | fip.bin |
PED | 0x09 | fip-b | Binary | nor0 | 0x00500000 | none |
PED | 0x0A | u-boot-env | Binary | nor0 | 0x00900000 | none |
PE | 0x0B | unused | Binary | nor0 | 0x00980000 | none |
P | 0x10 | bootfs | System | mmc0 | 0x00004400 | bootfs.ext4 |
P | 0x11 | vendorfs | FileSystem | mmc0 | TBD | vendorfs.ext4 |
P | 0x12 | rootfs | FileSystem | mmc0 | TBD | rootfs.ext4 |
P | 0x13 | userfs | FileSystem | mmc0 | TBD | userfs.ext4 |
The PartId 0x09 is empty/deleted in nor0 ('PED' flag), the second FIP slot is empty and cleared.
The PartId 0x0A is empty/deleted in nor0 ('PED' flag), the U-Boot environment is cleared.
The PartId 0x0B is an empty/free (user partition associated to 'nor_user' MTD partition in U-Boot ('PE' flag).
The 'System' partition 0x10 named "bootfs" is marked 'bootable'.
The partition 0x12 named "rootfs" has a specific PARTUUID.
3.2. NAND Flash memory[edit source]
The next example is compatible for any NAND device, as we align each partition size on max supported erase block size on NAND = 512 Kbyte and provides spare block for each partition on STMicrolectronics board, using NAND with 256 Kbyte erase block.
We have, based on the default MTD partitions on NAND, the MTD partitions:
- 2 for TF-A = 2 copy for failsafe update and redundancy
- 2 for metadata = 2 copy for failsafe update and redundancy
- 4 for FIP:
- 2 copies (1 and 2) for NAND redundancy of the each slot for FIP update support
- the first slot A is populated with the initial FIP file = fip.bin in fip-a1 and fip-a2
- the second slot B is empty: fip-b1 and fip-b2
- the number of remaining spare block, allowing to skip bad blocks in each FIP partition, depends of the size of the FIP
For parallel NAND, the MTD device is nand0:
Opt | Part | Name | Type | Device | Offset | Binary |
---|---|---|---|---|---|---|
- | 0x01 | fsbl-boot | Binary | none | 0x0 | tf-a-usb.stm32 |
- | 0x03 | fip-boot | FIP | none | 0x0 | fip.bin |
P | 0x04 | fsbl | Binary | nand0 | 0x00000000 | tf-a-nand.stm32 |
P | 0x05 | fsbl | Binary | nand0 | 0x00080000 | tf-a-nand.stm32 |
P | 0x06 | metadata1 | Binary | nand0 | 0x00100000 | metadata.bin |
P | 0x07 | metadata2 | Binary | nand0 | 0x00180000 | metadata.bin |
P | 0x08 | fip-a1 | FIP | nand0 | 0x00200000 | fip.bin |
P | 0x09 | fip-a2 | FIP | nand0 | 0x00600000 | fip.bin |
PED | 0x0A | fip-b1 | FIP | nand0 | 0x00A00000 | none |
PED | 0x0B | fip-b2 | FIP | nand0 | 0x00E00000 | none |
P | 0x10 | UBI | System | nand0 | 0x01200000 | ubi.bin |
For serial NAND, the MTD device is spi-nand0:
Opt | Part | Name | Type | Device | Offset | Binary |
---|---|---|---|---|---|---|
- | 0x01 | fsbl-boot | Binary | none | 0x0 | tf-a-usb.stm32 |
- | 0x03 | fip-boot | FIP | none | 0x0 | fip.bin |
P | 0x04 | fsbl | Binary | spi-nand0 | 0x00000000 | tf-a-spi-nand.stm32 |
P | 0x05 | fsbl | Binary | spi-nand0 | 0x00080000 | tf-a-spi-nand.stm32 |
P | 0x06 | metadata1 | Binary | spi-nand0 | 0x00100000 | metadata.bin |
P | 0x07 | metadata2 | Binary | spi-nand0 | 0x00180000 | metadata.bin |
P | 0x08 | fip-a1 | FIP | spi-nand0 | 0x00200000 | fip.bin |
P | 0x09 | fip-a2 | FIP | spi-nand0 | 0x00600000 | fip.bin |
PED | 0x0A | fip-b1 | FIP | spi-nand0 | 0x00A00000 | none |
PED | 0x0B | fip-b2 | FIP | spi-nand0 | 0x00E00000 | none |
P | 0x10 | UBI | System | spi-nand0 | 0x01200000 | ubi.bin |
This partitioning can be optimized for NAND with erase block size lower than 512kB.
Nota: If you increase the number of copie of FIP, you need to check the number spare block and perhaps update the MTD partition in U-Boot.
For OpenSTLinux, the name of UBI MTD partition names is required by the U-Boot UBI bootcmd and by CONFIG_ENV_UBI_PART.
System is required by for UBI support to erase the last block of the partition.
This partition have several UBI volumes as defined in NAND memory mapping:
Name | Type | Description |
---|---|---|
uboot_config | RAW | The RAW partition used by U-Boot to save its environment (CONFIG_ENV_IS_IN_UBI), the volume name is defined by CONFIG_ENV_UBI_VOLUME |
uboot_config_r | RAW | The RAW partition used by U-Boot to save its redundancy environment (CONFIG_ENV_IS_IN_UBI), the volume name is defined by CONFIG_ENV_UBI_VOLUME_REDUND |
boot | UBIFS | The partition used by U-Boot to boot the kernel, with extlnux.conf file; the volume name boot is required by the U-Boot UBI bootcmd: ubifs_boot |
vendorfs | UBIFS | A file system for third-party proprietary binaries |
rootfs | UBIFS | Linux root file system |
userfs | UBIFS | The user file system |
3.3. e•MMC[edit source]
TF-A is copied in the two boot area partitions of e•MMC (hidden partition) for failsafe update.
The GPT partitioning is used on the user area. The first partition offset starts just after the GPT header at 17-Kbyte offset.
OpenSTLinux defines by default the GPT partitions:
- 2 for TF-A metata: 2 copy for failsafe update
- 2 for FIP: only first slot is used, the second slot is empty
- 1 for U-Boot environment, named u-boot-env' on St Microelectronics boards
- the next partitions are pre-populated with ext4 partition: bootfs, vendorfs, rootfs, userfs
Opt | Part | Name | Type | Device | Offset | Binary |
---|---|---|---|---|---|---|
- | 0x01 | fsbl-boot | Binary | none | 0x0 | tf-a-usb.stm32 |
- | 0x03 | fip-boot | FIP | none | 0x0 | fip.bin |
P | 0x04 | fsbl1 | Binary | mmc1 | boot1 | tf-a-emmc.stm32 |
P | 0x05 | fsbl2 | Binary | mmc1 | boot2 | tf-a-emmc.stm32 |
P | 0x06 | metadata1 | FIP | mmc1 | 0x00080000 | metadata.bin |
P | 0x07 | metadata2 | FIP | mmc1 | 0x00100000 | metadata.bin |
P | 0x08 | fip-a | Binary | mmc1 | 0x00180000 | fip.bin |
PED | 0x09 | fip-b | Binary | mmc1 | 0x00580000 | none |
PED | 0x0A | u-boot-env | Binary | mmc1 | 0x00980000 | none |
P | 0x10 | bootfs | System | mmc1 | 0x00A00000 | bootfs.ext4 |
P | 0x11 | vendorfs | FileSytem | mmc1 | TDB | vendorfs.ext4 |
P | 0x12 | rootfs | FileSytem | mmc1 | TDB | rootfs.ext4 |
P | 0x13 | userfs | FileSytem | mmc1 | TDB | userfs.ext4 |
The FIP partitions named "fip-a" and "fip-b" have a specific PARTUUID.
The partition 0xA u-boot-env is erased before update with option D to clean the U-Boot environment.
The 'System' partition named "bootfs" is marked 'bootable'.
The partition named "rootfs" has a specific PARTUUID.
3.4. SD card[edit source]
OpenSTLinux defines by default the GPT partitions:
- 2 for TF-A partitions for fail safe update
- 2 for TF-A metata: 2 copy for failsafe update
- 2 for FIP: only first slot is used, the second slot is empty
- 1 for U-Boot environment, named u-boot-env' on St Microelectronics boards
- the next partitions are pre-populated with ext4 partition: bootfs, vendorfs, rootfs, userfs
The GPT partitioning is used so fsbl1 starts just after the GPT header at 17-Kbyte offset.
Opt | Part | Name | Type | Device | Offset | Binary |
---|---|---|---|---|---|---|
- | 0x01 | fsbl-boot | Binary | none | 0x0 | tf-a-usb.stm32 |
- | 0x03 | fip-boot | FIP | none | 0x0 | fip.bin |
P | 0x04 | fsbl1 | Binary | mmc0 | 0x00004400 | tf-a-sdcard.stm32 |
P | 0x05 | fsbl2 | Binary | mmc0 | 0x00044400 | tf-a-sdcard.stm32 |
P | 0x06 | medata1 | Binary | mmc0 | 0x00084400 | metadata.bin |
P | 0x07 | medata2 | Binary | mmc0 | 0x00084400 | metadata.bin |
P | 0x08 | fip-a | FIP | mmc0 | 0x000C4400 | fip.bin |
PED | 0x09 | fip-b | FIP | mmc0 | 0x00104400 | none |
PED | 0x0A | u-boot-env | Binary | mmc0 | 0x00504400 | none |
P | 0x10 | bootfs | System | mmc0 | 0x00904400 | bootfs.ext4 |
P | 0x11 | vendorfs | FileSytem | mmc0 | TBD | vendorfs.ext4 |
P | 0x12 | rootfs | FileSytem | mmc0 | TBD | rootfs.ext4 |
P | 0x13 | userfs | FileSytem | mmc0 | TBD | userfs.ext4 |
The FIP partitions named "fip-a" and "fip-b" have a specific PARTUUID.
The partition 0xA u-boot-env is erased before update with option D to clean the U-Boot environment.
The 'System' partition named "bootfs" is marked 'bootable'.
The partition named "rootfs" has a specific PARTUUID.
4. FlashLayout file to load and start U-Boot[edit source]
To be abble to load U-Boot with STM32CubeProgrammer, you can use this file:
For USB:
Opt | Part | Name | Type | Device | Offset | Binary |
---|---|---|---|---|---|---|
- | 0x01 | fsbl-boot | Binary | none | 0x0 | tf-a-usb.stm32 |
- | 0x03 | fip-boot | FIP | none | 0x0 | fip.bin |
For UART:
Opt | Part | Name | Type | Device | Offset | Binary |
---|---|---|---|---|---|---|
- | 0x01 | fsbl-boot | Binary | none | 0x0 | tf-a-uart.stm32 |
- | 0x03 | fip-boot | FIP | none | 0x0 | fip.bin |
5. FlashLayout file to load and start kernel[edit source]
Load programming service with Device=none.
Load kernel uImage and device tree in DDR, Device=ram0.
Opt | Part | Name | Type | Device | Offset | Binary |
---|---|---|---|---|---|---|
- | 0x01 | fsbl-boot | Binary | none | 0x0 | tf-a-usb.stm32 |
- | 0x03 | fip-boot | FIP | none | 0x0 | fip.bin |
P | 0x10 | kernel | System | ram0 | 0xC2000000 | uImage.bin |
P | 0x11 | dtb | FileSytem | ram0 | 0xC4000000 | stm32mp157f-ev1.dtb |
This Linux kernel is started by a bootm
command after the STM32CubeProgrammer DFU detach request, by using CLI -detach option.
For example on usb:
STM32_Programmer_CLI -c port=USB1 -d flashlayout.tsv STM32_Programmer_CLI -c port=USB1 -detach
To fully boot this Linux kernel, the used rootfs must be defined (it is a generic feature not explained in this WIKI):
- initramfs integrated in uImage.bin (with INITRD command in Linux build configuration file or with INITRAMFS_IMAGE_BUNDLE with YOCTO),
- an external roofs, with a location defined in command line provided in the provided Linux kernel device tree.
6. Using provided FlashLayout files[edit source]
The binary and the associated pre-defined FlashLayout files for STM32CubeProgrammer over USB are provided by ST in the Discovery kit.
For example, in STM32MP15 Discovery kits, you can find the distribution images as well as the file FlashLayout_sdcard_stm32mp157f-ev1-trusted.tsv:
#Opt Id Name Type IP Offset Binary - 0x01 fsbl-boot Binary none 0x0 arm-trusted-firmware/tf-a-stm32mp157f-ev1-usb.stm32 - 0x03 fip-boot Binary none 0x0 fip/fip-stm32mp157f-ev1-trusted.bin P 0x04 fsbl1 Binary mmc0 0x00004400 arm-trusted-firmware/tf-a-stm32mp157f-ev1-sdcard.stm32 P 0x05 fsbl2 Binary mmc0 0x00044400 arm-trusted-firmware/tf-a-stm32mp157f-ev1-sdcard.stm32 PD 0x06 fip Binary mmc0 0x00084400 fip/fip-stm32mp157f-ev1-trusted.bin P 0x10 boot System mmc0 0x00484400 st-image-bootfs-openstlinux-weston-stm32mp1.ext4 P 0x11 vendorfs FileSystem mmc0 0x04484400 st-image-vendorfs-openstlinux-weston-stm32mp1.ext4 P 0x12 rootfs FileSystem mmc0 0x05484400 st-image-weston-openstlinux-weston-stm32mp1.ext4 P 0x13 userfs FileSystem mmc0 0x33E84400 st-image-userfs-openstlinux-weston-stm32mp1.ext4
They are used to program over USB all the binary on the flash device . You can use these FlashLayout files as a starting point and simply modify them:
- #Using STM32Programmer over UART
- #Updating partitions
- #Updating partitions using official ST bootloaders
6.1. Using STM32Programmer over UART[edit source]
To use the provided STM32CubeProgrammer over UART, the TF-A BL2 binary with USB support tf-a-<board>-usb.stm32 must be replaced in the flashlayout file by the TF-A BL2 binary with UART support: tf-a-<board>-uart.stm32.
Opt | Part | Name | Type | Device | Offset | Binary |
---|---|---|---|---|---|---|
- | 0x01 | fsbl-boot | Binary | none | 0x0 | arm-trusted-firmware/tf-a-stm32mp157f-ev1-uart.stm32 |
- | 0x03 | fip-boot | Binary | none | 0x0 | fip/fip-stm32mp157f-ev1-trusted.bin |
P | 0x04 | fsbl1 | Binary | mmc0 | 0x00004400 | arm-trusted-firmware/tf-a-stm32mp157f-ev1-sdcard.stm32 |
P | 0x05 | fsbl2 | Binary | mmc0 | 0x00044400 | arm-trusted-firmware/tf-a-stm32mp157f-ev1-sdcard.stm32 |
PD | 0x06 | fip | Binary | mmc0 | 0x00084400 | fip/fip-stm32mp157f-ev1-trusted.bin |
P | 0x10 | bootfs | System | mmc0 | 0x00484400 | st-image-bootfs-openstlinux-weston-stm32mp1.ext4 |
P | 0x11 | vendorfs | FileSystem | mmc0 | 0x04484400 | st-image-vendorfs-openstlinux-weston-stm32mp1.ext4 |
P | 0x12 | rootfs | FileSystem | mmc0 | 0x05484400 | st-image-core-openstlinux-weston-stm32mp1.ext4 |
P | 0x13 | userfs | FileSystem | mmc0 | 0x33E84400 | st-image-userfs-openstlinux-weston-stm32mp1.ext4 |
The associated text file becomes :
#Opt Id Name Type IP Offset Binary - 0x01 fsbl-boot Binary none 0x0 arm-trusted-firmware/tf-a-stm32mp157f-ev1-uart.stm32 - 0x03 fip-boot Binary none 0x0 fip/fip-stm32mp157f-ev1-trusted.bin P 0x04 fsbl1 Binary mmc0 0x00004400 arm-trusted-firmware/tf-a-stm32mp157f-ev1-sdcard.stm32 P 0x05 fsbl2 Binary mmc0 0x00044400 arm-trusted-firmware/tf-a-stm32mp157f-ev1-sdcard.stm32 PD 0x06 fip Binary mmc0 0x00084400 fip/fip-stm32mp157f-ev1-trusted.bin P 0x10 boot System mmc0 0x00484400 st-image-bootfs-openstlinux-weston-stm32mp1.ext4 P 0x11 vendorfs FileSystem mmc0 0x04484400 st-image-vendorfs-openstlinux-weston-stm32mp1.ext4 P 0x12 rootfs FileSystem mmc0 0x05484400 st-image-weston-openstlinux-weston-stm32mp1.ext4 P 0x13 userfs FileSystem mmc0 0x33E84400 st-image-userfs-openstlinux-weston-stm32mp1.ext4
6.2. Updating partitions[edit source]
To update only some partitions, change the FlashLayout and only "select" the partitions that need to be updated:
Options field inside the FlashLayout is kept to P for partition(s) that need to be updated, others are changed to -.
Then execute STM32CubeProgrammer as before.
Example to update only U-Boot binary and st-image-bootfs filesystem :
Opt | Part | Name | Type | Device | Offset | Binary |
---|---|---|---|---|---|---|
- | 0x01 | fsbl-boot | Binary | none | 0x0 | arm-trusted-firmware/tf-a-stm32mp157f-ev1-usb.stm32 |
- | 0x03 | fip-boot | Binary | none | 0x0 | fip/fip-stm32mp157f-ev1-trusted.bin |
- | 0x04 | fsbl1 | Binary | mmc0 | 0x00004400 | arm-trusted-firmware/tf-a-stm32mp157f-ev1-sdcard.stm32 |
- | 0x05 | fsbl2 | Binary | mmc0 | 0x00044400 | arm-trusted-firmware/tf-a-stm32mp157f-ev1-sdcard.stm32 |
PD | 0x06 | fip | Binary | mmc0 | 0x00084400 | fip/fip-stm32mp157f-ev1-trusted.bin |
P | 0x10 | bootfs | System | mmc0 | 0x00484400 | st-image-bootfs-openstlinux-weston-stm32mp1.ext4 |
- | 0x11 | vendorfs | FileSystem | mmc0 | 0x04484400 | st-image-vendorfs-openstlinux-weston-stm32mp1.ext4 |
- | 0x12 | rootfs | FileSystem | mmc0 | 0x05484400 | st-image-core-openstlinux-weston-stm32mp1.ext4 |
- | 0x13 | userfs | FileSystem | mmc0 | 0x33E84400 | st-image-userfs-openstlinux-weston-stm32mp1.ext4 |
The associated text file becomes :
#Opt Id Name Type IP Offset Binary - 0x01 fsbl-boot Binary none 0x0 arm-trusted-firmware/tf-a-stm32mp157f-ev1-usb.stm32 - 0x03 fip-boot Binary none 0x0 fip/fip-stm32mp157f-ev1-trusted.bin - 0x04 fsbl1 Binary mmc0 0x00004400 arm-trusted-firmware/tf-a-stm32mp157f-ev1-sdcard.stm32 - 0x05 fsbl2 Binary mmc0 0x00044400 arm-trusted-firmware/tf-a-stm32mp157f-ev1-sdcard.stm32 PD 0x06 fip Binary mmc0 0x00084400 fip/fip-stm32mp157f-ev1-trusted.bin P 0x10 boot System mmc0 0x00484400 st-image-bootfs-openstlinux-weston-stm32mp1.ext4 - 0x11 vendorfs FileSystem mmc0 0x04484400 st-image-vendorfs-openstlinux-weston-stm32mp1.ext4 - 0x12 rootfs FileSystem mmc0 0x05484400 st-image-weston-openstlinux-weston-stm32mp1.ext4 - 0x13 userfs FileSystem mmc0 0x33E84400 st-image-userfs-openstlinux-weston-stm32mp1.ext4
6.3. Updating partitions using official ST bootloaders[edit source]
If TF-A or FIP are modified, and the STM32CubeProgrammer support is lost for any reason (for example if the stm32prog command is removed), you can still program these new files by selecting the correct binary setting for the partitions 0x01 and 0x03 with Device=none and change the Id for the binaries to program in Flash, as indicated in chapter "Field2: Id".
For example, with ST board, you can flash Customer-modified binary by using the ST original file. The new Layout file is:
Opt | Part | Name | Type | Device | Offset | Binary |
---|---|---|---|---|---|---|
- | 0x01 | fsbl-boot | Binary | none | 0x0 | arm-trusted-firmware/tf-a-stm32mp157f-ev1-usb.stm32 |
- | 0x03 | fip-boot | Binary | none | 0x0 | fip/fip-stm32mp157f-ev1-trusted.bin |
P | 0x04 | fsbl1 | Binary | mmc0 | 0x00004400 | <customer-tf-a>.stm32 |
P | 0x05 | fsbl2 | Binary | mmc0 | 0x00044400 | <customer-tf-a>.stm32 |
PD | 0x06 | fip | Binary | mmc0 | 0x00084400 | <customer-fip>.bin |
P | 0x10 | bootfs | System | mmc0 | 0x00484400 | st-image-bootfs-openstlinux-weston-stm32mp1.ext4 |
P | 0x11 | vendorfs | FileSystem | mmc0 | 0x04484400 | st-image-vendorfs-openstlinux-weston-stm32mp1.ext4 |
P | 0x12 | rootfs | FileSystem | mmc0 | 0x05484400 | st-image-core-openstlinux-weston-stm32mp1.ext4 |
P | 0x13 | userfs | FileSystem | mmc0 | 0x33E84400 | st-image-userfs-openstlinux-weston-stm32mp1.ext4 |
The associated text file becomes :
#Opt Id Name Type IP Offset Binary - 0x01 fsbl-boot Binary none 0x0 arm-trusted-firmware/tf-a-stm32mp157f-ev1-usb.stm32 - 0x03 fip-boot Binary none 0x0 fip/fip-stm32mp157f-ev1-trusted.bin P 0x04 fsbl1 Binary mmc0 0x00004400 customer-tf-a.stm32 P 0x05 fsbl2 Binary mmc0 0x00044400 customer-tf-a.stm32 PD 0x06 fip Binary mmc0 0x00084400 customer-fip.bin P 0x10 boot System mmc0 0x00484400 st-image-bootfs-openstlinux-weston-stm32mp1.ext4 P 0x11 vendorfs FileSystem mmc0 0x04484400 st-image-vendorfs-openstlinux-weston-stm32mp1.ext4 P 0x12 rootfs FileSystem mmc0 0x05484400 st-image-weston-openstlinux-weston-stm32mp1.ext4 P 0x13 userfs FileSystem mmc0 0x33E84400 st-image-userfs-openstlinux-weston-stm32mp1.ext4
7. Other FlashLayout examples[edit source]
7.1. NOR and NAND Flash memories[edit source]
NOR Flash memory in RAW: TF-A uses several partitions for failsafe update, then FIP.
NAND Flash memory in UBI: only one large MTD partition for UBI volumes and UBIFS.
Here, the update feature in TF-A is not supported, the metadata and fip-b partitions are absent.
Opt | Part | Name | Type | Device | Offset | Binary |
---|---|---|---|---|---|---|
- | 0x01 | fsbl-boot | Binary | none | 0x0 | tf-a-usb.stm32 |
- | 0x03 | fip-boot | FIP | none | 0x0 | fip.bin |
P | 0x04 | fsbl1 | Binary | nor0 | 0x000000 | tf-a-nor.stm32 |
P | 0x05 | fsbl2 | Binary | nor0 | 0x040000 | tf-a-nor.stm32 |
P | 0x06 | fip | FIP | nor0 | 0x080000 | fip.bin |
PED | 0x10 | env | Binary | nor0 | 0x480000 | none |
PE | 0x11 | unused | Binary | nor0 | 0x500000 | none |
P | 0x20 | UBI | System | nand0 | 0x00000000 | ubi.bin |
The PartId 0x11 is an empty/free user partition associated to 'nor_user' MTD partition in U-Boot.
7.2. SD card: FAT[edit source]
Below an example with FAT bootfs partition (kernel and RAMFS) and an empty userfs partition, deleted and formatted by Linux on first boot:
Opt | Part | Name | Type | Device | Offset | Binary |
---|---|---|---|---|---|---|
- | 0x01 | fsbl-boot | Binary | none | 0x0 | tf-a-usb.stm32 |
- | 0x03 | fip-boot | FIP | none | 0x0 | fip.bin |
P | 0x04 | fsbl1 | Binary | mmc0 | 0x000000 | tf-a-sdcard.stm32 |
P | 0x05 | fsbl2 | Binary | mmc0 | 0x040000 | tf-a-sdcard.stm32 |
P | 0x06 | fip | FIP | mmc0 | 0x080000 | fip.bin |
P | 0x10 | bootfs | System | mmc0 | 0x200000 | bootfs.vfat |
PED | 0x11 | userfs | Empty | mmc0 | 0x400000 | none |
7.3. RawImage[edit source]
The SD card content is exported as RAW device and updated with the image.sdcard file:
Opt | Part | Name | Type | Device | Offset | Binary |
---|---|---|---|---|---|---|
- | 0x01 | fsbl-boot | Binary | none | 0x0 | tf-a-usb.stm32 |
- | 0x03 | fip-boot | FIP | none | 0x0 | fip.bin |
P | 0x10 | sdcard | RawImage | mmc0 | 0x0 | image.sdcard |
You can also erase the device before performing the update, by adding D in option.
7.4. Deleting device content[edit source]
For example, NOR and NAND Flash memories are deleted with:
Opt | Part | Name | Type | Device | Offset | Binary |
---|---|---|---|---|---|---|
- | 0x01 | fsbl-boot | Binary | none | 0x0 | tf-a-usb.stm32 |
- | 0x03 | fip-boot | FIP | none | 0x0 | fip.bin |
PDE | 0x10 | nor | RawImage | nor0 | 0x0 | none |
PDE | 0x11 | nand | RawImage | nand0 | 0x0 | none |
To erase all other devices, including the e•MMC boot partition, proceed as follows:
Opt | Part | Name | Type | Device | Offset | Binary |
---|---|---|---|---|---|---|
- | 0x01 | fsbl-boot | Binary | none | 0x0 | tf-a-usb.stm32 |
- | 0x03 | fip-boot | FIP | none | 0x0 | fip.bin |
PDE | 0x10 | sdcard | RawImage | mmc0 | 0x0 | none |
PED | 0x20 | emmc_boot1 | Binary | mmc1 | boot1 | none |
DPE | 0x21 | emmc_boot2 | Binary | mmc1 | boot2 | none |
EPD | 0x22 | emmc | RawImage | mmc1 | 0x0 | none |
DPE | 0x30 | nand | RawImage | nand0 | 0x0 | none |
PDE | 0x40 | nor | RawImage | nor0 | 0x0 | none |
Warning: A timeout may occur in STM32CubeProgrammer since deleting NOR Flash memory might be slow. To avoid this issue you can delete only the used partitions (Option=PED), for example:
#Opt Id Name Type Device Offset Binary - 0x01 fsbl-boot Binary none 0x0 tf-a-usb.stm32 - 0x03 fip-boot FIP none 0x0 fip.bin #delete ALL devices EPD 0x10 sdcard RawImage mmc0 0x0 none PED 0x20 emmc_b1 Binary mmc1 boot1 none PED 0x21 emmc_b2 Binary mmc1 boot2 none PED 0x22 emmc RawImage mmc1 0x0 none PED 0x30 nand RawImage nand0 0x0 none # on NOR (slow device): delete ALL used MTD partitions PE 0x40 nor RawImage nor0 0x00000000 none PED 0x41 fsbl1 Binary nor0 0x00000000 none PED 0x42 fsbl2 Binary nor0 0x00040000 none PED 0x43 metadata1 Binary nor0 0x00080000 none PED 0x44 metadata2 Binary nor0 0x000C0000 none PED 0x45 fip-a FIP nor0 0x00100000 none PED 0x46 fip-b FIP nor0 0x00500000 none PED 0x47 u-boot-env Binary nor0 0x00900000 none PE 0x48 unused Binary nor0 0x00980000 none
7.5. Complex use case[edit source]
Update SD card (mmc0 on SDMMC1). The GPT partition is created since all partitions are selected and Userfs is deleted and empty.
Erase all other devices, including e•MMC hidden boot partition.
Opt | Part | Name | Type | Device | Offset | Binary |
---|---|---|---|---|---|---|
- | 0x01 | fsbl-boot | Binary | node | 0x0 | tf-a-usb.stm32 |
- | 0x03 | fip-boot | FIP | none | 0x0 | fip.bin |
P | 0x04 | fsbl1 | Binary | mmc0 | 0x00004400 | tf-a-sdcard.stm32 |
P | 0x05 | fsbl2 | Binary | mmc0 | 0x00044400 | tf-a-sdcard.stm32 |
P | 0x06 | medata1 | Binary | mmc0 | 0x00084400 | metadata.bin |
P | 0x07 | medata2 | Binary | mmc0 | 0x00084400 | metadata.bin |
P | 0x08 | fip-a | FIP | mmc0 | 0x000C4400 | fip.bin |
PED | 0x09 | fip-b}} | FIP | mmc0 | 0x00104400 | none |
PED | 0x0A | u-boot-env | Binary | mmc0 | 0x00504400 | none |
P | 0x09 | bootfs | System | mmc0 | 0x00904400 | bootfs.ext4 |
P | 0x10 | vendorfs | FileSytem | mmc0 | TBD | vendorfs.ext4 |
P | 0x12 | rootfs | FileSytem | mmc0 | TBD | rootfs.ext4 |
P | 0x13 | userfs | FileSytem | mmc0 | TBD | userfs.ext4 |
PED | 0x60 | emmc_boot1 | Binary | mmc1 | boot1 | none |
DPE | 0x61 | emmc_boot2 | Binary | mmc1 | boot2 | none |
EPD | 0x62 | emmc | RawImage | mmc1 | 0x0 | none |
EPD | 0x10 | nand | RawImage | nand0 | 0x0 | none |
8. Reference list[edit source]
- ↑ https://en.wikipedia.org/wiki/USB#Device_Firmware_Upgrade
- ↑ USB Device Class Specification for Device Firmware Upgrade, Version 1.1, (available at http://www.usb.org/developers/docs): https://www.usb.org/sites/default/files/DFU_1.1.pdf
- ↑ 3.0 3.1 https://en.wikipedia.org/wiki/GUID_Partition_Table
- ↑ 4.0 4.1 https://en.wikipedia.org/wiki/Universally_unique_identifier
- ↑ https://wiki.archlinux.org/index.php/persistent_block_device_naming