How to stream camera over network

Revision as of 12:04, 20 November 2023 by Registered User (→‎Overview)
Applicable for STM32MP13x lines, STM32MP15x lines

1. Overview[edit source]

This article will explain how to stream camera content over network thanks to GStreamer application on top of V4L2 Linux® kernel framework.

Capturing compressed JPEG pictures is an efficient way to send camera images to any local or remote player; JPEG pictures require a limited bandwidth while being fully interoperable.

Info white.png Information
This article focus on camera sensor which can directly output JPEG content, if it is not the case refer to How to stream RAW camera over network.

Find below some examples of command lines allowing to capture a continuous JPEG stream while playing it using various multimedia players, either local or remote.

2. Local streaming[edit source]

Here is an example of a local preview involving V4l2-ctl for JPEG pictures capture and gst-play GStreamer player for JPEG decoding and display. JPEG pictures are sent over a standard Linux pipe.

Warning white.png Warning
If Weston is configured with a "weston" user instead of a "root" user, please use the following command:
 su -l "weston" -c "your_weston_command"

Note: Above tips may not be necessary on Yocto Project® versions greater than or equal to 4.2 ("Mickledore").


For STM32MP135 line More info.png, setup the camera subsystem first:
 media-ctl -d /dev/media0 --set-v4l2 "'ov5640 1-003c':0[fmt:JPEG_1X8/640x480@1/30 field:none]"
media-ctl -d /dev/media0 --set-v4l2 "'dcmipp_parallel':0[fmt:JPEG_1X8/640x480]"
media-ctl -d /dev/media0 --set-v4l2 "'dcmipp_dump_postproc':0[fmt:JPEG_1X8/640x480]"
media-ctl -d /dev/media0 --set-v4l2 "'dcmipp_dump_postproc':1[fmt:JPEG_1X8/640x480]" 
media-ctl -d /dev/media0 --set-v4l2 "'dcmipp_dump_postproc':1[crop:(0,0)/640x480]"


Capture JPEG pictures then decode & display them:

 v4l2-ctl --set-parm=30;v4l2-ctl --set-fmt-video=width=640,height=480,pixelformat=JPEG --stream-mmap --stream-count=-1 --stream-to=- 2>/dev/null | gst-play-1.0 "fd://0"

--stream-to=- tells V4l2-ctl to output binary captured content to standard output, which is then sent to pipe |.

Special URI fd://0 tells gst-play GStreamer player to read data from the pipe.

Note the 2>/dev/null right after the V4l2-ctl command to remove the logs from console output.

3. UDP streaming[edit source]

An internet connection is required, for example by plugging an ethernet cable on the:

STM32MP135x-DK Discovery kit More info green.png CN4 Ethernet connector 1 or CN15 Ethernet connector 2
STM32MP157x-DKx Discovery kit More info green.png CN8 Ethernet connector
STM32MP157x-EV1 Evaluation board More info green.png CN3 Ethernet connector


For STM32MP135 line More info.png, setup the camera subsystem first:
 media-ctl -d /dev/media0 --set-v4l2 "'ov5640 1-003c':0[fmt:JPEG_1X8/640x480@1/30 field:none]"
media-ctl -d /dev/media0 --set-v4l2 "'dcmipp_parallel':0[fmt:JPEG_1X8/640x480]"
media-ctl -d /dev/media0 --set-v4l2 "'dcmipp_dump_postproc':0[fmt:JPEG_1X8/640x480]"
media-ctl -d /dev/media0 --set-v4l2 "'dcmipp_dump_postproc':1[fmt:JPEG_1X8/640x480]" 
media-ctl -d /dev/media0 --set-v4l2 "'dcmipp_dump_postproc':1[crop:(0,0)/640x480]"


Get the IP address aa.bb.cc.dd of the host PC using ifconfig command:

 ifconfig | grep "inet addr"
   inet addr:aa.bb.cc.dd  Bcast:10.201.23.255  Mask:255.255.252.0
   inet addr:127.0.0.1  Mask:255.0.0.0

Then fill the host= udpsink property with this IP address on the remote side:

 v4l2-ctl --set-parm=30;v4l2-ctl --set-fmt-video=width=640,height=480,pixelformat=JPEG --stream-mmap --stream-count=-1 --stream-to=- 2>/dev/null | gst-launch-1.0 fdsrc ! jpegparse ! rtpjpegpay ! udpsink host=aa.bb.cc.dd port=5000

Then play the UDP stream on host PC:

 gst-launch-1.0 udpsrc port=5000 ! application/x-rtp, encoding-name=JPEG ! rtpjpegdepay ! jpegparse ! decodebin ! videoconvert ! autovideosink

A new window will popup on host PC displaying the camera content.

Info white.png Information
Due to SDP protocol signaling, this solution is not fully interoperable because it needs a dedicated GStreamer command line to be played on host side