LVDS internal peripheral

Revision as of 10:12, 9 November 2023 by Registered User (→‎Peripheral overview)
Applicable for STM32MP25x lines

1. Article purpose[edit source]

The purpose of this article is to:

  • introduce briefly the LVDS peripheral and its main features,
  • indicate the peripheral instances assignment at boot time and their assignment at runtime (including whether instances can be allocated to secure contexts),
  • list the software frameworks and drivers managing the peripheral,
  • explain how to configure the peripheral.

2. Peripheral overview[edit source]

The LVDS display interface transmitter (LVDS) handles the LVDS protocol. It maps the pixels received from the upstream Pixel-DMA (LTDC[1]) onto the LVDS PHY.

It regroups three sub blocks.

  • LVDS host: it handles the LVDS protocol (FPD / OpenLDI) by mapping its input pixels onto the data lanes of the PHY.
  • LVDS PHY: it parallelizes the data and drives the LVDS data lanes.
  • LVDS wrapper: it handles the top-level settings.

The LVDS host supports the following high-level features:

  • FPD-Link-I and OpenLDI (v0.95) protocols
  • Single-Link or Dual-Link operation
  • Single-Display or Double-Display (with the same content duplicated on both)
  • Flexible Bit-Mapping, including JEIDA and VESA
  • RGB888 or RGB666 output
  • Synchronous design, with one input pixel per clock cycle
  • No resolution limitation.

The LVDS PHY supports the following high-level features:

  • FPD bitrate: 784 Mbps/lane (112 Mpixel/s/Link, 224 Mpixel/s if Dual Link)
  • OpenLDI bitrate: 1100 Mbps/lane (157 Mpixel/s/Link, 314 Mpixel/s if Dual Link)

Refer to the STM32 MPU reference manuals for the complete list of features, and to the software frameworks and drivers, introduced below, to see which features are implemented.

3. Peripheral usage[edit source]

This chapter is applicable in the scope of the OpenSTLinux BSP running on the Arm® Cortex®-A processor(s), and the STM32CubeMPU Package running on the Arm® Cortex®-M processor.

3.1. Boot time assignment[edit source]

The LVDS can be used at boot time for displaying a splash screen thanks to the U-Boot framework [2].

3.1.1. On STM32MP25x lines More info.png[edit source]

Click on How to.png to expand or collapse the legend...

  • means that the peripheral can be assigned to the given boot time context.
  • means that the peripheral is assigned by default to the given boot time context and that the peripheral is mandatory for the STM32 MPU Embedded Software distribution.
  • means that the peripheral can be assigned to the given boot time context, but this configuration is not supported in STM32 MPU Embedded Software distribution.
  • is used for system peripherals that cannot be unchecked because they are hardware connected in the device.

The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possibilities might be described in STM32MP25 reference manuals.

Domain Peripheral Boot time allocation Comment How to.png
Instance Cortex-A35
secure
(ROM code)
Cortex-A35
secure
(TF-A BL2)
Cortex-A35
non-secure
(U-Boot)
Visual LVDS LVDS

3.2. Runtime assignment[edit source]

3.2.1. On STM32MP25x lines More info.png[edit source]

Click on How to.png to expand or collapse the legend...

STM32MP25 internal peripherals

Check boxes illustrate the possible peripheral allocations supported by STM32 MPU Embedded Software:

  • means that the peripheral can be assigned to the given runtime context.
  • means that the peripheral is assigned by default to the given runtime context and that the peripheral is mandatory for the STM32 MPU Embedded Software distribution.
  • means that the peripheral can be assigned to the given runtime context, but this configuration is not supported in STM32 MPU Embedded Software distribution.
  • is used for system peripherals that cannot be unchecked because they are hardware connected in the device.

The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possibilities might be described in STM32MP25 reference manuals.

Domain Peripheral Runtime allocation Comment How to.png
Instance Cortex-A35
secure
(OP-TEE /
TF-A BL31)
Cortex-A35
non-secure
(Linux)
Cortex-M33
secure
(TF-M)
Cortex-M33
non-secure
(STM32Cube)
Cortex-M0+
Warning.png
(STM32Cube)
Visual LVDS LVDS OP-TEE

4. Software frameworks and drivers[edit source]

Below are listed the software frameworks and drivers managing the LVDS peripheral for the embedded software components listed in the above tables.

5. How to assign and configure the peripheral[edit source]

The peripheral assignment can be done via the STM32CubeMX graphical tool (and manually completed if needed).
This tool also helps to configure the peripheral by generating:

  • partial device trees (pin control and clock tree) for the OpenSTLinux software components,
  • HAL initialization code for the STM32CubeMPU Package.

The configuration is applied by the firmware running in the context in which the peripheral is assigned.

See also additional information in the LVDS device tree configuration article for Linux®.

6. How to go further[edit source]

Refer to the STM32 MPU reference manuals for a detailed description of the LVDS peripheral and applicable use-cases.

7. References[edit source]