IPCC internal peripheral

Revision as of 15:47, 27 September 2023 by Registered User (→‎On {{MicroprocessorDevice | device=25}})
Applicable for STM32MP15x lines, STM32MP25x lines

Warning white.png Warning
Concerning the STM32MP25x lines More info.png, only the boot time assignment table and the runtime assignment table have been updated.
The other chapters have not been updated yet.


1. Article purpose[edit source]

The purpose of this article is to:

  • briefly introduce the IPCC peripheral and its main features,
  • indicate the peripheral instances assignment at boot time and their assignment at runtime (including whether instances can be allocated to secure contexts),
  • list the software frameworks and drivers managing the peripheral,
  • explain how to configure the peripheral.

2. Peripheral overview[edit source]

The IPCC (inter-processor communication controller) peripheral is used to exchange data between two processors. It provides a non blocking signaling mechanism to post and retrieve information in an atomic way. Note that shared memory buffers are allocated in the MCU SRAM, which is not part of the IPCC block.

The IPCC peripheral provides a hardware support to manage inter-processor communication between two processor instances. Each processor owns specific register bank and interrupts.

The IPCC provides the signaling for six bidirectional channels.
Each channel is divided into two subchannels that offer a unidirectional signaling from the "sender" processor to the "receiver" processor:

  • P1_TO_P2 subchannel
  • P2_TO_P1 subchannel

A subchannel consists in:

  • One flag that toggles between occupied and free: the flag is set to occupied by the "sender" processor and cleared by the "receiver" processor.
  • Two associated interrupts (shared with the other channels):
    • RXO: RX channel occupied, connected to the "receiver" processor.
    • TXF: TX channel free, connected to the "sender" processor.
  • Two associated interrupt masks multiplexing channel IRQs.


IPCC peripheral.png
The IPCC supports the following channel operating modes:

  • Simplex communication mode:
    • Only one subchannel is used.
    • Unidirectional messages: once the "sender" processor has posted the communication data in the memory, it sets the channel status flag to occupied. The "receiver" processor clears the flag when the message is treated.
  • Half-duplex communication mode:
    • Only one subchannel is used.
    • Bidirectional messages: once the "sender" processor has posted the communication data in the memory, it sets the channel status flag to occupied. The "receiver" processor clears the flag when the message is treated and the response is available in shared memory.
  • Full-duplex communication mode:
    • The subchannels are used in Asynchronous mode.
    • Any processor can post asynchronously a message by setting the subchannel status flag to occupied. The "receiver" processor clears the flag when the message is treated. This mode can be considered as a combination of two simplex modes on a given channel.

Refer to the STM32MP15 reference manuals for the complete list of features, and to the software frameworks and drivers, introduced below, to see which features are implemented.

3. Peripheral usage[edit source]

This chapter is applicable in the scope of the OpenSTLinux BSP running on the Arm® Cortex®-A processor(s), and the STM32CubeMPU Package running on the Arm® Cortex®-M processor.

3.1. Boot time assignment[edit source]

3.1.1. On STM32MP1 series[edit source]

The IPCC peripheral is not used at boot time.

3.1.2. On STM32MP2 series[edit source]

Click on How to.png to expand or collapse the legend...

  • means that the peripheral can be assigned to the given boot time context.
  • means that the peripheral is assigned by default to the given boot time context and that the peripheral is mandatory for the STM32 MPU Embedded Software distribution.
  • means that the peripheral can be assigned to the given boot time context, but this configuration is not supported in STM32 MPU Embedded Software distribution.
  • is used for system peripherals that cannot be unchecked because they are hardware connected in the device.

The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possibilities might be described in STM32MP25 reference manuals.

Domain Peripheral Boot time allocation Comment How to.png
Instance Cortex-A35
secure
(ROM code)
Cortex-A35
secure
(TF-A BL2)
Cortex-A35
non-secure
(U-Boot)
Coprocessor IPCC Info.png IPCC1 Shareable at internal peripheral level thanks to the RIF: see the boot time allocation per feature
IPCC2 Shareable at internal peripheral level thanks to the RIF: see the boot time allocation per feature


The below table shows the possible boot time allocations for the features of the IPCC1 instance.

Feature Boot time allocation Info.png Comment
Cortex-A35
secure
(ROM code)
Cortex-A35
secure
(TF-A BL2)
Cortex-A35
non-secure
(U-Boot)
CPU1 channel 1
CPU1 channel 2
CPU1 channel 3
CPU1 channel 4
CPU1 channel 5
CPU1 channel 6
CPU1 channel 7
CPU1 channel 8
CPU1 channel 9
CPU1 channel 10
CPU1 channel 11
CPU1 channel 12
CPU1 channel 13
CPU1 channel 14
CPU1 channel 15
CPU1 channel 16
CPU2 channel 1
CPU2 channel 2
CPU2 channel 3
CPU2 channel 4
CPU2 channel 5
CPU2 channel 6
CPU2 channel 7
CPU2 channel 8
CPU2 channel 9
CPU2 channel 10
CPU2 channel 11
CPU2 channel 12
CPU2 channel 13
CPU2 channel 14
CPU2 channel 15
CPU2 channel 16


The below table shows the possible boot time allocations for the features of the IPCC2 instance.

Feature Boot time allocation Info.png Comment
Cortex-A35
secure
(ROM code)
Cortex-A35
secure
(TF-A BL2)
Cortex-A35
non-secure
(U-Boot)
CPU1 channel 1
CPU1 channel 2
CPU1 channel 3
CPU1 channel 4
CPU2 channel 1
CPU2 channel 2
CPU2 channel 3
CPU2 channel 4

3.2. Runtime assignment[edit source]

3.2.1. On STM32MP15x lines More info.png[edit source]

STMicroelectronics distribution uses the IPCC peripheral for inter-processor communication with the following configuration:

  • IPCC processor 1 interface is assigned to Arm® Cortex®-A7 non-secure context.
  • IPCC processor 2 interface is assigned to Arm® Cortex®-M4 context.


File:IPCC overview.png

It does not make sense to allocate the IPCC to a single runtime execution context. It is consequently enabled by default for both cores in the STM32CubeMX.

Click on How to.png to expand or collapse the legend...

STM32MP15 internal peripherals

Check boxes illustrate the possible peripheral allocations supported by STM32 MPU Embedded Software:

  • means that the peripheral can be assigned to the given runtime context.
  • means that the peripheral is assigned by default to the given runtime context and that the peripheral is mandatory for the STM32 MPU Embedded Software distribution.
  • means that the peripheral can be assigned to the given runtime context, but this configuration is not supported in STM32 MPU Embedded Software distribution.
  • is used for system peripherals that cannot be unchecked because they are hardware connected in the device.

Refer to How to assign an internal peripheral to an execution context for more information on how to assign peripherals manually or via STM32CubeMX.
The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possiblities might be described in STM32MP15 reference manuals.

Domain Peripheral Runtime allocation Comment How to.png
Instance Cortex-A7
secure
(OP-TEE)
Cortex-A7
non-secure
(Linux)
Cortex-M4

(STM32Cube)
Coprocessor IPCC IPCC Shared (none or both)

3.2.2. On STM32MP25x lines More info.png[edit source]

Click on How to.png to expand or collapse the legend...

STM32MP25 internal peripherals

Check boxes illustrate the possible peripheral allocations supported by STM32 MPU Embedded Software:

  • means that the peripheral can be assigned to the given runtime context.
  • means that the peripheral is assigned by default to the given runtime context and that the peripheral is mandatory for the STM32 MPU Embedded Software distribution.
  • means that the peripheral can be assigned to the given runtime context, but this configuration is not supported in STM32 MPU Embedded Software distribution.
  • is used for system peripherals that cannot be unchecked because they are hardware connected in the device.

The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possibilities might be described in STM32MP25 reference manuals.

Domain Peripheral Runtime allocation Comment How to.png
Instance Cortex-A35
secure
(OP-TEE /
TF-A BL31)
Cortex-A35
non-secure
(Linux)
Cortex-M33
secure
(TF-M)
Cortex-M33
non-secure
(STM32Cube)
Cortex-M0+
Warning.png
(STM32Cube)
Coprocessor IPCC Info.png IPCC1 OP-TEE Shareable at internal peripheral level thanks to the RIF: see the runtime allocation per feature
IPCC2 OP-TEE Shareable at internal peripheral level thanks to the RIF: see the runtime allocation per feature


The below table shows the possible runtime allocations for the features of the IPCC1 instance.

Feature Runtime allocation Info.png Comment
Cortex-A35
secure
(OP-TEE /
TF-A BL31)
Cortex-A35
non-secure
(Linux)
Cortex-M33
secure
(TF-M)
Cortex-M33
non-secure
(STM32Cube)
Cortex-M0+
Warning.png
(STM32Cube)
CPU1 channel 1 OP-TEE
CPU1 channel 2 OP-TEE
CPU1 channel 3 OP-TEE
CPU1 channel 4 OP-TEE
CPU1 channel 5 OP-TEE
CPU1 channel 6 OP-TEE
CPU1 channel 7 OP-TEE
CPU1 channel 8 OP-TEE
CPU1 channel 9 OP-TEE
CPU1 channel 10 OP-TEE
CPU1 channel 11 OP-TEE
CPU1 channel 12 OP-TEE
CPU1 channel 13 OP-TEE
CPU1 channel 14 OP-TEE
CPU1 channel 15 OP-TEE
CPU1 channel 16 OP-TEE
CPU2 channel 1
CPU2 channel 2
CPU2 channel 3
CPU2 channel 4
CPU2 channel 5
CPU2 channel 6
CPU2 channel 7
CPU2 channel 8
CPU2 channel 9
CPU2 channel 10
CPU2 channel 11
CPU2 channel 12
CPU2 channel 13
CPU2 channel 14
CPU2 channel 15
CPU2 channel 16


The below table shows the possible runtime allocations for the features of the IPCC2 instance.

Feature Runtime allocation Info.png Comment
Cortex-A35
secure
(OP-TEE /
TF-A BL31)
Cortex-A35
non-secure
(Linux)
Cortex-M33
secure
(TF-M)
Cortex-M33
non-secure
(STM32Cube)
Cortex-M0+
Warning.png
(STM32Cube)
CPU1 channel 1 OP-TEE
CPU1 channel 2 OP-TEE
CPU1 channel 3 OP-TEE
CPU1 channel 4 OP-TEE
CPU2 channel 1
CPU2 channel 2
CPU2 channel 3
CPU2 channel 4

4. Software frameworks and drivers[edit source]

Below are listed the software frameworks and drivers managing the IPCC peripheral for the embedded software components listed in the above tables.

5. How to assign and configure the peripheral[edit source]

The peripheral assignment can be done via the STM32CubeMX graphical tool (and manually completed if needed).
This tool also helps to configure the peripheral:

  • partial device trees (pin control and clock tree) generation for the OpenSTLinux software components,
  • HAL initialization code generation for the STM32CubeMPU Package.

The configuration is applied by the firmware running in the context in which the peripheral is assigned.

The IPCC peripheral is shared between the Arm Cortex-A and Cortex-M contexts. A particular attention must therefore be paid to have a complementary configuration on both contexts. In STMicroelectronics distribution, the IPCC is configured as described below. To ensure the coherency of the system, it is recommended to keep this configuration unchanged in your implementation.

  • Processor interface
Processor interface Context
Cortex-A7 non-secure
(Linux)
Cortex-M4
(STM32Cube)
Processor 1 interface
Processor 2 interface
  • Channel allocation
Channel Mode Usage Software client frameworks
Cortex-A7 non-secure
(Linux)
Cortex-M4
(STM32Cube)
Channel 1 Full-duplex communication RPMsg transfer from Cortex-M to Cortex-A
  • The Cortex-M core uses this channel to indicate that a message is available
  • The Cortex-A core uses this channel to indicate that the message is treated
RPMsg framework OpenAMP
Channel 2 Full-duplex communication RPMsg transfer from Cortex-A to Cortex-M
  • The Cortex-A core uses this channel to indicate that a message is available
  • The Cortex-M core uses this channel to indicate that the message is treated
RPmsg framework OpenAMP
Channel 3 Simplex communication Cortex-M4 shutdown request RemoteProc framework CprocSync cube utility
Channel 4 free
Channel 5 free
Channel 6 free