STM32MP13 RAM mapping

Revision as of 13:19, 24 January 2023 by Registered User (→‎Overview)
Applicable for STM32MP13x lines


1. Overview[edit source]

This article shows the default memory mapping defined by STMicroelectronics in STM32MPU Embedded Software. It uses a subset of all memory regions that are exposed at hardware level: customers may use other memory regions or aliases that are not shown here but are described in the STM32MP13 reference manuals.

2. Arm core characteristics[edit source]

The integration of Arm® Cortex® cores sets some constraints on the device memory mapping: the main ones are listed in this article.

2.1. Reset address[edit source]

Arm® Cortex® cores start running from address 0x00000000 on reset, which is why this address respectively points to:

3. Memory mapping[edit source]

3.1. Overall memory mapping[edit source]

The memory mapping below is a subset of all regions that are exposed at hardware level: it shows the default configuration used in OpenSTLinux but the customer may choose a different mapping to take advantage of other address ranges defined in STM32MP13 reference manuals.


DDRBackup registersBKPSRAMCAN SRAMSRAMSYSRAMROM
STM32MP13 memory mapping

4. Internal RAM mapping[edit source]

4.1. Overview[edit source]

SYSRAM and SRAM can be used by secure and non-secure Cortex-A7 contexts like described in SYSRAM internal memory and STM32MP13 SRAM internal memory articles.

4.2. How to do that in practice[edit source]

The memory usage is defined in both Cortex-A7 contexts:

  • on secure Cortex-A7: in OP-TEE device tree, using Reserved_memory mechanism
  • on non-secure Cortex-A7: in Linux device tree, using Reserved_memory mechanism

To ensure the consistency of the system, both memory declarations have to be updated according to the expected configuration.

4.2.1. SRAM[edit source]

By default part of the SRAM is reserved for DMA chaining for Linux features. It can be freed for some other purposes by removing following:

  • Linux device tree
Remove followings declarations:
&sram {
    dma_pool: dma_pool@0 {
    reg = <0x0 0x4000>;
    pool;
};
&dma1 {
	sram = <&dma_pool>;
};

&dma2 {
	sram = <&dma_pool>;
};