This page is a candidate for renaming (move). The requested new name is: How to transfer files to Discovery kit using Tera Term on Windows PC . The supplied reason is: Balance the verb complements better . -- Registered User (-) 09:38, 16 November 2022 (CET). Wiki maintainers: remember to update the pages that link this page before renaming (moving) it. |
The article is written as an extension to the article X-NUCLEO-NFC05A1 expansion board and X-NUCLEO-NFC06A1 expansion board. The purpose of this article is to specifically help users with steps to transfer any file from a Windows® PC to the STM32MP157C-DK2 Discovery kit using "Tera Term"[Ex1 1]. Download and install Tera Term on your Windows® PC and follow the steps listed below.
- Plug the power cable to power-up the STM32MP157C-DK2 .
- Connect the STM32MP157C-DK2 Discovery kit to your PC via a USB Micro-B cable through CN11.
- Check the Virtual COM port number visible in the device manager. For example, in the snapshot below, the COM port number is 14.
- Open Tera Term on your PC and select the COM port (as found in step 3 above). The baud rate must be 115200 bauds. The virtual terminal (remote access) is displayed as shown in the snapshot below.
- To transfer a file from the host PC to STM32MP157C-DK2 ,click on the File menu in the top-left corner of the Tera Term window and go to [File]>[Transfer]>[ZMODEM]>[Send]. Refer to the snapshot below.
- Select the file to be transferred from the pop-up window (see an example in the snapshot below) and click on the Open tab.
- A progress bar shows the file transfer status as shown in the snapshot below
Cite error: <ref>
tags exist for a group named "Ex1", but no corresponding <references group="Ex1"/>
tag was found