This page explains how to manually update OTP with the U-Boot fuse
command.
1. The fuse command[edit source]
The fuse
command allows you to update the OTP words in U-Boot:
- sense/program to directly access the OTP value (for a permanent update)
- read/override to access only the shadow cache value (for a temporary update).
help fuse fuse - Fuse sub-system Usage: fuse read <bank> <word> [<cnt>] - read 1 or 'cnt' fuse words, starting at 'word' fuse sense <bank> <word> [<cnt>] - sense 1 or 'cnt' fuse words, starting at 'word' fuse prog [-y] <bank> <word> <hexval> [<hexval>...] - program 1 or several fuse words, starting at 'word' (PERMANENT) fuse override <bank> <word> <hexval> [<hexval>...] - override 1 or several fuse words, starting at 'word'.
See doc/README.fuse for details.
2. STM32MP support[edit source]
The fuse</code command is implemented in drivers/misc/stm32mp_fuse.c :
- For the STM32MP15x lines with 2 banks:
- <bank> = SOC OTP: 0 #STM32MP1 OTP
- <bank> = PMIC NVM : 1 #STPMIC1 NVM
- For the STM32MP13x lines with 1 bank:
- <bank> = SOC OTP: 0 #STM32MP1 OTP
2.1. STM32MP OTP[edit source]
<bank> = 0 provides access to the 96 STM32MP13x or STM32MP15x OTP words with the BSEC driver: arch/arm/mach-stm32mp/bsec.c .
Refer to the STM32MP13 reference manuals or STM32MP15 reference manuals for the OTP layout.
The OTP<index> words value and lock status (0=unlocked, 1=locked) are available with <index> = 0 to 95 :
- for value: <word> = <index>
- for lock status: <word> = 0x10000000 + <index>
not shadowed, only support operation sense
and program
the status bit-field is same than STM32CubeProgrammer OTP management:
- [0]: 1 bit read error detected: 1 = OTP value isn't valid
- [26]: 1 bit lock error
- [27]: 1 bit sticky programming lock
- [28]: 1 bit shadow write sticky lock
- [29]: 1 bit shadow read sticky lock
- [30]: 1 bit permanent write lock
Only 32 lower OTPs words are accessible by default, the software needs to manage exceptions to allow some upper OTPs to be accessed by the non-secure world as described in BSEC_device_tree_configuration.
2.1.1. Simple OTP examples[edit source]
1) Read OTP value for OTP57 and 58 (2 OTP words)
fuse sense 0 57 2
Sensing bank 0:
Word 0x00000039: 42e18000 0000e448
2) Check lock status of OTP 57 - 60 (4 words at index 57 = 0x39)
fuse sense 0 0x10000039 4
Sensing bank 0:
Word 0x10000039: 40000000 40000000 40000000 00000000
3) Display shadow values for all OTPs
When only the 32 lower OTPs are accessible:
fuse read 0 0 32
Reading bank 0:
Word 0x00000000: 00000017 00008001 00000000 00000000
Word 0x00000004: 00000000 00000000 00000000 00000000
Word 0x00000008: 00000000 82004000 00000000 00000000
Word 0x0000000c: 7d04f0db 00470022 33385115 34383330
Word 0x00000010: 22986562 27010551 7a470140 06cc1608
Word 0x00000014: 5e560054 00000000 00000000 401a300c
Word 0x00000018: ffffffff ffffffff ffffffff ffffffff
Word 0x0000001c: ffffffff ffffffff ffffffff ffffffff
When all the 96 OTPs are available:
fuse read 0 0 96
Reading bank 0:
Word 0x00000000: 00000017 00008000 00000000 00000000
Word 0x00000004: 00000000 00000000 00000000 00000000
Word 0x00000008: 00000000 00000000 00000000 00000000
Word 0x0000000c: 7cf5f0f9 00410032 33385116 34383330
Word 0x00000010: 129675aa 2931215e 7a550000 069013ec
Word 0x00000014: 5e360042 00000000 00000000 40133023
Word 0x00000018: 00000000 00000000 00000000 00000000
Word 0x0000001c: 00000000 00000000 00000000 00000000
Word 0x00000020: 00000000 00000000 00000000 00000000
Word 0x00000024: 00000000 00000000 00000000 00000000
Word 0x00000028: aa333e40 b5e90dda f15f4678 8ab41400
Word 0x0000002c: b74efe3a f0a03b1b 01e016b3 d06a79dd
Word 0x00000030: 48b96fbe 20fbd352 6732dbf4 edc395f9
Word 0x00000034: cdf15575 418fd3d0 0bb7d994 8dc929d0
Word 0x00000038: 00000000 42e18000 0000e448 12722301
Word 0x0000003c: 00000000 00000000 00000000 00000000
Word 0x00000040: 00000000 00000000 00000000 00000000
Word 0x00000044: 00000000 00000000 00000000 00000000
Word 0x00000048: 00000000 00000000 00000000 00000000
Word 0x0000004c: 00000000 00000000 00000000 00000000
Word 0x00000050: 00000000 00000000 00000000 00000000
Word 0x00000054: 00000000 00000000 00000000 00000000
Word 0x00000058: 00000000 00000000 00000000 00000000
Word 0x0000005c: 00000000 00000000 00000000 00000000
4) Override value for one OTP
fuse override 0 0x0000005c 1
Overriding bank 0 word 0x0000005c with 0x00000001...
fuse read 0 0x0000005c
Reading bank 0:
Word 0x0000005c: 00000001
fuse sense 0 0x0000005c
Sensing bank 0:
Word 0x0000005c: 00000000
2.1.2. MAC address example for STM32MP15x[edit source]
For STM32MP15_boards, the MAC address[1] is retrieved in the 2 OTP words:
- OTP_57[31:0] = MAC_ADDR[31:0]
- OTP_58[15:0] = MAC_ADDR[47:32]
To program a MAC address on virgin OTP words above, you can use the fuse
command on bank 0 to access internal OTP words and lock them:
Prerequisite: check if a MAC address isn't yet programmed in OTP.
1) Check OTPs: their value must be equal to 0:
fuse sense 0 57 2
Sensing bank 0:
Word 0x00000039: 00000000 00000000
2) Check environment variable:
env print ethaddr
## Error: "ethaddr" not defined
3) Check lock status of OTP 57 & 58 (at 0x39, 0=unlocked, 1=locked):
fuse sense 0 0x10000039 2
Sensing bank 0:
Word 0x10000039: 00000000 00000000
Example to set MAC address "12:34:56:78:9a:bc"
1) Write OTP:
fuse prog -y 0 57 0x78563412 0x0000bc9a
2) Read OTP:
fuse sense 0 57 2
Sensing bank 0:
Word 0x00000039: 78563412 0000bc9a
3) Lock OTP:
fuse prog 0 0x10000039 0x40000000 0x40000000
fuse sense 0 0x10000039 2
Sensing bank 0:
Word 0x10000039: 40000000 40000000
4) OTP is used after REBOOT, in the trace:
### Setting environment from OTP MAC address = "12:34:56:78:9a:bc"
5) Check env update:
env print ethaddr
ethaddr=12:34:56:78:9a:bc
2.1.3. MAC address example for STM32MP13x[edit source]
For STM32MP13_boards, the two MAC address are retrieved in the 3 OTP words:
- OTP_57[31:0] = MAC_ADDR1[31:0]
- OTP_58[15:0] = MAC_ADDR1[47:32]
- OTP_58[31:16] = MAC_ADDR2[15:0]
- OTP_59[31:0] = MAC_ADDR2[47:16]
See the full sequence in previous chapter, with a added OTP, for example:
fuse prog -y 0 57 e17ae710 e71094a2 95a2e17a
fuse read 0 57 3
Reading bank 0:
Word 0x00000039: e17ae710 e71094a2 95a2e17a
env print
...
eth1addr=10:e7:7a:e1:a2:95
ethaddr=10:e7:7a:e1:a2:94
...
2.2. STPMIC1 NVM[edit source]
<bank> = 1 provides access to the non-volatile memory (NVM) of the PMIC on the board when PMIC is managed by U-Boot.
It is not the case in OpenSTLinux, when OP-TEE is used.
For STPMIC1, the NVM has 8 bytes as defined in datasheet: DS12792, with <word> = <0xf8> to <0xff>.
1) Read the values of the 8 NVM
fuse read 1 0xf8 8
Reading bank 1:
Word 0x000000f8: 000000ee 00000092 000000c0 00000002
Word 0x000000fc: 000000f2 00000080 00000002 00000033
2) Read 2 NVM shadow values
fuse sense 1 0xf9 2
Sensing bank 1:
Word 0x000000f9: 00000092 000000c0
3) Update the NVM at index 0xfc with value 0xf2
fuse prog 1 0xfc 0xf2
Programming bank 1 word 0x000000fc to 0x000000f2...
Warning: Programming fuses is an irreversible operation!
This may brick your system.
Use this command only if you are sure of what you are doing!
Really perform this fuse programming? <y/N>
y
3. References[edit source]