This article briefly describes the STM32MP15x lines support in U-Boot.
1. STM32MP15x lines
support[edit source]
For detailed information, please read the file in the delivered U-Boot code = doc/board/st/stm32mp1.rst or the stm32mp1 documentation generated by make htlmdocs
[1].
Also available in official U-Boot Git.
Code :
- arch/arm/mach-stm32mp : arch specific code for STM32 Arm® Cortex® MPUs
- arch/arm/mach-stm32mp/Kconfig : generic configuration for STM32 Arm® Cortex® MPUs
- arch/arm/mach-stm32mp/Kconfig.15x : specific configuration for STM32MP15x lines
- arch/arm/mach-stm32mp/Kconfig : generic configuration for STM32 Arm® Cortex® MPUs
- board/st/common : STMicroelectronics common code
- board/st/stm32mp1 : STMicroelectronics boards support for STM32MP1 series
- drivers/*/*stm32* : drivers
Configuration Files:
- defconfig file
- configs/stm32mp15_defconfig when FIP is used in OpenSTLinux
- config files
- include/configs/stm32mp15_common.h : generic for STM32MP15x lines
- include/configs/stm32mp15_st_common.h : STMicroelectronics board for STM32MP15x lines
- STM32_MPU_device_tree in arch/arm/dts : stm32mp15*.dts*
- <Device tree>.dts : same as kernel
- <Device tree>-u-boot.dtsi : addition for u-boot automatically included in build process
The two next defconfig are kept only for compatibility with upstream, don't use them:
- configs/stm32mp15_trusted_defconfig with stm32 image header support (CONFIG_STM32MP15x_STM32IMAGE)
- configs/stm32mp15_basic_defconfig when SPL is used
2. Selecting targets : choose defconfig and Device Tree[edit source]
The STM32 MPU boot chain is supported by one U-Boot configuration with defconfig = stm32mp15_defconfig
Several boards are supported with the associated device-tree (same name as kernel):
Board part number | Device tree | Description |
---|---|---|
STM32MP157A-EV1 Evaluation board ![]() |
stm32mp157a-ev1 | MB1262+MB1263 |
STM32MP157C-EV1 Evaluation board ![]() |
stm32mp157c-ev1 | |
STM32MP157D-EV1 Evaluation board ![]() |
stm32mp157d-ev1 | |
STM32MP157F-EV1 Evaluation board ![]() |
stm32mp157f-ev1 | |
STM32MP157A-DK1 Discovery kit ![]() |
stm32mp157a-dk1 | MB1272 |
STM32MP157D-DK1 Discovery kit ![]() |
stm32mp157d-dk1 | |
STM32MP157C-DK2 Discovery kit ![]() |
stm32mp157c-dk2 | MB1272+MB1407 |
STM32MP157F-DK2 Discovery kit ![]() |
stm32mp157f-dk2 |
For information the 'Evaluation' daughter-board only (MB1263 without MB1262) is also supported by stm32mp15*-ed1.dts device tree files.
3. Compilation[edit source]
See U-Boot_overview#U-Boot_build with the defconfig file: stm32mp15_defconfig
make stm32mp15_defconfig make DEVICE_TREE=<Device tree> all
The supported variables are:
- DEVICE_TREE: select in arch/arm/dts the device tree that is used
- KBUILD_OUTPUT: change the destination directory for the build
- EXT_DTB: select external device tree
The output files u-boot.dtb and u-boot-nodtb.bin are integrated in FIP.
Nota: All the compiled device tree are available in $KBUILD_OUTPUT/arch/arm/dts/*.dtb.
You can select them instead of u-boot.dtb without U-Boot recompilation.
The ouput file u-boot.stm32' is only generated for stm32mp15_trusted_defconfig with CONFIG_STM32MP15x_STM32IMAGE; it is not more used for ecosystem release ≥ v4.0.0 .
4. U-Boot integration in FIP[edit source]
U-Boot binary and its associated device tree are part of the FIP binary, created with TF-A Makefile option :
- BL33_CFG = u-boot.dtb
- BL33 = u-boot-nodtb.bin
or updated with fiptools
:
- --hw-config u-boot.dtb
- --nt-fw u-boot-nodtb.bin
Example for FIP update :
fiptool --verbose update --nt-fw u-boot-nodtb.bin \ --hw-config u-boot.dtb \ fip-<board>.bin DEBUG: Replacing nt-fw with.../u-boot-nodtb.bin DEBUG: Replacing hw-config with .../u-boot.dtb DEBUG: Metadata size: ... bytes DEBUG: Payload size: ... bytes
See How_to_configure_TF-A_FIP for details.
5. Examples[edit source]
5.1. STM32MP157F-EV1 Evaluation board
[edit source]
make stm32mp15_defconfig make DEVICE_TREE=stm32mp157f-ev1 all
An existing FIP file is updated with:
fiptool update --nt-fw u-boot-nodtb.bin --hw-config u-boot.dtb fip-stm32mp157f-ev1.bin
5.2. STM32MP157C-EV1 Evaluation board
[edit source]
make stm32mp15_defconfig make DEVICE_TREE=stm32mp157c-ev1 all
An existing FIP file is updated with:
fiptool update --nt-fw u-boot-nodtb.bin --hw-config u-boot.dtb fip-stm32mp157c-ev1.bin
5.3. STM32MP157D-DK1 Discovery kit
[edit source]
make stm32mp15_defconfig make DEVICE_TREE=stm32mp157d-dk1 all
An existing FIP file is updated with:
fiptool update --nt-fw u-boot-nodtb.bin --hw-config u-boot.dtb fip-stm32mp157d-dk1.bin
5.4. STM32MP157C-DK2 Discovery kit
[edit source]
Using export to select the device tree
export KBUILD_OUTPUT=../build/stm32mp15 export DEVICE_TREE=stm32mp157c-dk2 make stm32mp15_defconfig make all
An existing FIP file is updated with:
fiptool update --nt-fw $KBUILD_OUTPUT/u-boot-nodtb.bin --hw-config $KBUILD_OUTPUT/u-boot.dtb \ fip-stm32mp157c-dk2.bin
5.5. Custom board with external device tree[edit source]
make stm32mp15_defconfig make EXT_DTB=stm32mp151a-myboard.dtb all
Then you can create or update the FIP