LEDs and buttons on STM32 MPU boards

Revision as of 12:28, 4 November 2021 by Registered User (→‎LEDs)
Applicable for STM32MP13x lines, STM32MP15x lines

1. Introduction[edit source]

The following paragraphs describe the functional mapping of the LEDs and buttons.

2. Description[edit source]

2.1. LEDs[edit source]

LED color Purpose
Green
Can be used at runtime for Linux examples
Red
Used to show Cortex-A boot information[1]
Blue U-Boot entering / exit indication then Linux heartbeat, which blinks as long as Linux[2] is alive[1] on the Cortex-A
Orange Used for STM32Cube[3] examples verdict, on STM32MP15. Free for user on STM32MP13.

2.2. Buttons[edit source]

Button label Purpose
WAKE UP Allows the platform to be woken from any low-power mode[4]
USER1
Used at boot time by U-Boot to enter USB programming mode with STM32CubeProgrammer. This avoids manipulation of the boot pins when a valid U-Boot image is already present in the board.

Can be used at runtime for Linux examples or STM32Cube examples, on STM32MP15.

USER2
Used at boot time by U-Boot to enter Android Fastboot mode.

Used at runtime for Linux, on STM32MP13.

TAMPER Allows to generate an external tamper event. Only present on STM32MP13 board.

3. On STM32MP13x lines More info.png[edit source]

On STM32MP135F-DK Discovery kit, the GPIO assignment is as follow:

  • The green LED is on the IO expander pin GPB6
  • The red LED and USER2 button are on the pin PA13
  • The blue LED and USER1 button are on the pin PA14
  • The orange LED is on the IO expander pin GPB7
Warning white.png Warning
'Blue LED & USER1', 'Red LED & USER2' are respectively connected to the same GPIO, with inverted logic for the LED control (so the LED is switched on when the GPIO output is set low).

4. On STM32MP15x lines More info.png[edit source]

You can refer to the respective board-hardware descriptions to determine to which GPIO each function is mapped:

Warning white.png Warning
'Green LED & USER1', 'Red LED & USER2' are respectively connected to the same GPIO, with inverted logic for the LED control (so the LED is switched on when the GPIO output is set low).

5. References[edit source]