1. Article purpose[edit source]
The purpose of this article is to give information about the Arm® CoreSight™ hardware subsystem.
It explains what are the principle peripherals of this subsystem.
2. Peripheral overview[edit source]
Arm® CoreSight™ products include a wide range of trace macrocells for Arm® processors, system and software instrumentation and a comprehensive set of IP blocks to enable the debug & trace of the most complex, multi-core SoCs.
Arm® has defined an open CoreSight architecture to allow SoC designers to add debug & trace capabilities for other IP cores in to the CoreSight infrastructure.
2.1. Components description[edit source]
The debug features are based on Arm® CoreSight™ components
Arm® CoreSight™ components | STM32MP13x lines | STM32MP15x lines |
---|---|---|
SWJ-DP: JTAG/Serial-wire debug port | ||
AXI-AP: AXI access port | ||
AHB-AP: AHB access port | ||
APB-AP: APB access port | ||
ITM: Instrumentation Trace Macrocell | ||
DWT: Data Watchpoint and Trace | ||
ETM: Embedded Trace Macrocell | ||
ETF: Embedded Trace FIFO | ||
TPIU: Trace Port Interface Unit | ||
SWO: Serial Wire Output | ||
CTI: Cross Trigger Interface | ||
CTM: Cross Trigger Matrix | ||
TSGEN: Timestamp Generator | ||
STM: System Trace Macrocell |
More information about these components can be found in the Arm® website [1]
2.2. Features[edit source]
The supported debug features are described in the Debug support (DBG) chapter of the reference manual. Refer to:
- STM32MP13 reference manuals for STM32MP13x lines
- STM32MP15 reference manuals for STM32MP15x lines
3. References[edit source]