How to configure U-Boot for your board

Revision as of 17:02, 29 October 2020 by Registered User

This page explains how to configure the U-Boot source for your board.

Many existing ressources [1] [2] explain the porting of U-Boot on a new board. This article only provides basic guidelines for STM32MP1 Series.

To summarize, you need to configure U-Boot for your <VENDOR> <BOARD> with the following steps:

  1. Add your board device tree: arch/arm/dts/<board>.dts and <board>-u-boot.dtsi.
  2. Create your own board support directory: board/<vendor>/<board>.
  3. Add TARGET_<VENDOR> _<BOARD> in Kconfig.
  4. Create your board defconfig: defconfig/<board>_defconfig.
  5. Add your configuration file : include/configs/<board>.h.

1. Device tree[edit source]

Add the board device tree files <board>.dts and <board>-u-boot.dtsi in arch/arm/dts , following the steps below:

  • Copy the Linux kernel device tree in the directory arch/arm/dts : <board>.dts
 dtb-$(CONFIG_STM32MP15x) += \
 	<board>.dtb 
  • Add a U-Boot addon device tree for your board in the arch/arm/dts directory: <board>-u-boot.dtsi
    This file is automatically included during <board>.dts processing.
    It includes the <soc>-u-boot.dtsi file provided by STMicroelectronics (arch/arm/dts/stm32mp15-u-boot.dtsi for example) and add all the properties on nodes needed by U-Boot (added nodes, configs and attibutes: u-boot,dm-pre-reloc or u-boot,dm-pre-proper).

At this point you can use the generic STM32 MPU defconfig with the STMicroelectronics board directory, but with your board device tree.

The board-specific features are not correctly managed, but should be sufficient for a simple board derived from STMicroelectronics designs.

For example, on STM32MP15x lines More info.png, you can use the STMicroelectronics code with your device tree as follows:

  make stm32mp15_trusted_defconfig
  make DEVICE_TREE=<board> all

The next steps are required if the STMicroelectronics generic board does not comply with all of the expected behavioral aspects for your board (for example MAC address not located in OTP, specific PMIC, specific boot command).

1.1. Config node[edit source]

Some properties in the 'config' node are also used to dynamically configure the U-Boot behavior in the board device tree as follows:

  • Generic U-Boot configuration, managed in generic code:
    • u-boot,mmc-env-partition = name of partition used to save U-Boot environment
  • Some STMicroelectronics properties only managed in STMicroelectronics board code (in line with LEDs and buttons on STM32 MPU boards); they can only be used if your board reuses this code
    • u-boot,boot-led = name of boot-progress indicator LED
    • u-boot,error-led = name of error indicator LED
    • st,adc_usb_pd = ADC channels used to check USB power supply
    • st,stm32prog-gpios = GPIO used to force STM32CubeProgrammer mode
    • st,fastboot-gpios = GPIO used to force Android Fastboot mode

For example in arch/arm/dts/stm32mp157a-dk1-u-boot.dtsi

   	config {
   		u-boot,boot-led = "heartbeat";
   		u-boot,error-led = "error";
   		u-boot,mmc-env-partition = "ssbl";
   		st,adc_usb_pd = <&adc1 18>, <&adc1 19>;
   		st,fastboot-gpios = <&gpioa 13 GPIO_ACTIVE_LOW>;
   		st,stm32prog-gpios = <&gpioa 14 GPIO_ACTIVE_LOW>;
   	};

1.2. USB OTG node[edit source]

The U-Boot driver for USB OTG, with the compatible st,stm32mp1-hsotg, doesn't have a full OTG support so only the gadget is used in STM32 MPU board with drivers/usb/host/dwc2.c .

Two U-Boot specific properties are added to support the possible USB connection of ID pin and VBUS on the board:

  • u-boot,force-b-session-valid: force USB B session (deactivate the detection with ID pin) and deactivate VBus sensing; used when all those features are managed by the board (it is used on the STM32MP5X-DK2 board, using the USB type-C controller STUSB1600)
  • u-boot,force-vbus-detection: used to force Vbus sensing, when "u-boot,force-b-session-valid" is used (typically when ID pin is not correctly managed).

Examples of USB configuration in <board>-u-boot.dtsi:

  • To force B session = device mode and USB pin not used and the VBus sensing is deactivated.
 &usbotg_hs {
 	u-boot,force-b-session-valid;
 	dr_mode = "peripheral";
 };
  • To force B session and to force VBus sensing (deactived by default with "force-b-session-valid")
 &usbotg_hs {
 	u-boot,force-b-session-valid;
 	u-boot,force-vbus-detection;
 	dr_mode = "peripheral";
 };

2. Board subdirectory[edit source]

Create your own board support subdirectory = board/<vendor>/<board> and add a Makefile file.

You can add any source files needed for your board.

In this Makefile, you can compile the STMicroelectronics files (in board/st/stm32mp1 or in board/st/common) or just copy them as starting point then modify them.

For example board/dhelectronics/dh_stm32mp1/Makefile uses STMicroelectronics board files in ../../st/stm32mp1 directory and local file "board.c"

 ifdef CONFIG_SPL_BUILD
 obj-y += ../../st/stm32mp1/spl.o
 endif

 obj-y += ../../st/stm32mp1/board.o board.o

3. Kconfig[edit source]

You need to support your board in Kconfig with a new configuration flag: TARGET_<VENDOR>_<BOARD>

3.1. Arch Kconfig: arch/arm/mach-stm32mp/Kconfig [edit source]

  • Add new CONFIG_TARGET_<VENDOR>_<BOARD>
  • Select the required option (soc for example : CONFIG_STM32MP15x)
  • Include your board Kconfig in arch one (source "board/<vendor>/<board>/Kconfig")
 choice
 	prompt "STM32MP15x board select"
 	optional
   
   [...]
   
   config TARGET_<VENDOR>_<BOARD>
   	bool "<vendor> <board> board"
   	select STM32MP15x
   	help
 		target the <vendor> <board> board with SOC STM32MP15x
 		managed by board/<vendor>/<board>
 

To check the U-Boot behavior and the value of the generated variables, in a U-Boot console, you can execute the command "mtdparts".

   endchoice
 
  [...]
  source "board/st/stm32mp1/Kconfig"
  source "board/dhelectronics/dh_stm32mp1/Kconfig"
  source "board/<vendor>/<board>/Kconfig"
  
  endif

3.2. Board Kconfig: board/<vendor>/<board>/Kconfig[edit source]

The mininimal content of this file is:

 if TARGET_<VENDOR>_<BOARD>
 
 config SYS_BOARD
 	default "<board>"
 
 config SYS_VENDOR
 	default "<vendor>"
 
 config SYS_CONFIG_NAME
 	default "<config>"
 endif

See for example board/dhelectronics/dh_stm32mp1/Kconfig .

SYS_CONFIG_NAME is used to select the used configuration file: include/configs/SYS_CONFIG_NAME.h

4. Defconfig[edit source]

Add a new defconfig for your board in configs .

  • copy configs/stm32mp15_trusted_defconfig to your "<vendor>_<board>_defconfig"
  • select your new defconfig: make <vendor>_<board>_defconfig"
  • use make menuconfig to change your defconfig
    • remove CONFIG_TARGET_ST_STM32MP15x
    • add CONFIG_TARGET_<VENDOR>_<BOARD>
    • change CONFIG_DEFAULT_DEVICE_TREE from "stm32mp157c-ev1" to the name of the board device tree: "<board>"
  • save the updated defconfig: make savedefconfig
  • verify and copy the file "defconfig" in configs/<vendor>_<board>_defconfig

See for example the file configs/dh_stm32mp1/stm32mp15_dhcom_basic_defconfig .

5. Configuration file[edit source]

The configuration file is the include file in include/configs directory selected in Makefile.autoconf by CONFIG_SYS_CONFIG_NAME .

This file defines the CONFIG_ flags of boards that are not defined with Kconfig.

For example, in this configuration file, you can choose the initial U-Boot environment with CONFIG_EXTRA_ENV_SETTINGS, including the boot command.

For STMicroelectronics boards, CONFIG_SYS_CONFIG_NAME = stm32mp1; the configuration file is include/configs/stm32mp1.h .

This STMicroelectronics configuration file can be:

  • used in your project (with CONFIG_SYS_CONFIG_NAME="stm32mp1")
or
  • included in your board configuration file (#include "stm32mp1")
or
  • can be used a starting point for your configuration file (copy and update it).

6. Configuration example[edit source]

6.1. MTD partitions[edit source]

In U-Boot, all the mtd partitions are managed in U-Boot variables mtdparts and mtdids.

Then U-Boot dynamically updates the Linux kernel device tree with these information under CONFIG_OF_BOARD_SETUP in board/st/stm32mp1/stm32mp1.c ::ft_board_setup().

This device tree udpate allows to have MTD configuration aligned between U-Boot and Linux and avoids issue for STM32CubeProgrammer support as the MTD partition sizes need to be aligned with Flashlayout.

If the customer needs to define the MTD parttions in Linux device tree, CONFIG_OF_BOARD_SETUP can be deactivated in the customer defconfig (but with potential misalignment with U-Boot).

To simplify the STMicroelectronics board deployment (same software for boot with and without TEE and for any device) these variables mtdparts and mtdids are dynamically built under CONFIG_SYS_MTDPARTS_RUNTIME with :

To check this U-Boot behavior and the generated value of theses variables, execute the command mtdparts in a U-Boot console.

The default values of CONFIG_MTDPARTS_XXX are used for STMicroelectronics boards: see values in board/st/common/Kconfig .

But the customer can modify them in their defconfig if this file stm32mp_mtdparts.c is also used in board configuration file.

For example: CONFIG_MTDPARTS_NAND0_BOOT = "1m(u-boot),512k(params)" and the 'UBI' partition is automatically added at the end of the device.

But the MTD default configuration can also be hardcoded directly in the customer defconfig (stm32mp_mtdparts.c is not used).

  • deactivate CONFIG_SYS_MTDPARTS_RUNTIME
  • choose your MTDPARTS default configuration with
    • CONFIG_MTDPARTS_DEFAULT
    • CONFIG_MTDIDS_DEFAULT

For example:

  CONFIG_MTDPARTS_DEFAULT="mtdparts=nand0:1m(u-boot),512k(params),-(ubifs)"
  CONFIG_MTDIDS_DEFAULT="nand0=nand0"

For information, only mtdids_default and mtdparts_default are generated in mtdparts_init() / board_mtdparts_default() and these defaults values are used only if mtdpart/mtdids variables are empty.

So you can also define the MTD configuration directly with these U-Boot variables in your board configuraiton file, in CONFIG_EXTRA_ENV_SETTINGS:

  • mtdparts="mtdparts=nand0:2m(fsbl),2m(ssbl1),2m(ssbl2),-(UBI)"
  • mtdids="nand0=nand0"

It is a generic U-Boot configuration, see U-Boot documentation for details.

7. References[edit source]