SPDIFRX internal peripheral

Revision as of 17:52, 4 February 2020 by Registered User

1. Article purpose[edit source]

The purpose of this article is to:

  • briefly introduce the SPDIFRX peripheral and its main features
  • indicate the level of security supported by this hardware block
  • explain how each instance can be allocated to the three runtime contexts and linked to the corresponding software components
  • explain how to configure the SPDFIRX peripheral.

2. Peripheral overview[edit source]

The SPDIFRX peripheral, is designed to receive an S/PDIF flow compliant with IEC-60958 and IEC-61937. The SPDIFRX receiver provides two separated paths to retrieve the audio data and the user and channel information.

2.1. Features[edit source]

Refer to the STM32MP15 reference manuals for the complete feature list, and to the software components, introduced below, to see which features are implemented.

2.2. Security support[edit source]

The SPDFIRX is a non secure peripheral.

3. Peripheral usage and associated software[edit source]

3.1. Boot time[edit source]

The SPDFIRX is not used at boot time.

3.2. Runtime[edit source]

3.2.1. Overview[edit source]

The SPDIFRX instance can be allocated to:

Chapter #Peripheral assignment exposes which instance can be assigned to which context.

3.2.2. Software frameworks[edit source]

Internal peripherals software table template

| Audio
| SPDIFRX
| 
| ALSA framework
| STM32Cube SPDIFRX driver
|
|-
|}

3.2.3. Peripheral configuration[edit source]

The configuration is applied by the firmware running in the context to which the peripheral is assigned. The configuration can be done alone via the STM32CubeMX tool for all internal peripherals, and then manually completed (particularly for external peripherals), according to the information given in the corresponding software framework article.

3.2.3.1. Configuration in Cortex-A7 non-secure software[edit source]

When the Arm® Cortex®-A7 core operates in non-secure access mode, the SPDIFRX is controlled by the Linux kernel framework. Refer to the SPDIFRX Linux driver to drive the SPDIFRX through Linux kernel ALSA framework. Refer to Soundcard configuration and SPDIFRX device tree configuration to configure the SPDIFRX through Linux kernel device tree[1].

3.2.3.2. Arm® Cortex®-M4 software configuration[edit source]


3.2.4. Peripheral assignment[edit source]

Internal peripherals assignment table template

| rowspan="1" | Audio
| rowspan="1" | SPDIFRX
| SPDIFRX
| 
| 
| 
| Assignment (single choice)
|-
|}

4. How to go further[edit source]

The STM32H7 SPDIFRX training [2], introduces the STM32 S/PDIF Receiver interface on the STM32H7. This training also applies to the STM32 MPU SPDIFRX internal peripheral.

5. References[edit source]