STM32CubeIDE release note

Revision as of 13:00, 2 October 2019 by Registered User

Template:ArticleMainWriter


More information can be found in the detailed release notes referenced later in this article.

1. STM32CubeIDE 1.1.0 - MPU Support[edit source]

This release of STM32CubeIDE provides support of Cortex®-M core contained in the STM32MP1 Family.
It provides:

  • the target status widget,
  • the console management,
  • the project creation, compilation and debug in two modes:
    • Engineering Mode,
    • Production Mode, with Cortex®-M firmware download :
      • via Ethernet Network (LAN or Point-to-Point)
      • via Ethernet over USB
  • the remote system explorer configuration


It is available on Linux® and Windows® platforms.


STM32CubeIDE for Linux® host PC STM32CubeIDE for Windows® host PC
Download

Version 1.1.0

  • Download the preferred all-in-one Linux installer from my.st.com
    • en.st-stm32cubeide_1.1.0_xxxx_xxxxxxxx_xxxx_amd64.sh.zip
    • en.st-stm32cubeide_1.1.0_xxxx_xxxxxxxx_xxxx_amd64.deb_bundle.sh.zip
    • en.st-stm32cubeide_1.1.0_xxxx_xxxxxxxx_xxxx_amd64.rpm_bundle.sh.zip

Version 1.1.0

  • Download the all-in-one Windows installer from my.st.com
    • en.st-stm32cubeide_1.1.0_xxxx_xxxx_xxxxxxxx_x86_64.exe.zip
Installation
  • Run the installation script
$ chmod +x install_sw4stm32_linux_64bits-v2.8.run
$ ./install_sw4stm32_linux_64bits-v2.8.run
  • Run the installation exe
$ install_sw4stm32_win_64bits-v2.8.exe
Detailed release notes Details about the content of this tool version are available on my.st.com

Details about the content of this tool version are available on my.st.com