1. Configuring the Linux kernel[edit source]
To get debug symbols and add the GDB script (i.e. Linux® awareness), the Linux kernel configuration must activate CONFIG_DEBUG_INFO and CONFIG_GDB_SCRIPTS using the Linux kernel Menuconfig tool (Menuconfig or how to configure kernel):
Symbol: DEBUG_INFO [=y] Location: Kernel Hacking ---> Tracers --> [*] -> Compile time checks and compiler options Symbol: GDB_SCRIPTS [=y] Location: Kernel Hacking ---> Tracers --> [*] -> Compile-time checks and compiler options [*] Provide GDB scripts for kernel debugging
CONFIG_DEBUG_INFO and CONFIG_GDB_SCRIPTS are enabled by default in all STM32MPU software Packages, so you have nothing to do.
2. Kernel boot debugging issue[edit source]
Please refer to GDB page for Linux kernel boot base.
If the default setting of Setup.gdb file is used, the kernel stops in stext function.
...
define break_boot_linuxkernel
symadd_bl32 $bl32_load_addr
thbreak stext
c
end
...
If you prefer to break in another function from the Linux kernel boot, just update the function name in the above break point definition #04572F.
You can then proceed with program execution or set new break point(s). A description of all GDB commands can be found here.
To monitor and debug source code execution, you can also use GDB UI as Gdbgui.
3. Debugging the kernel after boot[edit source]
Please refer to GDB page for Linux kernel execution phase.
In this case, the GDB attaches the target on the current state.
You can then proceed with program execution or set new break point(s). A description of all GDB commands can be found here.
To monitor and debug source code execution, you can also use GDB UI as Gdbgui.
4. Debugging an already-probed kernel module[edit source]
Debugging an external Linux kernel module requires some specific actions, especially because the symbols for this module are not part of the main vmlinux symbol file.
4.1. Adding symbols manually and debugging[edit source]
4.1.1. Checking the module various ELF section addresses[edit source]
Information on where the module various ELF sections were loaded into the kernel space can be obtained by looking into the /sys/module/<module_name>/sections directory.
Below an example for the GPU driver:
ls -al /sys/module/galcore/sections/ total 0 drwxr-xr-x 2 root root 0 Jun 30 22:14 . drwxr-xr-x 7 root root 0 Jun 30 22:04 .. -r--r--r-- 1 root root 4096 Jun 30 22:14 .ARM.exidx -r--r--r-- 1 root root 4096 Jun 30 22:14 .ARM.exidx.exit.text -r--r--r-- 1 root root 4096 Jun 30 22:14 .ARM.exidx.init.text -r--r--r-- 1 root root 4096 Jun 30 22:14 .ARM.exidx.text.unlikely -r--r--r-- 1 root root 4096 Jun 30 22:14 .ARM.extab -r--r--r-- 1 root root 4096 Jun 30 22:14 .alt.smp.init -r--r--r-- 1 root root 4096 Jun 30 22:14 .bss (where the BSS section was loaded) -r--r--r-- 1 root root 4096 Jun 30 22:14 .data (where the data section was loaded) -r--r--r-- 1 root root 4096 Jun 30 22:14 .exit.text -r--r--r-- 1 root root 4096 Jun 30 22:14 .gnu.linkonce.this_module -r--r--r-- 1 root root 4096 Jun 30 22:14 .init.text -r--r--r-- 1 root root 4096 Jun 30 22:14 .note.gnu.build-id -r--r--r-- 1 root root 4096 Jun 30 22:14 .pv_table -r--r--r-- 1 root root 4096 Jun 30 22:14 .rodata -r--r--r-- 1 root root 4096 Jun 30 22:14 .rodata.str -r--r--r-- 1 root root 4096 Jun 30 22:14 .rodata.str1.4 -r--r--r-- 1 root root 4096 Jun 30 22:14 .strtab -r--r--r-- 1 root root 4096 Jun 30 22:14 .symtab -r--r--r-- 1 root root 4096 Jun 30 22:14 .text (where the text section was loaded) -r--r--r-- 1 root root 4096 Jun 30 22:14 .text.unlikely -r--r--r-- 1 root root 4096 Jun 30 22:14 __bug_table -r--r--r-- 1 root root 4096 Jun 30 22:14 __param
You can then retrieve the addresses where the required sections have been loaded, mainly .bss (optional), .data and .text.
cat .text .data .bss
Below an example for the GPU driver:
cat .text .data .bss 0xbf0ba000 --> .text 0xbf0ee000 --> .data 0xbf0fae40 --> .bss
4.1.2. Adding the module symbol file to the GDB environment[edit source]
This is done by using the add-symbol-file GDB command:
(gdb) add-symbol-file <module.ko_path> <address of module's text section> \ -s .data <address of module's data section> \ -s .bss <address of module's bss section if available>
Below an example for the GPU driver:
- If the symbol file is not available on your side, you can get it from the remote target:
scp root@ip_of_board>/lib/modules/4.19.4/extra/galcore.ko <your_path_to>/galcore.ko
- When the symbol file is available, add it to the GDB environment:
(gdb) add-symbol-file <your_path_to>/galcore.ko 0xbf0ba000 \
-s .data 0xbf0ee000 \
-s .bss 0xbf0fae40
- You can then search for a symbol belonging to the new module:
(gdb) p gpu_probe $3 = {int (struct platform_device *)} 0xbf0c4298 <gpu_probe>
- and set a debug breakpoint.
4.2. Adding symbols using the Linux awareness and debug[edit source]
- Enable Linux awareness (refer to Enabling Linux awareness paragraph).
- Load the symbol file.
# Go to your linux kernel build directory path.
(gdb) cd <your_linux_kernel_build_dir>
# Load the kernel symbol vmlinux and all the symbols of the loaded module(s)
(gdb) lx-symbols
You can search for a a symbol belonging to the new module (videobuf2-core.ko module in the example below):
(gdb) p vb2_core_queue_init $1 = {intt (struct vb2_queue *)} 0xbf089380 <vb2_core_queue_init>
and set a debug breakpoint.
- Specific configuration for external module driver
You can also use Linux awareness to debug an external module (source code out of the Linux kernel tree).
In that case, add an argument to lx-symbols command to provide the path to the external module .ko file (only path, not full path).
For example:
(gdb) cd <kernel_build_directory_path>
(gdb) lx-symbols /local/views/hands-on/openstlinux-distribution/openstlinux-hands-driver
5. Debugging a kernel module when probed[edit source]
You can debug an external module when it is inserted (probed) at Linux kernel runtime or during Linux kernel boot phase.
- The Linux awareness environment for GDB is required in this context. Please refer to Enabling Linux awareness paragraph.
- Load the symbol file. You have to specify the directory path for your module symbol file if it is not part of the standard Linux kernel build tree.
# Go to your linux kernel build directory path: (gdb) cd <your_linux_kernel_build_dir> # Load the kernel symbol vmlinux and all the symbols of the loaded module(s): (gdb) lx-symbols <your_symbol_file_path_if_required>
- Load source file paths
If your external module is not part of the standard Linux kernel tree, specify your source file path:
(gdb) directory <your_external_module_source_path>
- Add a breakpoint in the load_module function from the kernel/module.c Linux kernel source file
- This Linux kernel function loads the external module.
- Breakpoints have to be set at a specific line in the function. At this step, the module is prepared by the kernel but not yet started:
/* Now the module is in its final location, and you can initialize the linked lists. */
err = module_unload_init(mod);
if (err) --> please check the line number in the kernel/module.c file, i.e. line 3678
goto unlink_mod;
...
# Insert a breakpoint in the load_module function at line 3678
(gdb) b module.c:3678
(gdb) continue
- Check that the module is the one that you inserted, by printing the module name from the module structure:
(gdb) p mod->name
- If the module is not the expected one, proceed with software execution until the expected module is available.
- When the breakpoint defined in the load_module function is reached, set your breakpoint in your external module
- For example:
(gdb) b goodix_ts_probe
- Proceed with software execution until you reach the breakpoint in your external module driver:
(gdb) continue
6. Debugging Linux kernel decompression[edit source]
- Configure the GDB and the OpenOCD to be attached on the running target in U-Boot phase.
- Add a breakpoint in the boot_jump_linux function from U-Boot source file, arch/arm/lib/bootm.c.
- The U-Boot function jumps to the Linux kernel module previously loaded.
- Breakpoints have to be set at a specific line in the function:
...
kernel_entry(0, machid, r2); -> please check the line number in the arch/arm/lib/bootm.c file, i.e. line 400
...
# Insert a breakpoint in the load_module function: (gdb) b arch/arm/lib/bootm.c:400 Breakpoint 1 at 0xc0100c70: arch/arm/lib/bootm.c:400. (2 locations) (gdb) continue
- From the UART console, run the command to boot the Linux kernel image:
run bootcmd
- In the GDB, check that the software execution stopped at the expected breakpoint. You can then check the kernel_entry address (address of the Linux kernel compressed image that will be executed, i.e. zImage)
(gdb) p kernel_entry $1 = (void (*)(int, int, uint)) 0xc2000040
- Load the compressed Linux kernel symbol file (see symadd_vmlinux_compressed variable define in the path_env.gdb configuration file used in the GDB).
(gdb) symadd_vmlinux_compressed
- Set a breakpoint in the decompress_kernel function from Linux kernel:
(gdb) b decompress_kernel
Breakpoint 2 at 0xc2000ae4: file <your_linux_kernel_source_dir>/arch/arm/boot/compressed/misc.c, line 150
- Proceed with software execution. It then stops at the breakpoint set in the decompress_kernel function:
(gdb) continue
- From this point, you can start a debugging session.
7. Debugging using Linux awareness environment (Python plugin)[edit source]
To enhance debugging experience, Linux awareness provides the debugger with additional knowledge on the underlying operating system (e.g. location of the task list in memory or kernel log buffer).
7.1. Enabling Linux awareness[edit source]
It is highly recommended to use a Linux kernel compiled to get the Linux awareness environment, based on a Developer Package.
Refer to Install Linux kernel software package with STM32MPU Developer Package for detail.
- Add Linux kernel build directories for Python path:
(gdb) add-auto-load-safe-path <your_linux_kernel_build_dir>
- Launch the Linux awareness Python script:
(gdb) source <your_linux_kernel_build_dir>/vmlinux-gdb.py
7.2. Displaying dmesg[edit source]
(gdb) lx-dmesg [ 0.000000] Booting Linux on physical CPU 0x0 [ 0.000000] Linux version 4.14.48 (oe-user@oe-host) (gcc version 7.3.0 (GCC)) #1 SMP PREEMPT Thu Jul 5 07:37:20 UTC 2018 [ 0.000000] CPU: ARMv7 Processor [410fc075] revision 5 (ARMv7), cr=10c5387d [ 0.000000] CPU: div instructions available: patching division code [ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache [ 0.000000] OF: fdt: Machine model: STMicroelectronics STM32MP157C-EV1 pmic eval daughter on eval mother [ 0.000000] bootconsole [earlycon0] enabled ...
7.3. Displaying the module list[edit source]
(gdb) lx-lsmod Address Module Size Used by 0xbf0ba000 galcore 294912 0 0xbf0ad000 stm32_dcmi 28672 0 0xbf0a4000 videobuf2_dma_contig 20480 1 stm32_dcmi 0xbf09d000 videobuf2_memops 16384 1 videobuf2_dma_contig 0xbf094000 videobuf2_v4l2 20480 1 stm32_dcmi 0xbf086000 videobuf2_core 36864 2 stm32_dcmi,videobuf2_v4l2 0xbf078000 ov5640 36864 0 0xbf071000 v4l2_fwnode 16384 2 stm32_dcmi,ov5640 0xbf06a000 v4l2_common 16384 2 stm32_dcmi,ov5640 0xbf038000 videodev 139264 5 stm32_dcmi,videobuf2_v4l2,videobuf2_core,ov5640,v4l2_common 0xbf030000 stm32_cec 16384 0 0xbf022000 media 32768 2 ov5640,videodev 0xbf013000 cec 36864 1 stm32_cec 0xbf009000 snd_soc_stm32_spdifrx 20480 2 0xbf000000 goodix 16384 0
7.4. Displaying the current kernel processes[edit source]
(gdb) lx-ps 0xc1007580 <init_task> 0 swapper/0 0xee8b8000 1 systemd 0xee8b8680 2 kthreadd 0xee8b9380 4 kworker/0:0H 0xee8b9a00 5 kworker/u4:0 0xee8ba080 6 mm_percpu_wq 0xee8ba700 7 ksoftirqd/0 0xee8bad80 8 rcu_preempt 0xee8bb400 9 rcu_sched 0xee8bba80 10 rcu_bh ...
- Print task_struct information:
(gdb) p *(struct task_struct *)<addr_of_process, see above>
- For example:
(gdb) p *(struct task_struct *)0xee8ba080 $1 = {state = 1026, stack = 0xee8ca000, usage = {counter = 2}, flags = 69238880, ptrace = 0, wake_entry = {next = 0x0}, on_cpu = 0, wakee_flips = 0, wakee_flip_decay_ts = 0, ...
- Print the executable name, path excluded:
(gdb) p (*(struct task_struct *)0xee8ba080)->comm $7 = "mm_percpu_wq\000\000\000"
- Print the PID:
(gdb) p (*(struct task_struct *)0xee8ba080)->pid $8 = 6
- Print stack and thread information (ti)
(gdb) p *(struct thread_info *)(*(struct task_struct *)0xee8ba080)->stack $9 = {flags = 0, preempt_count = 2, addr_limit = 0, task = 0xee8ba080, cpu = 0, cpu_domain = 0, cpu_context = {r4 = 4017867840, r5 = 4002128000, r6 = 4002119680, r7 = 3238137856, r8 = 0, r9 = 0, sl = 3238767332, fp = 4002201396, sp = 4002201320, pc = 3232110636, extra = {0, 0}}, syscall = 0, used_cp = '\000' <repeats 15 times>, tp_value = {0, 4115157644}, fpstate = {hard = {save = {0 <repeats 35 times>}}, soft = {save = {0 <repeats 35 times>}}}, vfpstate = {hard = {fpregs = {0 <repeats 32 times>}, fpexc = 0, fpscr = 0, fpinst = 0, fpinst2 = 0, cpu = 0}}, thumbee_state = 0}
7.5. Container_of[edit source]
Each task contains a pointer towards the previous and next task. These pointers are actually pointing to the list itself and not the object.
To get the exact object address, kernel developers generally use container_of. The same macro is implemented in the plugin to quickly browse data structures.
Below an example to find the next task_struct:
(gdb) p $container_of(init_task.tasks.next, "struct task_struct", "tasks") $10 = (struct task_struct *) 0xee8b8000
7.6. Checking list consistency[edit source]
(gdb) p init_task.tasks $11 = {next = 0xee8b8278, prev = 0xedd495f8} (gdb) lx-list-check init_task.tasks Starting with: {next = 0xee8b8278, prev = 0xedd495f8} list is consistent: 92 node(s)
7.7. Loading symbols[edit source]
The lx-symbols command (re)loads the symbols of the Linux kernel and the currently loaded modules.
The kernel (vmlinux) is directly taken from the current working. Modules (.ko) are scanned recursively, starting in the same directory.
Optionally, the module search path can be extended by a list of paths separated by a space and passed to the lx-symbols command:
(gdb) cd <kernel_build_directory_path>
(gdb) lx-symbols [specific_module_symbol_path1] [specific_module_symbol_path2]...
7.8. Other commands[edit source]
You can get the list of commands for Linux awareness:
(gdb) apropos lx function lx_current -- Return current task function lx_module -- Find module by name and return the module variable function lx_per_cpu -- Return per-cpu variable function lx_task_by_pid -- Find Linux task by PID and return the task_struct variable function lx_thread_info -- Calculate Linux thread_info from task variable function lx_thread_info_by_pid -- Calculate Linux thread_info from task variable found by pid lx-cmdline -- Report the Linux Commandline used in the current kernel lx-cpus -- List CPU status arrays lx-dmesg -- Print Linux kernel log buffer lx-fdtdump -- Output Flattened Device Tree header and dump FDT blob to the filename lx-iomem -- Identify the IO memory resource locations defined by the kernel lx-ioports -- Identify the IO port resource locations defined by the kernel lx-list-check -- Verify a list consistency lx-lsmod -- List currently loaded modules lx-mounts -- Report the VFS mounts of the current process namespace lx-ps -- Dump Linux tasks lx-symbols -- (Re-)load symbols of Linux kernel and currently loaded modules lx-version -- Report the Linux Version of the current kernel
8. Hints[edit source]
8.1. RCU stall messages[edit source]
During kernel debugging, halting the CPU will cause the kernel to complain about RCU CPU stall once the CPU execution is restarted. To prevent this annoying messages, you can add the following to the kernel command line:
rcupdate.rcu_cpu_stall_suppress=1
8.2. Breakpoints cleared by kernel boot[edit source]
During kernel boot, Linux deletes the breakpoint unit and a breakpoint set before the boot can be missed. To prevent it, add to the kernel command line:
initcall_blacklist=arch_hw_breakpoint_init
8.3. Breakpoints in kernel code[edit source]
The Linux kernel sets the text segment as read-only. A debugger would be unable to add a SW breakpoint, so only HW breakpoints can be used.
To force GDB to set HW breakpoints through OpenOCD, type the following command in GDB console:
(gdb) monitor gdb_breakpoint_override hard
Please notice that only few HW breakpoints are available for Cortex®-A (usually 6 HW breakpoints on STM32 Arm® Cortex® MPUs ).
If more breakpoints are required, it is possible to run the kernel with the text segment in R/W more, by adding the kernel command line:
rodata=off
or by recompiling the kernel with the read-only protection disabled with:
# CONFIG_STRICT_KERNEL_RWX is not set
9. Reference[edit source]
- Useful external links
Document link | Document Type | Description |
---|---|---|
Gdb Kernel debugging | User guide | Documentation from kernel.org |