How to start the coprocessor from the bootloader

Revision as of 15:46, 23 November 2023 by Registered User (→‎STM32Cube)
Applicable for STM32MP15x lines, STM32MP25x lines

1. Introduction[edit source]

The coprocessor firmware can be loaded and started:

This article explains how the coprocessor firmware is loaded by U-Boot and started before the Linux kernel.

Info white.png Information

The STM32MPU Embedded Software distribution enables the loading of the following firmware format in U-Boot:

  • ELF firmware binary, on STM32MP15x lines More info.png only.
  • Signed firmware binary, on STM32MP15x lines More info.png and STM32MP15x lines More info.png.

2. Location of the coprocessor firmware[edit source]

With generic DISTRO configuration, U-Boot searches and loads the required binaries in the first GPT bootable partition for block device, which is bootfs in the OpenSTLinux distribution, or the boot UBIFS volume in UBI mtd partition (see STM32 MPU Flash mapping), so the coprocessor firmware must be installed in this partition.

For block device, the simplest way to do it consists in copying the firmware from the rootfs partition to the bootfs partition as follows.

  • Boot from an SD card:
 mount /dev/mmcblk0p6 /boot
 cp rproc-m4-fw.elf /boot/
 sync
Here with TF-A update support, bootfs is the 6th partition on SD card. To check the partition name, following commands can be used:
 ls -l /dev/disk/by-partlabel/
  • Boot from with UBI mtd partition "boot":
 mount -t ubifs ubi0:boot /mnt
 cp rproc-m4-fw.elf /mnt/
 sync

As an alternative method, you can use the Eclipse IDE, or transfer the firmware over the serial console or over the network.

Info white.png Information
The default firmware image name rproc-m4-fw.elf is used for the examples on this page. It can be replaced by another name, including the name of a signed firmware image.

3. Starting the coprocessor firmware[edit source]

U-Boot can boot the coprocessor before the kernel (coprocessor early boot) with remoteproc uclass . Several methods are possible:

  1. Manual start by using rproc commands
  2. Automatic start, at each boot by using

3.1. Manual start[edit source]

You can load and start the coprocessor firmware by using the rproc command in the U-Boot console (to access to the U-boot console, press any key during the U-Boot execution).

  rproc
 rproc - Control operation of remote processors in an SoC
 
 Usage:
 rproc  [init|list|load|start|stop|reset|is_running|ping]
 		 Where:
 		[addr] is a memory address
 		<id> is a numerical identifier for the remote processor
 		     provided by 'list' command.
 		Note: Remote processors must be initalized prior to usage
 		Note: Services depend on the driver capability
 		      'list' command shows the capability of each device
 
 	Subcommands:
 	init   - Enumerates and initializes the remote processors
 	list   - lists available remote processors
 	load <id> [addr] [size]- Loads the remote processor with
 			  image stored at address [addr] in memory
 	start <id>	- Starts the remote processor(must be loaded)
 	stop <id>	- Stops the remote processor
 	reset <id>	- Resets the remote processor
 	is_running <id> - Reports if the remote processor is running
 	ping <id>	- Pings the remote processor for communication

In this example, the firmware is loaded from an SD card into RAM (at ${kernel_addr_r}), and then launched.

 load mmc 0#bootfs ${kernel_addr_r} rproc-m4-fw.elf -> SD card is mmc 0, bootfs partition
 rproc init                                        -> initializes all coprocessors
 rproc load 0 ${kernel_addr_r} ${filesize}         -> loads firmware for coprocessor 0 (code part found in .elf)
 rproc start 0                                     -> starts coprocessor 0

You can then resume the normal boot process:

 run bootcmd

3.2. Automatic start[edit source]

3.2.1. Start from the bootcmd[edit source]

You can update the bootcmd which is exectued automatically: modify CONFIG_EXTRA_ENV_SETTINGS in your Configuration file (for example include/configs/stm32mp15_st_common.h for STM32MP15x STMicroelectronics board) and then recompile U-Boot.

For example, to boot a firmware from an SD card, proceed as follows:

#define CONFIG_EXTRA_ENV_SETTINGS \
	"stdin=serial\0" \
	"stdout=serial\0" \
	"stderr=serial\0" \
	...
	BOOTENV \
	"m4fw_name=rproc-m4-fw.elf\0" \
        "m4fw_addr=${kernel_addr_r}\0" \
	"boot_m4fw=rproc init; rproc load 0 ${m4fw_addr} ${filesize}; rproc start 0\0" \
        "boot_m4_mmc0=if load mmc 0#bootfs ${m4fw_addr} ${m4fw_name} ; then run boot_m4fw; fi;\0"
        "bootcmd=run boot_m4_mmc0; run bootcmd_mmc0\0"

Note: It is recommended to check STM32MP15_U-Boot or STM32MP25_U-Boot for compilation.

3.2.2. Start from a generic DISTRO boot script[edit source]

Without U-boot recompilation, you can also use a DISTRO boot script boot.scr.uimg to automatically load and run the firmware.

For example, use the following script boot.scr.cmd to boot from mmc 0 with GPT partition bootfs:

 env set m4fw_name "rproc-m4-fw.elf"
 env set m4fw_addr ${kernel_addr_r}
 
 #load M4 firmware
 if load mmc 0#bootfs ${m4fw_addr} ${m4fw_name}
 then
   rproc init
   rproc load 0 ${m4fw_addr} ${filesize}
   rproc start 0
 fi
 
 #load kernel and device tree
 load mmc 0#bootfs  ${kernel_addr_r} uImage
 load mmc 0#bootfs  ${fdt_addr_r}  ${board_name}.dtb
 
 # start kernel 
 env set bootargs root=/dev/mmcblk0p6 rootwait rw console=ttySTM0,115200
 bootm ${kernel_addr_r} - ${fdt_addr_r}

or this one to boot from a nand 0 with UBI mtd partition and boot UBI volume mounted as ubi 0:

# M4 Firmware load
env set m4fw_name "rproc-m4-fw.elf"
env set m4fw_addr ${kernel_addr_r}

# mount UBIFS on boot UBI volume is not required: it is already done in DISTRO bootcmd
# ubi part UBI
# ubifsmount ubi0:boot 

if load ubi 0 ${m4fw_addr} ${m4fw_name}
then
   rproc init
   rproc load 0 ${m4fw_addr} ${filesize}
   rproc start 0
fi
 
#load kernel and device tree
load ubi 0 ${kernel_addr_r} uImage
load ubi 0 ${fdt_addr_r} ${board_name}.dtb

# start kernel 
env set bootargs ubi.mtd=UBI rootfstype=ubifs root=ubi0:rootfs rootwait rw console=ttySTM0,115200
bootm ${kernel_addr_r} - ${fdt_addr_r}

Then generate the associated image using mkimage U-Boot tool:

 mkimage -T script -C none -A arm -d boot.scr.cmd boot.scr.uimg

Lastly, install boot.scr.uimg in the bootfs partition (following the same procedure used for coprocessor firmware)

 mount /dev/mmcblk0p6 /boot
 cp boot.scr.uimg  /boot/
 sync
Info white.png Information
The name of boot.scr.uimg may be adapted according to your configuration. For example, it may be mmc0_boot.scr.uimg.'
The distro variables can be used in script ${devtype} ${devnum}:${distro_bootpart} to identify the boot device and have more generic script

.

Warning white.png Warning
The 'boot.scr.uimg' U-Boot script is executed only if 'extlinux/extlinux.conf' is not found (scan_dev_for_scripts is called after scan_dev_for_extlinux)
You should remove pre-existing file in bootfs partition:
 mount /dev/mmcblk0p6 /boot
 rm -r /boot/extlinux
 sync

3.2.3. Start from the FIT image[edit source]

The coprocessor firmware can also be included in the new U-Boot image format, Flattened uImage Tree (FIT) . This firmware is then automatically loaded when it is detected by U-Boot.

Info white.png Information
Please note that the upstreaming of this example is in progress, only a part of the files are present in the U-boot sources provided by STMicroelectronics

Refer to chapter 'Coprocessor firmware' in board/st/stm32mp1/README : it contains an example of '.its' file, <U-Boot directory>/board/st/stm32mp1/fit_copro_kernel_dtb.its, and shows how to generate the FIT with U-Boot mkimage tool:

 mkimage -f fit_copro_kernel_dtb.its fit_copro_kernel_dtb.itb

You can load the generated FIT using:

To go deeper, read:

4. Synchronizing the remote firmware with Linux[edit source]

The STM32MPU Embedded Software distribution provides the ability to detect and manage a firmware loaded by U-Boot thanks to the remoteproc Linux framework.

4.1. STM32Cube[edit source]

The developer must pay attention to how he/she implements the Arm Cortex-M firmware (Arm Cortex-M4 or Arm Cortex-M33), if the RPMsg is used to communicate with Linux. In this case a synchronization is required. The Arm Cortex-M core has to wait until Linux is booted to start RPMsg communications. When Linux is ready, the Linux kernel automatically updates the vdev status in the resource table, and sends a signal to the Arm Cortex-M core using the IPCC peripheral.
Two methods can be implemented to wait for the synchronization:

  • Blocking method: the firmware is blocked on MX_OPENAMP_Init call (by the rproc_virtio_wait_remote_ready function) until the Linux kernel is ready to communicate (update of the vdev status in the resource table).
  • Non-blocking method: when it is ready to communicate, the Linux kernel generates an interrupt towards the Arm Cortex-M core using the IPCC peripheral. This interrupt can be used by the Arm Cortex-M firmware to initialize the OpenAMP middleware and start the RPMsg protocol.

4.2. Linux kernel[edit source]

On Linux kernel boot, The Linux remoteproc framework is able to detect if a firmware is already running on the Arm Cortex-M of the STM32 Arm® Cortex® MPUs More info.png (Arm Cortex-M4 or Arm Cortex-M33). If detected, the remoteproc state is set to "detached".

 cat >/sys/class/remoteproc/remoteproc0/state
detached
  • To manually attach to the Cortex-M and start the RPMsg communication, the state has to be updated to "running":
 echo start > /sys/class/remoteproc/remoteproc0/state
 cat /sys/class/remoteproc/remoteproc0/state
running
&m4_rproc {
	st,auto-boot = <1>;
};

or

&m33_rproc {
	st,auto-boot = <1>;
};