1. Article purpose[edit source]
The purpose of this article is to:
- briefly introduce the EXTI peripheral and its main features,
- indicate the peripheral instances assignment at boot time and their assignment at runtime (including whether instances can be allocated to secure contexts),
- list the software frameworks and drivers managing the peripheral,
- explain how to configure the peripheral.
2. Peripheral overview[edit source]
The EXTI peripheral is used to get an interrupt when a GPIO is toggling. It can also wake up the system from Stop low power mode, by means of the PWR internal peripheral when a wake up event occurs, before (eventualy - see the note below) propagating an interrupt to the client processor (Cortex-A7 GIC or Cortex-M4 NVIC in case of STM32MP15). The wake up events can be internal (from other IPs clocked by the LSE, LSI or HSI from RCC), or external (from GPIO).
Notice that:
- Up to 16 GPIO pins can be configured as external interrupts: for each index between 0 and 15, one EXTI can be selected among all banks (EXTI<index> = GPIO<one_bank><index>).
- On STM32MP13x lines
: The 16 GPIO and one internal peripheral events ( AVD/PVD), can generate interrupts connected to the GIC. All the other internal peripheral events can wake up the system, but the EXTI does not generate any interrupt to the GIC; in such cases, another peripheral interrupt has to be used as a trigger via the GIC.
- On STM32MP15x lines
: The 16 GPIO and 5 internal peripheral events (AVD/PVD, CPU1 SEV, CPU2 SEV, WWDG1 reset, CPU2 SYSRESETREQ) can generate interrupts connected to the GIC and NVIC. All the other internal peripheral events can wake up the system, but the EXTI does not generate any interrupt to the GIC or NVIC for them; in such cases, another peripheral interrupt has to be used as a trigger via the GIC or NVIC.
- By default, at reset, all EXTI wake up events are non-secure.
Refer to the STM32 MPU reference manuals for the complete list of features, and to the software frameworks and drivers, introduced below, to see which features are implemented.
3. Peripheral usage[edit source]
This chapter is applicable in the scope of the OpenSTLinux BSP running on the Arm® Cortex®-A processor(s), and the STM32CubeMPU Package running on the Arm® Cortex®-M processor.
3.1. Boot time assignment[edit source]
3.1.1. On STM32MP13x lines
[edit source]
The EXTI peripheral is not used at boot time, but is configured during Linux initialization.
3.1.2. On STM32MP15x lines
[edit source]
The EXTI peripheral is not used at boot time, but is configured during Linux initialization.
Since wake-up event configuration is done via register bit-field reads and writes, concurrent accesses from Linux and the coprocessor are not possible at boot time:
- Linux configures all EXTI events during their respective consumer driver probing
- The coprocessor uses the resource management mechanisms to request and configure the EXTI events it needs.
3.1.3. On STM32MP2 series[edit source]
Click on to expand or collapse the legend...
- ☐ means that the peripheral can be assigned to the given boot time context.
- ☑ means that the peripheral is assigned by default to the given boot time context and that the peripheral is mandatory for the STM32 MPU Embedded Software distribution.
- ⬚ means that the peripheral can be assigned to the given boot time context, but this configuration is not supported in STM32 MPU Embedded Software distribution.
- ✓ is used for system peripherals that cannot be unchecked because they are hardware connected in the device.
The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possibilities might be described in STM32MP25 reference manuals.
Domain | Peripheral | Boot time allocation | Comment ![]() | |||
---|---|---|---|---|---|---|
Instance | Cortex-A35 secure (ROM code) |
Cortex-A35 secure (TF-A BL2) |
Cortex-A35 non-secure (U-Boot) | |||
Core/Interrupts | EXTI ![]() |
EXTI1 | ☐ | ☐ | ☐ | Shareable at internal peripheral level thanks to the RIF: see the boot time allocation per feature |
EXTI2 | ☐ | ☐ | ☐ | Shareable at internal peripheral level thanks to the RIF: see the boot time allocation per feature |
The below table shows the possible boot time allocations for the features of the EXTI1 instance.
Feature | Boot time allocation ![]() |
Comment | ||
---|---|---|---|---|
Cortex-A35 secure (ROM code) |
Cortex-A35 secure (TF-A BL2) |
Cortex-A35 non-secure (U-Boot) | ||
EXTI1[0] | ⬚ | |||
EXTI1[1] | ⬚ | |||
EXTI1[2] | ⬚ | |||
EXTI1[3] | ⬚ | |||
EXTI1[4] | ⬚ | |||
EXTI1[5] | ⬚ | |||
EXTI1[6] | ⬚ | |||
EXTI1[7] | ⬚ | |||
EXTI1[8] | ⬚ | |||
EXTI1[9] | ⬚ | |||
EXTI1[10] | ⬚ | |||
EXTI1[11] | ⬚ | |||
EXTI1[12] | ⬚ | |||
EXTI1[13] | ⬚ | |||
EXTI1[14] | ⬚ | |||
EXTI1[15] | ⬚ | |||
PVD | ⬚ | |||
PVM | ⬚ | |||
VDDGPU_VD | ⬚ | |||
RCC_HSI_FMON | ⬚ | |||
I2C1 | ⬚ | |||
I2C2 | ⬚ | |||
I2C3 | ⬚ | |||
I2C4 | ⬚ | |||
I2C5 | ⬚ | |||
USART1 | ⬚ | |||
USART2 | ⬚ | |||
USART3 | ⬚ | |||
USART6 | ⬚ | |||
UART4 | ⬚ | |||
UART5 | ⬚ | |||
UART7 | ⬚ | |||
UART8 | ⬚ | |||
UART9 | ⬚ | |||
SPI1 | ⬚ | |||
SPI2 | ⬚ | |||
SPI3 | ⬚ | |||
SPI4 | ⬚ | |||
SPI5 | ⬚ | |||
SPI6 | ⬚ | |||
SPI7 | ⬚ | |||
USBH | ⬚ | |||
USB3DR | ⬚ | |||
COMBOPHY | ⬚ | |||
UCPD | ⬚ | |||
LPTIM1 | ⬚ | |||
LPTIM2 | ⬚ | |||
I2C6 | ⬚ | |||
I2C7 | ⬚ | |||
WKUP1 wakeup | ⬚ | |||
WKUP2 wakeup | ⬚ | |||
WKUP3 wakeup | ⬚ | |||
WKUP4 wakeup | ⬚ | |||
WKUP5 wakeup | ⬚ | |||
WKUP6 wakeup | ⬚ | |||
IPCC1 non secure interrupt CPU1 | ⬚ | |||
IPCC1 non secure interrupt CPU2 | ||||
IPCC1 secure interrupt CPU1 | ||||
IPCC1 secure interrupt CPU2 | ||||
CPU2 SEV interrupt | ⬚ | |||
CPU1 SEV interrupt | ||||
WWDG1 Reset | ⬚ | |||
ETH1_PMT wakeup | ⬚ | |||
ETH1_SBD | ⬚ | |||
ETH2_PMT wakeup | ⬚ | |||
ETH2_SBD | ⬚ | |||
DTS | ⬚ | |||
CPU2 SYSRESETREQ local CPU2 reset | ||||
I3C1 | ||||
I3C2 | ||||
I3C3 | ||||
HPDMA1 Channel 0 to 15 CPU1 irq | ⬚ | |||
HPDMA2 Channel 0 to 15 CPU1 irq | ⬚ | |||
HPDMA3 Channel 0 to 15 CPU1 irq | ⬚ | |||
HPDMA1 Channel 0 to 15 CPU2 irq | ||||
HPDMA2 Channel 0 to 15 CPU2 irq | ||||
HPDMA3 Channel 0 to 15 CPU2 irq | ||||
UCPD VBUS DETECT | ⬚ | |||
UCPD VBUS VSAFE5V | ⬚ |
The below table shows the possible boot time allocations for the features of the EXTI2 instance.
Feature | Boot time allocation ![]() |
Comment | ||
---|---|---|---|---|
Cortex-A35 secure (ROM code) |
Cortex-A35 secure (TF-A BL2) |
Cortex-A35 non-secure (U-Boot) | ||
EXTI2[0] | ⬚ | |||
EXTI2[1] | ⬚ | |||
EXTI2[2] | ⬚ | |||
EXTI2[3] | ⬚ | |||
EXTI2[4] | ⬚ | |||
EXTI2[5] | ⬚ | |||
EXTI2[6] | ⬚ | |||
EXTI2[7] | ⬚ | |||
EXTI2[8] | ⬚ | |||
EXTI2[9] | ⬚ | |||
EXTI2[10] | ⬚ | |||
EXTI2[11] | ⬚ | |||
EXTI2[12] | ⬚ | |||
EXTI2[13] | ⬚ | |||
EXTI2[14] | ⬚ | |||
EXTI2[15] | ⬚ | |||
TAMP non secure tamper CPU1 | ⬚ | |||
RTC global non secure Wakeup CPU1 | ⬚ | |||
TAMP non secure tamper CPU2 | ||||
RTC global non secure Wakeup CPU2 | ||||
TAMP non secure tamper CPU3 | ||||
TAMP secure tamper CPU1 | ||||
RTC global secure Wakeup CPU1 | ||||
TAMP secure tamper CPU2 | ||||
RTC global secure Wakeup CPU2 | ||||
I2C8 | ⬚ | |||
LPUART1 | ⬚ | |||
SPI8 | ⬚ | |||
LPTIM3 | ⬚ | |||
LPTIM4 | ⬚ | |||
LPTIM5 | ⬚ | |||
ADF1 | ⬚ | |||
IPCC2 non secure interrupt CPU1 | ⬚ | |||
IPCC2 non secure interrupt CPU2 | ||||
IPCC2 non secure interrupt CPU3 | ||||
IPCC2 secure interrupt CPU1 | ||||
IPCC2 secure interrupt CPU2 | ||||
HSEM1 non secure interrupt | ⬚ | |||
HSEM2 non secure interrupt | ||||
HSEM3 non secure interrupt | ||||
HSEM1 secure interrupt | ||||
HSEM2 secure interrupt | ||||
WWDG2 reset | ⬚ | |||
IWDG1 reset | ||||
IWDG2 reset | ||||
IWDG3 reset | ⬚ | |||
IWDG4 reset | ⬚ | |||
IWDG5 reset | ⬚ | |||
IWDG1 early wake | ⬚ | |||
IWDG2 early wake | ⬚ | |||
IWDG3 early wake | ||||
IWDG4 early wake | ||||
IWDG5 early wake | ||||
CM33 SEV interrupt to CPU3 | ||||
CA35 SEV interrupt to CPU3 | ||||
CM0 SEV interrupt | ⬚ | |||
IAC interrupt CPU1 | ||||
IAC interrupt CPU2 | ||||
VDDCPU_VD | ⬚ | |||
VDDCORE_VD | ⬚ | |||
RETRAM CRC error wakeup | ||||
lpdma_ch0123_cpu1_irq | ⬚ | |||
lpdma_ch0123_cpu2_irq | ||||
lpdma_ch0123_cpu3_irq | ||||
I3C4 | ⬚ | |||
CDBGPWRUPREQ | ⬚ |
3.2. Runtime assignment[edit source]
3.2.1. On STM32MP13x lines
[edit source]
Click on to expand or collapse the legend...
Check boxes illustrate the possible peripheral allocations supported by STM32 MPU Embedded Software:
- ☐ means that the peripheral can be assigned to the given runtime context.
- ☑ means that the peripheral is assigned by default to the given runtime context and that the peripheral is mandatory for the STM32 MPU Embedded Software distribution.
- ⬚ means that the peripheral can be assigned to the given runtime context, but this configuration is not supported in STM32 MPU Embedded Software distribution.
- ✓ is used for system peripherals that cannot be unchecked because they are hardware connected in the device.
Refer to How to assign an internal peripheral to an execution context for more information on how to assign peripherals manually or via STM32CubeMX.
The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possibilities might be described in STM32MP13 reference manuals.
Domain | Peripheral | Runtime allocation | Comment ![]() | ||
---|---|---|---|---|---|
Instance | Cortex-A7 secure (OP-TEE) |
Cortex-A7 non-secure (Linux) | |||
Core/Interrupts | EXTI | EXTI | ☐ | ☐ |
3.2.2. On STM32MP15x lines
[edit source]
Click on to expand or collapse the legend...
Check boxes illustrate the possible peripheral allocations supported by STM32 MPU Embedded Software:
- ☐ means that the peripheral can be assigned to the given runtime context.
- ☑ means that the peripheral is assigned by default to the given runtime context and that the peripheral is mandatory for the STM32 MPU Embedded Software distribution.
- ⬚ means that the peripheral can be assigned to the given runtime context, but this configuration is not supported in STM32 MPU Embedded Software distribution.
- ✓ is used for system peripherals that cannot be unchecked because they are hardware connected in the device.
Refer to How to assign an internal peripheral to an execution context for more information on how to assign peripherals manually or via STM32CubeMX.
The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possiblities might be described in STM32MP15 reference manuals.
Domain | Peripheral | Runtime allocation | Comment ![]() | |||
---|---|---|---|---|---|---|
Instance | Cortex-A7 secure (OP-TEE) |
Cortex-A7 non-secure (Linux) |
Cortex-M4 (STM32Cube) | |||
Core/Interrupts | EXTI | EXTI | ☐ | ☐ | ☐ | Shared |
The OP-TEE EXTI driver is not activated and not used by OpenSTLinux on STM32MP15x lines .
3.2.3. On STM32MP25x lines
[edit source]
Click on to expand or collapse the legend...
Check boxes illustrate the possible peripheral allocations supported by STM32 MPU Embedded Software:
- ☐ means that the peripheral can be assigned to the given runtime context.
- ☑ means that the peripheral is assigned by default to the given runtime context and that the peripheral is mandatory for the STM32 MPU Embedded Software distribution.
- ⬚ means that the peripheral can be assigned to the given runtime context, but this configuration is not supported in STM32 MPU Embedded Software distribution.
- ✓ is used for system peripherals that cannot be unchecked because they are hardware connected in the device.
The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possibilities might be described in STM32MP25 reference manuals.
Domain | Peripheral | Runtime allocation | Comment ![]() | |||||
---|---|---|---|---|---|---|---|---|
Instance | Cortex-A35 secure (OP-TEE / TF-A BL31) |
Cortex-A35 non-secure (Linux) |
Cortex-M33 secure (TF-M) |
Cortex-M33 non-secure (STM32Cube) |
Cortex-M0+![]() (STM32Cube) | |||
Core/Interrupts | EXTI ![]() |
EXTI1 | ☐OP-TEE | ☐ | ☐ | ☐ | ☐ | Shareable at internal peripheral level thanks to the RIF: see the runtime allocation per feature |
EXTI2 | ☐OP-TEE | ☐ | ☐ | ☐ | ☐ | Shareable at internal peripheral level thanks to the RIF: see the runtime allocation per feature |
The below table shows the possible runtime allocations for the features of the EXTI1 instance.
Feature | Runtime allocation ![]() |
Comment | ||||
---|---|---|---|---|---|---|
Cortex-A35 secure (OP-TEE / TF-A BL31) |
Cortex-A35 non-secure (Linux) |
Cortex-M33 secure (TF-M) |
Cortex-M33 non-secure (STM32Cube) |
Cortex-M0+![]() (STM32Cube) | ||
EXTI1[0] | ☐OP-TEE | ☐ | ☐ | ☐ | ||
EXTI1[1] | ☐OP-TEE | ☐ | ☐ | ☐ | ||
EXTI1[2] | ☐OP-TEE | ☐ | ☐ | ☐ | ||
EXTI1[3] | ☐OP-TEE | ☐ | ☐ | ☐ | ||
EXTI1[4] | ☐OP-TEE | ☐ | ☐ | ☐ | ||
EXTI1[5] | ☐OP-TEE | ☐ | ☐ | ☐ | ||
EXTI1[6] | ☐OP-TEE | ☐ | ☐ | ☐ | ||
EXTI1[7] | ☐OP-TEE | ☐ | ☐ | ☐ | ||
EXTI1[8] | ☐OP-TEE | ☐ | ☐ | ☐ | ||
EXTI1[9] | ☐OP-TEE | ☐ | ☐ | ☐ | ||
EXTI1[10] | ☐OP-TEE | ☐ | ☐ | ☐ | ||
EXTI1[11] | ☐OP-TEE | ☐ | ☐ | ☐ | ||
EXTI1[12] | ☐OP-TEE | ☐ | ☐ | ☐ | ||
EXTI1[13] | ☐OP-TEE | ☐ | ☐ | ☐ | ||
EXTI1[14] | ☐OP-TEE | ☐ | ☐ | ☐ | ||
EXTI1[15] | ☐OP-TEE | ☐ | ☐ | ☐ | ||
PVD | ☑OP-TEE | ⬚ | ☐ | ⬚ | ||
PVM | ☑OP-TEE | ⬚ | ☐ | ⬚ | ||
VDDGPU_VD | ☑OP-TEE | ⬚ | ⬚ | ⬚ | ||
RCC_HSI_FMON | ☑OP-TEE | ⬚ | ☐ | ⬚ | ||
I2C1 | ☐OP-TEE | ☐ | ☐ | ☐ | ||
I2C2 | ☐OP-TEE | ☐ | ☐ | ☐ | ||
I2C3 | ☐OP-TEE | ☐ | ☐ | ☐ | ||
I2C4 | ☐OP-TEE | ☐ | ☐ | ☐ | ||
I2C5 | ☐OP-TEE | ☐ | ☐ | ☐ | ||
USART1 | ☐OP-TEE | ☐ | ☐ | ☐ | ||
USART2 | ☐OP-TEE | ☐ | ☐ | ☐ | ||
USART3 | ☐OP-TEE | ☐ | ☐ | ☐ | ||
USART6 | ☐OP-TEE | ☐ | ☐ | ☐ | ||
UART4 | ☐OP-TEE | ☐ | ☐ | ☐ | ||
UART5 | ☐OP-TEE | ☐ | ☐ | ☐ | ||
UART7 | ☐OP-TEE | ☐ | ☐ | ☐ | ||
UART8 | ☐OP-TEE | ☐ | ☐ | ☐ | ||
UART9 | ☐OP-TEE | ☐ | ☐ | ☐ | ||
SPI1 | ☐OP-TEE | ☐ | ☐ | ☐ | ||
SPI2 | ☐OP-TEE | ☐ | ☐ | ☐ | ||
SPI3 | ☐OP-TEE | ☐ | ☐ | ☐ | ||
SPI4 | ☐OP-TEE | ☐ | ☐ | ☐ | ||
SPI5 | ☐OP-TEE | ☐ | ☐ | ☐ | ||
SPI6 | ☐OP-TEE | ☐ | ☐ | ☐ | ||
SPI7 | ☐OP-TEE | ☐ | ☐ | ☐ | ||
USBH | ⬚OP-TEE | ☐ | ☐ | ☐ | ||
USB3DR | ⬚OP-TEE | ☐ | ☐ | ☐ | ||
COMBOPHY | ⬚OP-TEE | ☑ | ⬚ | ⬚ | ||
UCPD | ⬚OP-TEE | ⬚ | ⬚ | ☑ | ||
LPTIM1 | ☐OP-TEE | ☐ | ☐ | ☐ | ||
LPTIM2 | ☐OP-TEE | ☐ | ☐ | ☐ | ||
I2C6 | ☐OP-TEE | ☐ | ☐ | ☐ | ||
I2C7 | ☐OP-TEE | ☐ | ☐ | ☐ | ||
WKUP1 wakeup | ☐OP-TEE | ☐ | ☐ | ☐ | ||
WKUP2 wakeup | ☐OP-TEE | ☐ | ☐ | ☐ | ||
WKUP3 wakeup | ☐OP-TEE | ☐ | ☐ | ☐ | ||
WKUP4 wakeup | ☐OP-TEE | ☐ | ☐ | ☐ | ||
WKUP5 wakeup | ☐OP-TEE | ☐ | ☐ | ☐ | ||
WKUP6 wakeup | ☐OP-TEE | ☐ | ☐ | ☐ | ||
IPCC1 non secure interrupt CPU1 | ✓ | |||||
IPCC1 non secure interrupt CPU2 | ✓ | |||||
IPCC1 secure interrupt CPU1 | ✓OP-TEE | |||||
IPCC1 secure interrupt CPU2 | ✓ | |||||
CPU2 SEV interrupt | ☐OP-TEE | ☐ | ||||
CPU1 SEV interrupt | ☐ | ☐ | ||||
WWDG1 Reset | ⬚OP-TEE | ☐ | ||||
ETH1_PMT wakeup | ⬚OP-TEE | ☐ | ⬚ | ☐ | ||
ETH1_SBD | ⬚OP-TEE | ☐ | ⬚ | ☐ | ||
ETH2_PMT wakeup | ⬚OP-TEE | ☐ | ⬚ | ☐ | ||
ETH2_SBD | ⬚OP-TEE | ☐ | ⬚ | ☐ | ||
DTS | ☐OP-TEE | ⬚ | ☐ | ⬚ | ||
CPU2 SYSRESETREQ local CPU2 reset | ||||||
I3C1 | ☐OP-TEE | ☐ | ☐ | ☐ | ||
I3C2 | ☐OP-TEE | ☐ | ☐ | ☐ | ||
I3C3 | ☐OP-TEE | ☐ | ☐ | ☐ | ||
HPDMA1 Channel 0 to 15 CPU1 irq | ☐OP-TEE | ☐ | ||||
HPDMA2 Channel 0 to 15 CPU1 irq | ☐OP-TEE | ☐ | ||||
HPDMA3 Channel 0 to 15 CPU1 irq | ☐OP-TEE | ☐ | ||||
HPDMA1 Channel 0 to 15 CPU2 irq | ☐ | ☐ | ||||
HPDMA2 Channel 0 to 15 CPU2 irq | ☐ | ☐ | ||||
HPDMA3 Channel 0 to 15 CPU2 irq | ☐ | ☐ | ||||
UCPD VBUS DETECT | ⬚OP-TEE | ⬚ | ⬚ | ☑ | ||
UCPD VBUS VSAFE5V | ⬚OP-TEE | ⬚ | ⬚ | ☑ |
The below table shows the possible runtime allocations for the features of the EXTI2 instance.
Feature | Runtime allocation ![]() |
Comment | ||||
---|---|---|---|---|---|---|
Cortex-A35 secure (OP-TEE / TF-A BL31) |
Cortex-A35 non-secure (Linux) |
Cortex-M33 secure (TF-M) |
Cortex-M33 non-secure (STM32Cube) |
Cortex-M0+![]() (STM32Cube) | ||
EXTI2[0] | ☐OP-TEE | ☐ | ☐ | ☐ | ☐ | |
EXTI2[1] | ☐OP-TEE | ☐ | ☐ | ☐ | ☐ | |
EXTI2[2] | ☐OP-TEE | ☐ | ☐ | ☐ | ☐ | |
EXTI2[3] | ☐OP-TEE | ☐ | ☐ | ☐ | ☐ | |
EXTI2[4] | ☐OP-TEE | ☐ | ☐ | ☐ | ☐ | |
EXTI2[5] | ☐OP-TEE | ☐ | ☐ | ☐ | ☐ | |
EXTI2[6] | ☐OP-TEE | ☐ | ☐ | ☐ | ☐ | |
EXTI2[7] | ☐OP-TEE | ☐ | ☐ | ☐ | ☐ | |
EXTI2[8] | ☐OP-TEE | ☐ | ☐ | ☐ | ☐ | |
EXTI2[9] | ☐OP-TEE | ☐ | ☐ | ☐ | ☐ | |
EXTI2[10] | ☐OP-TEE | ☐ | ☐ | ☐ | ☐ | |
EXTI2[11] | ☐OP-TEE | ☐ | ☐ | ☐ | ☐ | |
EXTI2[12] | ☐OP-TEE | ☐ | ☐ | ☐ | ☐ | |
EXTI2[13] | ☐OP-TEE | ☐ | ☐ | ☐ | ☐ | |
EXTI2[14] | ☐OP-TEE | ☐ | ☐ | ☐ | ☐ | |
EXTI2[15] | ☐OP-TEE | ☐ | ☐ | ☐ | ||
TAMP non secure tamper CPU1 | ⬚ | |||||
RTC global non secure Wakeup CPU1 | ✓ | |||||
TAMP non secure tamper CPU2 | ☐ | |||||
RTC global non secure Wakeup CPU2 | ☐ | |||||
TAMP non secure tamper CPU3 | ☐ | |||||
TAMP secure tamper CPU1 | ✓OP-TEE | |||||
RTC global secure Wakeup CPU1 | ✓OP-TEE | |||||
TAMP secure tamper CPU2 | ☐ | |||||
RTC global secure Wakeup CPU2 | ☐ | |||||
I2C8 | ☐OP-TEE | ☐ | ☐ | ☐ | ☐ | |
LPUART1 | ☐OP-TEE | ☐ | ☐ | ☐ | ☐ | |
SPI8 | ☐OP-TEE | ☐ | ☐ | ☐ | ☐ | |
LPTIM3 | ☐OP-TEE | ☐ | ☐ | ☐ | ☐ | |
LPTIM4 | ☐OP-TEE | ☐ | ☐ | ☐ | ☐ | |
LPTIM5 | ☐OP-TEE | ☐ | ☐ | ☐ | ☐ | |
ADF1 | ☐OP-TEE | ☐ | ☐ | ☐ | ☐ | |
IPCC2 non secure interrupt CPU1 | ☑ | |||||
IPCC2 non secure interrupt CPU2 | ☑ | |||||
IPCC2 non secure interrupt CPU3 | ☑ | |||||
IPCC2 secure interrupt CPU1 | ☑OP-TEE | |||||
IPCC2 secure interrupt CPU2 | ☑ | |||||
HSEM1 non secure interrupt | ☑ | |||||
HSEM2 non secure interrupt | ☑ | |||||
HSEM3 non secure interrupt | ☑ | |||||
HSEM1 secure interrupt | ☑OP-TEE | |||||
HSEM2 secure interrupt | ☑ | |||||
WWDG2 reset | ☐OP-TEE | ☐ | ☐ | ☐ | ||
IWDG1 reset | ||||||
IWDG2 reset | ☑OP-TEE | ☐ | ☐ | |||
IWDG3 reset | ☐OP-TEE | ☐ | ||||
IWDG4 reset | ☐OP-TEE | ☐ | ☑ | |||
IWDG5 reset | ☐OP-TEE | ☐ | ☐ | ☐ | ||
IWDG1 early wake | ☑OP-TEE | ☐ | ||||
IWDG2 early wake | ☐OP-TEE | ☑ | ||||
IWDG3 early wake | ☑ | ☐ | ||||
IWDG4 early wake | ☐ | ☑ | ||||
IWDG5 early wake | ☑ | |||||
CM33 SEV interrupt to CPU3 | ☑ | |||||
CA35 SEV interrupt to CPU3 | ☑ | |||||
CM0 SEV interrupt | ☐OP-TEE | ☐ | ☐ | ☐ | ||
IAC interrupt CPU1 | ✓OP-TEE | |||||
IAC interrupt CPU2 | ||||||
VDDCPU_VD | ☐OP-TEE | ⬚ | ☐ | ☐ | ||
VDDCORE_VD | ☐OP-TEE | ⬚ | ☐ | ☐ | ☐ | |
RETRAM CRC error wakeup | ||||||
lpdma_ch0123_cpu1_irq | ⬚OP-TEE | ⬚ | ||||
lpdma_ch0123_cpu2_irq | ☐ | ☐ | ||||
lpdma_ch0123_cpu3_irq | ☐ | |||||
I3C4 | ☐OP-TEE | ☐ | ☐ | ☐ | ☐ | |
CDBGPWRUPREQ | ☐OP-TEE | ☐ | ☐ | ☐ | ☐ |
4. Software frameworks and drivers[edit source]
Below are listed the software frameworks and drivers managing the EXTI peripheral for the embedded software components listed in the above tables.
- Linux®: interrupts framework
- OP-TEE: OP-TEE EXTI driver
- STM32Cube: HAL EXTI driver
5. How to assign and configure the peripheral[edit source]
The peripheral assignment can be done via the STM32CubeMX graphical tool (and manually completed if needed).
This tool also helps to configure the peripheral:
- partial device trees (pin control and clock tree) generation for the OpenSTLinux software components,
- HAL initialization code generation for the STM32CubeMPU Package.
The configuration is applied by the firmware running in the context in which the peripheral is assigned.
See also additional information in the Interrupt device tree configuration article for Linux®.