USB3DR internal peripheral

Revision as of 21:44, 9 September 2023 by Registered User
Applicable for STM32MP25x lines

Warning white.png Warning
Concerning the STM32MP25x lines More info.png, only the boot time assignment table and the runtime assignment table have been updated.
The other chapters have not been updated yet.


1. Article purpose[edit source]

The purpose of this article is to:

  • briefly introduce the USB3DR peripheral and its main features,
  • indicate the peripheral instances assignment at boot time and their assignment at runtime (including whether instances can be allocated to secure contexts),
  • list the software frameworks and drivers managing the peripheral,
  • explain how to configure the peripheral.

2. Peripheral overview[edit source]

The USB3DR peripheral is used to interconnect other systems with STM32 MPU devices, using USB standard. USB3DR (as name implies) supports USB3 and lower versions of the standard

The USB3DR peripheral is a USB Dual-Role Device (DRD) controller that supports both device and host functions.

USB3DR speeds supported SS (5000 Mb/s) HS (480 Mb/s) FS (12 Mb/s) LS (1.5 Mb/s)
Host mode Yes Yes Yes Yes
Device mode Yes Yes Yes

USB3DR supports the following PHY interfaces:

USB3DR peripheral PHY interfaces STM32MP25x lines More info.png
UTMI interface connected to internal HS PHY for HS/FS/LS speeds Yes
PIPE interface connected to internal SS PHY for SS speeds Yes

The USB3DR peripheral is fully compliant with

  • Universal Serial Bus Revision 2.0 Specification[1], Revision 2.0, April 27, 2000
  • Universal Serial Bus Revision 3.0 Specification[2], Revision 3.0, November 12, 2008
  • USB 2.0 Link Power Management Addendum Engineering Change Notice to the USB 2.0 specification[3], July 16, 2007
  • USB 2.0 Transceiver Macrocell Interface (UTMI) Specification[4], Version 1.05, March 29, 2001
  • UTMI+ Specification[5], Revision 1.0, February 25, 2004
  • Physical Interface for PCI Express (PIPE) Specification[6]

Refer to the STM32 MPU reference manuals for the complete list of features, and to the software frameworks and drivers, introduced below, to see which features are implemented.

3. Peripheral usage[edit source]

This chapter is applicable in the scope of the OpenSTLinux BSP running on the Arm® Cortex®-A processor(s), and the STM32CubeMPU Package running on the Arm® Cortex®-M processor.

3.1. Boot time assignment[edit source]

3.1.1. On STM32MP2 series[edit source]

Click on How to.png to expand or collapse the legend...

  • means that the peripheral can be assigned to the given boot time context.
  • means that the peripheral is assigned by default to the given boot time context and that the peripheral is mandatory for the STM32 MPU Embedded Software distribution.
  • means that the peripheral can be assigned to the given boot time context, but this configuration is not supported in STM32 MPU Embedded Software distribution.
  • is used for system peripherals that cannot be unchecked because they are hardware connected in the device.

The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possibilities might be described in STM32MP25 reference manuals.

Domain Peripheral Boot time allocation Comment How to.png
Instance Cortex-A35
secure
(ROM code)
Cortex-A35
secure
(TF-A BL2)
Cortex-A35
non-secure
(U-Boot)
High speed interface USB3DR USB3DR

3.2. Runtime assignment[edit source]

3.2.1. On STM32MP25x lines More info.png[edit source]

Click on How to.png to expand or collapse the legend...

STM32MP25 internal peripherals

Check boxes illustrate the possible peripheral allocations supported by STM32 MPU Embedded Software:

  • means that the peripheral can be assigned to the given runtime context.
  • means that the peripheral is assigned by default to the given runtime context and that the peripheral is mandatory for the STM32 MPU Embedded Software distribution.
  • means that the peripheral can be assigned to the given runtime context, but this configuration is not supported in STM32 MPU Embedded Software distribution.
  • is used for system peripherals that cannot be unchecked because they are hardware connected in the device.

The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possibilities might be described in STM32MP25 reference manuals.

Domain Peripheral Runtime allocation Comment How to.png
Instance Cortex-A35
secure
(OP-TEE /
TF-A BL31)
Cortex-A35
non-secure
(Linux)
Cortex-M33
secure
(TF-M)
Cortex-M33
non-secure
(STM32Cube)
Cortex-M0+
Warning.png
(STM32Cube)
High speed interface USB3DR USB3DR OP-TEE

4. Software frameworks and drivers[edit source]

Below are listed the software frameworks and drivers managing the USB3DR peripheral for the embedded software components listed in the above tables.

Under construction.png Coming soon

5. How to assign and configure the peripheral[edit source]

The peripheral assignment can be done via the STM32CubeMX graphical tool (and manually completed if needed).
This tool also helps to configure the peripheral by generating:

  • partial device trees (pin control and clock tree) for the OpenSTLinux software components,
  • HAL initialization code for the STM32CubeMPU Package.

The configuration is applied by the firmware running in the context in which the peripheral is assigned.

Under construction.png Coming soon

6. How to go further[edit source]

Under construction.png Coming soon

7. References[edit source]