This article lists all internal peripherals embedded in STM32MP25x lines and shows the assignment possibilities to the runtime contexts for each one of them.
From this article, you can also access to individual peripheral articles with information related to the overview and configuration aspects.
1. Internal peripherals overview[edit source]
The figure below shows all peripherals embedded in STM32MP25x lines , grouped per functional domains that are reused in many places of this wiki to structure the articles.
Several runtime contexts exist on STM32MP25x lines [1], corresponding to the different Arm cores and associated security modes:
- Arm dual core Cortex-A35 secure (Trustzone), running OP-TEE
- Arm dual core Cortex-A35 non secure , running Linux
- Arm Cortex-M33 secure (Trustzone), running TF-M
- Arm Cortex-M4 non-secure , running STM32Cube
The legend below shows how assigned and shared peripherals are identified in the assignment diagram that follows:
Both the diagram below and the following summary table (in Internal peripherals assignment chapter below) are clickable in order to jump to each peripheral overview articles and get more detailed information (like software frameworks used to control them). They list STMicroelectronics recommendations. The STM32MP25 reference manual [2] may expose more possibilities than what is shown here.
2. Internal peripherals runtime assignment[edit source]
Click on to expand or collapse the legend...
Check boxes illustrate the possible peripheral allocations supported by STM32 MPU Embedded Software:
- ☐ means that the peripheral can be assigned to the given runtime context.
- ☑ means that the peripheral is assigned by default to the given runtime context and that the peripheral is mandatory for the STM32 MPU Embedded Software distribution.
- ⬚ means that the peripheral can be assigned to the given runtime context, but this configuration is not supported in STM32 MPU Embedded Software distribution.
- ✓ is used for system peripherals that cannot be unchecked because they are hardware connected in the device.
The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possibilities might be described in STM32MP25 reference manuals.
Domain | Peripheral | Runtime allocation | Comment | |||||
---|---|---|---|---|---|---|---|---|
Instance | Cortex-A35 secure (OP-TEE / TF-A BL31) |
Cortex-A35 non-secure (Linux) |
Cortex-M33 secure (TF-M) |
Cortex-M33 non-secure (STM32Cube) |
Cortex-M0+ (STM32Cube) | |||
Core/Processors | Arm® Cortex®-A35 | Arm® Cortex®-A35 | ✓OP-TEE ✓TF-A BL31 |
✓ | ||||
Core/Processors | Arm® Cortex®-M33 (coprocessor) | Arm® Cortex®-M33 (coprocessor) | ☐OP-TEE | ☐ | ☐ | ✓ | Controlled by LInux or OP-TEE. Running the STM32CubeMP2 firmware. | |
Core/Processors | Arm® Cortex®-M0+ (coprocessor) | Arm® Cortex®-M0+ (coprocessor) | ☐OP-TEE | ☐ | ☐ | ☐ | ||
Analog | VREFBUF | VREFBUF | ☑OP-TEE | ☐ | ☐ | ☐ | OP-TEE offers SCMI regulator service to manage VREFBUF | |
Analog | ADC | ADC12 | ⬚ | ☐ | ⬚ | ☐ | ||
ADC3 | ⬚ | ☐ | ⬚ | ☑ | ADC3 may be used by the UCSI firmware to measure the Vbus level on the Type-C connector. | |||
Analog | MDF | MDF1 | ⬚OP-TEE | ☐ | ⬚ | ☐ | ||
Low speed interface or audio |
SPI | SPI2S1 | ⬚OP-TEE | ☐ | ⬚ | ☐ | ||
SPI2S2 | ⬚OP-TEE | ☐ | ⬚ | ☐ | ||||
SPI2S3 | ⬚OP-TEE | ☐ | ⬚ | ☐ | ||||
SPI4 | ⬚OP-TEE | ☐ | ⬚ | ☐ | ||||
SPI5 | ⬚OP-TEE | ☐ | ⬚ | ☐ | ||||
SPI6 | ⬚OP-TEE | ☐ | ⬚ | ☐ | ||||
SPI7 | ⬚OP-TEE | ☐ | ⬚ | ☐ | ||||
SPI8 | ⬚OP-TEE | ☐ | ⬚ | ☐ | ☐ | |||
Audio | ADF | ADF1 | ⬚OP-TEE | ☐ | ⬚ | ☐ | ☐ | |
Audio | SPDIFRX | SPDIFRX | ⬚OP-TEE | ☐ | ⬚ | ☐ | ||
Audio | SAI | SAI1 | ⬚OP-TEE | ☐ | ⬚ | ☐ | ||
SAI2 | ⬚OP-TEE | ☐ | ⬚ | ☐ | ||||
SAI3 | ⬚OP-TEE | ☐ | ⬚ | ☐ | ||||
SAI4 | ⬚OP-TEE | ☐ | ⬚ | ☐ | ||||
Coprocessor | IPCC | IPCC1 | ☐OP-TEE | ☐ | ☐ | ☐ | Shareable at internal peripheral level thanks to the RIF: see the runtime allocation per feature | |
IPCC2 | ☐OP-TEE | ☐ | ☐ | ☐ | ☐ | Shareable at internal peripheral level thanks to the RIF: see the runtime allocation per feature | ||
Core | STGEN | STGEN | ☑OP-TEE ☑TF-A BL31 |
Read-only (STGENR) |
Read-only (STGENR) |
Read-only (STGENR) |
||
Core | SYSCFG | SYSCFG | ☑ | ☑ | ☑ | ☑ | ||
Core | RTC | RTC | ☐OP-TEE | ☐ | ☐ | ☐ | ☐ | Shareable at internal peripheral level thanks to the RIF: see the runtime allocation per feature |
Core/DMA | HPDMA | HPDMAx (x = 1 to 3) | ☐OP-TEE | ☐ | ☐ | ☐ | ☐ | Shareable at internal peripheral level thanks to the RIF: see the runtime allocation per feature |
Core/DMA | LPDMA | LPDMA | ☐OP-TEE | ☐ | ☐ | ☐ | ☐ | Shareable at internal peripheral level thanks to the RIF: see the runtime allocation per feature |
Core/Interrupts | EXTI | EXTI1 | ☐OP-TEE | ☐ | ☐ | ☐ | ☐ | Shareable at internal peripheral level thanks to the RIF: see the runtime allocation per feature |
EXTI2 | ☐OP-TEE | ☐ | ☐ | ☐ | ☐ | Shareable at internal peripheral level thanks to the RIF: see the runtime allocation per feature | ||
Core/Interrupts | NVIC | NVIC CM33 | ✓ | ✓ | ||||
NVIC CM0+ | ✓ | |||||||
Core/Interrupts | GIC | GIC | ✓OP-TEE ✓TF-A BL31 |
✓ | ||||
Core/IOs | GPIO | GPIOA-K | ☐OP-TEE ☐TF-A BL31 |
☐ | ☐ | ☐ | Shareable at internal peripheral level thanks to the RIF: see the runtime allocation per feature | |
GPIOZ | ☐OP-TEE ☐TF-A BL31 |
☐ | ☐ | ☐ | ☐ | Shareable at internal peripheral level thanks to the RIF: see the runtime allocation per feature | ||
Core/RAM | SYSRAM | SYSRAM | ☑BL31 ☐OP-TEE |
☑ | ☐ | ☐ |
Cortex-A35 secure section required for low power entry and exit | |
Core/RAM | DDRCTRL | DDR | ☑TF-A BL31 | ⬚ | ☐ | ⬚ | ||
Core/RAM | BKPSRAM | BKPSRAM | ⬚OP-TEE
☑TF-A BL31 |
⬚ | ☑ | ⬚ | TF-M uses BKPSRAM for ITS (Internal Trusted Storage) | |
Core/RAM | RETRAM | RETRAM | ☐OP-TEE
☐TF-A BL31 |
⬚ | ☑ | ☐ | ||
Core/Timers | TIM | TIM1 | ⬚OP-TEE | ☐ | ⬚ | ☐ | ||
TIM10 | ⬚OP-TEE | ☐ | ⬚ | ☐ | ||||
TIM11 | ⬚OP-TEE | ☐ | ⬚ | ☐ | ||||
TIM12 | ⬚OP-TEE | ☐ | ⬚ | ☐ | ||||
TIM13 | ⬚OP-TEE | ☐ | ⬚ | ☐ | ||||
TIM14 | ⬚OP-TEE | ☐ | ⬚ | ☐ | ||||
TIM15 | ⬚OP-TEE | ☐ | ⬚ | ☐ | ||||
TIM16 | ⬚OP-TEE | ☐ | ⬚ | ☐ | ||||
TIM17 | ⬚OP-TEE | ☐ | ⬚ | ☐ | ||||
TIM2 | ⬚OP-TEE | ☐ | ⬚ | ☐ | ||||
TIM20 | ⬚OP-TEE | ☐ | ⬚ | ☐ | ||||
TIM3 | ⬚OP-TEE | ☐ | ⬚ | ☐ | ||||
TIM4 | ⬚OP-TEE | ☐ | ⬚ | ☐ | ||||
TIM5 | ⬚OP-TEE | ☐ | ⬚ | ☐ | ||||
TIM6 | ⬚OP-TEE | ☐ | ⬚ | ☐ | ||||
TIM7 | ⬚OP-TEE | ☐ | ⬚ | ☐ | ||||
TIM8 | ⬚OP-TEE | ☐ | ⬚ | ☐ | ||||
Core/Timers | LPTIM | LPTIM1 | ☐OP-TEE | ☐ | ⬚ | ☐ | LPTIM1 can be used for HSE monitoring. | |
LPTIM2 | ☐OP-TEE | ☐ | ⬚ | ☐ | ||||
LPTIM3 | ☐OP-TEE | ☐ | ⬚ | ☐ | ☐ | |||
LPTIM4 | ☐OP-TEE | ☐ | ⬚ | ☐ | ☐ | |||
LPTIM5 | ☐OP-TEE | ☐ | ⬚ | ☐ | ☐ | |||
Core/Watchdog | IWDG | IWDG1 | ☑OP-TEE ☑TF-A BL31 |
☐ | ||||
IWDG2 | ☐OP-TEE ☐TF-A BL31 |
☐ | ||||||
IWDG3 | ☐ | ☐ | ||||||
IWDG4 | ☐ | ☐ | ||||||
IWDG5 | ☐ | |||||||
Core/Watchdog | WWDG | WWDG1 | ⬚ | ☐ | ||||
WWDG2 | ☐ | |||||||
High speed interface | USB3DR | USB3DR | ⬚OP-TEE | ☐ | ⬚ | ⬚ | The USB3DR running at USB3 speed and the PCIe are mutually exclusive. Both require to use the ComboPHY. | |
High speed interface | USBH | USBH | ⬚OP-TEE | ☐ | ⬚ | ⬚ | ||
High speed interface | COMBOPHY | COMBOPHY | ⬚OP-TEE | ☐ | ⬚ | ⬚ | COMBOPHY can be assigned to either the USB3DR or the PCIe. | |
High speed interface | PCIe | PCIe | ⬚OP-TEE | ☐ | The PCIe and the USB3DR running at USB3 speed are mutually exclusive. Both require using the ComboPHY. | |||
Low speed interface | USART | UART4 | ☐OP-TEE ☐TF-A BL31 |
☐ | ☐ | ☐ | ||
UART5 | ☐OP-TEE ☐TF-A BL31 |
☐ | ☐ | ☐ | ||||
UART7 | ☐OP-TEE ☐TF-A BL31 |
☐ | ☐ | ☐ | ||||
UART8 | ☐OP-TEE ☐TF-A BL31 |
☐ | ☐ | ☐ | ||||
UART9 | ☐OP-TEE ☐TF-A BL31 |
☐ | ☐ | ☐ | ||||
USART1 | ☐OP-TEE ☐TF-A BL31 |
☐ | ☐ | ☐ | ||||
USART2 | ☐OP-TEE ☐TF-A BL31 |
☐ | ☐ | ☐ | ||||
USART3 | ☐OP-TEE ☐TF-A BL31 |
☐ | ☐ | ☐ | ||||
USART6 | ☐OP-TEE ☐TF-A BL31 |
☐ | ☐ | ☐ | ||||
Low speed interface | I2C | I2C1 | ☐OP-TEE ⬚TF-A BL31 |
☐ | ☐ | ☐ | ||
I2C2 | ☐OP-TEE ⬚TF-A BL31 |
☐ | ☐ | ☐ | ||||
I2C3 | ☐OP-TEE ⬚TF-A BL31 |
☐ | ☐ | ☐ | ||||
I2C4 | ☐OP-TEE ⬚TF-A BL31 |
☐ | ☐ | ☐ | ||||
I2C5 | ☐OP-TEE ⬚TF-A BL31 |
☐ | ☐ | ☐ | ||||
I2C6 | ☐OP-TEE ⬚TF-A BL31 |
☐ | ☐ | ☐ | ||||
I2C7 | ☐OP-TEE ⬚TF-A BL31 |
☐ | ☐ | ☐ | ||||
I2C8 | ☐OP-TEE ⬚TF-A BL31 |
☐ | ☐ | ☐ | ☐ | |||
Low speed interface | I3C | I3C1 | ⬚OP-TEE ⬚TF-A BL31 |
☐ | ⬚ | ☐ | ||
I3C2 | ⬚OP-TEE ⬚TF-A BL31 |
☐ | ⬚ | ☐ | ||||
I3C3 | ⬚OP-TEE ⬚TF-A BL31 |
☐ | ⬚ | ☐ | ||||
I3C4 | ⬚OP-TEE ⬚TF-A BL31 |
☐ | ⬚ | ☐ | ☐ | |||
Mass storage | OCTOSPI | OCTOSPI1 | ⬚OP-TEE | ☐ | ☐ | ☐ | OP-TEE need to access OCTOSPI1 at boot time to set OSPIM mode | |
OCTOSPI2 | ⬚OP-TEE | ☐ | ☐ | ☐ | OP-TEE need to access OCTOSPI2 at boot time to set OSPIM mode | |||
Mass storage | OCTOSPIM | OCTOSPIM | ☐OP-TEE | ☐ | ☐ | ☐ | ||
Mass storage | FMC | FMC | ☐OP-TEE | ☐ | ☐ | ☐ | ☐ | Shareable at internal peripheral level thanks to the RIF: see the runtime allocation per feature |
Mass storage | SDMMC | SDMMC1 | ⬚OP-TEE | ☐ | ⬚ | ☐ | ||
SDMMC2 | ⬚OP-TEE | ☐ | ⬚ | ☐ | ||||
SDMMC3 | ⬚OP-TEE | ☐ | ⬚ | ☐ | ||||
Networking | FDCAN | FDCAN1 | ⬚OP-TEE | ☐ | ⬚ | ☐ | ||
FDCAN2 | ⬚OP-TEE | ☐ | ⬚ | ☐ | ||||
FDCAN3 | ⬚OP-TEE | ☐ | ⬚ | ☐ | ||||
Networking | ETHSW | ETHSW | ⬚OP-TEE | ☐ | ⬚ | ⬚ | ||
Networking | ETH | ETH1 | ⬚OP-TEE | ☐ | ⬚ | ☐ | ||
ETH2 | ⬚OP-TEE | ☐ | ⬚ | ☐ | ||||
Power & Thermal | RCC | RCC | ✓OP-TEE ✓TF-A BL31 |
✓ | ✓ | ✓ | ✓ | Shareable at internal peripheral level thanks to the RIF: see the runtime allocation per feature |
Power & Thermal | PWR | PWR | ☐OP-TEE ☐TF-A BL31 |
☐ | ☐ | ☐ | ☐ | Shareable at internal peripheral level thanks to the RIF: see the runtime allocation per feature |
Power & Thermal | DTS | DTS | ⬚OP-TEE | ☐ | ⬚ | |||
Security | BSEC | BSEC | ✓OP-TEE ✓TF-A BL31 |
|||||
Security | RNG | RNG | ☑OP-TEE | ☐ | ☐ | ⬚ | ||
Security | HASH | HASH | ☐OP-TEE | ☐ | ☐ | ☐ | ||
Security | CRYP | CRYP1 | ☐OP-TEE | ☐ | ⬚ | ☐ | ||
CRYP2 | ☐OP-TEE | ☐ | ⬚ | ☐ | ||||
Security | CRC | CRC | ⬚OP-TEE | ☐ | ⬚ | ☐ | ||
Security | SAES | SAES | ☐OP-TEE | ⬚ | ☐ | ⬚ | ||
Security | TAMP | TAMP | ✓OP-TEE | ⬚ | ⬚ | ⬚ | Shareable at internal peripheral level thanks to the RIF: see the runtime allocation per feature | |
Security | OTFDEC | OTFDEC1 | ⬚OP-TEE | ⬚ | ⬚ | ⬚ | ||
OTFDEC2 | ⬚OP-TEE | ⬚ | ⬚ | ⬚ | ||||
Security | PKA | PKA | ☐OP-TEE | ⬚ | ☐ | ⬚ | ||
Trace & Debug | HDP | HDP | ⬚OP-TEE | ☑ | ⬚ | ⬚ | ||
Trace & debug | SERC | SERC | ☑OP-TEE | ⬚ | ||||
Security | IAC | IAC | ✓OP-TEE | ⬚ | Fixed to TDCID | |||
Trace & Debug | DDRPERFM | DDRPERFM | ⬚OP-TEE | ☐ | ⬚ | ⬚ | ||
Visual | GPU | GPU | ⬚OP-TEE | ☑ | ⬚ | ⬚ | ||
Visual | DSI | DSI | ☐OP-TEE | ☐ | ☐ | ☐ | ☐ | Shareable at internal peripheral level thanks to the RIF: see the runtime allocation per feature |
Visual | LTDC | LTDC | ☐OP-TEE | ☐ | ☐ | ☐ | ☐ | Shareable at internal peripheral level thanks to the RIF: see the runtime allocation per feature |
Visual | DCMI | DCMI | ⬚OP-TEE | ☑ | ⬚ | ☐ | ||
Visual | CSI | CSI | ⬚OP-TEE | ☑ | ⬚ | ☐ | ||
Visual | LVDS | LVDS | ⬚OP-TEE | ☑ | ⬚ | ☐ | ||
Visual | DCMIPP | DCMIPP | ⬚OP-TEE | ☑ | ⬚ | ☐ | ||
Visual | VENC | VENC | ⬚OP-TEE | ☑ | ⬚ | ⬚ | ||
Visual | VDEC | VDEC | ⬚OP-TEE | ☑ | ⬚ | ⬚ |
3. Internal peripherals boot time assignment[edit source]
Click on to expand or collapse the legend...
- ☐ means that the peripheral can be assigned to the given boot time context.
- ☑ means that the peripheral is assigned by default to the given boot time context and that the peripheral is mandatory for the STM32 MPU Embedded Software distribution.
- ⬚ means that the peripheral can be assigned to the given boot time context, but this configuration is not supported in STM32 MPU Embedded Software distribution.
- ✓ is used for system peripherals that cannot be unchecked because they are hardware connected in the device.
The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possibilities might be described in STM32MP25 reference manuals.
Domain | Peripheral | Boot time allocation | Comment | |||||
---|---|---|---|---|---|---|---|---|
Instance | Cortex-A35 secure (ROM code) |
Cortex-A35 secure (TF-A BL2) |
Cortex-A35 non-secure (U-Boot) | |||||
Core/Processors | Arm® Cortex®-A35 | Arm® Cortex®-A35 | ✓ | ✓ | ✓ | |||
Core/Processors | Arm® Cortex®-M33 (coprocessor) | Arm® Cortex®-M33 (coprocessor) | ⬚ | ☐ | How to start the coprocessor from the bootloader How_to_protect_the_coprocessor_firmware | |||
Core/Processors | Arm® Cortex®-M0+ (coprocessor) | Arm® Cortex®-M0+ | ⬚ | ☐ | ||||
Analog | VREFBUF | VREFBUF | ☐ | |||||
Analog | ADC | ADC12 | ⬚ | ☐ | ||||
ADC3 | ⬚ | ☐ | ||||||
Analog | MDF | MDF1 | ⬚ | |||||
Low speed interface or audio |
SPI | SPI2S1 | ⬚ | ☐ | ||||
SPI2S2 | ⬚ | ☐ | ||||||
SPI2S3 | ⬚ | ☐ | ||||||
SPI4 | ⬚ | ☐ | ||||||
SPI5 | ⬚ | ☐ | ||||||
SPI6 | ⬚ | ☐ | ||||||
SPI7 | ⬚ | ☐ | ||||||
SPI8 | ⬚ | ☐ | ||||||
Audio | ADF | ADF1 | ⬚ | |||||
Audio | SPDIFRX | SPDIFRX | ⬚ | |||||
Audio | SAI | SAI1 | ⬚ | |||||
SAI2 | ⬚ | |||||||
SAI3 | ⬚ | |||||||
SAI4 | ⬚ | |||||||
Coprocessor | IPCC | IPCC1 | ⬚ | ⬚ | Shareable at internal peripheral level thanks to the RIF: see the boot time allocation per feature | |||
IPCC2 | ⬚ | ⬚ | Shareable at internal peripheral level thanks to the RIF: see the boot time allocation per feature | |||||
Core | STGEN | STGEN | ✓ | ☑ | Read-only (STGENR) |
|||
Core | SYSCFG | SYSCFG | ✓ | ☑ | ☑ | |||
Core | RTC | RTC | ⬚ | ☐ | Shareable at internal peripheral level thanks to the RIF: see the boot time allocation per feature | |||
Core/DMA | HPDMA | HPDMAx (x = 1 to 3) | ☐ | ☐ | ☐ | Shareable at internal peripheral level thanks to the RIF: see the boot time allocation per feature | ||
Core/DMA | LPDMA | LPDMA | ☐ | ☐ | ☐ | Shareable at internal peripheral level thanks to the RIF: see the boot time allocation per feature | ||
Core/Interrupts | EXTI | EXTI1 | ☐ | ☐ | ☐ | Shareable at internal peripheral level thanks to the RIF: see the boot time allocation per feature | ||
EXTI2 | ☐ | ☐ | ☐ | Shareable at internal peripheral level thanks to the RIF: see the boot time allocation per feature | ||||
Core/Interrupts | GIC | GIC | ⬚ | ⬚ | ||||
Core/IOs | GPIO | GPIOA-K | ✓ | ☐ | ☐ | Shareable at internal peripheral level thanks to the RIF: see the boot time allocation per feature | ||
GPIOZ | ☐ | ☐ | Shareable at internal peripheral level thanks to the RIF: see the boot time allocation per feature | |||||
Core/RAM | SYSRAM | SYSRAM | ☑BL31 ☐OP-TEE |
☑ | ☐ | ☐ |
Cortex-A35 secure section required for low power entry and exit | |
Core/RAM | DDRCTRL | DDR | ☑ | ⬚ | ||||
Core/RAM | BKPSRAM | BKPSRAM | ☑ | ⬚ | ||||
Core/Timers | TIM | TIMx (x = 1 to 8, 10 to 17, 20) | ⬚ | ⬚ | ||||
Core/Timers | LPTIM | LPTIMx (x = 1 to 5) | ⬚ | ⬚ | LPTIM are not used at boot time. | |||
Core/Watchdog | IWDG | IWDG1 | ✓ | ☑ | ☐ | |||
IWDG2 | ✓ | ☐ | ☐ | |||||
IWDG3 | ||||||||
IWDG4 | ||||||||
IWDG5 | ||||||||
High speed interface | USB3DR | USB3DR | ☐ | ☐ | ☐ | The USB3DR can be used by ROM code, FSBL and SSBL in DFU mode to support serial boot. It can be used also in U-boot with command line tools. | ||
High speed interface | USBH | USBH | ⬚ | ☐ | ||||
High speed interface | COMBOPHY | COMBOPHY | ☐ | |||||
High speed interface | UCPD | UCPD1 | ⬚ | ⬚ | ||||
High speed interface | PCIe | PCIe | ☐ | The PCIe and the USB3DR running at USB3 speed are mutually exclusive. Both require using the ComboPHY. | ||||
Low speed interface | USART | UART4 | ☐ | ☐ | ☐ | |||
UART5 | ☐ | ☐ | ☐ | |||||
UART7 | ☐ | ☐ | ☐ | |||||
UART8 | ☐ | ☐ | ☐ | |||||
UART9 | ☐ | ☐ | ☐ | |||||
USART1 | ☐ | ☐ | ☐ | |||||
USART2 | ☐ | ☐ | ☐ | |||||
USART3 | ☐ | ☐ | ☐ | |||||
USART6 | ☐ | ☐ | ☐ | |||||
Low speed interface | I2C | Any instance | ☐ | ☐ | ||||
Low speed interface | I3C | I3C1 | ⬚ | ☐ | ||||
I3C2 | ⬚ | ☐ | ||||||
I3C3 | ⬚ | ☐ | ||||||
I3C4 | ⬚ | ☐ | ||||||
Mass storage | OCTOSPI | OCTOSPI1 | ☐ | ☐ | ☐ | |||
OCTOSPI2 | ☐ | ☐ | ||||||
Mass storage | OCTOSPIM | OCTOSPIM | ☐ | ⬚ | ☐ | TF-A BL2 relies on OCTOSPIM configuration applied by ROM code | ||
Mass storage | FMC | FMC | ☐ | ☐ | ☐ | Shareable at internal peripheral level thanks to the RIF: see the boot time allocation per feature | ||
Mass storage | SDMMC | SDMMC1 | ☐ | ☐ | ☐ | |||
SDMMC2 | ☐ | ☐ | ☐ | |||||
SDMMC3 | ☐ | |||||||
Networking | FDCAN | FDCAN1 | ⬚ | |||||
FDCAN2 | ⬚ | |||||||
FDCAN3 | ⬚ | |||||||
Networking | ETHSW | ETHSW | ⬚ | |||||
Networking | ETH | ETH1 | ☐ | |||||
ETH2 | ☐ | |||||||
Power & Thermal | RCC | RCC | ✓ | ✓ | ☐ | Shareable at internal peripheral level thanks to the RIF: see the boot time allocation per feature | ||
Power & Thermal | PWR | PWR | ☐ | ☐ | ☐ | Shareable at internal peripheral level thanks to the RIF: see the boot time allocation per feature | ||
Power & Thermal | DTS | DTS | ⬚ | |||||
Security | BSEC | BSEC | ✓ | ✓ | ||||
Security | RNG | RNG | ✓ | ☑ | ☐ | |||
Security | HASH | HASH | ✓ | ☑ | ☐ | |||
Security | CRYP | CRYP1 | ☑ | ☑ | ⬚ | ROM code allocation is managed with the bit 8 in OTP 16 | ||
CRYP2 | ⬚ | |||||||
Security | SAES | SAES | ☐ | ☑ | ⬚ | ROM code allocation is managed with the bit 8 in OTP 16 | ||
Security | TAMP | TAMP | ☐ | ☐ | ☐ | Shareable at internal peripheral level thanks to the RIF: see the boot time allocation per feature | ||
Security | OTFDEC | OTFDEC1 | ⬚ | ⬚ | ||||
OTFDEC2 | ⬚ | ⬚ | ||||||
Security | PKA | PKA | ✓ | ☑ | ⬚ | Assignment is mandatory only for secure boot | ||
Trace & Debug | DBGMCU | DBGMCU | ⬚ | ⬚ | ⬚ | |||
Trace & Debug | HDP | HDP | ⬚ | ⬚ | ||||
Trace & debug | SERC | SERC | ⬚ | |||||
Security | IAC | IAC | ⬚ | Fixed to TDCID | ||||
Trace & Debug | DDRPERFM | DDRPERFM | ⬚ | ⬚ | ||||
Visual | GPU | GPU | ⬚ | |||||
Visual | DSI | DSI | ☐ | ☐ | ☐ | Shareable at internal peripheral level thanks to the RIF: see the boot time allocation per feature | ||
Visual | LTDC | LTDC | ☐ | ☐ | ☐ | Shareable at internal peripheral level thanks to the RIF: see the boot time allocation per feature | ||
Visual | DCMI | DCMI | ⬚ | |||||
Visual | CSI | CSI | ⬚ | |||||
Visual | LVDS | LVDS | ☑ | |||||
Visual | DCMIPP | DCMIPP | ⬚ | |||||
Visual | VENC | VENC | ⬚ | |||||
Visual | VDEC | VDEC | ⬚ |
4. References[edit source]