How to build LVGL applications using STM32CubeIDE

Applicable for STM32MP13x lines, STM32MP15x lines

This article gives information about how to easily develop a LVGL application on STM32MP1 using STM32CubeIDE.

1. Architecture overview[edit source]

The following diagram summarizes all the configurations of the LVGL library. In this article we will detail each of the possibilities and we will see how to generate the SDK.

1.1. Component presentation[edit source]

1.1.1. LVGL[edit source]

LVGL (Light and Versatile Graphics Library) is an open-source embedded GUI library that is written in C (with C++ compatibility) and is released under the MIT license. It’s optimized for deployment on micro-controllers and bare metal (no OS) devices, but on this article, we will see how to develop LVGL applications for our STM32MP1 microprocessor that runs the OpenSTLinux linux distribution.

1.1.2. SDL2[edit source]


  • SDL or Simple Direct Media Layer is a cross-platform development library designed to provide low level access to audio, keyboard, mouse, joystick, and graphics hardware. It allows to show windows, show images, play sounds, manage keyboards...
  • SDL is written in C, works natively with C++, and there are bindings available for several other languages, including C# and Python.
  • SDL 2.0 is distributed under the zlib license. This license allows you to use SDL freely in any software.

1.1.3. Wayland / Weston[edit source]

  • Wayland is a protocol that allows a composer to communicate with multiple windows. It works only with systems using KMS (Kernel-based mode-setting), a kernel feature dependent on the graphics card driver used, hence the need to use a composer.
  • A composer implementing the Wayland protocol (Mutter, Kwin, Enlightenment, Weston...) is necessary (otherwise Wayland alone does nothing, and it is always an X server that would be used).
  • The composer is a window manager who uses a buffer in memory to manage each window and apply visual effects to it.
  • Weston is the reference implementation of a graphical composer window manager for the Wayland display protocol, its existence is justified by the need to develop Wayland without depending on the ups and downs of the development of libraries and environments, by the need to be able to rigorously test Wayland without experiencing bugs independent of Wayland.



1.1.4. DRM / KMS[edit source]

For more information about drm /kms, you can see the following article: DRM/KMS

1.2. Different configurations[edit source]

1.2.1. Weston Wayland SDL2 configuration with GPU[edit source]

1.2.2. DRM-KMS / SDL2 configuration with GPU[edit source]

1.2.3. DRM-KMS / SDL2 configuration without GPU[edit source]

1.2.4. Direct DRM-KMS configuration without GPU[edit source]

2. How to generate SDK and the flash image for the configuration[edit source]

2.1. Purpose to generate SDK and the flash image[edit source]

  • SDK or Software development kit is a programming package that enables a programmer to develop applications for a specific platform .
  • In our case, this SDK will allow us to use the SDL2 library, without the need to download it, and include it in our LVGL project.
Info white.png Information
Usage of GPU depends on SDL2 configuration in SDK and on SDL2 library hosted on board.
Info white.png Information
Since STM32 MPU ecosystem release v4.1.0 , SDL2 library are integrated on SDK and Starter Package

2.2. Generate SDK for SDL2 with GPU configuration[edit source]

  • Before generating the SDK, we will start by creating a recipe append file for the SDL2 library in our distribution package.
 mkdir /local/STM32MP15-Ecosystem-v4.0.0/Distribution-Package/openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/layers/meta-st/meta-st-openstlinux/recipes-graphics/libsdl2
 cd /local/STM32MP15-Ecosystem-v4.0.0/Distribution-Package/openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/layers/meta-st/meta-st-openstlinux/recipes-graphics/libsdl2
 touch libsdl2_%.bbappend
  • To configure SDL2 for stm32mp1 platform and Vivante GPU, copy or modify the following script into the recipe.
FILESEXTRAPATHS:prepend := "${THISDIR}/files:"

SRC_URI += "file://0001-Correction-of-bad-dlopen-for-libEGL.patch"

PACKAGECONFIG_GL = ""
PACKAGECONFIG ??= " \
    ${PACKAGECONFIG_GL} \
    ${@bb.utils.filter('DISTRO_FEATURES', 'alsa pulseaudio', d)} \
    ${@bb.utils.contains('DISTRO_FEATURES', 'wayland', 'wayland gles2', '', d)} \
    ${@bb.utils.contains("TUNE_FEATURES", "neon","arm-neon","",d)} \
    kmsdrm \
"
 
EXTRA_OECONF += " \
    -DSDL_VIVANTE=OFF \
    -DSDL_VULKAN=OFF \
    -DSDL_OPENGL=OFF \
"
  • To solve some problems of reading the symbols for the lib libegl , we need to create a patch called by the recipe .
  • On the same directory (workspace) , we create a subdirectory with the name of files and in it we create our patch with the name of 0001-Correction-of-bad-dlopen-for-libEGL.patch
  • Copy the following script into our patch.
--- a/src/loadso/dlopen/SDL_sysloadso.c
+++ b/src/loadso/dlopen/SDL_sysloadso.c
@@ -46,8 +46,13 @@ SDL_LoadObject(const char *sofile)
         return NULL;
     }
#endif
+    // SDL will skip dlopen'ing libEGL.so after it spots EGL symbols on our
+    // wrapper, so force loading it here.
+    if (strncmp(sofile, "libEGL.so", 9) != 0)
+        handle = dlopen(sofile, RTLD_NOW|RTLD_LOCAL | RTLD_GLOBAL | RTLD_LAZY);
+    else
+        handle = dlopen(sofile, RTLD_NOW|RTLD_LOCAL);

-    handle = dlopen(sofile, RTLD_NOW|RTLD_LOCAL);
     loaderror = dlerror();
     if (handle == NULL) {
         SDL_SetError("Failed loading %s: %s", sofile, loaderror);
  • Add libsdl2 to our image (if it's not alreay made) for sdk in CORE_IMAGE_EXTRA_INSTALL variable:
  cd /local/STM32MP15-Ecosystem-v4.0.0/Distribution-Package/openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/layers/meta-st/meta-st-openstlinux/packagegroups/

  • Modify the script of 'packagegroup-framework-core-base.bb as follows :
...
SUMMARY:packagegroup-framework-core-base-display = "Framework core base components for display" 
RDEPENDS:packagegroup-framework-core-base-display = "\
   libdrm          \
   libdrm-tests    \
   \
   ${@bb.utils.contains('DISTRO_FEATURES', 'opengl', 'libsdl2', , d)} \
   "
...


  • To create SDK :
 cd /local/STM32MP15-Ecosystem-v4.0.0/Distribution-Package/openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15
 DISTRO=openstlinux-weston MACHINE=stm32mp1 source layers/meta-st/scripts/envsetup.sh
 bitbake -c populate_sdk st-image-weston
  • Bitbake generates the sdk in the following directory:
  cd /local/STM32MP15-Ecosystem-v4.0.0/Distribution-Package/openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/build-openstlinuxweston-stm32mp1/tmp-glibc/deploy/sdk
  • To give the right of execution :
 chmod +x st-image-weston-openstlinux-weston-stm32mp1-x86_64-toolchain-yocto-kirkstone-mp1-v22.06.15-snapshot.sh
  • Run the SDK and copy it back to the developer package.
 ./st-image-weston-openstlinux-weston-stm32mp1-x86_64-toolchain-yocto-kirkstone-mp1-v22.06.15-snapshot.sh -d /local/STM32MP15-Ecosystem-v4.0.0/Developer-Package/SDK_SDL2_WITH_GPU

2.3. Generate SDK for SDL2 without GPU configuration[edit source]

To generate the SDK for sdl2 without using GPU , you can follow the same steps as with GPU , just add a line in the recipe that disables the GPU :

PACKAGECONFIG:remove = "gles2"

2.4. Flash image associated to your SDK on the board[edit source]

  • To create flash image associated to your SDK
 cd /local/STM32MP15-Ecosystem-v4.0.0/Distribution-Package/openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15
 DISTRO=openstlinux-weston MACHINE=stm32mp1 source layers/meta-st/scripts/envsetup.sh
 bitbake -st-image-weston
  • Bitbake generates the image in the following directory:
  cd /local/STM32MP15-Ecosystem-v4.0.0/Distribution-Package/openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/build-openstlinuxweston-stm32mp1/tmp-glibc/deploy/image

You need to flash this new image on your board

3. How to build LVGL project with STM32CubeIDE[edit source]

3.1. Get LVGL project[edit source]

  • Create a new folder.
  • Open a terminal in this folder.
  • Download the LVGL project with the following command:
 git clone --recursive https://github.com/lvgl/lv_port_pc_eclipse.git
 git checkout -b WORKING origin/release/v8.1
 git submodule init
 git submodule update

If you are using Windows, you can go to LVGL's GitHub and download the folder and unzip it.

  • Import your project :

Click on file ==> Import ==> Projects from folder or archive ==> Next==> Directory ==> upload your LVGL project.

Chemin.png
  • Change the toolchain .

By default, stm32CubeIDE uses a Tool Chain for a x86_64 architecture, in our case we want to compile for our microprocessor with an ARM architecture. For this we need to change it:

Right-Click on you project ==> Properties ==> C/C++ Build ==> Tool Chain Editor ==> select OpenSTLinux SDK ==> Apply and Close

Toolchain.png

3.2. Configure CubeIDE with SDK[edit source]

  • To be able to use the SDK that we have generated , stm32CubeIDE needs the absolute path to access it :

Right-click on you project ==> Properties ==> C/C++ Build ==>Environment ==> Double click on SDKPATH ==> Paste the the absolute path ==> click on "OK" ==> click on "Apply an close "

SDK.png

3.2.1. For usage of direct DRM/KMS configuration[edit source]

  • Add include path (for libdrm) :

Right-click on you project ==> Properties ==> C/C++ Build ==>Settings ==> MPU GCC Compiler ==> Include paths == > add the followings path :

"${SDKPATH}/sysroots/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/usr/include/libdrm/"
Path.png
  • Add drm library for linker :

Right-click on you project ==> Properties ==> C/C++ Build ==>Settings ==> MPU GCC Linker ==> Libraries== > add a new library that we call drm

Drmm.png
  • Remove SDL2 and SDL2 Main libraries for linker

Right-click on you project ==> Properties ==> C/C++ Build ==>Settings ==> MPU GCC Linker ==> Libraries== >Remove SDL2main and SDL2

3.2.2. For usage of SDL2 configuration[edit source]

  • Remove SDL2 Main libraries for linker

Right-click on you project ==> Properties ==> C/C++ Build ==>Settings ==> MPU GCC Linker ==> Libraries== >Remove SDL2main

Drmm.png

3.3. Proposed modifications on LVGL project (common for all configuration)[edit source]

To adapt LVGL to our stmp32mp1 board some modification are needed.
The following modification are common for all the configuration described on this pages (SDL2 configuration or direct DRM/KMS configuration)

3.3.1. Adaptation of example source code (aka main.c)[edit source]

  • Replace the content of the main file of your project , by the following script :
/**
 * @file main.c
 *
 */
/*********************
 *      INCLUDES
 *********************/
#define _DEFAULT_SOURCE /* needed for usleep() */
#include <stdlib.h>
#include <unistd.h>

// For SDL2 usage
#define SDL_MAIN_HANDLED /*To fix SDL's "undefined reference to WinMain" issue*/
#include <SDL2/SDL.h>
#include "lvgl/lvgl.h"
#include "lvgl/examples/lv_examples.h"
#include "lv_demos/lv_demo.h"
#include "lv_drivers/sdl/sdl.h"

// For USE DRM usage
#include "lv_drivers/display/drm.h"
#include "lv_drivers/indev/evdev.h"

/**********************
 *  STATIC PROTOTYPES
 **********************/
static void hal_init(void);
static int tick_thread(void *data);


/*********************
 *      DEFINES
 *********************/
/* select which demo you would like to execute */
#define COMPILE_WIDGET 1
//#define COMPILE_MUSIC 1
//#define COMPILE_KEYPAD 1


/**********************
 *   GLOBAL FUNCTIONS
 **********************/
int main(int argc, char **argv)
{
    (void)argc; /*Unused*/
    (void)argv; /*Unused*/

    /*Initialize LVGL*/
    lv_init();

    /*Initialize the HAL (display, input devices, tick) for LVGL*/
    hal_init();

#ifdef COMPILE_WIDGET
    lv_demo_widgets();
#endif
#ifdef COMPILE_MUSIC
    lv_demo_music();
#endif
#ifdef COMPILE_KEYPAD
    lv_demo_keypad_encoder();
 #endif

    while(1) {
        /* Periodically call the lv_task handler.
         * It could be done in a timer interrupt or an OS task too.*/
        lv_timer_handler();
        usleep(5 * 1000);
    }

    return 0;
}

/**********************
 *   STATIC FUNCTIONS
 **********************/
/**
 * Initialize the Hardware Abstraction Layer (HAL) for the LVGL graphics
 * library
 */
static void hal_init(void)
{
#if USE_DRM
    drm_init();
#endif
#if USE_SDL
    sdl_init();
#endif

    /* Tick init.
     * You have to call 'lv_tick_inc()' in periodically to inform LittelvGL about
     * how much time were elapsed Create an SDL thread to do this*/
    SDL_CreateThread(tick_thread, "tick", NULL);

    /* Create a display buffer */
    static lv_disp_draw_buf_t disp_buf1;

#if USE_DRM
    static lv_color_t buf1_1[128 * 1024];
    lv_disp_draw_buf_init(&disp_buf1, buf1_1, NULL, 128 * 1024);
#endif
#if USE_SDL
    static lv_color_t buf1_1[SDL_HOR_RES * 100];
    lv_disp_draw_buf_init(&disp_buf1, buf1_1, NULL, SDL_HOR_RES * 100);
#endif

    /*Create a display*/
    static lv_disp_drv_t disp_drv;
    lv_disp_drv_init(&disp_drv); /*Basic initialization*/
    disp_drv.draw_buf = &disp_buf1;
#if USE_DRM
    disp_drv.flush_cb   = drm_flush;
    lv_coord_t drm_width, drm_height;
    /* get size from DRM/KMS backend */
    uint32_t drm_dpi;
    drm_get_sizes(&drm_width, &drm_height, &drm_dpi);
    disp_drv.hor_res    = drm_width;
    disp_drv.ver_res    = drm_height;
#endif
#if USE_SDL
    disp_drv.flush_cb = sdl_display_flush;
    disp_drv.hor_res = SDL_HOR_RES;
    disp_drv.ver_res = SDL_VER_RES;
#endif
    fprintf(stderr, "SCREEN SIZE ----> %d x %d\n", disp_drv.hor_res, disp_drv.ver_res);
    lv_disp_t * disp = lv_disp_drv_register(&disp_drv);

    lv_theme_t * th = lv_theme_default_init(disp,
                                            lv_palette_main(LV_PALETTE_BLUE),
                                            lv_palette_main(LV_PALETTE_RED),
                                            LV_THEME_DEFAULT_DARK, LV_FONT_DEFAULT);
    lv_disp_set_theme(disp, th);

#if USE_EVDEV
    /* warning: EVDEV_NAME on lv_drv_conf.h MUST be adapted to the correct input devince on board */
    evdev_init();
    static lv_indev_drv_t indev_drv;
    lv_indev_drv_init(&indev_drv);
    indev_drv.type = LV_INDEV_TYPE_POINTER;
    indev_drv.read_cb = evdev_read;
    lv_indev_drv_register(&indev_drv);
#endif

#if USE_SDL
    lv_group_t * g = lv_group_create();
    lv_group_set_default(g);

    /* Add the mouse as input device
     * Use the 'mouse' driver which reads the PC's mouse*/
    static lv_indev_drv_t indev_drv_1;
    lv_indev_drv_init(&indev_drv_1); /*Basic initialization*/
    indev_drv_1.type = LV_INDEV_TYPE_POINTER;

    /* This function will be called periodically (by the library) to get the mouse position and state */
    indev_drv_1.read_cb = sdl_mouse_read;
    lv_indev_t *mouse_indev = lv_indev_drv_register(&indev_drv_1);

    static lv_indev_drv_t indev_drv_2;
    lv_indev_drv_init(&indev_drv_2); /*Basic initialization*/
    indev_drv_2.type = LV_INDEV_TYPE_KEYPAD;
    indev_drv_2.read_cb = sdl_keyboard_read;
    lv_indev_t *kb_indev = lv_indev_drv_register(&indev_drv_2);
    lv_indev_set_group(kb_indev, g);

    static lv_indev_drv_t indev_drv_3;
    lv_indev_drv_init(&indev_drv_3); /*Basic initialization*/
    indev_drv_3.type = LV_INDEV_TYPE_ENCODER;
    indev_drv_3.read_cb = sdl_mousewheel_read;
    lv_indev_t * enc_indev = lv_indev_drv_register(&indev_drv_3);
    lv_indev_set_group(enc_indev, g);

    /* Set a cursor for the mouse*/
    LV_IMG_DECLARE(mouse_cursor_icon); /*Declare the image file.*/
    lv_obj_t * cursor_obj = lv_img_create(lv_scr_act()); /*Create an image object for the cursor */
    lv_img_set_src(cursor_obj, &mouse_cursor_icon);           /*Set the image source*/
    lv_indev_set_cursor(mouse_indev, cursor_obj);             /*Connect the image  object to the driver*/
#endif
}

/**
 * A task to measure the elapsed time for LVGL
 * @param data unused
 * @return never return
 */
static int tick_thread(void *data) {
    (void)data;

    while(1) {
        SDL_Delay(5);
        lv_tick_inc(5); /*Tell LittelvGL that 5 milliseconds were elapsed*/
    }
    return 0;
}

3.3.2. Configuration of demo for LVGL (aka lv_demo_conf.h)[edit source]

  • The file lv_demo_conf.h must be aligned with the template present on lv_demos/lv_demo_conf_template.h
 cp lv_demos/lv_demo_conf_template.h lv_demo_conf.h
  • Adapt configuration

Enable demo configuration , demo Benchmark, demo Music (with Lanscape) and demo Keypad

#if 1 /*Set it to "1" to enable the content*/
#define LV_USE_DEMO_WIDGETS        1
#define LV_USE_DEMO_KEYPAD_AND_ENCODER    1
#define LV_USE_DEMO_MUSIC      1
# define LV_DEMO_MUSIC_LANDSCAPE    1

3.3.3. Configuration of LVGL (aka lv_conf)[edit source]

  • The file lv_conf.h must be aligned with the template present on lvgl/lv_conf_template.h
 cp lvgl/lv_conf_template.h lv_conf.h
  • Adapt configuration

Enable lvgl configuration, force color depth to 32, enable font for demo

#if 1 /*Set it to "1" to enable content*/

Force Color Depth

#define LV_COLOR_DEPTH     32

Enable font (could be adapted on function of fonts requested by elements used on demo)

#define LV_FONT_MONTSERRAT_8     1
#define LV_FONT_MONTSERRAT_10    1
#define LV_FONT_MONTSERRAT_12    1
#define LV_FONT_MONTSERRAT_14    1
#define LV_FONT_MONTSERRAT_16    1
#define LV_FONT_MONTSERRAT_18    1
#define LV_FONT_MONTSERRAT_20    1
#define LV_FONT_MONTSERRAT_22    1
#define LV_FONT_MONTSERRAT_24    1
#define LV_FONT_MONTSERRAT_26    1
#define LV_FONT_MONTSERRAT_28    1
#define LV_FONT_MONTSERRAT_30    1
#define LV_FONT_MONTSERRAT_32    1
#define LV_FONT_MONTSERRAT_34    1
#define LV_FONT_MONTSERRAT_36    1
#define LV_FONT_MONTSERRAT_38    1
#define LV_FONT_MONTSERRAT_40    1
#define LV_FONT_MONTSERRAT_42    1
#define LV_FONT_MONTSERRAT_44    1
#define LV_FONT_MONTSERRAT_46    1
#define LV_FONT_MONTSERRAT_48    1
#define LV_FONT_MONTSERRAT_12_SUBPX      1
#define LV_FONT_MONTSERRAT_28_COMPRESSED 1  /*bpp = 3*/
#define LV_FONT_DEJAVU_16_PERSIAN_HEBREW 1  /*Hebrew, Arabic, Perisan letters and all their forms*/
#define LV_FONT_SIMSUN_16_CJK            1  /*1000 most common CJK radicals*/
#define LV_FONT_UNSCII_8        1
#define LV_FONT_UNSCII_16       1
#define LV_FONT_FMT_TXT_LARGE   1
#define LV_USE_FONT_COMPRESSED  1
#define LV_USE_FONT_SUBPX       1
#define LV_USE_BIDI         1

If you like to see performance monitor, you can activate:

#define LV_USE_MEM_MONITOR 1

3.4. Proposed modifications on LVGL project for configuration 1 to 3 (SDL2 configuration)[edit source]

To adapt LVGL to our stmp32mp1 board some modification are needed.
The following modification are valid only for SDL2 configuration.

3.4.1. Configuration of driver for LVGL (aka lv_drv_conf.h)[edit source]

  • The file lv_conf.h must be aligned with the template present on lv_drivers/lv_drv_conf_template.h
 cp lv_drivers/lv_drv_conf_template.h lv_drv_conf.h
  • Adapt configuration

Enable driver configuration, SDL configuration and display size configuration:

#if 1 /*Set it to "1" to enable the content*/
# define USE_SDL 1
#  define SDL_HOR_RES     800
#  define SDL_VER_RES     480
Info white.png Information
The size of screen must be adapted to the size of screen present on board:
stm32mp157f-dk2: 800x400
stm32mp157f-ev1: 1280x720
stm32mp135f-dk: 480x272

3.5. Proposed modifications on LVGL project for configuration 4 (direct DRM/KMS)[edit source]

To adapt LVGL to our stmp32mp1 board some modification are needed.
The following modification are valid only for direct DRM/KMS configuration.

3.5.1. Configuration of driver for LVGL (aka lv_drv_conf.h)[edit source]

  • The file lv_conf.h must be aligned with the template present on lv_drivers/lv_drv_conf_template.h
 cp lv_drivers/lv_drv_conf_template.h lv_drv_conf.h
  • Adapt configuration

Enable driver configuration, drm configuration and EVDEV configuration:

#if 1 /*Set it to "1" to enable the content*/
#  define USE_DRM           1
#  define USE_EVDEV       1    
Info white.png Information
For EVDEV configuration, EVDEV_NAME MUST be adapted to the input device available on board
#  define EVDEV_NAME   "/dev/input/event0" /* touch screen on stm32mp157f-dk2 */
#  define EVDEV_NAME   "/dev/input/event1" /* touch screen on stm32mp135f-dk */ 

3.5.2. Adaptation of Makefile (aka Makefile)[edit source]

On Makefile, the CFLAGS and LDFLAGS MUST adapated to the usage of librdm instead of SDL2 library:

CFLAGS ?= -O3 -I$(LVGL_DIR)/ $(WARNINGS) 
LDFLAGS ?= -lm -ldrm

3.6. Proposed modifications on LVGL project for configuration 4 (DRM/KMS only configuration)[edit source]

To adapt LVGL to our stmp32mp1 board some modification are needed.

  • Remplace the content of the main file of your project , by the following script :

#include <stdio.h>
#include <stdlib.h>

#include "lvgl/lvgl.h"
#include "lv_drivers/display/fbdev.h"
#include "lv_drivers/display/drm.h"
#include "lv_drivers/indev/evdev.h"
#include "lv_demo_conf.h"
#include <unistd.h>
#include <pthread.h>
#include <time.h>
#include <sys/time.h>

#define DISP_BUF_SIZE (128 * 1024)

#define COMPILE_WIDGET 1
//#define COMPILE_MUSIC 1
//#define COMPILE_KEYPAD 1

int main(void)
{
    /*LittlevGL init*/
    lv_init();

#if USE_FBDEV
    /*Linux frame buffer device init*/
    fbdev_init();
#endif
#if USE_DRM
    drm_init();
#endif

    /*A small buffer for LittlevGL to draw the screen's content*/
    static lv_color_t buf[DISP_BUF_SIZE];

    /*Initialize a descriptor for the buffer*/
    static lv_disp_draw_buf_t disp_buf;
    lv_disp_draw_buf_init(&disp_buf, buf, NULL, DISP_BUF_SIZE);

    /*Initialize and register a display driver*/
    static lv_disp_drv_t disp_drv;
    lv_disp_drv_init(&disp_drv);
    disp_drv.draw_buf   = &disp_buf;
#if USE_FBDEV
    disp_drv.flush_cb   = fbdev_flush;
#endif
#if USE_DRM
    disp_drv.flush_cb   = drm_flush;
#endif

    const char *width, *height, *rotate;
    width = getenv("LVGL_DRM_WIDTH");
    height = getenv("LVGL_DRM_HEIGHT");
fprintf(stderr, " ----> %s %s\n", width, height);
    if (width && height) {
        disp_drv.hor_res    = atoi(width);
        disp_drv.ver_res    = atoi(height);
    } else {
        disp_drv.hor_res    = 480;
        disp_drv.ver_res    = 800;
    }
    lv_disp_drv_register(&disp_drv);


    evdev_init();
#if USE_EVDEV
  const char *device_evdev;
  device_evdev = getenv("LVGL_EVDEV");
  if (device_evdev) 
     evdev_init_with_device(device_evdev);
  else
     evdev_init();
  static lv_indev_drv_t indev_drv;
  lv_indev_drv_init(&indev_drv);
  indev_drv.type = LV_INDEV_TYPE_POINTER;
  indev_drv.read_cb = evdev_read;
  lv_indev_t *evdev_indev = lv_indev_drv_register(&indev_drv);
#endif



#ifdef COMPILE_WIDGET
    lv_demo_widgets();
#endif
#ifdef COMPILE_MUSIC
    lv_demo_music();
#endif
#ifdef COMPILE_KEYPAD
    lv_demo_keypad_encoder();
#endif

    /*Handle LitlevGL tasks (tickless mode)*/
    while(1) {
        lv_task_handler();
        usleep(5000);
    }

    return 0;
}



/*Set in lv_conf.h as `LV_TICK_CUSTOM_SYS_TIME_EXPR`*/
uint32_t custom_tick_get(void)
{
    static uint64_t start_ms = 0;
    if(start_ms == 0) {
        struct timeval tv_start;
        gettimeofday(&tv_start, NULL);
        start_ms = (tv_start.tv_sec * 1000000 + tv_start.tv_usec) / 1000;
    }

    struct timeval tv_now;
    gettimeofday(&tv_now, NULL);
    uint64_t now_ms;
    now_ms = (tv_now.tv_sec * 1000000 + tv_now.tv_usec) / 1000;

    uint32_t time_ms = now_ms - start_ms;
    return time_ms;
}
  • Remplace the content of the Makefile of your project , by the following script :
#
# Makefile
#
CC ?= gcc
LVGL_DIR_NAME ?= lvgl
LVGL_DIR ?= ${shell pwd}
CFLAGS += -O3 -g0 -I$(LVGL_DIR)/ -Wall -Wshadow -Wundef -Wmissing-prototypes -Wno-discarded-qualifiers -Wall -Wextra -Wno-unused-function -Wno-error=strict-prototypes -Wpointer-arith -fno-strict-aliasing -Wno-error=cpp -Wuninitialized -Wmaybe-uninitialized -Wno-unused-parameter -Wno-missing-field-initializers -Wtype-limits -Wsizeof-pointer-memaccess -Wno-format-nonliteral -Wno-cast-qual -Wunreachable-code -Wno-switch-default -Wreturn-type -Wmultichar -Wformat-security -Wno-ignored-qualifiers -Wno-error=pedantic -Wno-sign-compare -Wno-error=missing-prototypes -Wdouble-promotion -Wclobbered -Wdeprecated -Wempty-body -Wtype-limits -Wshift-negative-value -Wstack-usage=2048 -Wno-unused-value -Wno-unused-parameter -Wno-missing-field-initializers -Wuninitialized -Wmaybe-uninitialized -Wall -Wextra -Wno-unused-parameter -Wno-missing-field-initializers -Wtype-limits -Wsizeof-pointer-memaccess -Wno-format-nonliteral -Wpointer-arith -Wno-cast-qual -Wmissing-prototypes -Wunreachable-code -Wno-switch-default -Wreturn-type -Wmultichar -Wno-discarded-qualifiers -Wformat-security -Wno-ignored-qualifiers -Wno-sign-compare
LDFLAGS += -lm -ldrm
BIN = demo


#Collect the files to compile
MAINSRC = ./main.c

include $(LVGL_DIR)/lvgl/lvgl.mk
include $(LVGL_DIR)/lv_drivers/lv_drivers.mk
include $(LVGL_DIR)/lv_demos/lv_demo.mk

OBJEXT ?= .o

AOBJS = $(ASRCS:.S=$(OBJEXT))
COBJS = $(CSRCS:.c=$(OBJEXT))

MAINOBJ = $(MAINSRC:.c=$(OBJEXT))

SRCS = $(ASRCS) $(CSRCS) $(MAINSRC)
OBJS = $(AOBJS) $(COBJS)

## MAINOBJ -> OBJFILES

all: default

%.o: %.c
	@echo "$(CC) $(CFLAGS) -c $< -o $@"
	@$(CC)  $(CFLAGS) -c $< -o $@
    
default: $(AOBJS) $(COBJS) $(MAINOBJ)
	$(CC) -o $(BIN) $(MAINOBJ) $(AOBJS) $(COBJS) $(LDFLAGS)

clean: 
	rm -f $(BIN) $(AOBJS) $(COBJS) $(MAINOBJ)

  • Create a file in the project with the name of lv_demo_conf.h and copy the following script into it :
/**
 * @file lv_demo_conf.h
 * Configuration file for v8.1.0-dev
 *
 */
/*
 * COPY THIS FILE AS lv_demo_conf.h
 */

#if 1 /*Set it to "1" to enable the content*/

#ifndef LV_EX_CONF_H
#define LV_EX_CONF_H


/*******************
 * GENERAL SETTING
 *******************/
#define LV_EX_PRINTF       0       /*Enable printf-ing data in demoes and examples*/
#define LV_EX_KEYBOARD     0       /*Add PC keyboard support to some examples (`lv_drivers` repository is required)*/
#define LV_EX_MOUSEWHEEL   0       /*Add 'encoder' (mouse wheel) support to some examples (`lv_drivers` repository is required)*/

/*********************
 * DEMO USAGE
 *********************/

/*Show some widget*/
#define LV_USE_DEMO_WIDGETS        1
#if LV_USE_DEMO_WIDGETS
#define LV_DEMO_WIDGETS_SLIDESHOW  0
#endif

/*Printer demo, optimized for 800x480*/
#define LV_USE_DEMO_PRINTER     1

/*Demonstrate the usage of encoder and keyboard*/
#define LV_USE_DEMO_KEYPAD_AND_ENCODER     1

/*Benchmark your system*/
#define LV_USE_DEMO_BENCHMARK   1

/*Stress test for LVGL*/
#define LV_USE_DEMO_STRESS      1

/*Music player demo*/
#define LV_USE_DEMO_MUSIC      1
#if LV_USE_DEMO_MUSIC
# define LV_DEMO_MUSIC_LANDSCAPE    0
# define LV_DEMO_MUSIC_LARGE        0
#define LV_DEMO_MUSIC_AUTO_PLAY     0
#endif

#endif /*LV_EX_CONF_H*/

#endif /*End of "Content enable"*/

we create a new patch that we rename 0001-extend-evdev.patch and we copy the following script :

From a9b0e2008e35e23910238bd1bac562c36499f765 Mon Sep 17 00:00:00 2001
From: Christophe Priouzeau <christophe.priouzeau@foss.st.com>
Date: Mon, 23 Aug 2021 09:42:17 +0200
Subject: [PATCH] extend evdev

---
 indev/evdev.c | 15 +++++++++++++++
 indev/evdev.h |  2 ++
 2 files changed, 17 insertions(+)

diff --git a/lv_drivers/indev/evdev.c b/lv_drivers/indev/evdev.c
index e85b7f4..b6f4f13 100644
--- a/lv_drivers/indev/evdev.c
+++ b/lv_drivers/indev/evdev.c
@@ -75,6 +75,21 @@ void evdev_init(void)
     evdev_key_val = 0;
     evdev_button = LV_INDEV_STATE_REL;
 }
+void evdev_init_with_device(char *device)
+{
+    evdev_fd = open(device, O_RDWR | O_NOCTTY | O_NDELAY);
+    if(evdev_fd == -1) {
+        perror("unable open evdev interface:");
+        return;
+    }
+
+    fcntl(evdev_fd, F_SETFL, O_ASYNC | O_NONBLOCK);
+    evdev_root_x = 0;
+    evdev_root_y = 0;
+    evdev_key_val = 0;
+    evdev_button = LV_INDEV_STATE_REL;
+}
+
 /**
  * reconfigure the device file for evdev
  * @param dev_name set the evdev device filename
diff --git a/lv_drivers/indev/evdev.h b/lv_drivers/indev/evdev.h
index dcb9114..bc82cb4 100644
--- a/lv_drivers/indev/evdev.h
+++ b/lv_drivers/indev/evdev.h
@@ -45,6 +45,8 @@ extern "C" {
  * Initialize the evdev
  */
 void evdev_init(void);
+void evdev_init_with_device(char *device);
+
 /**
  * reconfigure the device file for evdev
  * @param dev_name set the evdev device filename
-- 
2.25.1
  • Apply patch 0001-extend-evdev.patch in lvgl root directory
 patch -p1 < 0001-extend-evdev.patch
  • In lvgl root directory (in file lv_conf.h ), we apply the following changes:

Replace this part of the code :

 /*Use a custom tick source that tells the elapsed time in milliseconds.
  *It removes the need to manually update the tick with `lv_tick_inc()`)*/
#define LV_TICK_CUSTOM 0
#if LV_TICK_CUSTOM
#define LV_TICK_CUSTOM_INCLUDE "Arduino.h"         /*Header for the system time function*/ #define LV_TICK_CUSTOM_SYS_TIME_EXPR (millis())    /*Expression evaluating to current system time in ms*/
*Expression evaluating to current system time in ms*/
 #endif   /*LV_TICK_CUSTOM*/

with :

  /*Use a custom tick source that tells the elapsed time in milliseconds.
  *It removes the need to manually update the tick with `lv_tick_inc()`)*/
uint32_t custom_tick_get(void);

#define LV_TICK_CUSTOM     1
 #if LV_TICK_CUSTOM
#define LV_TICK_CUSTOM_INCLUDE  <stdint.h>         /*Header for the system time function*/
#define LV_TICK_CUSTOM_SYS_TIME_EXPR (custom_tick_get())     /*Expression evaluating to current system time in ms*/
 #endif   /*LV_TICK_CUSTOM*/


Change maximum buffer size to allocate for rotation by replacing the following line :

#define LV_DISP_ROT_MAX_BUF (32*1024)

with :

#define LV_DISP_ROT_MAX_BUF (10*1024)
  • In lvgl root directory (in lv_drv_conf.h ), we apply the following changes:

Change the resolution by modifying the following parameters :

#if USE_MONITOR
#  define MONITOR_HOR_RES     480
#  define MONITOR_VER_RES     320

with :

#if USE_MONITOR
#  define MONITOR_HOR_RES     800
#  define MONITOR_VER_RES     480

we choose to use DRM/KMS by changing :

#  define USE_DRM           0

with :

#  define USE_DRM           1

we choose to use EVDEV by replacing :

#  define USE_EVDEV           0

with :

#  define USE_EVDEV          1

Replacing the following part of code :

#if USE_EVDEV || USE_BSD_EVDEV
#  define EVDEV_NAME   "/dev/input/event0"        /*You can use the "evtest" Linux tool to get the list of devices and test them*/

with :

#if USE_EVDEV || USE_BSD_EVDEV
#  define EVDEV_NAME   "/dev/input/event1"        /*You can use the "evtest" Linux tool to get the list of devices and test them*/

4. Run the demo[edit source]

  • You need to build binary for your configuration
  • Build the project

Right-Click on you project ==> Build project

  • If everything works well, in your project (folder "Debug") you find the binary file.
  • Setup terminal on the board.
 minicom  -D /dev/ttyACM0
  • To get the IP address of your target, type the following commands:
 ifconfig 
...
eth1      Link encap:Ethernet  HWaddr 10:E7:7A:E3:47:C8  
         inet addr:10.48.1.145  Bcast:10.48.3.255  Mask:255.255.252.0
         inet6 addr: fe80::12e7:7aff:fee3:47c8/64 Scope:Link
inet is the ip address of your target

or

  ip addr
 ...
3: eth1: <BROADCAST,MULTICAST,UP,LOWER_UP> mtu 1500 qdisc mq state UP group default qlen 1000
   link/ether 10:e7:7a:e3:47:c8 brd ff:ff:ff:ff:ff:ff
   inet 10.48.1.145/22 metric 10 brd 10.48.3.255 scope global dynamic eth1


  • You can copy binary to the board by using the following command:
 scp <name_of_your_binary> root@<IP_address>:/usr/local/

To force binary writting on the sdcard

 sync

4.1. Run your binary with SDL2 configuration (configuration 1, 2, 3)[edit source]

For using SDL, you need to precise to SDL2 library which backend you would like to use: here wayland or kmsdrm

  • In configuration 1: Weston Wayland SDL2 configuration with GPU
The environment variable for SDK2 videodriver must be set to wayland

The binary need to be executed with weston permision:

  su -l weston -c "SDL_VIDEODRIVER=wayland /usr/local/<name_of_your_binary >"

To kill the binary execution:

 CTRL + c
  • In configuration 2,3: DRM-KMS / SDL2 configuration with GPU or without GPU

For this configuration, you MUST stop Weston service before to run your binary

 systemctl stop weston-launch
 export SDL_VIDEODRIVER=kmsdrm 

To run the binary :

 /usr/local/<name_of_your_binary >

To kill the current project:

 CTRL + c
  • As a summary, to run the different configurations

Log as weston user in OpenSTLinux4.0.

In configuration 1: Weston Wayland SDL2 configuration with GPU

 su -l weston 
 export SDL_VIDEODRIVER=wayland
 <path to binary>/<name_of_your_binary >

In configuration 2: DRM-KMS / SDL2 configuration with GPU

 systemctl stop weston-launch
 export SDL_VIDEODRIVER=kmsdrm 
 <path to binary>/<name_of_your_binary>

In configuration 3: DRM-KMS / SDL2 configuration without GPU

 systemctl stop weston-launch 
 export SDL_VIDEODRIVER=kmsdrm 
 <path to binary>/<name_of_your_binary>

In configuration 4: direct DRM/KMS

 <path to binary>/<name_of_your_binary >

4.2. Display performances[edit source]

To measure performances, you will need two terminals, the first to launch the application and the second to display the performances in real time.

  • After copying the binary, we launch the first terminal on the board with the following commands :
  minicom  -D /dev/ttyACM0
   ./<name_of_your_binary>
  • we launch the second terminal with SSH .
  ssh root@<IP_address>

on the same terminal paste and run the following script :


 (while true; do \
 
gpu_last_gc=$(cat /sys/kernel/debug/gc/idle); \
 
m=$(mpstat 4 1 | grep "Average:     all" | awk -F" " '{print "cpu load " $3 "%"}'); \
 
echo "-------------------------"; \
 
export fps=`cat /sys/kernel/debug/dri/0/state | grep fps -m1 | grep -o '[0-9]\+'`; echo display  ${fps}fps; \
 
gpu_on=$(echo $gpu_last_gc | tr -d '\n' | tr -d ',' | awk -F" " '{printf("%f\n", $2)}'); \
 
gpu_start=$(echo $gpu_last_gc | tr -d '\n' | tr -d ',' | awk -F" " '{printf("%f\n", ($2+$5+$8+$11))}'); \
 
tr -d '\n' < /sys/kernel/debug/gc/idle | tr -d ',' | awk -v on=$gpu_on -v start=$gpu_start -F" " '{printf ("gpu load %.0f%%\n", ($2 - on) * 100/($2+$4+$6+$8 - start));}'; \
 
echo $m; \
 
done) &

to stop the script: Click on

                      > 'f' +'g'+ ENTER  
                      > CTRL+C

5. References[edit source]

"LVGL official web site"[1] "LVGL Get Started"[2] "LVGL demos"[3] "LVGL demos github" [4] "LVGL project examples"[5] "Learn LVGL"[6] "LVGL forum"[7] "SDL official web site"[8] "Wayland official web site"[9]