1. Article purpose[edit source]
The purpose of this article is to
- briefly introduce the SDMMC peripheral and its main features
- indicate the level of security supported by this hardware block
- explain how each instance can be allocated to the runtime contexts and linked to the corresponding software components
- explain, when necessary, how to configure the SDMMC peripheral.
2. Peripheral overview[edit source]
The SDMMC peripheral is used to interconnect STM32 MPU to SD memory cards, SDIO and MMC devices.
2.1. Features[edit source]
Refer to the STM32MP13 reference manuals or STM32MP15 reference manuals for the complete list of features, and to the software components, introduced below, to see which features are implemented.
2.2. Security support[edit source]
2.2.1. On STM32MP13x lines [edit source]
The SDMMC1/2 instances are secure peripherals (under ETZPC control).
2.2.2. On STM32MP15x lines [edit source]
The SDMMC1/2/3 instances are non-secure peripherals.
3. Peripheral usage and associated software[edit source]
3.1. Boot time[edit source]
SDMMC1/2 instances can be used to support memory boot on SD or MMC Flash devices.
The SDMMC3 (only present on STM32MP15x lines ) is not used at boot time.
3.2. Runtime[edit source]
3.2.1. Overview[edit source]
On STM32MP13x lines only, the SDMMC1/2 instances can be allocated to the Arm® Cortex®-A7 secure context but this is not supported in OpenSTLinux.
All the SDMMC instances can be allocated to the Arm® Cortex®-A7 non-secure core to be controlled in Linux® by the MMC framework.
On STM32MP15x lines only, SDMMC3 can be allocated to the Arm® Cortex®-M4 to be controlled in STM32Cube MPU Package by STM32Cube SDMMC driver.
Chapter #Peripheral assignment describes which peripheral instance can be assigned to which context.
3.2.2. Software frameworks[edit source]
3.2.2.1. On STM32MP13x lines [edit source]
Domain | Peripheral | Software components | Comment | |
---|---|---|---|---|
OP-TEE | Linux | |||
Mass storage | SDMMC | Linux MMC framework |
3.2.2.2. On STM32MP15x lines [edit source]
Internal peripherals software table template
| Mass storage | SDMMC | | Linux MMC framework | STM32Cube SDMMC driver | |- |}
3.2.3. Peripheral configuration[edit source]
The configuration is applied by the firmware running in the context to which the peripheral is assigned. The configuration can be done alone via the STM32CubeMX tool for all internal peripherals, and then manually completed (particularly for external peripherals), according to the information given in the corresponding software framework article.
For Linux® kernel configuration, please refer to SDMMC device tree configuration.
3.2.4. Peripheral assignment[edit source]
Internal peripherals assignment table template
| rowspan="3" | Mass storage | rowspan="3" | SDMMC | SDMMC1 | | ☐ | | |- | SDMMC2 | | ☐ | | |- | SDMMC3 | | ☐ | ☐ | Assignment (single choice) |-
|}
4. How to go further[edit source]
5. References[edit source]