This article briefly describes the STM32MP15x lines support in U-Boot.
1. STM32MP15x lines support[edit source]
For detailed information, please read the file in the delivered U-Boot code = doc/board/st/stm32mp1.rst or the stm32mp1 documentation generated by make htlmdocs
[1].
Also available in official U-Boot Git.
Code :
- arch/arm/mach-stm32mp : arch specific code for STM32 Arm® Cortex® MPUs
- board/st/common : STMicroelectronics common code
- board/st/stm32mp1 : generic STMicroelectronics board for STM32MP1 series
- drivers/*/*stm32* : drivers
Configuration Files:
- defconfig file
- config files
- STM32MP15_device_tree in arch/arm/dts : stm32mp15*.dts*
- <Device tree>.dts : same as kernel
- <Device tree>-u-boot.dtsi : addition for u-boot automatically included in build process
2. Selecting targets : choose defconfig and Device Tree[edit source]
The STM32 MPU boot chain is supported by one U-Boot configuration with defconfig = stm32mp15_trusted_defconfig
Several boards are supported with the associated device-tree (same name as kernel):
Board part number | Device tree | Description |
---|---|---|
STM32MP157A-EV1 Evaluation board | stm32mp157a-ev1 | MB1262+MB1263 |
STM32MP157C-EV1 Evaluation board | stm32mp157c-ev1 | |
STM32MP157D-EV1 Evaluation board | stm32mp157d-ev1 | |
STM32MP157F-EV1 Evaluation board | stm32mp157f-ev1 | |
STM32MP157A-DK1 Discovery kit | stm32mp157a-dk1 | MB1272 |
STM32MP157D-DK1 Discovery kit | stm32mp157d-dk1 | |
STM32MP157C-DK2 Discovery kit | stm32mp157c-dk2 | MB1272+MB1407 |
STM32MP157F-DK2 Discovery kit | stm32mp157f-dk2 |
For information the 'Evaluation' daughter-board only (MB1263 without MB1262) is also supported by stm32mp15*-ed1.dts device tree files.
3. Compilation[edit source]
see U-Boot_overview#U-Boot_build
With the defconfig file: stm32mp15_trusted_defconfig
make stm32mp15_trusted_defconfig make DEVICE_TREE=<Device tree> all
The supported variables are:
- DEVICE_TREE: select in arch/arm/dts the device tree that is used
- KBUILD_OUTPUT: change the destination directory for the build
- EXT_DTB: select external device tree
Nota: All the compiled device tree are available in $KBUILD_OUTPUT/arch/arm/dts/*.dtb.
You can select them instead of u-boot.dtb without U-Boot recompilation.
The ouput file is u-boot.stm32 for ecosystem release ≤ v2.1.0 or if you activate CONFIG_STM32MP15x_STM32IMAGE in your defconfig for ecosystem release v3.0.0 (this temporary option is only introduced to facilitate the FIP migration but it will be removed in the next EcosystemRelease).
With FIP support for ecosystem release v3.0.0 , the offset on U-Boot environment in NOR are defined in the defconfig with:
CONFIG_ENV_OFFSET=0x480000 CONFIG_ENV_OFFSET_REDUND=0x4C0000
Without FIP support these MTD partition offsets in NOR for default flashlayout change and to reuse the ecosystem release ≤ v2.1.0 flashlayout the defconfig options become:
CONFIG_STM32MP15x_STM32IMAGE=y CONFIG_ENV_OFFSET=0x280000 CONFIG_ENV_OFFSET_REDUND=0x2C0000
4. U-Boot integration in FIP[edit source]
U-Boot binary and its associated device tree are part of the FIP binary, created or updated with TF-A Makefile or with fiptools
:
- BL33_CFG or --hw-config = u-boot.dtb
- BL33 or --nt-fw = u-boot-nodtb.bin
5. SPL compilation[edit source]
The alternate boot chain with SPL is also supported by "stm32mp15_basic_defconfig" but only for U-Boot_SPL:_DDR_interactive_mode
With the defconfig file: stm32mp15_basic_defconfig
make stm32mp15_basic_defconfig make DEVICE_TREE=<Device tree> all
The resulting U-Boot files are located in your build directory:
- u-boot-spl.stm32 : FSBL = SPL binary with STM32 image header, loaded by ROM code
- u-boot.img : SSBL = U-Boot binary with U-Boot image header (uImage), loaded by SPL
6. Examples[edit source]
6.1. STM32MP157F-EV1 Evaluation board [edit source]
make stm32mp15_trusted_defconfig make DEVICE_TREE=stm32mp157f-ev1 all
6.2. STM32MP157C-EV1 Evaluation board [edit source]
make stm32mp15_trusted_defconfig make DEVICE_TREE=stm32mp157c-ev1 all
6.3. STM32MP157D-DK1 Discovery kit [edit source]
make stm32mp15_trusted_defconfig make DEVICE_TREE=stm32mp157d-dk1 all
6.4. STM32MP157C-DK2 Discovery kit [edit source]
Using export to select the device tree
export KBUILD_OUTPUT=../build/stm32mp15_trusted export DEVICE_TREE=stm32mp157c-dk2 make stm32mp15_trusted_defconfig make all
6.5. Custom board with external device tree[edit source]
make stm32mp15_trusted_defconfig make EXT_DTB=stm32mp151a-myboard.dtb all
6.6. SPL for STM32MP157F-EV1 Evaluation board [edit source]
make stm32mp15_basic_defconfig
make DEVICE_TREE=stm32mp157f-ev1 all