How to load U-Boot with STM32CubeProgrammer

Revision as of 12:29, 16 February 2021 by Registered User (Nathalie Sangouard moved page How to load U-Boot with STM32cubeProgrammer to How to load U-Boot with STM32CubeProgrammer without leaving a redirect)

This page explains how to load and start U-Boot with STM32CubeProgrammer over uart or usb.

1. Overview[edit source]

To load and execute U-Boot in DDR with STM32CubeProgrammer, you need to follow the steps described in AN5275: USB DFU/USART protocols used in STM32MP1 Series bootloaders, load and start FSBL and SSBL to start the programming service:

  1. phase 0x1 loaded by ROM code is the FSBL = TF-A BL2
  2. phase 0x3 loaded by FSBL is the FIP file including the SSBL image: U-Boot

The FSBL, SSBL and FIP definitions can be found in the Boot chain overview (FIP include the required SSBL).

This feature can be used to debug U-Boot features required for programming service (USB support, flash devcie support,...) during board bringup.

See FAQ of STM32CubeProgrammer for specific question on this tools.

2. Prepare U-Boot to use the console[edit source]

By default in the STM32 boot command the stm32prog command is executed when the boot device is uart or usb to allow U-Boot (the programming service) to communicate with STM32CubeProgrammer.

To access to U-Boot console when U-Boot is loaded with STM32CubeProgrammer:

  • For USB boot you can easily interrupt this command stm32prog usb 0by pressing Ctr + C in the console without U-Boot modification.
  • For UART boot, the U-Boot console is deactivated to execute the stm32prog serial ${boot_instance} command in the bootcmd.
    To use the U-Boot console after STM32cubeProgrammer load, you can deactivate this behavior by
    • deactivate CONFIG_CMD_STM32PROG_SERIAL:
      • Use make menuconfig as explain in Kbuild
      • Add the line # CONFIG_CMD_STM32PROG_SERIAL is not set in your defconfig (stm32mp15_trusted_defconfig for example)
    • recompile U-Boot

Before ecosystem release v3.0.0 :

As CONFIG_CMD_STM32PROG_SERIAL don't exist, you need to

  • deactivate the support of the stm32prog command (for usb and uart device) with a line #CONFIG_CMD_STM32PROG is not set in your defconfig
  • patch the code, in arch/arm/mach-stm32mp/cpu.c (vv2020.01-stm32mp-r2)::arch_cpu_init(), and remove the console deactivation: gd->flags |= GD_FLG_SILENT | GD_FLG_DISABLE_CONSOLE;

3. Load U-Boot using Flashlayout[edit source]

You can use a minimal "FlashLayout.tsv" files for <dev> serial boot (see STM32CubeProgrammer_flashlayout for file format details):

 #Opt	id	Name	Type		IP		Offset		Binary
 -	0x01	fsbl		Binary		none	0x00000000	tf-a_<dev>.stm32
 -	0x03	fip		Binary		none	0x00000000	fip.bin

Then you use it with STM32CubeProgrammer command:

  STM32_Programmer_CLI -c port=<dev_port> -w FlashLayout.tsv

With

  • For USB: <dev> = usb and <dev_port>=usb1
  • For UART: <dev> =uart and <dev_port>= uart Interface identifier (ex COM1, /dev/ttyS0,...)

4. Load U-Boot using CLI[edit source]

You can also use the -d/--download option to load each phase and -s/--start option to start them without flashlayout.

For USB serial boot, <dev>=usb device with port=usb1.

  STM32_Programmer_CLI -c port=usb1 \
    -d tf-a_usb.stm32 0x1 -s 0x1 \
    -d flashlayout.stm32 0x0 -s 0x0 \
    -d fip.bin 0x3 -s 0x3

It is the same for uart serial boot with <dev> =uart and port = the uart Interface identifier.

For information, loading a flashlayout file with STM32 header for phase 0x0, even empty, is mandatory today but it will be removed in future release.

You can generate this empty flashlayout.stm32 file with U-Boot mkimage with commands on Linux shell:

 echo "" > flashlayout.tsv
 mkimage -T stm32image -a 0xC0000000 -e 0xC0000000 -d flashlayout.tsv flashlayout.stm32