This article explains the way STM32CubeIDE is managing Yocto SDK provided by OpenSTLinux.
1. Overview[edit source]
Two flavors are proposed for installing Yocto SDK:
- Yocto SDK is already installed on host workstation, after a download of the STM32MP1 OpenSTLinux Developer Package. In that case, only a setup is needed for STM32CubeIDE to use it.
- Yocto SDK is not present on host workstation, it can be installed via STM32CubeIDE:
- embedded inside the STM32CubeIDE; Yocto SDK removal is managed by STM32CubeIDE
- external, on host workstation disk, outside STM32CubeIDE scope; Yocto SDK removal is under final user responsibility
2. Using already installed Yocto SDK[edit source]
The choice is made proposed after the Setup OpenSTLinux menu, selecting Use existing.
You have then to give the Yocto SDK Install Root Path in the STM32Cube Preferences.
3. Installing Yocto SDK via STM32CubeIDE[edit source]
.