Template:Maintainer Template:ReviewersList Template:ArticleApprovedVersion
This category groups together articles explaining how to customize software for the STM32MPU Embedded Software distribution, and the STM32 MPUs microprocessor devices and boards.
Pages in category "How to customize software"
The following 29 pages are in this category, out of 29 total.
H
- How to add a customer application
- How to add a new parallel or serial NAND flash memory device in Yocto
- How to adjust USBPHYC settings using USB Eye Diagram
- How to assign an internal peripheral to an execution context
- How to avoid proxy issues
- How to change the CPU frequency
- How to compile the device tree with the Distribution Package
- How to configure a 256MB DDR mapping from STM32 MPU Distribution Package
- How to configure system resources
- How to configure U-Boot for your board
- How to configure UEFI boot with the Distribution Package
- How to configure uniprocessor mode
- How to create a new open embedded layer
- How to create your board device tree
- How to create your own distribution
- How to create your own image
- How to customize the Linux kernel
- How to develop an OP-TEE Trusted Application
- How to disable one CPU
- How to enable secure boot on STM32 MPU
- How to install X-TouchGFX MPU Addon
- How to optimize the boot time
- How to perform Secure Boot from Distribution package
- How to protect the coprocessor firmware
- How to use LTDC layers from CM33 and CA35 simultaneously
- How to use the DCMIPP ISP
- How to use the secure display feature