1. Developer package : build AI application from the X-LINUX-AI add-on SDK[edit source]
In order to easily develop and build an AI application without using the Yocto build system, X-LINUX-AI comes with a SDK add-on extending the OpenSTLinux SDK with AI functionality. To install and use the X-LINUX-AI SDK Add-on please refer to the following steps.
2. Prerequisites[edit source]
2.1. Install the OpenSTLinux SDK[edit source]
First of all, you must download and install the OpenSTLinux SDK, which contains all the basis needed for the X-LINUX-AI add-on. To do this, follow instructions given in STM32MPU Developer Package : Installing the SDK chapter. Once this has been done, you should have a directory containing the OpenSTLinux SDK.
3. X-LINUX-AI SDK add-on installation[edit source]
3.1. Download the X-LINUX-AI SDK add-on[edit source]
To add the Artificial Intelligence part into the OpenSTLinux SDK, you must download and install the X-LINUX-AI SDK add-on. The add-on is delivered through a tarball file that can be downloaded here: X-LINUX-AI SDK add-on.
3.2. Install the X-LINUX-AI SDK add-on[edit source]
Install add-on for STM32MP1 series
Once the X-LINUX-AI SDK add-on is downloaded, uncompress the add-on:
cd ~/Downloads/
tar xzf unknown package
Then, copy the .sh script to your OpenSTLinux SDK directory:
cp unknown package/unknown package <working directory absolute path>/Developer-Package/SDK
Finally, run the script contained in the tarball:
cd <working directory absolute path>/Developer-Package/SDK ./unknown package
Optionally, once the script is executed, you can delete it.
rm *.sh
Install add-on for STM32MP25x lines
Once the X-LINUX-AI SDK add-on is downloaded, uncompress the add-on:
cd ~/Downloads/
tar xzf unknown package
Then, copy the .sh script to your OpenSTLinux SDK directory:
cp unknown package/unknown package <working directory absolute path>/Developer-Package/SDK
Finally, run the script contained in the tarball:
cd <working directory absolute path>/Developer-Package/SDK ./unknown package
Optionally, once the script is executed, you can delete it.
rm *.sh
3.3. Start the SDK[edit source]
The add-on is now installed into the OpenSTLinux SDK. You can start the SDK. Go to your OpenSTLinux SDK directory and source the environment:
cd <working directory absolute path>/Developer-Package/SDK
source environment-setup-cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi
Check that the SDK is properly installed:
x-linux-ai -v
X-LINUX-AI version: 5.1.0
4. Use the SDK[edit source]
4.1. Build an application with the SDK[edit source]
Once the SDK is correctly set up, the applications can be built easily. In this example, it is the image classification application that is built.
Download the github repository:
git clone https://github.com/PRG-MPU-ALPHA/meta-st-x-linux-ai
Go to the image classification directory:
cd meta-st-x-linux-ai/recipes-samples/image-classification/files/tflite
Export ARCHITECTURE variable to build AI applications with NPU acceleration :
export ARCHITECTURE=stm32mp2_npu
Then, use the make command to build the application:
make
A new file is displayed, named tflite_image_classification. This is a binary file, which has been generated using the make command. It is compiled for the STM32MP2x architecture. It must now be transferred to the board.
4.2. Use the application[edit source]
Once the STM32MP2x board is correctly set up and the X-LINUX-AI packages are installed with the right version, it is possible to send the application to the board.
To do it, use the following command using your own IP address:
scp -r -p tflite_image_classification root@<ip_address>:/usr/local/demo-ai/image-classification/tflite
Then, use the ssh protocol to connect to the board:
ssh root@<ip_address>
On the board, go to the right directory and use the image classification script to launch the application:
cd /usr/local/demo-ai/image-classification/tflite ./launch_bin_image_classification.sh
This script is using the tflite_image_classification application that has been compiled before.