EXTI internal peripheral

Revision as of 12:07, 20 November 2023 by Registered User (→‎Peripheral overview)
Applicable for STM32MP13x lines, STM32MP15x lines, STM32MP25x lines

Warning white.png Warning
Concerning the STM32MP25x lines More info.png, only the boot time assignment table and the runtime assignment table have been updated.
The other chapters have not been updated yet.

1. Article purpose[edit source]

The purpose of this article is to:

  • briefly introduce the EXTI peripheral and its main features,
  • indicate the peripheral instances assignment at boot time and their assignment at runtime (including whether instances can be allocated to secure contexts),
  • list the software frameworks and drivers managing the peripheral,
  • explain how to configure the peripheral.

2. Peripheral overview[edit source]

The EXTI peripheral is used to get an interrupt when a GPIO is toggling. It can also wake up the system from Stop low power mode, by means of the PWR internal peripheral when a wake up event occurs, before (eventualy - see the note below) propagating an interrupt to the (Cortex-A GIC or Cortex-M NVIC). The wake up events can be internal (from other IPs clocked by the LSE, LSI or HSI from RCC), or external (from GPIO).

Notice that:

  • Up to 16 GPIO pins can be configured as external interrupts: for each index between 0 and 15, one EXTI can be selected among all banks (EXTI<index> = GPIO<one_bank><index>).
  • On STM32MP13x lines More info.png: The 16 GPIO and one internal peripheral events ( AVD/PVD), can generate interrupts connected to the GIC. All the other internal peripheral events can wake up the system, but the EXTI does not generate any interrupt to the GIC; in such cases, another peripheral interrupt has to be used as a trigger via the GIC.
  • On STM32MP15x lines More info.png: The 16 GPIO and 5 internal peripheral events (AVD/PVD, CPU1 SEV, CPU2 SEV, WWDG1 reset, CPU2 SYSRESETREQ) can generate interrupts connected to the GIC and NVIC. All the other internal peripheral events can wake up the system, but the EXTI does not generate any interrupt to the GIC or NVIC for them; in such cases, another peripheral interrupt has to be used as a trigger via the GIC or NVIC.
  • By default, at reset, all EXTI wake up events are non-secure.

Refer to the STM32 MPU reference manuals for the complete list of features, and to the software frameworks and drivers, introduced below, to see which features are implemented.

3. Peripheral usage[edit source]

This chapter is applicable in the scope of the OpenSTLinux BSP running on the Arm® Cortex®-A processor(s), and the STM32CubeMPU Package running on the Arm® Cortex®-M processor.

3.1. Boot time assignment[edit source]

3.1.1. On STM32MP13x lines More info.png[edit source]

The EXTI peripheral is not used at boot time, but is configured during Linux initialization.

3.1.2. On STM32MP15x lines More info.png[edit source]

The EXTI peripheral is not used at boot time, but is configured during Linux initialization.

Since wake-up event configuration is done via register bit-field reads and writes, concurrent accesses from Linux and the coprocessor are not possible at boot time:

  • Linux configures all EXTI events during their respective consumer driver probing
  • The coprocessor uses the resource management mechanisms to request and configure the EXTI events it needs.

3.1.3. On STM32MP2 series[edit source]

Click on How to.png to expand or collapse the legend...

  • means that the peripheral can be assigned to the given boot time context.
  • means that the peripheral is assigned by default to the given boot time context and that the peripheral is mandatory for the STM32 MPU Embedded Software distribution.
  • means that the peripheral can be assigned to the given boot time context, but this configuration is not supported in STM32 MPU Embedded Software distribution.
  • is used for system peripherals that cannot be unchecked because they are hardware connected in the device.

The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possibilities might be described in STM32MP25 reference manuals.

Domain Peripheral Boot time allocation Comment How to.png
Instance Cortex-A35
secure
(ROM code)
Cortex-A35
secure
(TF-A BL2)
Cortex-A35
non-secure
(U-Boot)
Core/Interrupts EXTI Info.png EXTI1 Shareable at internal peripheral level thanks to the RIF: see the boot time allocation per feature
EXTI2 Shareable at internal peripheral level thanks to the RIF: see the boot time allocation per feature

The below table shows the possible boot time allocations for the features of the EXTI1 instance.

Feature Boot time allocation Info.png Comment
Cortex-A35
secure
(ROM code)
Cortex-A35
secure
(TF-A BL2)
Cortex-A35
non-secure
(U-Boot)
EXTI1[0]
EXTI1[1]
EXTI1[2]
EXTI1[3]
EXTI1[4]
EXTI1[5]
EXTI1[6]
EXTI1[7]
EXTI1[8]
EXTI1[9]
EXTI1[10]
EXTI1[11]
EXTI1[12]
EXTI1[13]
EXTI1[14]
EXTI1[15]
PVD
PVM
VDDGPU_VD
RCC_HSI_FMON
I2C1
I2C2
I2C3
I2C4
I2C5
USART1
USART2
USART3
USART6
UART4
UART5
UART7
UART8
UART9
SPI1
SPI2
SPI3
SPI4
SPI5
SPI6
SPI7
USBH
USB3DR
COMBOPHY
UCPD
LPTIM1
LPTIM2
I2C6
I2C7
WKUP1 wakeup
WKUP2 wakeup
WKUP3 wakeup
WKUP4 wakeup
WKUP5 wakeup
WKUP6 wakeup
IPCC1 non secure interrupt CPU1
IPCC1 non secure interrupt CPU2
IPCC1 secure interrupt CPU1
IPCC1 secure interrupt CPU2
CPU2 SEV interrupt
CPU1 SEV interrupt
WWDG1 Reset
ETH1_PMT wakeup
ETH1_SBD
ETH2_PMT wakeup
ETH2_SBD
DTS
CPU2 SYSRESETREQ local CPU2 reset
I3C1
I3C2
I3C3
HPDMA1 Channel 0 to 15 CPU1 irq
HPDMA2 Channel 0 to 15 CPU1 irq
HPDMA3 Channel 0 to 15 CPU1 irq
HPDMA1 Channel 0 to 15 CPU2 irq
HPDMA2 Channel 0 to 15 CPU2 irq
HPDMA3 Channel 0 to 15 CPU2 irq
UCPD VBUS DETECT
UCPD VBUS VSAFE5V

The below table shows the possible boot time allocations for the features of the EXTI2 instance.

Feature Boot time allocation Info.png Comment
Cortex-A35
secure
(ROM code)
Cortex-A35
secure
(TF-A BL2)
Cortex-A35
non-secure
(U-Boot)
EXTI2[0]
EXTI2[1]
EXTI2[2]
EXTI2[3]
EXTI2[4]
EXTI2[5]
EXTI2[6]
EXTI2[7]
EXTI2[8]
EXTI2[9]
EXTI2[10]
EXTI2[11]
EXTI2[12]
EXTI2[13]
EXTI2[14]
EXTI2[15]
TAMP non secure tamper CPU1
RTC global non secure Wakeup CPU1
TAMP non secure tamper CPU2
RTC global non secure Wakeup CPU2
TAMP non secure tamper CPU3
TAMP secure tamper CPU1
RTC global secure Wakeup CPU1
TAMP secure tamper CPU2
RTC global secure Wakeup CPU2
I2C8
LPUART1
SPI8
LPTIM3
LPTIM4
LPTIM5
ADF1
IPCC2 non secure interrupt CPU1
IPCC2 non secure interrupt CPU2
IPCC2 non secure interrupt CPU3
IPCC2 secure interrupt CPU1
IPCC2 secure interrupt CPU2
HSEM1 non secure interrupt
HSEM2 non secure interrupt
HSEM3 non secure interrupt
HSEM1 secure interrupt
HSEM2 secure interrupt
WWDG2 reset
IWDG1 reset
IWDG2 reset
IWDG3 reset
IWDG4 reset
IWDG5 reset
IWDG1 early wake
IWDG2 early wake
IWDG3 early wake
IWDG4 early wake
IWDG5 early wake
CM33 SEV interrupt to CPU3
CA35 SEV interrupt to CPU3
CM0 SEV interrupt
IAC interrupt CPU1
IAC interrupt CPU2
VDDCPU_VD
VDDCORE_VD
RETRAM CRC error wakeup
lpdma_ch0123_cpu1_irq
lpdma_ch0123_cpu2_irq
lpdma_ch0123_cpu3_irq
I3C4
CDBGPWRUPREQ

3.2. Runtime assignment[edit source]

3.2.1. On STM32MP13x lines More info.png[edit source]

Click on How to.png to expand or collapse the legend...

STM32MP13 internal peripherals

Check boxes illustrate the possible peripheral allocations supported by STM32 MPU Embedded Software:

  • means that the peripheral can be assigned to the given runtime context.
  • means that the peripheral is assigned by default to the given runtime context and that the peripheral is mandatory for the STM32 MPU Embedded Software distribution.
  • means that the peripheral can be assigned to the given runtime context, but this configuration is not supported in STM32 MPU Embedded Software distribution.
  • is used for system peripherals that cannot be unchecked because they are hardware connected in the device.

Refer to How to assign an internal peripheral to an execution context for more information on how to assign peripherals manually or via STM32CubeMX.
The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possibilities might be described in STM32MP13 reference manuals.

Domain Peripheral Runtime allocation Comment How to.png
Instance Cortex-A7
secure
(OP-TEE)
Cortex-A7
non-secure
(Linux)
Core/Interrupts EXTI EXTI

3.2.2. On STM32MP15x lines More info.png[edit source]

Click on How to.png to expand or collapse the legend...

STM32MP15 internal peripherals

Check boxes illustrate the possible peripheral allocations supported by STM32 MPU Embedded Software:

  • means that the peripheral can be assigned to the given runtime context.
  • means that the peripheral is assigned by default to the given runtime context and that the peripheral is mandatory for the STM32 MPU Embedded Software distribution.
  • means that the peripheral can be assigned to the given runtime context, but this configuration is not supported in STM32 MPU Embedded Software distribution.
  • is used for system peripherals that cannot be unchecked because they are hardware connected in the device.

Refer to How to assign an internal peripheral to an execution context for more information on how to assign peripherals manually or via STM32CubeMX.
The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possiblities might be described in STM32MP15 reference manuals.

Domain Peripheral Runtime allocation Comment How to.png
Instance Cortex-A7
secure
(OP-TEE)
Cortex-A7
non-secure
(Linux)
Cortex-M4

(STM32Cube)
Core/Interrupts EXTI EXTI Shared
Info white.png Information
The EXTI peripheral is not listed in STM32CubeMX peripherals list because its configuration is partly embedded in the Device tree (for all internal EXTI sources, coming from peripherals with wake up capabilities) and completed with the GPIO configuration that comes from STM32CubeMX pinout view

The OP-TEE EXTI driver is not activated and not used by OpenSTLinux on STM32MP15x lines More info.png.

3.2.3. On STM32MP25x lines More info.png[edit source]

Click on How to.png to expand or collapse the legend...

STM32MP25 internal peripherals

Check boxes illustrate the possible peripheral allocations supported by STM32 MPU Embedded Software:

  • means that the peripheral can be assigned to the given runtime context.
  • means that the peripheral is assigned by default to the given runtime context and that the peripheral is mandatory for the STM32 MPU Embedded Software distribution.
  • means that the peripheral can be assigned to the given runtime context, but this configuration is not supported in STM32 MPU Embedded Software distribution.
  • is used for system peripherals that cannot be unchecked because they are hardware connected in the device.

The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possibilities might be described in STM32MP25 reference manuals.

Domain Peripheral Runtime allocation Comment How to.png
Instance Cortex-A35
secure
(OP-TEE /
TF-A BL31)
Cortex-A35
non-secure
(Linux)
Cortex-M33
secure
(TF-M)
Cortex-M33
non-secure
(STM32Cube)
Cortex-M0+
Warning.png
(STM32Cube)
Core/Interrupts EXTI Info.png EXTI1 OP-TEE Shareable at internal peripheral level thanks to the RIF: see the runtime allocation per feature
EXTI2 OP-TEE Shareable at internal peripheral level thanks to the RIF: see the runtime allocation per feature

The below table shows the possible runtime allocations for the features of the EXTI1 instance.

Feature Runtime allocation Info.png Comment
Cortex-A35
secure
(OP-TEE /
TF-A BL31)
Cortex-A35
non-secure
(Linux)
Cortex-M33
secure
(TF-M)
Cortex-M33
non-secure
(STM32Cube)
Cortex-M0+
Warning.png
(STM32Cube)
EXTI1[0] OP-TEE
EXTI1[1] OP-TEE
EXTI1[2] OP-TEE
EXTI1[3] OP-TEE
EXTI1[4] OP-TEE
EXTI1[5] OP-TEE
EXTI1[6] OP-TEE
EXTI1[7] OP-TEE
EXTI1[8] OP-TEE
EXTI1[9] OP-TEE
EXTI1[10] OP-TEE
EXTI1[11] OP-TEE
EXTI1[12] OP-TEE
EXTI1[13] OP-TEE
EXTI1[14] OP-TEE
EXTI1[15] OP-TEE
PVD OP-TEE
PVM OP-TEE
VDDGPU_VD OP-TEE
RCC_HSI_FMON OP-TEE
I2C1 OP-TEE
I2C2 OP-TEE
I2C3 OP-TEE
I2C4 OP-TEE
I2C5 OP-TEE
USART1 OP-TEE
USART2 OP-TEE
USART3 OP-TEE
USART6 OP-TEE
UART4 OP-TEE
UART5 OP-TEE
UART7 OP-TEE
UART8 OP-TEE
UART9 OP-TEE
SPI1 OP-TEE
SPI2 OP-TEE
SPI3 OP-TEE
SPI4 OP-TEE
SPI5 OP-TEE
SPI6 OP-TEE
SPI7 OP-TEE
USBH OP-TEE
USB3DR OP-TEE
COMBOPHY OP-TEE
UCPD OP-TEE
LPTIM1 OP-TEE
LPTIM2 OP-TEE
I2C6 OP-TEE
I2C7 OP-TEE
WKUP1 wakeup OP-TEE
WKUP2 wakeup OP-TEE
WKUP3 wakeup OP-TEE
WKUP4 wakeup OP-TEE
WKUP5 wakeup OP-TEE
WKUP6 wakeup OP-TEE
IPCC1 non secure interrupt CPU1
IPCC1 non secure interrupt CPU2
IPCC1 secure interrupt CPU1 OP-TEE
IPCC1 secure interrupt CPU2
CPU2 SEV interrupt OP-TEE
CPU1 SEV interrupt
WWDG1 Reset OP-TEE
ETH1_PMT wakeup OP-TEE
ETH1_SBD OP-TEE
ETH2_PMT wakeup OP-TEE
ETH2_SBD OP-TEE
DTS OP-TEE
CPU2 SYSRESETREQ local CPU2 reset
I3C1 OP-TEE
I3C2 OP-TEE
I3C3 OP-TEE
HPDMA1 Channel 0 to 15 CPU1 irq OP-TEE
HPDMA2 Channel 0 to 15 CPU1 irq OP-TEE
HPDMA3 Channel 0 to 15 CPU1 irq OP-TEE
HPDMA1 Channel 0 to 15 CPU2 irq
HPDMA2 Channel 0 to 15 CPU2 irq
HPDMA3 Channel 0 to 15 CPU2 irq
UCPD VBUS DETECT OP-TEE
UCPD VBUS VSAFE5V OP-TEE

The below table shows the possible runtime allocations for the features of the EXTI2 instance.

Feature Runtime allocation Info.png Comment
Cortex-A35
secure
(OP-TEE /
TF-A BL31)
Cortex-A35
non-secure
(Linux)
Cortex-M33
secure
(TF-M)
Cortex-M33
non-secure
(STM32Cube)
Cortex-M0+
Warning.png
(STM32Cube)
EXTI2[0] OP-TEE
EXTI2[1] OP-TEE
EXTI2[2] OP-TEE
EXTI2[3] OP-TEE
EXTI2[4] OP-TEE
EXTI2[5] OP-TEE
EXTI2[6] OP-TEE
EXTI2[7] OP-TEE
EXTI2[8] OP-TEE
EXTI2[9] OP-TEE
EXTI2[10] OP-TEE
EXTI2[11] OP-TEE
EXTI2[12] OP-TEE
EXTI2[13] OP-TEE
EXTI2[14] OP-TEE
EXTI2[15] OP-TEE
TAMP non secure tamper CPU1
RTC global non secure Wakeup CPU1
TAMP non secure tamper CPU2
RTC global non secure Wakeup CPU2
TAMP non secure tamper CPU3
TAMP secure tamper CPU1 OP-TEE
RTC global secure Wakeup CPU1 OP-TEE
TAMP secure tamper CPU2
RTC global secure Wakeup CPU2
I2C8 OP-TEE
LPUART1 OP-TEE
SPI8 OP-TEE
LPTIM3 OP-TEE
LPTIM4 OP-TEE
LPTIM5 OP-TEE
ADF1 OP-TEE
IPCC2 non secure interrupt CPU1
IPCC2 non secure interrupt CPU2
IPCC2 non secure interrupt CPU3
IPCC2 secure interrupt CPU1 OP-TEE
IPCC2 secure interrupt CPU2
HSEM1 non secure interrupt
HSEM2 non secure interrupt
HSEM3 non secure interrupt
HSEM1 secure interrupt OP-TEE
HSEM2 secure interrupt
WWDG2 reset OP-TEE
IWDG1 reset
IWDG2 reset OP-TEE
IWDG3 reset OP-TEE
IWDG4 reset OP-TEE
IWDG5 reset OP-TEE
IWDG1 early wake OP-TEE
IWDG2 early wake OP-TEE
IWDG3 early wake
IWDG4 early wake
IWDG5 early wake
CM33 SEV interrupt to CPU3
CA35 SEV interrupt to CPU3
CM0 SEV interrupt OP-TEE
IAC interrupt CPU1 OP-TEE
IAC interrupt CPU2
VDDCPU_VD OP-TEE
VDDCORE_VD OP-TEE
RETRAM CRC error wakeup
lpdma_ch0123_cpu1_irq OP-TEE
lpdma_ch0123_cpu2_irq
lpdma_ch0123_cpu3_irq
I3C4 OP-TEE
CDBGPWRUPREQ OP-TEE

4. Software frameworks and drivers[edit source]

Below are listed the software frameworks and drivers managing the EXTI peripheral for the embedded software components listed in the above tables.


5. How to assign and configure the peripheral[edit source]

The peripheral assignment can be done via the STM32CubeMX graphical tool (and manually completed if needed).
This tool also helps to configure the peripheral:

  • partial device trees (pin control and clock tree) generation for the OpenSTLinux software components,
  • HAL initialization code generation for the STM32CubeMPU Package.

The configuration is applied by the firmware running in the context in which the peripheral is assigned.

See also additional information in the Interrupt device tree configuration article for Linux®.